diff --git a/src/hw/gpio/gpio.c b/src/hw/gpio/gpio.c
index 27f8df49ce890db2668f2cc9ca2758f3fc123395..196ec97c0373b4bad22acef50c51312c2d100f71 100644 (file)
--- a/src/hw/gpio/gpio.c
+++ b/src/hw/gpio/gpio.c
* Pre-Condition: The GPIO[7:0] should be configured as input
*
*****************************************************************************/
-Uint8 hwGpioReadDataBus( void )
+Uint32 hwGpioReadDataBus( void )
{
- Uint8* puchGpioInput = (Uint8*)GPIO_IN_DATA_REG;
+ Uint32* puchGpioInput = (Uint32*)GPIO_IN_DATA_REG;
return *puchGpioInput;
}