index 391cc20a1becac38691bd08ba6c9a115861d1e89..1786ab322ccd282f6fac77e94da428ce3fdbe2d1 100644 (file)
--- a/src/interp/btbl/btblpr.c
+++ b/src/interp/btbl/btblpr.c
void boot_proc_boot_tbl_addr(BOOT_TBL_CB_T* p_inst);
void boot_proc_boot_tbl_data(BOOT_TBL_CB_T* p_inst);
void boot_proc_boot_tbl_flush(BOOT_TBL_CB_T* p_inst);
+void boot_proc_boot_tbl_pad(BOOT_TBL_CB_T* p_inst);
/*******************************************************************************
* Local variables
p_inst->data_size_uint16--;
}
+/*******************************************************************************
+ * FUNCTION PURPOSE: Process the boot table in the PAD state
+ *******************************************************************************
+ * DESCRIPTION: Toss data bytes to advance to the next section
+ *******************************************************************************/
+#define MIN(a,b) (a)<(b) ? (a) : (b)
+void boot_proc_boot_tbl_pad(BOOT_TBL_CB_T* p_inst)
+{
+ UINT32 num_bytes;
+ UINT32 num_uint16_words;
+
+ num_bytes = MIN (p_inst->section_size_bytes, CHIP_UINT16_TO_BYTES(p_inst->data_size_uint16));
+ num_uint16_words = CHIP_BYTES_TO_UINT16(num_bytes);
+
+ /* Update instance variables for the next code section */
+ p_inst->data_size_uint16 -= num_uint16_words;
+ p_inst->p_data += num_uint16_words;
+
+ p_inst->section_addr += num_bytes;
+ p_inst->section_size_bytes -= num_bytes;
+
+ if(p_inst->section_size_bytes == 0)
+ {
+ p_inst->state = BOOT_TBL_STATE_SIZE;
+
+ /* Chip specific post block handling. Can be defined to an empty statement */
+ chipBtblBlockDone();
+ }
+}
+
+
+
/*******************************************************************************
* FUNCTION PURPOSE: Process the boot table in DATA State
*******************************************************************************
* BOOT_TBL_CB_T *p_inst) - A pointer to Boot Table Control instance
*
*****************************************************************************/
-#define MIN(a,b) (a)<(b) ? (a) : (b)
void boot_proc_boot_tbl_data(BOOT_TBL_CB_T* p_inst)
{
- UINT32 num_bytes; /* number of bytes to be copy */
- UINT32 num_uint16_words; /* number of 16 bit words to copy */
+ UINT32 num_bytes; /* number of bytes to be copy */
+ UINT32 num_uint16_words; /* number of 16 bit words to copy */
+ UINT32 num_uint16_words_pad; /* number of 16 bit words, rounded up to a multiple of 4 bytes */
+ UINT32 pad_uint16; /* The amount of pad present */
UINT16 error;
num_bytes = MIN (p_inst->section_size_bytes, CHIP_UINT16_TO_BYTES(p_inst->data_size_uint16));
num_uint16_words = CHIP_BYTES_TO_UINT16(num_bytes);
/* Some processors add padding to the memwidth used in the rom (created by tools) */
- num_uint16_words = chipAddBtblUint16Pad (num_uint16_words);
+ num_uint16_words_pad = chipAddBtblUint16Pad (num_uint16_words);
+ pad_uint16 = num_uint16_words_pad - num_uint16_words;
/*
* Record the last UINT16 word and copy the data to the destination
p_inst->section_addr += num_bytes;
p_inst->section_size_bytes -= num_bytes;
-
+
if(p_inst->section_size_bytes == 0)
{
- p_inst->state = BOOT_TBL_STATE_SIZE;
- /* Chip specific post block handling. Can be defined to an empty statement */
- chipBtblBlockDone();
+ if (pad_uint16)
+ {
+ p_inst->state = BOOT_TBL_STATE_PAD;
+ p_inst->section_size_bytes = CHIP_UINT16_TO_BYTES(pad_uint16);
+ }
+ else
+ {
+ p_inst->state = BOOT_TBL_STATE_SIZE;
+
+ /* Chip specific post block handling. Can be defined to an empty statement */
+ chipBtblBlockDone();
+ }
}
/* update statistics */
*****************************************************************************/
void boot_init_boot_tbl_inst(BOOT_TBL_CB_T *p_btbl_inst)
{
- memset(p_btbl_inst, 0, sizeof(BOOT_TBL_CB_T));
+ btblMemset(p_btbl_inst, 0, sizeof(BOOT_TBL_CB_T));
p_btbl_inst->state = BOOT_TBL_STATE_INIT;
/*
btbl_st_proc_fcn[BOOT_TBL_STATE_SIZE] = boot_proc_boot_tbl_size;
btbl_st_proc_fcn[BOOT_TBL_STATE_ADDR] = boot_proc_boot_tbl_addr;
btbl_st_proc_fcn[BOOT_TBL_STATE_DATA] = boot_proc_boot_tbl_data;
+ btbl_st_proc_fcn[BOOT_TBL_STATE_PAD] = boot_proc_boot_tbl_pad;
btbl_st_proc_fcn[BOOT_TBL_STATE_FLUSH] = boot_proc_boot_tbl_flush;
} /* end of boot_init_boot_tbl_inst() */