author | Mike Line <m-line1@ti.com> | |
Mon, 1 Nov 2010 17:42:30 +0000 (13:42 -0400) | ||
committer | Mike Line <m-line1@ti.com> | |
Mon, 1 Nov 2010 17:42:30 +0000 (13:42 -0400) | ||
commit | 63895f7b3f64958a0948cdce0f5fbbb07082b7cd | |
tree | 014a9c728423235881722fc075336e257490b447 | tree | snapshot (tar.xz tar.gz zip) |
parent | 6143ef43e41f7d6291235c348594958c0ca70ca5 | commit | diff |
Two stage load of ibl from I2C
A two stage load of the ibl is done. The first stage loaded is an
endian independent program which then loads the rest of the ibl
(endian dependent). The PLL is also setup in the first stage
which will increase the load time for the c6455
A two stage load of the ibl is done. The first stage loaded is an
endian independent program which then loads the rest of the ibl
(endian dependent). The PLL is also setup in the first stage
which will increase the load time for the c6455
12 files changed: