Documentation updates
authorSandeep Nair <sandeep_n@ti.com>
Tue, 24 May 2011 13:55:57 +0000 (09:55 -0400)
committerSandeep Nair <sandeep_n@ti.com>
Tue, 24 May 2011 13:55:57 +0000 (09:55 -0400)
doc/evmc6670-instructions.txt
doc/evmc6678-instructions.txt
doc/release_info.txt
src/util/btoccs/Makefile

index 352c01cc01f0a72a7660dd58687102cc511dc388..5ed7e0bf32995eaa08194d0e416295a070de635a 100644 (file)
@@ -43,7 +43,7 @@ Steps to use IBL on the c6670 EVM
     SW4(on, on, on, on), 
     SW5(on, on, on, off),
     SW6(on, on, on, on)
-   This will set the boot para index to 0 to boot the NOR image, by default
+   This will set the boot param index to 0 to boot the NOR image, by default
    the boot configuration table sets the NOR offset address to be 0 and 
    image format to be ELF for image 0.
    
@@ -53,7 +53,7 @@ Steps to use IBL on the c6670 EVM
     SW4(on, off, on, on), 
     SW5(on, on, on, off),
     SW6(on, on, on, on)
-   This will set the boot para index to 2 to boot the NAND image, by default
+   This will set the boot param index to 2 to boot the NAND image, by default
    the boot configuration table sets the NAND offset address to be 16384 
    (start of block 1) and image format to be BBLOB for image 0.
 
@@ -63,7 +63,7 @@ Steps to use IBL on the c6670 EVM
     SW4(on, on, off, on), 
     SW5(on, on, on, off),
     SW6(on, on, on, on)
-   This will set the boot para index to 4 to boot an image from a remote TFTP
+   This will set the boot param index to 4 to boot an image from a remote TFTP
    server, by default the boot configuration table sets the server IP to be 
    192.168.2.101, board IP to be 192.168.2.100 and image format to be BBLOB.
 
index 15567cb40a957e2b71350b061397c2fe2ca41412..b61b090bde31227e4edf110d7845e733d4813980 100644 (file)
@@ -43,7 +43,7 @@ Steps to use IBL on the c6678 EVM
     SW4(on, on, on, on), 
     SW5(on, on, on, off),
     SW6(on, on, on, on)
-   This will set the boot para index to 0 to boot the NOR image, by default
+   This will set the boot param index to 0 to boot the NOR image, by default
    the boot configuration table sets the NOR offset address to be 0 and 
    image format to be ELF for image 0.
    
@@ -53,7 +53,7 @@ Steps to use IBL on the c6678 EVM
     SW4(on, off, on, on), 
     SW5(on, on, on, off),
     SW6(on, on, on, on)
-   This will set the boot para index to 2 to boot the NAND image, by default
+   This will set the boot param index to 2 to boot the NAND image, by default
    the boot configuration table sets the NAND offset address to be 16384 
    (start of block 1) and image format to be BBLOB for image 0.
 
@@ -63,7 +63,7 @@ Steps to use IBL on the c6678 EVM
     SW4(on, on, off, on), 
     SW5(on, on, on, off),
     SW6(on, on, on, on)
-   This will set the boot para index to 4 to boot an image from a remote TFTP
+   This will set the boot param index to 4 to boot an image from a remote TFTP
    server, by default the boot configuration table sets the server IP to be 
    192.168.2.101, board IP to be 192.168.2.100 and image format to be BBLOB.
 
index 4fb438ea9e2ee9e7a954acf3a1319c17b02f7e27..135c5beb4642e64a3f9221b84a883a92e27af347 100644 (file)
@@ -15,24 +15,31 @@ May 2011
     - little
 
 3) Required toolset
-    - If building in Windows environment - MinGW MSYS v1.0.11
-      (http://downloads.sourceforge.net/mingw/MSYS-1.0.11.exe)
     - TI CGEN compiler CGT_C6000_7.2.0
-NOTE: TI CGEN compiler CGT_C6000_6.1.12 has to be used for building IBL with
-ENDIAN mode "both".
+
+   Requirements for building IBL on Windows:
+   For building on a Windows machine, a GNU development environment is
+   required. MinGW installation is required for this. 
+   MinGW project link: http://www.mingw.org/
+   MinGW installer can be obtained from the following link
+   http://sourceforge.net/projects/mingw/files/Automated%20MinGW%20Installer/mingw-get-inst/mingw-get-inst-20110316/mingw-get-inst-20110316.exe/download
+   While installing MinGW following options have to be chosen:
+    1.  MinGw Compiler Suite
+        -   C Compiler
+    2. MinGW Developer Toolkit 
  
 4) Build Instructions
 
     - Change directory to ibl\src\make
     - Modify the environment setup script to match the tool chain installation
       directory:
-        For building in Cygwin environment modify setupenv.bat 
         For building in MINGW-MSYS Bash shell modify setupenvMsys.sh 
         For building in Linux Bash shell modify setupenvLnx.sh 
-    - Set the environment by running "setupenv.bat" or "source setupenvLnx.sh"
-      or "source setupenvMsys.sh"
+    - Set the environment variables:
+         On a Linux Bash shell run  "source setupenvLnx.sh"
+         On a MinGW-MSYS Bash shell "source setupenvMsys.sh"
     - For building run the following make command:
-    C6678/C6670 EVM:
+    For C6678/C6670 Low Cost EVM:
         make evm_c667x_i2c ENDIAN=little I2C_BUS_ADDR=0x51 
       or:
         make <TARGET>  ENDIAN=[little|big]
index 7aa9bf989fef0c28b4396008f8c7d3b8c8206a46..0c489f629355b5350598c2fde47a1e3431ffb7b0 100644 (file)
@@ -57,4 +57,4 @@ ccs2bin.exe: ccs2bin.c
 
 
 clean:
-       -rm -f b2ccs.exe b2i2c.exe ccs2b.exe bfaddsect.exe bfmerge.exe ccs2bin.exe ccs2bin
+       -rm -f b2ccs b2i2c ccs2b bfaddsect bfmerge ccs2bin *.exe