Merge branch 'master' of git@gtgit01.gt.design.ti.com:git/teams/mmi/ibl DEV.MAD_UTILS.IBL.01.00.00.06
authorSandeep Nair <sandeep_n@ti.com>
Fri, 17 Jun 2011 22:21:29 +0000 (18:21 -0400)
committerSandeep Nair <sandeep_n@ti.com>
Fri, 17 Jun 2011 22:21:29 +0000 (18:21 -0400)
doc/README.txt
src/device/c66x/c66xinit.c
src/device/c66x/target.h
src/driver/nand/nand.c
src/make/ibl_c66x/i2crom.map.pre
src/make/setupenv.bat [deleted file]

index 2aedf9a6686372356645237f53b896edc3a919ca..0ae550200f03f6248411378b997cbd280d853b22 100644 (file)
@@ -1,7 +1,7 @@
 =====================================================
 C6x Intermediate Bootloader (IBL)
-Version: 1.0.0.5
-May 2011
+Version: 1.0.0.6
+June 2011
 =====================================================
 
 This directory contains the following documents:
index deae692f3c2f42e578ce33024915ec02ced341b6..6488f1eb30721c44b5cfe2d2f08c73307f25a0ac 100644 (file)
@@ -152,9 +152,122 @@ void iblEnableEDC ()
        *(volatile unsigned int *)(SMEDCC) |= 0x40000000;       //Set ECM(bit30)=1      
 }
 
+#ifdef IBL_ENABLE_PCIE_WORKAROUND
+
+/* undocumented register in data manual 
+ * Bit 0 of this register is supposed to give the status of PCIe PLL lock*/
+#define PCIE_STS_REG    0x262015C
+
+/* Workaround for PCIe boot mode support for C6678/C6670 */
+/* This is a temporary workaround should be removed once fixed in RBL */
+
+/* PCIe Config register base on C6678/C6670 */
+#define PCIE_BASE_ADDR 0x21800000
+
+/* PCIe Application registers */
+#define PCIE_APP_CMD_STATUS  0x4
+#define PCIE_OB_SIZE         0x30
+#define PCIE_APP_SERDES_CFG0 0x390
+#define PCIE_APP_SERDES_CFG1 0x394
+
+/* PCIe Local Configuration registers */
+#define PCIE_VENDER_DEVICE_ID   0x1000
+#define PCIE_STATUS_CMD         0x1004
+#define PCIE_CLASSCODE_REVID    0x1008
+#define PCIE_BAR0               0x1010
+#define PCIE_BAR1               0x1014
+#define PCIE_BAR2               0x1018
+#define PCIE_BAR3               0x101c
+#define PCIE_DEVICE_CAP         0x1074
+#define PCIE_DEV_STAT_CTRL     0x1078
+#define PCIE_LINK_STAT_CTRL     0x1080
+#define PCIE_ACCR                  0x1118
+#define PCIE_DEBUG0             0x1728
+#define PCIE_PL_GEN2            0x180C
+
+/* SERDES Configuration registers */
+#define PCIE_SERDES_CFG_PLL 0x2620358
+
+#define MAGIC_ADDR (*(volatile unsigned int *)0x87fffc)
+
+/* */
+
+extern cregister volatile unsigned int IER;
+
+void waitForBoot(void)
+{
+    void (*escape)();
+    UINT32  i;
+
+    /* Disable interrupts */
+    IER = 1;
+       MAGIC_ADDR = 0;
+
+    do {
+        for (i=0; i < 100; i++)
+            asm("    nop");
+    } while (MAGIC_ADDR == 0);
+
+    escape = (void (*)())(MAGIC_ADDR);
+    (*escape)();
+}
+
+void iblPCIeWorkaround()
+{
+    UINT32  cmd_stat;
+    UINT32  reg,i;
+
+     /* Power up PCIe */
+    devicePowerPeriph (TARGET_PWR_PCIE);
+    for(i=0; i<1000; i++) asm (" NOP");
+
+    DEVICE_REG32_W ((PCIE_BASE_ADDR + PCIE_APP_SERDES_CFG0), 0x00062320);  /* ss clock */
+    DEVICE_REG32_W ((PCIE_BASE_ADDR + PCIE_APP_SERDES_CFG1), 0x00022320);  /* ss clock */
+      
+    /* Wait for PCIe PLL lock */
+    while(!(DEVICE_REG32_R(PCIE_STS_REG) & 1));
+
+    DEVICE_REG32_W ((PCIE_BASE_ADDR + PCIE_CLASSCODE_REVID), 0x04800001);  /* class = 4 */ 
+    DEVICE_REG32_W ((PCIE_BASE_ADDR + PCIE_LINK_STAT_CTRL),  0x10110080);  /* extended synch */
+
+    DEVICE_REG32_W ((PCIE_BASE_ADDR + PCIE_VENDER_DEVICE_ID),  0x8888104c); 
+    DEVICE_REG32_W ((PCIE_BASE_ADDR + PCIE_DEVICE_CAP),  0x288701); 
+
+       DEVICE_REG32_W ((PCIE_BASE_ADDR + PCIE_OB_SIZE),  0x00000003);          /* OB_SIZE = 8M */ 
+       DEVICE_REG32_W ((PCIE_BASE_ADDR + PCIE_PL_GEN2),  0x0000000F);
+
+    DEVICE_REG32_W ((PCIE_BASE_ADDR + PCIE_APP_CMD_STATUS), 0x0020); /* Set dbi_cs2 to allow access to the BAR registers */ 
+    DEVICE_REG32_W ((PCIE_BASE_ADDR + PCIE_BAR0), 0x00003FFF);
+    DEVICE_REG32_W ((PCIE_BASE_ADDR + PCIE_BAR1), 0x0007FFFF);
+    DEVICE_REG32_W ((PCIE_BASE_ADDR + PCIE_BAR2), 0x003FFFFF);
+    DEVICE_REG32_W ((PCIE_BASE_ADDR + PCIE_BAR3), 0x00FFFFFF);
+
+       DEVICE_REG32_W ((PCIE_BASE_ADDR + PCIE_APP_CMD_STATUS), 0x0);          /* dbi_cs2=0 */
+
+       DEVICE_REG32_W ((PCIE_BASE_ADDR + PCIE_STATUS_CMD), 0x00100146);
+    DEVICE_REG32_W ((PCIE_BASE_ADDR + PCIE_DEV_STAT_CTRL), 0x0000281F);
+    DEVICE_REG32_W ((PCIE_BASE_ADDR + PCIE_ACCR), 0x000001E0);
+    DEVICE_REG32_W ((PCIE_BASE_ADDR + PCIE_BAR0), 0);
+
+    DEVICE_REG32_W ((PCIE_BASE_ADDR + PCIE_APP_CMD_STATUS), 0x0000007);    /* enable LTSSM, IN, OB */
+    while((DEVICE_REG32_R(PCIE_BASE_ADDR + PCIE_DEBUG0) & 0x11)!=0x11);    /* Wait for training to complete */
+    /* Wait for the Boot from Host */
+    waitForBoot();
+
+    /* Will never reach here */
+    return;
+}
+
+#endif
+
 #define FPGA_BM_GPI_STATUS_LO_REG           4   /* Boot Mode GPI Status (07-00 Low Byte) Register */
 #define FPGA_BM_GPI_STATUS_HI_REG           5   /* Boot Mode GPI Status (15-08 High Byte) Register */
+#define FPGA_ICS557_SEL_CTRL_REG            0x50 /* ICS 557 Clock Selection
+                                                    Control Register*/
 #define FPGA_READ_REG_CMD(x)                ((x | 0x80) << 8)
+#define FPGA_WRITE_REG_CMD(addr,byte)       (((addr & 0x7f) << 8) | (byte & 0xff))
+
 /**
  * @brief
  *      Enter the ROM boot loader if the FPGA boot register
@@ -163,7 +276,6 @@ void iblEnableEDC ()
  */
 void iblEnterRom ()
 {
-    uint32      reg =  DEVICE_REG32_R (DEVICE_REG_DEVSTAT);
     uint32      v, dev_stat, bm_lo, bm_hi;
     void        (*exit)();
 
@@ -192,7 +304,7 @@ void iblEnterRom ()
     DEVICE_REG32_W (DEVICE_SPI_BASE(0) + SPI_REG_SPIGCR1, 0x01000003);
 
     /* Read the BM status lo register */
-       DEVICE_REG32_W(DEVICE_SPI_BASE(0) + 0x38, FPGA_READ_REG_CMD(FPGA_BM_GPI_STATUS_LO_REG));
+       DEVICE_REG32_W(DEVICE_SPI_BASE(0) + SPI_REG_SPIDAT0, FPGA_READ_REG_CMD(FPGA_BM_GPI_STATUS_LO_REG));
     chipDelay32(10000);
     v = DEVICE_REG32_R(DEVICE_SPI_BASE(0) + SPI_REG_SPIFLG);
     if ( v & 0x100)
@@ -205,7 +317,7 @@ void iblEnterRom ()
     }
 
     /* Read the BM status hi register */
-       DEVICE_REG32_W(DEVICE_SPI_BASE(0) + 0x38, FPGA_READ_REG_CMD(FPGA_BM_GPI_STATUS_HI_REG));
+       DEVICE_REG32_W(DEVICE_SPI_BASE(0) + SPI_REG_SPIDAT0, FPGA_READ_REG_CMD(FPGA_BM_GPI_STATUS_HI_REG));
     chipDelay32(10000);
     v = DEVICE_REG32_R(DEVICE_SPI_BASE(0) + SPI_REG_SPIFLG);
     if ( v & 0x100)
@@ -217,8 +329,6 @@ void iblEnterRom ()
         return;
     }
 
-    /* Reset SPI */
-    DEVICE_REG32_W (DEVICE_SPI_BASE(0) + SPI_REG_SPIGCR0, SPI_REG_VAL_SPIGCR0_RESET);
 
     if ( (BOOT_READ_BITFIELD(bm_lo,3,1) != 0x5)     ||
          (BOOT_READ_BITFIELD(bm_hi,3,3) == 0x0) )    
@@ -233,6 +343,27 @@ void iblEnterRom ()
         /* Update the DEVSTAT register for the intended Boot Device and i2c Addr */
         DEVICE_REG32_W (DEVICE_REG_DEVSTAT, dev_stat);
 
+#ifdef IBL_ENABLE_PCIE_WORKAROUND
+#define BOOT_DEVICE_MASK    0xE
+#define DEVSTAT_BOOTDEVICE_SHIFT    1
+#define PCI_BOOT_MODE   0x4
+
+        if (((dev_stat & BOOT_DEVICE_MASK)>>DEVSTAT_BOOTDEVICE_SHIFT) == PCI_BOOT_MODE) {
+            /* Write ICS 557 Clock Selection Control Register in the FPGA */
+            /* 1 : FPGA_ICS557_SEL s driven high */
+               DEVICE_REG32_W(DEVICE_SPI_BASE(0) + SPI_REG_SPIDAT0,
+                           FPGA_WRITE_REG_CMD(FPGA_ICS557_SEL_CTRL_REG,1));
+            chipDelay32(10000);
+            /* Reset SPI */
+            DEVICE_REG32_W (DEVICE_SPI_BASE(0) + SPI_REG_SPIGCR0, SPI_REG_VAL_SPIGCR0_RESET);
+
+            iblPCIeWorkaround();
+            /* Will never reach here */
+        }
+#endif
+        /* Reset SPI */
+        DEVICE_REG32_W (DEVICE_SPI_BASE(0) + SPI_REG_SPIGCR0, SPI_REG_VAL_SPIGCR0_RESET);
+
         exit = (void (*)())BOOT_ROM_ENTER_ADDRESS;
         (*exit)();        
     }
@@ -241,6 +372,9 @@ void iblEnterRom ()
         /* Update the DEVSTAT register for the actual boot configuration */
         DEVICE_REG32_W (DEVICE_REG_DEVSTAT, ((bm_hi << 8) | bm_lo));
     }
+
+    /* Reset SPI */
+    DEVICE_REG32_W (DEVICE_SPI_BASE(0) + SPI_REG_SPIGCR0, SPI_REG_VAL_SPIGCR0_RESET);
 }
 
 #if (!defined(EXCLUDE_NOR_SPI) || !defined(EXCLUDE_NAND_SPI))
@@ -301,7 +435,5 @@ void deviceLoadInitSpiConfig (void *vcfg)
     }
 
 }
-
-
-
 #endif
+
index 403cfe86103506576a6c6c6833dea1d453f71f84..853a4a073373d1063f2f59235036d9952af03f60 100644 (file)
  */
 #define TARGET_PWR_GPIO     -1
 
+/**
+ *  @brief
+ *      The LPSC number for PCIe. PCIe is 10 for C6678/C6770
+ */
+#define TARGET_PWR_PCIE    10 
+
 /**
  * @brief
  *  Flag to indicate timer 0 power up requested. The time is always on in the 6472
@@ -365,6 +371,13 @@ Int32 targetMacRcv (void *ptr_device, UINT8 *buffer);
 #define deviceConfigureForNor()    0
 
 
+/****************************************************************
+ *
+ * NOTE: Following build flags enable DEVICE specific workarounds
+ * and have code which is specific to C6670/C6678 LC EVMs
+ *
+ ****************************************************************/
+
 /**
  *  @brief
  *      Support for PLL workaround to re-enter ROM boot loader.
@@ -377,4 +390,11 @@ Int32 targetMacRcv (void *ptr_device, UINT8 *buffer);
  */
 #define IBL_ENABLE_EDC             1 
 
+/**
+ *  @brief
+ *      Support for enabling PCIe workarond for C6678/C6670.
+ */
+#define IBL_ENABLE_PCIE_WORKAROUND 1
+
 #endif /* _TARGET_H */
+
index 19a2399f3efc785ab800bc45834c2c0764e019da..2edf19542ab0a3bb1bade26a58622975acc619e1 100644 (file)
@@ -288,13 +288,13 @@ Int32 nand_open (void *ptr_driver, void (*asyncComplete)(void *))
     
 
     /* Construct the logical to physical block array */  
-    for (i = j = startBlock; i < nandmcb.devInfo.totalBlocks; i++)  {
+    for (i = startBlock, j = 0; i < nandmcb.devInfo.totalBlocks; i++)  {
         if (nandmcb.blocks[i] != 0xff)
             nandmcb.logicalToPhysMap[j++] = i;
     }
 
     /* Construct the physical to logical block array */
-    for (i = j = startBlock; i < nandmcb.devInfo.totalBlocks; i++)  {
+    for (i = startBlock, j = 0; i < nandmcb.devInfo.totalBlocks; i++)  {
         if (nandmcb.blocks[i] == 0xff)
             nandmcb.physToLogicalMap[i] = 0xff;
         else
@@ -307,7 +307,7 @@ Int32 nand_open (void *ptr_driver, void (*asyncComplete)(void *))
     nandmcb.currentLogicalBlock = 0xffffffff;
     nandmcb.currentPage         = 0xffffffff;
 
-    nand_seek (ibln->bootAddress[iblEndianIdx][iblImageIdx], 0);
+    nand_seek (0, 0);
             
     return (0);
 
index 8f8f83f04ab24786c2a2e1f325cdb0d82d60e164..cf22cc07089c10bb68d1b2b0ddc8f4ffa7b21a25 100644 (file)
@@ -14,9 +14,9 @@ section
 {
   param_index    = 0
   boot_mode      = 40
-  sw_pll_prediv         = 1
-  sw_pll_mult    = 16
-  sw_pll_postdiv = 2
+  sw_pll_prediv         = 0
+  sw_pll_mult    = 0
+  sw_pll_postdiv = 0
   options        = 1
 
   core_freq_mhz    = 100
@@ -34,9 +34,9 @@ section
 {
   param_index    = 1
   boot_mode      = 40
-  sw_pll_prediv         = 1
-  sw_pll_mult    = 16
-  sw_pll_postdiv = 2
+  sw_pll_prediv         = 0
+  sw_pll_mult    = 0
+  sw_pll_postdiv = 0
   options        = 1
 
   core_freq_mhz    = 100
@@ -54,9 +54,9 @@ section
 {
   param_index    = 2
   boot_mode      = 40
-  sw_pll_prediv         = 1
-  sw_pll_mult    = 16
-  sw_pll_postdiv = 2
+  sw_pll_prediv         = 0
+  sw_pll_mult    = 0
+  sw_pll_postdiv = 0
   options        = 1
 
   core_freq_mhz    = 100
@@ -74,9 +74,9 @@ section
 {
   param_index    = 3
   boot_mode      = 40
-  sw_pll_prediv         = 1
-  sw_pll_mult    = 16
-  sw_pll_postdiv = 2
+  sw_pll_prediv         = 0
+  sw_pll_mult    = 0
+  sw_pll_postdiv = 0
   options        = 1
 
   core_freq_mhz    = 100
@@ -94,9 +94,9 @@ section
 {
   param_index    = 4
   boot_mode      = 40
-  sw_pll_prediv         = 1
-  sw_pll_mult    = 16
-  sw_pll_postdiv = 2
+  sw_pll_prediv         = 0
+  sw_pll_mult    = 0
+  sw_pll_postdiv = 0
   options        = 1
 
   core_freq_mhz    = 100
@@ -114,9 +114,9 @@ section
 {
   param_index    = 5
   boot_mode      = 40
-  sw_pll_prediv         = 1
-  sw_pll_mult    = 16
-  sw_pll_postdiv = 2
+  sw_pll_prediv         = 0
+  sw_pll_mult    = 0
+  sw_pll_postdiv = 0
   options        = 1
 
   core_freq_mhz    = 100
@@ -134,9 +134,9 @@ section
 {
   param_index    = 6
   boot_mode      = 40
-  sw_pll_prediv         = 1
-  sw_pll_mult    = 16
-  sw_pll_postdiv = 2
+  sw_pll_prediv         = 0
+  sw_pll_mult    = 0
+  sw_pll_postdiv = 0
   options        = 1
 
   core_freq_mhz    = 100
@@ -154,9 +154,9 @@ section
 {
   param_index    = 7
   boot_mode      = 40
-  sw_pll_prediv         = 1
-  sw_pll_mult    = 16
-  sw_pll_postdiv = 2
+  sw_pll_prediv         = 0
+  sw_pll_mult    = 0
+  sw_pll_postdiv = 0
   options        = 1
 
   core_freq_mhz    = 100
diff --git a/src/make/setupenv.bat b/src/make/setupenv.bat
deleted file mode 100644 (file)
index 5dd5ff1..0000000
+++ /dev/null
@@ -1,39 +0,0 @@
-@REM ******************************************************************************
-@REM * FILE PURPOSE: Environment Setup for building Bootloader
-@REM ******************************************************************************
-@REM * FILE NAME: setupenv.bat
-@REM *
-@REM * DESCRIPTION: 
-@REM *  Configures and sets up the Build Environment for Bootloader in DOS environment. 
-@REM *  
-@REM *  Customers are expected to modify this file as per their build environment.
-@REM *
-@REM * USAGE:
-@REM *  setupenv.bat  
-@REM *
-@REM * Copyright (C) 2010, Texas Instruments, Inc.
-@REM *****************************************************************************
-
-@echo off
-
-REM  Setup the ibl build environment if using cygwin for build
-
-REM Modify following lines based on target environment for the toolset installed 
-REM Dependency is related to path for Cygwin and CGEN installed
-
-REM Specify the path to cygwin binaries and the code gen tools
-REM If the path has directory names with spaces use the below format to specify
-REM for e.g PATH=G:\cygwin\bin;C:\PROGRA~1\TEXASI~1\C6000C~1.12\bin
-set PATH=G:\cygwin\bin;t:\c6xx\cgen6_1_12\c6000\cgtools\bin
-
-REM Specify the base directory of the c6000 compiler with UNIX style path separator
-set TOOLSC6X=t:/c6xx/cgen6_1_12/c6000/cgtools
-
-REM Specify the base directory of the c6000 compiler with DOS style path separator
-set TOOLSC6XDOS=t:\c6xx\cgen6_1_12\c6000\cgtools
-
-REM # Don't modify the below variables. They are derived from the above definitions 
-set PATH=%PATH%;%SystemRoot%\system32;%SystemRoot%;
-set BISONSKEL=yacc.c
-
-