Updated romparse utility to specify device address
authorMike Line <m-line1@ti.com>
Wed, 20 Oct 2010 22:52:17 +0000 (18:52 -0400)
committerMike Line <m-line1@ti.com>
Wed, 20 Oct 2010 22:52:17 +0000 (18:52 -0400)
The romparse utility was updated to handle the c6455 case. Here the i2c
parameter table always lives at i2c address 0x50, the little endian image
lives at 0x50, but the big endian image lives at 0x51. The change allows the
specification of the i2c device address instead of a file name, so
manual placement of the image can be done.


No differences found