/****************************************************************************** * FILE PURPOSE: Build description for the iolink Driver ****************************************************************************** * FILE NAME: package.bld * * DESCRIPTION: * This file contains the build specification and description for the iolink driver * * The file takes the following parameters from the command line through the * XDCARGS variable. * XDCARGS[0] = Driver Install Type * Valid Values are "TAR" or "SETUP" * DEFAULT is "SETUP" * * Example for a valid command: * xdc XDCARGS="SETUP" release * * Copyright (C) 2018, Texas Instruments, Inc. *****************************************************************************/ /* List of all subdirectories that combine to make the iolink Socket Driver Package. */ var subDirectories = [ "src", "docs", "soc", "test", "firmware" ]; var driverInstallType; /* Determine if we need to create the InstallJammer Application or not? * iolink LLD Deliverables be either of the following formats: * - TAR Ball Package * - Setup Executable * DEFAULT is a SETUP Executable. */ if ((arguments[0] != "TAR") && (arguments[0] != "SETUP")) driverInstallType = "TAR"; else driverInstallType = arguments[0]; /* Irrespective of the InstallType we always create a TAR Ball Package as a part * of the RTSC Build. Here we determine the name of the TAR Ball Package * Format is as follows: * iolink_ */ var iolinkRTSCFileName = "iolink" + "_" + driverReleaseVersion[0] + "_" + driverReleaseVersion[1] + "_" + driverReleaseVersion[2] + "_" + driverReleaseVersion[3]; /****************************************************************** ************************ Release Banner ************************** ******************************************************************/ print ("************* iolink Socket Driver Build Information *************"); print ("iolink Socket Driver Install : " + driverInstallType); print ("iolink Socket Driver LLD Version : " + driverReleaseVersion); print ("RTSC File Name : " + iolinkRTSCFileName); print ("iolink Socket Driver LLD Path : " + driverPath); print ("C66 Tools Directory : " + c66ToolsBaseDir); print ("M4 Tools Directory : " + m4ToolsBaseDir); print ("A15 Tools Directory : " + a15ToolsBaseDir); if (pOpts == 1) { print ("CC LE opts : " + C66LE.ccOpts.prefix); print ("CC BE opts : " + C66BE.ccOpts.prefix); print ("M4 LE opts : " + M4LE.ccOpts.prefix); print ("A15 basic opts : " + A15LE.ccOpts.prefix); } print ("****************************************************************"); /* Create the release package for the iolink LLD */ Pkg.defaultRelease = Pkg.addRelease (iolinkRTSCFileName, {prefix: "./packages/"}); /* Moving forward we need to set the Archiver of the package to be ZIP. This is currently * not supported in the XDC tools being used. Currenly builds need to be done with the * following options:- * xdc MK_FIXLISTOPTS=-t release * ZIP is a better option as it works natively with INSTALL Jammer and we can remove the * uncompression into a temporary directory. XDC Tools with xdc-rXX support the ZIP archiver. */ //Pkg.attrs = {archiver : "zip"}; /* Cycle through all the sub-directories and build all the files */ for (var i = 0; i < subDirectories.length; i++) { /* Load the capsule in the sub directory. */ var caps = xdc.loadCapsule (subDirectories[i]+"/Module.xs"); print ("Building directory " + subDirectories[i]); /* Build the capsule. */ caps.modBuild(); /* Package the module.xs files for building via package */ Pkg.otherFiles[Pkg.otherFiles.length++] = subDirectories[i]+"/Module.xs"; } /* Package the remaining files */ Pkg.otherFiles[Pkg.otherFiles.length++] = "config.bld"; Pkg.otherFiles[Pkg.otherFiles.length++] = "config_mk.bld"; Pkg.otherFiles[Pkg.otherFiles.length++] = "package.bld"; Pkg.otherFiles[Pkg.otherFiles.length++] = "package.xdc"; Pkg.otherFiles[Pkg.otherFiles.length++] = "package.xs"; Pkg.otherFiles[Pkg.otherFiles.length++] = "Settings.xdc"; Pkg.otherFiles[Pkg.otherFiles.length++] = "Settings.xdc.xdt"; Pkg.otherFiles[Pkg.otherFiles.length++] = "IOLINK.h"; Pkg.otherFiles[Pkg.otherFiles.length++] = "IOLINKver.h"; Pkg.otherFiles[Pkg.otherFiles.length++] = "IOLINKver.h.xdt"; Pkg.otherFiles[Pkg.otherFiles.length++] = "docs/Doxyfile"; Pkg.otherFiles[Pkg.otherFiles.length++] = "docs/doxyfile.xdt"; Pkg.otherFiles[Pkg.otherFiles.length++] = "build/buildlib.xs"; Pkg.otherFiles[Pkg.otherFiles.length++] = "makefile"; Pkg.otherFiles[Pkg.otherFiles.length++] = "build/makefile.mk"; Pkg.otherFiles[Pkg.otherFiles.length++] = "build/makefile_indp.mk"; Pkg.otherFiles[Pkg.otherFiles.length++] = "build/makefile_profile_indp.mk"; Pkg.otherFiles[Pkg.otherFiles.length++] = "build/makefile_profile.mk"; Pkg.otherFiles[Pkg.otherFiles.length++] = "build/makefile_icss_iolink.mk"; Pkg.otherFiles[Pkg.otherFiles.length++] = "src/src_files_common.mk"; Pkg.otherFiles[Pkg.otherFiles.length++] = "iolink_component.mk"; Pkg.otherFiles[Pkg.otherFiles.length++] = "./lib"; /* Generate Users Manual Doxyfile */ var tplt = xdc.loadTemplate("./docs/doxyfile.xdt"); tplt.genFile("./docs/Doxyfile",driverReleaseVersion); /* Generate Settings.xdc */ var tplt = xdc.loadTemplate("./Settings.xdc.xdt"); tplt.genFile("./Settings.xdc",driverReleaseVersion); /* Generate paver.h */ var tplt = xdc.loadTemplate("./IOLINKver.h.xdt"); tplt.genFile("./IOLINKver.h",driverReleaseVersion);