5 years agoMerge pull request #2 in PROCESSOR-SDK/iqn2-lld from Doc_ver_update_5.0 to master DEV.IQN_LLD.01.00.00.11 DEV.PROCESSOR-SDK.05.01.00.10 DEV.PROCESSOR-SDK.05.01.00.11 DEV.PROCESSOR-SDK.05.02.00.07 DEV.PROCESSOR-SDK.05.03.00.05 DEV.PROCESSOR-SDK.06.00.00.05
Merge pull request #2 in PROCESSOR-SDK/iqn2-lld from Doc_ver_update_5.0 to master
* commit '47e7003399642eff026a49bf4eb9686003e0f020':
Documentation and version updates for procsdk 5.0 release
* commit '47e7003399642eff026a49bf4eb9686003e0f020':
Documentation and version updates for procsdk 5.0 release
Documentation and version updates for procsdk 5.0 release
Merge pull request #1 in PROCESSOR-SDK/iqn2-lld from PRSDK-2194 to master
* commit 'ca514cbf7a0e5fef318399b275832511839881b4':
PRSDK-2194 Added RULES_MAKE macro
* commit 'ca514cbf7a0e5fef318399b275832511839881b4':
PRSDK-2194 Added RULES_MAKE macro
PRSDK-2194 Added RULES_MAKE macro
Added RULES_MAKE macro to support build based on custom Rules.make
location
Added RULES_MAKE macro to support build based on custom Rules.make
location
iqn2: update RN and iqn2ver.h for release 1.0.0.10
Signed-off-by: Hao Zhang <hzhang@ti.com>
Signed-off-by: Hao Zhang <hzhang@ti.com>
iqn2: test: fix the include path error for CSL headers
Signed-off-by: Hao Zhang <hzhang@ti.com>
Signed-off-by: Hao Zhang <hzhang@ti.com>
iqn2: modulue.xs: fix the wrong test project name
Signed-off-by: Hao Zhang <hzhang@ti.com>
Signed-off-by: Hao Zhang <hzhang@ti.com>
iqn2: k2l: rename the test project name to contain "C66"
The pdkProjectCreate script support project creation for both ARM and DSP,
The DSP project name should contain "C66"
Signed-off-by: Hao Zhang <hzhang@ti.com>
The pdkProjectCreate script support project creation for both ARM and DSP,
The DSP project name should contain "C66"
Signed-off-by: Hao Zhang <hzhang@ti.com>
support SECTTI as an environment and CGT variable update
preparing for v1.0.0.9
Merge branch 'master' of git://gtgit01.gt.design.ti.com/git/projects/iqn2-lld
cosmetic
renaming CpType None
renamed additions for the broadmarket support
Merge branch 'master' of git://gtgit01.gt.design.ti.com/git/projects/iqn2-lld
fix for custom packet size
comments
fix for custom sampling rate for broad
Merge branch 'master' of git://gtgit01.gt.design.ti.com/git/projects/iqn2-lld
add support for broad custom sampling rate
added exception disabling functions
updated test utilities for generic serdes csl
release number now using decimal numbers
8 years agoMerge branch 'master' of git://gtgit01.gt.design.ti.com/git/projects/iqn2-lld DEV.IQN_LLD.01.00.00.08C
Merge branch 'master' of git://gtgit01.gt.design.ti.com/git/projects/iqn2-lld
change comment for new function
reset static variables from iqn2 resync procedure when exception counters are reset
Merge branch 'master' of git://gtgit01.gt.design.ti.com/git/projects/iqn2-lld
fix for UL and DL translation
8 years agoChange of the DFE PLL programming to match the PLL user guide recommendations DEV.IQN_LLD.01.00.00.08B
Change of the DFE PLL programming to match the PLL user guide recommendations
8 years agoMerge branch 'master' of git://gtgit01.gt.design.ti.com/git/projects/iqn2-lld DEV.IQN_LLD.01.00.00.08A
Merge branch 'master' of git://gtgit01.gt.design.ti.com/git/projects/iqn2-lld
resetting DFE object before call to Dfe_open()
Merge branch 'master' of git://gtgit01.gt.design.ti.com/git/projects/iqn2-lld
fix for multiple strobe
fix to be able to set ictl rate control for AID2 and AIL0/1 to zero
still supported non sysbios cache apis
Merge branch 'master' of git://gtgit01.gt.design.ti.com/git/projects/iqn2-lld
more doc for 1.0.0.8
updating documentation prior to 1.0.0.8 release
add secure test to the list
add secure support in regression
Merge branch 'master' of git://gtgit01.gt.design.ti.com/git/projects/iqn2-lld
change the way that dio engine is supported to enable LTE dio mode
manual merge
added custom parameter in radio timer object for Wcdma mode, to be able to set up TTI ticks bigger than 10ms
addd test case for lte dio
add support for lte dio mode
9 years agoreversed the order of operations to disable the iqn2 and dfe power domains DEV.IQN_LLD.01.00.00.07A
reversed the order of operations to disable the iqn2 and dfe power domains
Defined DFE LLD object in sysbios tests to fix the system tests
AT clocked from Dfe if AID is enabled
fix in DIO SI to take into account the egress and ingress direction inversion
releasing iqn2 lld v1.0.0.7
Merge branch 'master' of git://gtgit01.gt.design.ti.com/git/projects/iqn2-lld
change from float to uint32_t for custom sample rate
Merge branch 'master' of git://gtgit01.gt.design.ti.com/git/projects/iqn2-lld
Change on Dfe exceoption reporting
added support for custom sample rate
merge
9 years agochanges in test code following debugging of cpp dma from arm linux rfsdk2 DEV.IQN_LLD.01.00.00.06
changes in test code following debugging of cpp dma from arm linux rfsdk2
Merge branch 'master' of git://gtgit01.gt.design.ti.com/git/projects/iqn2-lld
getting 1.0.0.6 release ready
added new ingress cell id property of AxC object in the spec
doxygen change
Merge branch 'master' of git://gtgit01.gt.design.ti.com/git/projects/iqn2-lld
changed fifo depth in iqn2 pktdma for test utilities
changed iq order for Wcdma channels in AID2
document the changes for multi strobe support
Merge branch 'master' of git://gtgit01.gt.design.ti.com/git/projects/iqn2-lld
adding cellId for ingress in order to do dual strobe
Merge branch 'master' of git://gtgit01.gt.design.ti.com/git/projects/iqn2-lld
adding pktdma status information to the test utilities
fix merge
add CB ctl support in AID test
host packet descriptors for CTL traffic with AID2 works only if the packet descriptors are located in DSP local L2
Merge branch 'master' of git://gtgit01.gt.design.ti.com/git/projects/iqn2-lld
changed the per-channel exceptions to report current error status instead of accumulated errors
Merge branch 'master' of git://gtgit01.gt.design.ti.com/git/projects/iqn2-lld
changing test code to reflect the resync procedure change
updated spec to reflect the changes on the sync procedure
Merge branch 'master' of git://gtgit01.gt.design.ti.com/git/projects/iqn2-lld
during resync procedure, do not re-enable radio timers, and let the application do it at the appropriate point of time
fixes for AID2 CTL channels when used for power meters with host packet descriptors
fixed data swap issue for AID2 CTL channels
fix in IQN2_resyncProcedure() on offset calculations
debugging power meters via CPP DMA
for TAC, block address stride of DIO egress (field DMA_BLK_ADDR_STRIDE of the register DIO2_E_DMA_CFG1) needs to be set to 0
fix pdk build issues
fix warning in aid.c
merge changes for CPPDMA
support for CPPDMA
coverity fix
fix in iqn2fl for dio reconfiguration
fix following system testing
fix following initial tests with Dfe exception monitoring
updating documentation for release 1.0.0.5
AID2: now using AID2_UAT_EVT_RADT_CMP_CFG to implement egress and ingress delay compensation because ingress axc offset in AID2 is only a 2-bit field, which is not enough for LTE PHY
changed lld version number
spec update with the 2 new Inq2Fl APIs
added 2 new Iqn2Fl APIs to reconfigure either egress or ingress DIO2 engine (to be used by WCDMA PHY)
addition OSAL functions for RM module
fix post local regression suite on sysbios