summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 1234f95)
raw | patch | inline | side by side (parent: 1234f95)
author | Sandeep Nair <sandeep_n@ti.com> | |
Tue, 24 Apr 2012 15:12:07 +0000 (11:12 -0400) | ||
committer | Sandeep Nair <sandeep_n@ti.com> | |
Tue, 24 Apr 2012 15:12:07 +0000 (11:12 -0400) |
doc/Release.txt | patch | blob | history | |
mad-loader/README.txt | patch | blob | history | |
mad-loader/examples/build_examples_msys.sh | patch | blob | history |
diff --git a/doc/Release.txt b/doc/Release.txt
index 98054b25580576e96b212ee1c5e5c19b373e3e3d..7f1607292333d46290108e86484427fb9ef0fe01 100644 (file)
--- a/doc/Release.txt
+++ b/doc/Release.txt
MAD Utils User guide is available at:
http://processors.wiki.ti.com/index.php/MAD_Utils_User_Guide
+Changes in release 01.00.01.00:
+------------------------------
+1. Added support for C6657 device
+
Changes in release 01.00.00.05:
------------------------------
1. MAP tool now creates a CCS GEL file which enables symbolic debugging of the
diff --git a/mad-loader/README.txt b/mad-loader/README.txt
index 9da7790ddf0fac1cec960480d45967989c0d3757..77ff7b304e7846efa06862e53c42219c2cc294f0 100644 (file)
--- a/mad-loader/README.txt
+++ b/mad-loader/README.txt
- ./build_loader_lnx.sh device_name
For big endian build the script is invoked as:
- ./build_loader_lnx.sh device_name big
-where device name can be C6670 or C6678
+where device name can be C6670/C6678/C6657
Example applications:
supported device numbers are
C6670
C6678
+ C6657
MAD loader application:
-----------------------
supported device numbers are
C6670
C6678
+ C6657
NOTE: MAD loader application needs to be XIP (eXecute In Place) in DDR. The linker command file
"lnk_<device number>.cmd" is used to ensure that the MAD loader app is bound to XIP address in DDR.
supported device numbers are
C6670
C6678
+ C6657
NOTE: Since NML is XIP in DDR, it has to be ensured that the NML code segments are bound to virtual address
which is XIP in DDR. NML is a part of the ROM file system loaded on DDR. if the offset of the
diff --git a/mad-loader/examples/build_examples_msys.sh b/mad-loader/examples/build_examples_msys.sh
index 80fe14373b517e894ea17d164773bc9e088b4b50..0f83f240f56a572cf7a1d021abe1363191215a9d 100755 (executable)
\r
export C_DIR='"C:/Program Files/Texas Instruments/C6000 Code Generation Tools 7.2.4"'\r
\r
-export PATH=/c/Program\ Files/Texas\ Instruments/C6000\ Code\ Generation\ Tools\ 7.2.4/bin:$PATH\r
+export PATH=$PATH:/c/Program\ Files/Texas\ Instruments/C6000\ Code\ Generation\ Tools\ 7.2.4/bin\r
\r
mkdir -p bin/$1/$endian\r
\r