updating mcbsp driver to take tx data delay into account
[keystone-rtos/mcbsp-lld.git] / mcbsp_osal.h
1 /**
2  *   @file  mcbsp_osal.h
3  *
4  *   @brief   
5  *      This is the sample OS Adaptation layer which is used by the MCBSP
6  *      driver. The OSAL layer can be ported in either of the following 
7  *      manners to a native OS:
8  *
9  *      <b> Approach 1: </b>
10  *      @n  Use Prebuilt Libraries
11  *           - Ensure that the provide an implementation of all 
12  *             Osal_XXX API for their native OS.
13  *           - Link the prebuilt libraries with their application.
14  *           - Refer to the "example" directory for an example of this
15  *       @n <b> Pros: </b>
16  *           - Customers can reuse prebuilt TI provided libraries
17  *       @n <b> Cons: </b>
18  *           - Level of indirection in the API to get to the actual OS call
19  *              
20  *      <b> Approach 2: </b>
21  *      @n  Rebuilt Library 
22  *           - Create a copy of this file and modify it to directly 
23  *             inline the native OS calls
24  *           - Rebuild the MCBSP Driver library; ensure that the Include 
25  *             path points to the directory where the copy of this file 
26  *             has been provided.
27  *           - Please refer to the "test" directory for an example of this 
28  *       @n <b> Pros: </b>
29  *           - Optimizations can be done to remove the level of indirection
30  *       @n <b> Cons: </b>
31  *           - MCBSP Libraries need to be rebuilt by the customer.
32  *
33  *  \par
34  *  NOTE:
35  *      (C) Copyright 2012 Texas Instruments, Inc.
36  * 
37  *  Redistribution and use in source and binary forms, with or without 
38  *  modification, are permitted provided that the following conditions 
39  *  are met:
40  *
41  *    Redistributions of source code must retain the above copyright 
42  *    notice, this list of conditions and the following disclaimer.
43  *
44  *    Redistributions in binary form must reproduce the above copyright
45  *    notice, this list of conditions and the following disclaimer in the 
46  *    documentation and/or other materials provided with the   
47  *    distribution.
48  *
49  *    Neither the name of Texas Instruments Incorporated nor the names of
50  *    its contributors may be used to endorse or promote products derived
51  *    from this software without specific prior written permission.
52  *
53  *  THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS 
54  *  "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT 
55  *  LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
56  *  A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT 
57  *  OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, 
58  *  SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT 
59  *  LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
60  *  DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
61  *  THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT 
62  *  (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE 
63  *  OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
64  *
65  *  \par
66 */
67 #ifndef __MCBSP_OSAL_H__
68 #define __MCBSP_OSAL_H__
70 #include <string.h>
71 #include <ti/drv/mcbsp/mcbsp_drv.h>
73 /** @addtogroup MCBSP_OSAL_API
74  @{ */
76 /**********************************************************************
77  ************************* Extern Declarations ************************
78  **********************************************************************/
80 extern void* Osal_mcbspMalloc(uint32_t numBytes);
81 extern void  Osal_mcbspFree (void* ptr, uint32_t size);
82 extern void* Osal_mcbspDataBufferMalloc(uint32_t numBytes);
83 extern void  Osal_mcbspDataBufferFree(void* ptr, uint32_t numBytes);
84 extern void  Osal_mcbspLog(char* fmt, ... );
85 extern void* Osal_mcbspCreateSem(void);
86 extern void  Osal_mcbspDeleteSem(void* semHandle);
87 extern void  Osal_mcbspPendSem(void* semHandle);
88 extern void  Osal_mcbspPostSem(void* semHandle);
89 extern void* Osal_mcbspEnterMultipleCoreCriticalSection(void);
90 extern void  Osal_mcbspExitMultipleCoreCriticalSection(void* critSectHandle);
91 extern void* Osal_mcbspEnterSingleCoreCriticalSection();
92 extern void  Osal_mcbspExitSingleCoreCriticalSection(void* critSectHandle);
93 extern void  Osal_mcbspBeginMemAccess(void* ptr, uint32_t size);
94 extern void  Osal_mcbspEndMemAccess(void* ptr, uint32_t size);
96 extern Bool  Osal_mcbspQueueEmpty(void* handle);
97 extern void* Osal_mcbspQueueGet(void* handle);
98 extern void  Osal_mcbspQueuePut(void* handle, Mcbsp_QueueElem* elem);
99 extern void  Osal_mcbspWaitNBitClocks(uint32_t nticks);
100 extern void *Osal_local2Global (void *addr);
101 /**
102  * @brief   The macro is used by the MCBSP driver to create a semaphore for 
103  * each MCBSP socket opened in blocking mode. Semaphores created should 
104  * *initially* be created with a count of 0 i.e. unavailable. 
105  *
106  * <b> Prototype: </b>
107  *  The following is the C prototype for the expected OSAL API.
108  *
109  *  @verbatim
110        void* Osal_mcbspCreateSem(void);
111     @endverbatim
112  *
113  *  <b> Parameter </b>
114  *  @n Not Applicable
115  *
116  *  <b> Return Value </b>
117  *  @n Semaphore Handle
118  */
119 #define Mcbsp_osalCreateSem()        Osal_mcbspCreateSem()
121 /**
122  * @brief   The macro is used by the MCBSP driver to delete a previously 
123  * created semaphore. This is called when a MCBSP socket opened in blocking mode
124  * is being closed.
125  *
126  * <b> Prototype: </b>
127  *  The following is the C prototype for the expected OSAL API.
128  *
129  *  @verbatim
130        void Osal_mcbspDeleteSem(void* semHandle)
131     @endverbatim
133  *  <b> Parameter </b>
134  *  @n  Semaphore Handle returned by the create semaphore
135  *
136  *  <b> Return Value </b>
137  *  @n  Not Applicable
138  */
139 #define Mcbsp_osalDeleteSem(X)       Osal_mcbspDeleteSem(X)
141 /**
142  * @brief   The macro is used by the MCBSP driver to pend on a semaphore
143  * This is called when an application tries to receive data on a blocking
144  * socket when there is no data available. Since all semaphores are initially
145  * created to be unavailable; this will cause the application to block.
146  *
147  * <b> Prototype: </b>
148  *  The following is the C prototype for the expected OSAL API.
149  *
150  *  @verbatim
151        void Osal_mcbspPendSem(void* semHandle)
152     @endverbatim
153  *
154  *  <b> Parameter </b>
155  *  @n  Semaphore Handle
156  *
157  *  <b> Return Value </b>
158  *  @n  Not Applicable
159  */
160 #define Mcbsp_osalPendSem(X)         Osal_mcbspPendSem(X)
162 /**
163  * @brief   The macro is used by the MCBSP driver to post the semaphore
164  * The driver posts the semaphore once data is received on a specific 
165  * socket.  
166  *
167  * <b> Prototype: </b>
168  *  The following is the C prototype for the expected OSAL API.
169  *
170  *  @verbatim
171        void Osal_mcbspPostSem(void* semHandle)
172     @endverbatim
173  *      
174  *  <b> Parameter </b>
175  *  @n  Semaphore Handle
176  *
177  *  <b> Return Value </b>
178  *  @n  Not Applicable
179  */
180 #define Mcbsp_osalPostSem(X)     Osal_mcbspPostSem(X)
182 /**
183  * @brief   The macro is used by the MCBSP driver to allocate memory
184  * The MCBSP driver uses this macro to allocate memory for its internal 
185  * driver structures. This is invoked during the driver initialization
186  * and startup process.
187  *
188  * <b> Prototype: </b>
189  *  The following is the C prototype for the expected OSAL API.
190  *
191  *  @verbatim
192        void* Osal_mcbspMalloc(uint32_t numBytes)
193     @endverbatim
194  *      
195  *  <b> Parameter </b>
196  *  @n  Number of bytes to be allocated
197  *
198  *  <b> Return Value </b>
199  *  @n  Pointer to the allocated block size
200  *
201  *  @sa
202  *      Mcbsp_osalDataBufferMalloc
203  */
204 #define Mcbsp_osalMalloc(X)      Osal_mcbspMalloc(X)
206 /**
207  * @brief   The macro is used by the MCBSP driver to free a previously
208  * allocated block of memory
209  *
210  * <b> Prototype: </b>
211  *  The following is the C prototype for the expected OSAL API.
212  *
213  *  @verbatim
214        void Osal_mcbspFree(void* ptr, uint32_t numBytes)
215     @endverbatim
216  *      
217  *  <b> Parameter </b>
218  *  @n  Pointer to the block of memory to be cleaned up.
219  *  @n  Size of the allocated memory which is being freed.
220  *
221  *  <b> Return Value </b>
222  *  @n  Not applicable.
223  */
224 #define Mcbsp_osalFree(X, Y)     Osal_mcbspFree(X, Y)
226 /**
227  * @brief   The macro is used by the MCBSP driver to allocate memory
228  * for the data buffers in Driver Managed Configuration. All data
229  * buffers should allocated should be in the global address space. 
230  * This macro is invoked during the data path.
231  *
232  * <b> Prototype: </b>
233  *  The following is the C prototype for the expected OSAL API.
234  *
235  *  @verbatim
236        void* Osal_mcbspDataBufferMalloc(uint32_t numBytes)
237     @endverbatim
238  *      
239  *  <b> Parameter </b>
240  *  @n  Number of bytes to be allocated
241  *
242  *  <b> Return Value </b>
243  *  @n  Pointer to the allocated block size
244  */
245 #define Mcbsp_osalDataBufferMalloc(X)      Osal_mcbspDataBufferMalloc(X)
247 /**
248  * @brief   The macro is used by the MCBSP driver to convert local address
249  * to Global address space
250  *
251  * <b> Prototype: </b>
252  *  The following is the C prototype for the expected OSAL API.
253  *
254  *  @verbatim
255        void *Osal_local2Global (void *addr)
256     @endverbatim
257  *      
258  *  <b> Parameter </b>
259  *  @n  Local address pointer
260  *
261  *  <b> Return Value </b>
262  *  @n  Global address pointer
263  */
265 #define Mcbsp_osalLocal2Global(X) Osal_local2Global(X)
266 /**
267  * @brief   The macro is used by the MCBSP driver to free a previously
268  * allocated block data buffer. This macro is used to clean up previously
269  * allocated data buffers and is invoked during the data path.
270  *
271  * <b> Prototype: </b>
272  *  The following is the C prototype for the expected OSAL API.
273  *
274  *  @verbatim
275        void Osal_mcbspDataBufferFree(void* ptr, uint32_t numBytes)
276     @endverbatim
277  *      
278  *  <b> Parameter </b>
279  *  @n  Pointer to the block of memory to be cleaned up.
280  *  @n  Size of the allocated memory which is being freed.
281  *
282  *  <b> Return Value </b>
283  *  @n  Not applicable.
284  */
285 #define Mcbsp_osalDataBufferFree(X, Y)     Osal_mcbspDataBufferFree(X, Y)
287 /**
288  * @brief   The macro is used by the MCBSP driver to log various 
289  * messages. 
290  *
291  * <b> Prototype: </b>
292  *  The following is the C prototype for the expected OSAL API.
293  *
294  *  @verbatim
295        void Osal_mcbspLog( char* fmt, ... ) 
296     @endverbatim
297  *
298  *  <b> Parameter </b>
299  *  @n  printf-style format string 
300  *
301  *  <b> Return Value </b>
302  *  @n  Not applicable.
303  */
304 #define Mcbsp_osalLog            Osal_mcbspLog
306 /**
307  * @brief   The macro is used by the MCBSP Driver to protect its shared resources
308  * access from MULTIPLE CORES. This is required if the MCBSP Driver API's are being
309  * invoked from multiple cores. If this is not the case then these macros can be
310  * defined to be NOP.
311  *
312  * <b> Prototype: </b>
313  *  The following is the C prototype for the expected OSAL API.
314  *
315  *  @verbatim
316        void* Osal_mcbspEnterMultipleCoreCriticalSection(void)
317     @endverbatim
318  *
319  *  <b> Parameter </b>
320  *  @n  None
321  *
322  *  <b> Return Value </b>
323  *  @n  Opaque Handle used for holding critical section locking information
324  */
325 #define Mcbsp_osalEnterMultipleCoreCriticalSection      Osal_mcbspEnterMultipleCoreCriticalSection
327 /**
328  * @brief   The macro is used by the MCBSP driver to end the protection of its 
329  * internal shared "resources" from MULTIPLE CORE access.
330  *
331  * <b> Prototype: </b>
332  *  The following is the C prototype for the expected OSAL API.
333  *
334  *  @verbatim
335        void  Osal_mcbspExitMultipleCoreCriticalSection(void* critSectHandle)
336     @endverbatim
337  *
338  *  <b> Parameter </b>
339  *  @n  Opaque Handle used for holding critical section locking information
340  *
341  *  <b> Return Value </b>
342  *  @n  None
343  */
344 #define Mcbsp_osalExitMultipleCoreCriticalSection      Osal_mcbspExitMultipleCoreCriticalSection
346 /**
347  * @brief   The macro is used by the MCBSP driver to protect its internal shared
348  * resources from SINGLE CORE MULTIPLE CONTEXT (thread or ISR) access. If all 
349  * the MCBSP Driver APIs are being called from threads then this API could 
350  * use semaphores. However if the MCBSP driver API's are being called from 
351  * both ISR & Thread context then the critical section here would need to 
352  * disable/enable interrupts. 
353  *
354  * <b> Prototype: </b>
355  *  The following is the C prototype for the expected OSAL API.
356  *
357  *  @verbatim
358        void* Osal_mcbspEnterSingleCoreCriticalSection()
359     @endverbatim
360  *
361  *  <b> Parameter </b>
362  *  @n  None
363  *
364  *  <b> Return Value </b>
365  *  @n  Opaque Handle used for holding critical section locking information
366  */
367 #define Mcbsp_osalEnterSingleCoreCriticalSection     Osal_mcbspEnterSingleCoreCriticalSection
369 /**
370  * @brief   The macro is used to denote the end of the protection of the internal
371  * shared resource from SINGLE CORE MULTIPLE CONTEXT access.
372  *
373  * <b> Prototype: </b>
374  *  The following is the C prototype for the expected OSAL API.
375  *
376  *  @verbatim
377        void  Osal_mcbspExitSingleCoreCriticalSection(void* critSectHandle)
378     @endverbatim
379  *
380  *  <b> Parameter </b>
381  *  @n  critSectHandle - Opaque Handle used for holding critical section locking information
382  *
383  *  <b> Return Value </b>
384  *  @n  None
385  */
386 #define Mcbsp_osalExitSingleCoreCriticalSection      Osal_mcbspExitSingleCoreCriticalSection
388 /**
389  * @brief   The macro is used by the MCBSP driver to indicate that a block
390  * of memory is about to be accessed. If the memory block is cached then
391  * this indicates that the application would need to ensure that the cache
392  * is updated with the data from the actual memory.
393  *
394  * <b> Prototype: </b>
395  *  The following is the C prototype for the expected OSAL API.
396  *
397  *  @verbatim
398        void  Osal_mcbspBeginMemAccess(void* ptr, uint32_t size)
399     @endverbatim
400  *
401  *  <b> Parameter </b>
402  *  @n  ptr  - Pointer to the memory
403  *  @n  size - Size of the memory being accessed.
404  *
405  *  <b> Return Value </b>
406  *  @n  None
407  */
408 #define Mcbsp_osalBeginMemAccess      Osal_mcbspBeginMemAccess
410 /**
411  * @brief   The macro is used by the MCBSP driver to indicate that  the block of 
412  * memory has finished being accessed. If the memory block is cached then the 
413  * application would need to ensure that the contents of the cache are updated
414  * immediately to the actual memory.
415  *
416  * <b> Prototype: </b>
417  *  The following is the C prototype for the expected OSAL API.
418  *
419  *  @verbatim
420        void  Osal_mcbspEndMemAccess(void* ptr, uint32_t size)
421     @endverbatim
422  *
423  *  <b> Parameter </b>
424  *  @n  ptr  - Pointer to the memory 
425  *  @n  size - Size of the memory
426  *
427  *  <b> Return Value </b>
428  *  @n  None
429  */
430 #define Mcbsp_osalEndMemAccess       Osal_mcbspEndMemAccess
432 /**
433  * @brief   The macro is used by the MCBSP driver to test for an 
434  *          empty queue.
435  *
436  * <b> Prototype: </b>
437  *  The following is the C prototype for the expected OSAL API.
438  *
439  *  @verbatim
440        void  Osal_mcbspQueueEmpty(void* handle)
441     @endverbatim
442  *
443  *  <b> Parameter </b>
444  *  @n  handle - Handle of a previously created Queue instance object 
445  *
446  *  <b> Return Value </b>
447  *  @n  TRUE - If the queue is empty
448  */
449 #define Mcbsp_osalQueueEmpty         Osal_mcbspQueueEmpty
451 /**
452  * @brief   The macro is used by the MCBSP driver to get an 
453  *          element from the front of queue. The function 
454  *          removes the element from the front of queue and
455  *          returns a pointer to it.
456  *
457  * <b> Prototype: </b>
458  *  The following is the C prototype for the expected OSAL API.
459  *
460  *  @verbatim
461        void*  Osal_mcbspQueueGet(void* handle)
462     @endverbatim
463  *
464  *  <b> Parameter </b>
465  *  @n  handle - Handle of a previously created Queue instance object 
466  *
467  *  <b> Return Value </b>
468  *  @n  Handle (pointer) to former first element
469  */
470 #define Mcbsp_osalQueueGet           Osal_mcbspQueueGet
472 /**
473  * @brief   The macro is used by the MCBSP driver to put an 
474  *          element at the end of queue. 
475  *
476  * <b> Prototype: </b>
477  *  The following is the C prototype for the expected OSAL API.
478  *
479  *  @verbatim
480        void Osal_mcbspQueuePut(void* handle, Mcbsp_QueueElem* elem)
481     @endverbatim
482  *
483  *  <b> Parameter </b>
484  *  @n  handle - Handle of a previously created Queue instance object 
485  *  @n  elem - Pointer to new queue element 
486  *
487  *  <b> Return Value </b>
488  *  @n  None
489  */
490 #define Mcbsp_osalQueuePut           Osal_mcbspQueuePut
492 /**
493  * @brief   The macro is used by the MCBSP driver to wait 'n' 
494  *          bit clocks to ensure proper synchronization internally. 
495  *
496  * <b> Prototype: </b>
497  *  The following is the C prototype for the expected OSAL API.
498  *
499  *  @verbatim
500        void Osal_mcbspWaitNBitClocks(uint32_t nticks)
501     @endverbatim
502  *
503  *  <b> Parameter </b>
504  *  @n  nticks - Number of bit clocks to wait 
505  *
506  *  <b> Return Value </b>
507  *  @n  None
508  */
509 #define Mcbsp_osalWaitNBitClocks     Osal_mcbspWaitNBitClocks
510 /**
511 @}
512 */
514 #endif /* __MCBSP_OSAL_H__ */