1 /******************************************************************************
2 * FILE PURPOSE: Build description for the MCBSP Driver
3 ******************************************************************************
4 * FILE NAME: package.bld
5 *
6 * DESCRIPTION:
7 * This file contains the build specification and description for the MCBSP driver
8 *
9 * The file takes the following parameters from the command line through the
10 * XDCARGS variable.
11 * XDCARGS[0] = MCBSP Driver Install Type
12 * Valid Values are "TAR" or "SETUP"
13 * DEFAULT is "SETUP"
14 *
15 * Example for a valid command:
16 * xdc XDCARGS="SETUP" release
17 *
18 * Copyright (C) 2012, Texas Instruments, Inc.
19 *****************************************************************************/
21 /* List of all subdirectories that combine to make the MCBSP Driver Package. */
22 var subDirectories = [ "src", "docs", "include","device","example" ];
24 var mcbspDriverInstallType;
26 /* Determine if we need to create the InstallJammer Application or not?
27 * MCBSP LLD Deliverables be either of the following formats:
28 * - TAR Ball Package
29 * - Setup Executable
30 * DEFAULT is a SETUP Executable. */
32 if ((arguments[0] != "TAR") && (arguments[0] != "SETUP"))
33 mcbspDriverInstallType = "TAR";
34 else
35 mcbspDriverInstallType = arguments[0];
37 /* Irrespective of the InstallType we always create a TAR Ball Package as a part
38 * of the RTSC Build. Here we determine the name of the TAR Ball Package
39 * Format is as follows:
40 * mcbsp_<version> */
41 var mcbspRTSCFileName = "mcbsp" + "_" +
42 mcbspDriverReleaseVersion[0] + "_" + mcbspDriverReleaseVersion[1] + "_" +
43 mcbspDriverReleaseVersion[2] + "_" + mcbspDriverReleaseVersion[3];
45 /******************************************************************
46 ************************ Release Banner **************************
47 ******************************************************************/
49 print ("************* MCBSP Driver Build Information *************");
50 print ("MCBSP Driver Install : " + mcbspDriverInstallType);
51 print ("MCBSP Driver LLD Version : " + mcbspDriverReleaseVersion);
52 print ("Tools Directory : " + toolsBaseDir);
53 print ("RTSC File Name : " + mcbspRTSCFileName);
54 print ("MCBSP Driver LLD Path : " + driverPath);
55 if (pOpts == 1)
56 {
57 print ("CC LE opts : " + C66LE.ccOpts.prefix);
58 print ("CC BE opts : " + C66BE.ccOpts.prefix);
59 print ("****************************************************************");
60 }
62 /* Create the release package for the MCBSP LLD */
63 Pkg.defaultRelease = Pkg.addRelease (mcbspRTSCFileName, {prefix: "./packages/"});
65 /* Moving forward we need to set the Archiver of the package to be ZIP. This is currently
66 * not supported in the XDC tools being used. Currenly builds need to be done with the
67 * following options:-
68 * xdc MK_FIXLISTOPTS=-t release
69 * ZIP is a better option as it works natively with INSTALL Jammer and we can remove the
70 * uncompression into a temporary directory. XDC Tools with xdc-rXX support the ZIP archiver. */
71 //Pkg.attrs = {archiver : "zip"};
73 /* Cycle through all the sub-directories and build all the files */
74 for (var i = 0; i < subDirectories.length; i++)
75 {
76 /* Load the capsule in the sub directory. */
77 var caps = xdc.loadCapsule (subDirectories[i]+"/Module.xs");
79 print ("Building directory " + subDirectories[i]);
81 /* Build the capsule. */
82 caps.modBuild();
84 /* Package the module.xs files for building via package */
85 Pkg.otherFiles[Pkg.otherFiles.length++] = subDirectories[i]+"/Module.xs";
86 }
88 /* Package the remaining files */
89 Pkg.otherFiles[Pkg.otherFiles.length++] = "config.bld";
90 Pkg.otherFiles[Pkg.otherFiles.length++] = "config_mk.bld";
91 Pkg.otherFiles[Pkg.otherFiles.length++] = "package.bld";
92 Pkg.otherFiles[Pkg.otherFiles.length++] = "package.xdc";
93 Pkg.otherFiles[Pkg.otherFiles.length++] = "package.xs";
94 Pkg.otherFiles[Pkg.otherFiles.length++] = "Settings.xdc";
95 Pkg.otherFiles[Pkg.otherFiles.length++] = "Settings.xdc.xdt";
96 Pkg.otherFiles[Pkg.otherFiles.length++] = "mcbsp_drv.h";
97 Pkg.otherFiles[Pkg.otherFiles.length++] = "mcbsp_osal.h";
98 Pkg.otherFiles[Pkg.otherFiles.length++] = "mcbsp_types.h";
99 Pkg.otherFiles[Pkg.otherFiles.length++] = "mcbspver.h";
100 Pkg.otherFiles[Pkg.otherFiles.length++] = "mcbspver.h.xdt";
101 Pkg.otherFiles[Pkg.otherFiles.length++] = "docs/Doxyfile";
102 Pkg.otherFiles[Pkg.otherFiles.length++] = "docs/doxyfile.xdt";
103 Pkg.otherFiles[Pkg.otherFiles.length++] = "build/buildlib.xs";
104 Pkg.otherFiles[Pkg.otherFiles.length++] = "makefile";
105 Pkg.otherFiles[Pkg.otherFiles.length++] = "build/makefile.mk";
106 Pkg.otherFiles[Pkg.otherFiles.length++] = "src/src_files_common.mk";
107 Pkg.otherFiles[Pkg.otherFiles.length++] = "mcbsp_component.mk";
109 /* Generate Users Manual Doxyfile */
110 var tplt = xdc.loadTemplate("./docs/doxyfile.xdt");
111 tplt.genFile("./docs/Doxyfile",mcbspDriverReleaseVersion);
113 /* Generate Settings.xdc */
114 var tplt = xdc.loadTemplate("./Settings.xdc.xdt");
115 tplt.genFile("./Settings.xdc",mcbspDriverReleaseVersion);
117 /* Generate paver.h */
118 var tplt = xdc.loadTemplate("./mcbspver.h.xdt");
119 tplt.genFile("./mcbspver.h",mcbspDriverReleaseVersion);