/* * sample_init.c * * Sample Initialization for the EDMA3 Driver for BIOS 6 based applications. * It should be MANDATORILY done once before EDMA3 usage. * * Copyright (C) 2009 Texas Instruments Incorporated - http://www.ti.com/ * * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the * distribution. * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR * A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT * OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, * SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT * LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, * DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY * THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT * (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. * */ #include #include #include #include /** @brief EDMA3 Driver Instance specific Semaphore handle */ extern EDMA3_OS_Sem_Handle semHandle[EDMA3_MAX_EDMA3_INSTANCES]; /** To Register the ISRs with the underlying OS, if required. */ extern void registerEdma3Interrupts (uint32_t edma3Id); /** To Unregister the ISRs with the underlying OS, if previously registered. */ extern void unregisterEdma3Interrupts (uint32_t edma3Id); /* To find out the DSP# */ extern uint16_t determineProcId(void); /** * To check whether the global EDMA3 configuration is required or not. * It should be done ONCE by any of the masters present in the system. * This function checks whether the global configuration is required by the * current master or not. In case of many masters, it should be done only * by one of the masters. Hence this function will return TRUE only once * and FALSE for all other masters. */ extern uint16_t isGblConfigRequired(uint32_t dspNum); /** * DSP instance number on which the executable is running. Its value is * determined by reading the processor specific register DNUM. */ uint32_t dsp_num; /** * Shadow Region on which the executable is runnig. Its value is populated * with the DSP Instance Number here in this case. */ uint32_t region_id; /* Number of EDMA3 controllers present in the system */ extern const uint32_t numEdma3Instances; /* External Global Configuration Structure */ extern EDMA3_DRV_GblConfigParams sampleEdma3GblCfgParams[EDMA3_MAX_EDMA3_INSTANCES]; /* External Instance Specific Configuration Structure */ extern EDMA3_DRV_InstanceInitConfig sampleInstInitConfig[EDMA3_MAX_EDMA3_INSTANCES][EDMA3_MAX_REGIONS]; #ifdef DMA_XBAR_AVAILABLE extern EDMA3_DRV_Result sampleInitXbarEvt(EDMA3_DRV_Handle hEdma, uint32_t edma3Id); #endif /** * \brief EDMA3 Initialization * * This function initializes the EDMA3 Driver and registers the * interrupt handlers. * * \return EDMA3_DRV_SOK if success, else error code */ EDMA3_DRV_Handle edma3init (uint32_t edma3Id, EDMA3_DRV_Result *errorCode) { EDMA3_DRV_Result edma3Result = EDMA3_DRV_E_INVALID_PARAM; Semaphore_Params semParams; EDMA3_DRV_GblConfigParams *globalConfig = NULL; EDMA3_DRV_InitConfig initCfg; EDMA3_RM_MiscParam miscParam; EDMA3_DRV_Handle hEdma = NULL; if ((edma3Id >= numEdma3Instances) || (errorCode == NULL)) { hEdma = NULL; } else { /* DSP instance number */ dsp_num = determineProcId(); globalConfig = &sampleEdma3GblCfgParams[edma3Id]; /* Configure it as master, if required */ miscParam.isSlave = isGblConfigRequired(dsp_num); edma3Result = EDMA3_DRV_create (edma3Id, globalConfig , (void *)&miscParam); if (edma3Result == EDMA3_DRV_SOK) { /** * Driver Object created successfully. * Create a semaphore now for driver instance. */ Semaphore_Params_init(&semParams); initCfg.drvSemHandle = NULL; edma3Result = edma3OsSemCreate((int32_t)1, &semParams, &initCfg.drvSemHandle); } if (edma3Result == EDMA3_DRV_SOK) { /* Save the semaphore handle for future use */ semHandle[edma3Id] = initCfg.drvSemHandle; /* Driver instance specific config NULL */ initCfg.drvInstInitConfig = NULL; #ifndef EDMA3_DRV_USE_DEF_RM_CFG /* Hook for running examples with default RM config */ /* configuration structure for the Driver */ initCfg.drvInstInitConfig = &sampleInstInitConfig[edma3Id][dsp_num]; #endif initCfg.isMaster = TRUE; /* Choose shadow region according to the DSP# */ initCfg.regionId = (EDMA3_RM_RegionId)dsp_num; /*Saving the regionId for using it in the sample_cs.c file */ region_id = (EDMA3_RM_RegionId)dsp_num; /* Driver instance specific config NULL */ initCfg.gblerrCb = NULL; initCfg.gblerrData = NULL; /* Open the Driver Instance */ hEdma = EDMA3_DRV_open (edma3Id, (void *) &initCfg, &edma3Result); } #ifdef DMA_XBAR_AVAILABLE { if((hEdma != NULL) && (edma3Result == EDMA3_DRV_SOK)) { edma3Result = sampleInitXbarEvt(hEdma, edma3Id); } } #endif if((hEdma != NULL) && (edma3Result == EDMA3_DRV_SOK)) { /** * Register Interrupt Handlers for various interrupts * like transfer completion interrupt, CC error * interrupt, TC error interrupts etc, if required. */ registerEdma3Interrupts(edma3Id); } *errorCode = edma3Result; } return hEdma; } /** * \brief EDMA3 De-initialization * * This function removes the EDMA3 Driver instance and unregisters the * interrupt handlers. * * \return EDMA3_DRV_SOK if success, else error code */ EDMA3_DRV_Result edma3deinit (uint32_t edma3Id, EDMA3_DRV_Handle hEdma) { EDMA3_DRV_Result edma3Result = EDMA3_DRV_E_INVALID_PARAM; /* Unregister Interrupt Handlers first */ unregisterEdma3Interrupts(edma3Id); /* Delete the semaphore */ edma3Result = edma3OsSemDelete(semHandle[edma3Id]); if (EDMA3_DRV_SOK == edma3Result ) { /* Make the semaphore handle as NULL. */ semHandle[edma3Id] = NULL; /* Now, close the EDMA3 Driver Instance */ edma3Result = EDMA3_DRV_close (hEdma, NULL); } if (EDMA3_DRV_SOK == edma3Result ) { /* Now, delete the EDMA3 Driver Object */ edma3Result = EDMA3_DRV_delete (edma3Id, NULL); } return edma3Result; } /* End of File */