/* * mcbsp_drv.h * * This file contains Application programming interface for the Mcbsp driver and * command/macro definitions used by the Mcbsp driver. * * Copyright (C) 2012 Texas Instruments Incorporated - http://www.ti.com/ * * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the * distribution. * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR * A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT * OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, * SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT * LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, * DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY * THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT * (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. * */ /** * \file mcbsp_drv.h * * \brief McBSP driver interface definition file * * This file contains the interfaces, data types and symbolic * definitions that are needed by the application to utilize the * services of the McBSP device driver. * * (C) Copyright 2012, Texas Instruments, Inc * */ #ifndef _MCBSP_DRV_H_ #define _MCBSP_DRV_H_ /*============================================================================*/ /* INCLUDE FILES */ /*============================================================================*/ #ifdef __cplusplus extern "C" { #endif /* CSL RL includes */ #include // Freon has no cslr_device.h #include // Freon only has cslr directory #include "mcbspver.h" /*============================================================================*/ /* MACRO TYPES */ /*============================================================================*/ /** * \def MCBSP_LOOPJOB_ENABLE * To enable loop job mode support in the MCBSP driver, uncomment * following compiler switch and rebuild the MCBSP LLD. */ /* #define MCBSP_LOOPJOB_ENABLE */ /** * \def Mcbsp_POLLED_RETRYCOUNT * This macro specifies the default retry count to be used by the Mcbsp * driver when polling for any hardware bit to be set or reset. * * \note This default value used by the driver can be changed by an IOCTL * "Mcbsp_Ioctl_SET_TIMEOUT". */ #define Mcbsp_POLLED_RETRYCOUNT (0xFFFFu) /** * \def MCBSP_CACHE_LENGTH * Defines the Maximum length of cache line that is possible. */ #define MCBSP_CACHE_LENGTH (128u) /** * \def MCBSP_MAX_CACHE_ALIGN * Defines the Maximum cache line size for alignment. */ #define MCBSP_MAX_CACHE_ALIGN (128u) /** * \def MCBSP_COMPILE_TIME_SIZE_CHECK * This macro generates compiler error if postulate is false, so * allows 0 overhead compile time size check. This "works" when * the expression contains sizeof() which otherwise doesn't work * with preprocessor. */ #define MCBSP_COMPILE_TIME_SIZE_CHECK(postulate) \ do { \ typedef struct { \ uint8_t McbspNegativeSizeIfPostulateFalse[((int)(postulate))*2 - 1]; \ } McbspPostulateCheck_t; \ } \ while (0) /*============================================================================*/ /* ENUMERATED DATA TYPES */ /*============================================================================*/ /** * \brief Mcbsp device operational mode. * * This enum is used to define the operational mode of the mcbsp device * like normal mcbsp device. */ typedef enum Mcbsp_DevMode_t { Mcbsp_DevMode_McBSP = (0u) /**< Option to operate in normal McBSP mode */ }Mcbsp_DevMode; /**< Mcbsp device operational mode. */ /** * \brief Mcbsp driver operational mode * * Enumeration of the different modes of operation available for the * Mcbsp device driver.(Mcbsp driver supports only EDMA mode). */ typedef enum Mcbsp_OpMode_t { Mcbsp_OpMode_POLLED = 0, /**< Polled Mode */ Mcbsp_OpMode_INTERRUPT, /**< Interrupt Mode */ Mcbsp_OpMode_DMAINTERRUPT /**< DMA Mode */ }Mcbsp_OpMode; /**< Mcbsp driver operational mode */ /** * \brief Mcbsp Emulation mode settings * * Use this symbol to set the Emulation Mode to Free mode or any other * mode. * * \note The SOFT mode settings are applicable only is the FREE mode is * disabled.Hence if the soft mode is selected (both enable or disable) * the driver will internally disable the FREE mode. */ typedef enum Mcbsp_EmuMode_t { Mcbsp_EmuMode_SOFT_ABORT = (0u), /**< SOFT mode is disabled. */ Mcbsp_EmuMode_SOFT_STOP = (1u), /**< SOFT mode is enabled */ Mcbsp_EmuMode_FREE = (2u) /**< FREE mode is enabled */ }Mcbsp_EmuMode; /**< Mcbsp emulation modes */ /** * \brief McBSP digital loopback mode selection * * Enum to select the enable/disable of Loopback mode of the mcbsp. */ typedef enum Mcbsp_Loopback_t { Mcbsp_Loopback_DISABLE = 0, /**< loopback mode off */ Mcbsp_Loopback_ENABLE = 1 /**< loopback mode on */ } Mcbsp_Loopback; /**< McBSP digital loopback mode selection */ /** * \brief ENUM for receive data justification settings * * Use this symbol for setting up RCV sign-extension and justification * mode */ typedef enum Mcbsp_Rxjust_t { Mcbsp_RxJust_RZF = (0u), /**< RCV setting - right justify, fill MSBs with zeros */ Mcbsp_RxJust_RSE = (1u), /**< RCV setting - right justify, sign-extend the data into MSBs */ Mcbsp_RxJust_RxJUST_LZF = (2u) /**< RCV setting - left justify, fill LSBs with zeros */ }Mcbsp_Rxjust; /**< Enumeration for the Receive data justification */ /** * \brief Transmit pin mode configuration * * DX pin settings used for setting the pin in high impedance mode. */ typedef enum Mcbsp_DxEna_t { Mcbsp_DxEna_OFF = (0), /**< DX enabler is OFF */ Mcbsp_DxEna_ON = (1u) /**< DX enabler is ON */ }Mcbsp_DxEna; /**< DX pin High impedance enable/disable option */ /** * \brief Polarity of the CLKS pin * * Enum to Set the polarity of the CLKS pin used to generate Frame Sync * and bit clock */ typedef enum Mcbsp_ClkSPol_t { Mcbsp_ClkSPol_RISING_EDGE = 0, /**< Rising edge of CLKS generates CLKG and FSG. */ Mcbsp_ClkSPol_FALLING_EDGE = 1 /**< Falling edge of CLKS generates CLKG and FSG. */ }Mcbsp_ClkSPol; /**< Polarity of the CLKS pin */ /** * \brief SRG clock source * * Use this symbol to select input clock source for Sample Rate * Generator */ typedef enum Mcbsp_SrgClk_t { Mcbsp_SrgClk_CLKS = (0u), /**< input clock source for Sample Rate Generator is CLKS pin */ Mcbsp_SrgClk_CLKCPU = (1u), /**< input clock source for Sample Rate Generator is CPU */ Mcbsp_SrgClk_CLKR = (2u), /**< input clock source for Sample Rate Generator is BCLKR pin */ Mcbsp_SrgClk_CLKX = (3u) /**< input clock source for Sample Rate Generator is BCLKX pin */ }Mcbsp_SrgClk; /**< SRG clock source selection */ /** * \brief Enum to specify the supported buffer formats. * * Interleaved and non-interleaved is standard format, this enumeration * captures the standard and custom data formats. */ typedef enum Mcbsp_BufferFormat_t { /* This mode is used for buffer containing the data in continous * * memory locations where each sample is "wordWidth" long. This * * format is supported for following configurations * * Note : interleaved and non interleaved does not apply for this * * buffer format */ Mcbsp_BufferFormat_1SLOT, /* This is used for transfer of data with multiple slots.please note * * that the slot data is not interleaved in this format. */ Mcbsp_BufferFormat_MULTISLOT_NON_INTERLEAVED, /* This is used for transfer of data for multiple slots.please note * * that the slot data is interleaved in this format. */ Mcbsp_BufferFormat_MULTISLOT_INTERLEAVED }Mcbsp_BufferFormat; /**< Mcbsp supported buffer formats */ /** * \brief Mcbsp PHASE control enums * * \note These enums are used to control the Phase settings of the MCBSP. */ typedef enum Mcbsp_Phase_t { Mcbsp_Phase_SINGLE = (0u), /**< Single phase for frame */ Mcbsp_Phase_DUAL = (1u) /**< Dual phase for frame */ } Mcbsp_Phase; /**< Mcbsp frame phase selection ENUMERATION */ /** * \brief Mcbsp supported wordlength. * * Enumerated constant for wordlength supported by the MCBSP device */ typedef enum Mcbsp_WordLength_t { Mcbsp_WordLength_8 = 8u, /**< Word length of 8 bits */ Mcbsp_WordLength_12 = 12u, /**< Word length of 12 bits */ Mcbsp_WordLength_16 = 16u, /**< Word length of 16 bits */ Mcbsp_WordLength_20 = 20u, /**< Word length of 20 bits */ Mcbsp_WordLength_24 = 24u, /**< Word length of 24 bits */ Mcbsp_WordLength_32 = 32u /**< Word length of 32 bits */ }Mcbsp_WordLength; /**< Mcbsp supported wordlength. */ /** * \brief Frame sync ignore status enum * * \note Use this symbol to detect or ignore frame synchronisation */ typedef enum Mcbsp_FrmSync_t { Mcbsp_FrmSync_DETECT = (0u), /**< detect frame synchronisation */ Mcbsp_FrmSync_IGNORE = (1u) /**< ignore frame synchronisation */ }Mcbsp_FrmSync; /**< Frame sync detection options ENUMERATION */ /** * \brief Enum to select Data delay in bits * * Use this Enum to set XMT/RCV Data Delay (in bits) */ typedef enum Mcbsp_DataDelay_t { Mcbsp_DataDelay_0_BIT = (0u), /**< sets XMT/RCV Data Delay to 0 bits */ Mcbsp_DataDelay_1_BIT = (1u), /**< sets XMT/RCV Data Delay to 1 bits */ Mcbsp_DataDelay_2_BIT = (2u) /**< sets XMT/RCV Data Delay to 2 bits */ } Mcbsp_DataDelay; /**< Enum to select Data delay in bits */ /** * \brief Enum to select the companding law * * Use this Enum to select the appropriate companding rule applicable. */ typedef enum Mcbsp_Compand_t { Mcbsp_Compand_OFF_MSB_FIRST = (0u), /**< No companding, data transfer starts with MSB first. */ Mcbsp_Compand_OFF_LSB_FIRST = (1u), /**< No companding, 8-bit data transfer starts with LSB first. */ Mcbsp_Compand_MULAW = (2u), /**< mu-law comapanding enable for channel */ Mcbsp_Compand_ALAW = (3u) /**< A-law comapanding enable for channel */ }Mcbsp_Compand; /**< Enum to select the companding law */ /** * \brief McBSP 32-bit reversal feature * * This ENUM allows the user to select the option of BIT reversal. */ typedef enum Mcbsp_BitReversal_t { Mcbsp_BitReversal_DISABLE = (0u), /**< 32-bit reversal disabled */ Mcbsp_BitReversal_ENABLE = (1u) /**< 32-bit reversal enabled. 32-bit data is received LSB first. Word * * length should be set for 32-bit operation; else operation undefined */ }Mcbsp_BitReversal; /**< McBSP 32-bit reversal feature */ /** * \brief Frame sync clock source * * Use this ENUM to set the frame sync clock source as internal or * external */ typedef enum Mcbsp_FsClkMode_t { Mcbsp_FsClkMode_EXTERNAL = (0u), /**< frame sync clock source as internal */ Mcbsp_FsClkMode_INTERNAL = (1u), /**< frame sync clock source as external */ Mcbsp_FsClkMode_DXR_XSR = (2u) /**< frame sync is generated on DXR_XSR copy */ } Mcbsp_FsClkMode; /**< Frame sync clock source */ /** * \brief Clock source selection ENUM * * Use this symbol to set the clock source as internal or external */ typedef enum Mcbsp_TxRxClkMode_t { Mcbsp_TxRxClkMode_EXTERNAL = (0u), /**< clock source as internal */ Mcbsp_TxRxClkMode_INTERNAL = (1u) /**< clock source as external */ } Mcbsp_TxRxClkMode; /**< Clock source selection ENUM */ /** * \brief Clock polarity * * Use this symbol to set XMT or RCV clock polarity as rising or * falling edge */ typedef enum Mcbsp_ClkPol_t { Mcbsp_ClkPol_RISING_EDGE = (0u), /**< Data sampled on rising edge of the bit Clock */ Mcbsp_ClkPol_FALLING_EDGE = (1u), /**< Data sampled on falling edge of the bit Clock */ Mcbsp_ClkPol_SRG_RISING_EDGE = (0u), /**< SRG clock polarity is rising edge */ Mcbsp_ClkPol_SRG_FALLING_EDGE = (1u) /**< SRG clock polarity Is falling edge */ } Mcbsp_ClkPol; /**< Clock polarity */ /** * \brief Frame sync polarity * * Use this symbol to set frame sync polarity as active-high or * active-low */ typedef enum Mcbsp_FsPol_t { Mcbsp_FsPol_ACTIVE_HIGH = (0u), /**< frame sync polarity is active-high */ Mcbsp_FsPol_ACTIVE_LOW = (1u) /**< frame sync polarity is active-low */ }Mcbsp_FsPol; /**< Frame sync polarity */ /** * \brief MCBSP Interrupt mode * * Use this symbol to set Interrupt mode (i.e. source of interrupt * generation).This symbol is used on both RCV and XMT for RINT and * XINT generation mode. */ typedef enum Mcbsp_IntMode_t { Mcbsp_IntMode_ON_READY = (0u), /**< Interrupt generated on RRDY of RCV or XRDY of XMT */ Mcbsp_IntMode_ON_EOB = (1u), /**< Interrupt generated on end of 16-channel block transfer in * * multichannel mode */ Mcbsp_IntMode_ON_FSYNC = (2u), /**< Interrupt generated on frame sync */ Mcbsp_IntMode_ON_SYNCERR = (3u) /**< Interrupt generated on synchronisation error */ }Mcbsp_IntMode; /**< MCBSP Interrupt mode */ /** * \brief Transmit multichannel selection mode bit. * * MCM determines whether all channels or only selected channels are * enabled and unmasked for transmission/reception. * */ typedef enum Mcbsp_McmMode_t { Mcbsp_McmMode_ALL_CHAN_ENABLED_UNMASKED = (0u), /**< All the 128 channels are enabled */ Mcbsp_McmMode_ALL_CHAN_DISABLED_UNMASKED = (1u), /**< All channels are disabled unless selected by enable mask */ Mcbsp_McmMode_ALL_CHAN_ENABLED_MASKED = (2u), /**< All channels are enabled but masked unless selected by Enable mask */ Mcbsp_McmMode_ALL_CHAN_DISABLED_MASKED = (3u) /**< Symmetric transmission and reception */ }Mcbsp_McmMode; /**< Transmit multichannel selection mode bit. */ /** * \brief Partition A/B block channel selection bit. */ typedef enum Mcbsp_PartitionSel_t { Mcbsp_PartitionMode_CHAN_0_15 = (0u), /**< Select the channel 0-15 in block A */ Mcbsp_PartitionMode_CHAN_16_31 = (0u), /**< Select the channel 16-31 in block B */ Mcbsp_PartitionMode_CHAN_32_47 = (1u), /**< Select the channel 32-47 in block A */ Mcbsp_PartitionMode_CHAN_48_63 = (1u), /**< Select the channel 48-63 in block B */ Mcbsp_PartitionMode_CHAN_64_79 = (2u), /**< Select the channel 64-79 in block A */ Mcbsp_PartitionMode_CHAN_80_95 = (2u), /**< Select the channel 80-95 in block B */ Mcbsp_PartitionMode_CHAN_96_111 = (3u), /**< Select the channel 96-111 in block A */ Mcbsp_PartitionMode_CHAN_112_127 = (3u) /**< Select the channel 112-127 in block B */ }Mcbsp_PartitionSel; /**< Partition A/B block selection bit. */ /** * \brief Multichannel partition mode selection. * * Multichannel mode allows selection of either an 2 partition mode or * 8 partition mode.This enum allows the user to select the required * partition mode of choice. */ typedef enum Mcbsp_PartitionMode_t { Mcbsp_PartitionMode_2 = (0u), /**< 2-partition mode. Only partitions A and B are used. */ Mcbsp_PartitionMode_8 = (1u) /**< 8-partition mode. All partitions (A through H) are used */ }Mcbsp_PartitionMode; /**< Multichannel partition mode selction */ /*============================================================================*/ /* DATA STRUCTURES */ /*============================================================================*/ /** * \brief McBSP sample rate generator configuration structure * * Configurations for the Sample rate generator to generate the BCLK * and Frame Sync signals are specified using this structure. */ typedef struct Mcbsp_srgConfig_t { Bool gSync; /**< sample rate generator clock syncronization bit (only if CLKS is used)*/ Mcbsp_ClkSPol clksPolarity; /**< CLKS polarity used to drive the CLKG and FSG clocks */ Mcbsp_SrgClk srgInputClkMode; /**< Source for the Sample rate generator (CLKS,CPU,CLKX,CLKR) */ uint32_t srgrInputFreq; /**< input clock frequency for the SRGR (freq of CLKS or CLKX etc..) */ uint32_t srgFrmPulseWidth; /**< Set the Frame Sync Pulse width in terms of FSG clock */ } Mcbsp_srgConfig; /**< McBSP sample rate generator configuration structure */ /** * \brief Mcbsp TX/RX section configuration structure. * * This strcuture specifies the configuration for the McBSP data stream * including the whether it is single phase or dual phase, number of * frames,the word length in each phase and data delay etc. */ typedef struct Mcbsp_DataConfig_t { Mcbsp_Phase phaseNum; /**< Phase of the McBSP data stream */ Mcbsp_WordLength wrdLen1; /**< Length of the data word in first phase */ Mcbsp_WordLength wrdLen2; /**< Length of the data word in second when dual phase is selected */ uint32_t frmLen1; /**< Length of the data frame in first phase */ uint32_t frmLen2; /**< Length of the data frame in second phase */ Mcbsp_FrmSync frmSyncIgn; /**< Frame sync ignore bit */ Mcbsp_DataDelay dataDelay; /**< Data delay to be configured in number of Bits */ Mcbsp_Compand compandSel; /**< companding selection */ Mcbsp_BitReversal bitReversal; /**< Transmit 32-bit bit reversal feature enable bit. */ Mcbsp_IntMode intMode; /**< Event for which the interrupt is to be generated */ Mcbsp_Rxjust rjust; /**< Receive sign extension and justification settings (RX only setting) */ Mcbsp_DxEna dxState; /**< High impedance enable/disbale bit for the DX pin (TX only setting) */ }Mcbsp_DataConfig; /**< Mcbsp TX/RX section configuration structure. */ /** * \brief Mcbsp multi channel control settings * * structure to configure the multi channel settings for the mcbsp.used * when the multi channel configuration is to be enabled. */ typedef struct Mcbsp_McrSetup_t { Mcbsp_McmMode multiChanMode; /**< Multi channel mode to be selcted */ Mcbsp_PartitionSel partitionSelA; /**< Channel selection for partition A */ Mcbsp_PartitionSel partitionSelB; /**< Channel selection for partition B */ Mcbsp_PartitionMode partitionMode; /**< Channel partition mode selection */ }Mcbsp_McrSetup; /**< Mcbsp multi channel control settings */ /** * \brief Mcbsp clock settings setup structure. * * This structure contains the information required to configure the * clocks for the Mcbsp.Both the frame sync settings and the bit clock * settings can be configured in this structure. */ typedef struct Mcbsp_ClkSetup_t { Mcbsp_FsClkMode frmSyncMode; /**< Frame sync mode bit (FSXM/FSRM)(Internal/External) */ uint32_t samplingRate; /**< Frame sync frequency */ Mcbsp_TxRxClkMode clkMode; /**< Bit clock mode (internal or external) */ Mcbsp_FsPol frmSyncPolarity; /**< frmSyncTxPolarity */ Mcbsp_ClkPol clkPolarity; /**< clkTxPolarity */ }Mcbsp_ClkSetup; /**< Mcbsp clock settings setup structure */ /** * \brief Mcbsp Hardware specific information Object * * This structure maintains the information specific to the hardware instance * of the Mcbsp. information like the base address and the cpu event numbers * and DMA events is specific to the instance. This structure is a collection * of such information. */ typedef struct { uint32_t instNum; /**< Instance of MCBSP being referred by this object */ CSL_McbspRegsOvly regs; /**< Pointer to the register overlay structure of the MCBSP */ CSL_BfifoRegsOvly fifoRegs; /**< Fifo address of the mcbsp instance */ CSL_BdataRegsOvly dataAddress; /**< Mcbsp data registers address */ uint32_t edmaTxEventNum; /**< edma Transmit event number */ uint32_t edmaRxEventNum; /**< edma Receive event number */ uint32_t cpuTxEventNum; /**< Transmit interrupt number */ uint32_t cpuRxEventNum; /**< Receive interrupt number */ }Mcbsp_HwInfo_Unpadded; typedef struct { /** Data structure without padding, so sizeof() can compute padding */ Mcbsp_HwInfo_Unpadded obj; /** Pad out to end of MCBSP_MAX_CACHE_ALIGN bytes to prevent something else * from being placed on same cache line as Mcbsp_HwInfo. Note that pad[0] * is illegal, so must add full MCBSP_MAX_CACHE_ALIGN if structure is * already padded by chance. */ uint8_t pad[MCBSP_MAX_CACHE_ALIGN - (sizeof(Mcbsp_HwInfo_Unpadded) % MCBSP_MAX_CACHE_ALIGN)]; } Mcbsp_HwInfo; /**< Mcbsp Hardware specific information Object */ /** * \brief Loop job buffer structure. * This structure defines the format of the Loop job buffer. * * \note Loop job buffer is a buffer used by the mcbsp in edma mode. The * Mcbsp uses this buffer when no iobufs are present and the mcbsp * is also not stopped. In this condition the Mcbsp utilises the * loop job buffer to transmit a known pattern of data from the loopjob * buffer or receives the data in to a loop job buffer */ typedef struct Mcbsp_TempBuffer_t { Uint8 scratchBuf[(4u) + MCBSP_CACHE_LENGTH]; /**< This buffer will be aligned and also the same buffer will be used * for all slots and also only 4 bytes are required because the * max wordwidth is 4 and the cache length is used for buffer alignment */ uint32_t *scratchBuffer; /**< Pointer to hold the aligned buffer */ }Mcbsp_TempBuffer; /**< loop job buffer format. */ /*============================================================================*/ /* DATA TYPES */ /*============================================================================*/ /** * \brief Global error callback function protype * * This is the global error callback function for the McBSP driver. * This function is called directly called from ISR context in case of * error. * \note Since this function is called from an ISR context,care should be taken * that this function conforms to ISR coding guidelines. */ typedef void (*Mcbsp_GblErrCallback)(uint32_t Arg1,uint32_t Arg2,uint32_t Arg3); /** * \brief McBSP channel setup params * * This structure holds configuration to be used for * creating a channel of the Mcbsp. These parameters need to be * specified during the creation of the channel. */ typedef struct Mcbsp_ChanParams_t { uint32_t wordWidth; /**< This parameter informs the driver what is the width word (not * * slot) and this help driver indirectly to decided no. of bytes to * * be transfered for each slot- This is very * * important parameter - in case of invalid value default value * * driver will assume is 32 */ void* userLoopJobBuffer; /**< Buffer to be transferred when the loop job is running. */ uint16_t userLoopJobLength; /**< Number of bytes of the userloopjob buffer for each slot * Please note that this is no. of bytes and this should be * pre-calcuated properly for word width of slot - Please refer the * wordWidth of this structure */ Mcbsp_GblErrCallback gblCbk; /**< callback required when global error occurs - must be callable * * directly from the ISR context */ void* edmaHandle; /**< Handle to the EDMA Driver */ uint32_t edmaEventQue; /**< EDMA event queue to be used by the channel */ uint32_t hwiNumber; /**< Variable to specify the Hwi number to be used by the driver */ Mcbsp_BufferFormat dataFormat; /**< Format of the application supplied buffer */ Bool enableHwFifo; /**< Option to enable/disable the Hardware FIFO */ Mcbsp_DataConfig *chanConfig; /**< settings to configure the TX or RX hardware sections */ Mcbsp_ClkSetup *clkSetup; /**< clock setup for the RX or the TX section */ Mcbsp_McrSetup *multiChanCtrl; /**< multiple channel control settings */ uint32_t chanEnableMask[4]; /**< Mask of the channels to be enabled or disabled */ uint32_t numEnabledChannels; /**< Number of channels enabled with multichannel mode * Note: This should match the number of bits in chanEnable Mask if in * Mcbsp_McmMode_ALL_CHAN_DISABLED_UNMASKED mode */ }Mcbsp_ChanParams; /**< Mcbsp Channel setup parameters */ /** * \brief McBSP device create params * * This structure holds the configuration to be used for the * creation of the Mcbsp device instance.This configuration need to be * supplied during the creation of the device instance. */ typedef struct Mcbsp_Params_t { Mcbsp_DevMode mode; /**< Mode in which mcbsp instance needs to be created */ Mcbsp_OpMode opMode; /**< Operation mode of driver i.e. interrupt or EDMA.Mcbsp supports only * EDMA mode */ Bool enablecache; /**< whether the cache operations are to be performed on the application * buffers or not */ Mcbsp_EmuMode emulationMode; /**< Emulation mode settings for the Mcbsp */ Mcbsp_Loopback dlbMode; /**< digital loop back mode (ENABLE/DISABLE) */ Mcbsp_srgConfig *srgSetup; /**< configuration for the sample rate generator configurations */ void* txQPendingList; /**< Queue to hold the pending buffers received from the application */ void* txQFloatingList; /**< Queue to manage floating buffers in DMA */ void* rxQPendingList; /**< Queue to hold the pending buffers received from the application */ void* rxQFloatingList; /**< Queue to manage floating buffers in DMA */ } Mcbsp_Params; /**< McBSP device setup params */ /** * \brief McBSP queue element * * Doubly linked list for queue elements. * Required for Mcbsp_IOBuf structure. */ typedef struct Mcbsp_QueueElem_t { struct Mcbsp_QueueElem_t* volatile next; struct Mcbsp_QueueElem_t* volatile prev; } Mcbsp_QueueElem; /** * \brief McBSP frame object params * * Mcbsp_IOBuf structures are managed by the driver. MCBSP * buffers are the basis for all I/O operations. 'cmd' field * contains the command id for the driver. 'status' is filled * in by the driver and contains the status of the commmand. */ typedef struct Mcbsp_IOBuf_t { Mcbsp_QueueElem link; /**< queue link */ void* addr; /**< buffer address */ uint32_t size; /**< buffer size */ uint32_t arg; /**< arg to be used by end app */ uint32_t cmd; /**< command for driver - READ, WRITE, ABORT or FLUSH */ int32_t status; /**< status of command */ uint32_t misc; /**< reserved for driver */ } Mcbsp_IOBuf; /**< Mcbsp frame object params */ /** * \brief MCBSP driver callback function * * This is the driver's callback function. The driver will * call a function of this type whenever an I/O operation * is over. */ typedef void (*Mcbsp_CallbackFxn)(void* arg, Mcbsp_IOBuf *ioBuf); /*============================================================================*/ /* IOCTL COMMANDS */ /*============================================================================*/ /** * \brief McBSP Ioctl commands * * List of all the ioctl commands supported by the Mcbsp driver. * */ typedef enum Mcbsp_IOCTL_t { Mcbsp_IOCTL_START = 128, /**< Starts the data transfer */ Mcbsp_IOCTL_SAMPLE_RATE_CHANGE, /**< Command to chnage the sample rate */ Mcbsp_IOCTL_STOP, /**< Stops the data transfer */ Mcbsp_IOCTL_SRGR_START, /**< Start the McBSP SRG */ Mcbsp_IOCTL_SRGR_STOP, /**< Stop the McBSP SRG */ Mcbsp_IOCTL_FSGR_START, /**< Start the McBSP FSG */ Mcbsp_IOCTL_FSGR_STOP, /**< Stop the McBSP FSG */ Mcbsp_IOCTL_SET_TIMEOUT, /**< Modify the timeout value in the driver */ Mcbsp_IOCTL_MUTE_ON, /**< Mute ON the transfer */ Mcbsp_IOCTL_MUTE_OFF, /**< Take out of Muted state */ Mcbsp_IOCTL_PAUSE, /**< Pause the playback operation */ Mcbsp_IOCTL_RESUME, /**< Resume the playback operation */ Mcbsp_IOCTL_CHAN_RESET, /**< Reset an I/O channel */ Mcbsp_IOCTL_DEVICE_RESET, /**< Reset both input and output channel */ Mcbsp_IOCTL_SET_CLKMODE, /**< Set Bit clock mode for the McBSP */ Mcbsp_IOCTL_SET_FRMSYNCMODE, /**< Set Frame Sync mode for the McBSP */ Mcbsp_IOCTL_CONFIG_SRGR, /**< configure Sample Rate Generator */ Mcbsp_IOCTL_SET_BCLK_POL, /**< Set the CLKR or CLKX clock polarity */ Mcbsp_IOCTL_SET_FRMSYNC_POL, /**< Set the FSR and FSX polarity */ Mcbsp_IOCTL_MODIFY_LOOPJOB, /**< Enable/disable the loopjob */ Mcbsp_IOCTL_SYNCERR_INT_ENABLE, /**< Enable/disable the sync error */ Mcbsp_IOCTL_LOOPBACK, /**< enable/disable the loop back mode */ Mcbsp_IOCTL_CANCEL_PENDING_IO /**< Cancel all the current pending IO in the driver */ } Mcbsp_IOCTL; /**< McBSP Ioctl commands list */ /*============================================================================*/ /* MCBSP MODES */ /*============================================================================*/ /** * \brief McBSP Create Modes * * Mcbsp driver create functions take a mode parameter. * */ /** * \def MCBSP_MODE_INPUT * Defines the mode as input. */ #define MCBSP_MODE_INPUT 0x0001 /** * \def MCBSP_MODE_OUTPUT * Defines the mode as output. */ #define MCBSP_MODE_OUTPUT 0x0002 /** * \def MCBSP_MODE_INOUT * Defines the mode as input and output. */ #define MCBSP_MODE_INOUT (MCBSP_MODE_INPUT | MCBSP_MODE_OUTPUT) /*============================================================================*/ /* MCBSP STATUS CODES */ /*============================================================================*/ /** * \brief McBSP Driver Status Codes * * Mcbsp driver status codes. * */ /** * \def MCBSP_STATUS_COMPLETED * Defines the status as completed successfully. */ #define MCBSP_STATUS_COMPLETED 0 /** * \def MCBSP_STATUS_PENDING * Defines the status as queued and pending. */ #define MCBSP_STATUS_PENDING 1 /** * \def MCBSP_STATUS_FLUSHED * Defines the status as request flushed. Queued writes * will be completed w/ MCBSP_STATUS_COMPLETED. Queued * read requests return w/ MCBSP_STATUS_FLUSHED. */ #define MCBSP_STATUS_FLUSHED 2 /** * \def MCBSP_STATUS_ABORTED * Defines the status as request aborted. Non-completed * read or write requests return w/ MCBSP_STATUS_ABORTED. */ #define MCBSP_STATUS_ABORTED 3 /*============================================================================*/ /* MCBSP DRIVER ERROR CODES */ /*============================================================================*/ /** * \brief McBSP Driver Error Codes * * Mcbsp driver error codes. * */ /** * \def MCBSP_ERR_BADIO * Generic failure condition */ #define MCBSP_ERR_BADIO -1 /** * \def MCBSP_ERR_TIMEOUT * Timeout occurred */ #define MCBSP_ERR_TIMEOUT -2 /** * \def MCBSP_ERR_NOIOBUFFERS * No buffers available for I/O */ #define MCBSP_ERR_NOIOBUFFERS -3 /** * \def MCBSP_ERR_FREE * Unable to free resources */ #define MCBSP_ERR_FREE -4 /** * \def MCBSP_ERR_ALLOC * Unable to allocate resource */ #define MCBSP_ERR_ALLOC -5 /** * \def MCBSP_ERR_ABORT * I/O was aborted before completed */ #define MCBSP_ERR_ABORT -6 /** * \def MCBSP_ERR_BADMODE * Invalid device mode */ #define MCBSP_ERR_BADMODE -7 /** * \def MCBSP_ERR_EOF * End-of-File was encountered */ #define MCBSP_ERR_EOF -8 /** * \def MCBSP_ERR_NOTIMPL * Operation not implemented or supported */ #define MCBSP_ERR_NOTIMPL -9 /** * \def MCBSP_ERR_BADARGS * Invalid arguments specified */ #define MCBSP_ERR_BADARGS -10 /** * \def MCBSP_ERR_TIMEOUTUNREC * Unrecoverable timeout occurred */ #define MCBSP_ERR_TIMEOUTUNREC -11 /** * \def MCBSP_ERR_INUSE * Device already in use */ #define MCBSP_ERR_INUSE -12 /** * \brief McBSP Driver Buffer Frame Command Codes * * Mcbsp driver frame command codes. * */ /** * \def Mcbsp_IOBuf_Cmd_READ * Read command */ #define Mcbsp_IOBuf_Cmd_READ 0 /** * \def Mcbsp_IOBuf_Cmd_WRITE * Write command */ #define Mcbsp_IOBuf_Cmd_WRITE 1 /** * \def Mcbsp_IOBuf_Cmd_ABORT * Abort command */ #define Mcbsp_IOBuf_Cmd_ABORT 2 /** * \def Mcbsp_IOBuf_Cmd_FLUSH * Flush command */ #define Mcbsp_IOBuf_Cmd_FLUSH 3 /** * \brief McBSP Driver Command Codes Reserved for Control * * Mcbsp driver command codes reserved for control. * */ /** * \def MCBSP_CTRL_CHAN_RESET * Reset channel only */ #define MCBSP_CTRL_CHAN_RESET 0 /** * \def MCBSP_CTRL_CHAN_TIMEDOUT * Channel timeout occured */ #define MCBSP_CTRL_CHAN_TIMEDOUT 1 /** * \def MCBSP_CTRL_DEVICE_RESET * Reset entire device */ #define MCBSP_CTRL_DEVICE_RESET 2 /********************************************************************** **************************** EXPORTED API **************************** **********************************************************************/ int32_t mcbspInit (void); int32_t mcbspBindDev(void* *devp, int32_t devid, void* devParams); int32_t mcbspUnBindDev(void* devp); int32_t mcbspCreateChan(void* *chanp, void* devp, int32_t mode, void* chanParams, Mcbsp_CallbackFxn cbFxn, void* cbArg); int32_t mcbspDeleteChan(void* chanp); int32_t mcbspSubmitChan(void* chanp, Mcbsp_IOBuf *const ioBuf); int32_t mcbspControlChan(void* chanp, Mcbsp_IOCTL cmd, void* arg); void mcbspGblXmtIsr(void *hChan); void mcbspGblRcvIsr(void *hChan); #ifdef __cplusplus } #endif /* extern "C" */ #endif /* _MCBSP_DRV_H_ */ /*============================================================================*/ /* END OF FILE */ /*============================================================================*/