diff --git a/Settings.xdc.xdt b/Settings.xdc.xdt
index 60fdf81bf6f750bbc9bc7edddaf8b2c3d8062611..e422bfbe246cb752a66c8592edd22e37606133a7 100644 (file)
--- a/Settings.xdc.xdt
+++ b/Settings.xdc.xdt
module Settings
{
+ /*! This is the McBSP Version */
config string mcbspVersionString = `packageVersion`;
+
+ /*! This variable is to control the device type selection.
+ * By default this variable is set to NULL.
+ *
+ * To use MCBSP for the selected device, add the following lines to config
+ * file and set the deviceType correctly:
+ *
+ * var hlink = xdc.useModule ('ti.drv.mcbsp.Settings');
+ * hlink.deviceType = "k2g";
+ *
+ * If this is not set, then hyperlink will use device independent
+ * library where user must supply compiled device_mcbsp_loopback.obj
+ */
+ metaonly config string deviceType = "";
+
+ /*! This variable is to control the device library type selection.
+ * By default this variable is set to release.
+ *
+ * To use CSL to use the debug/release library, add the following lines to config
+ * file and set the library profile accordingly:
+ *
+ * var mcbspSettings = xdc.useModule ('ti.mcbsp.Settings');
+ * mcbspSettings.libProfile = "debug";
+ *
+ */
+ metaonly config string libProfile = "release";
}