diff --git a/config_mk.bld b/config_mk.bld
--- /dev/null
+++ b/config_mk.bld
@@ -0,0 +1,43 @@
+/******************************************************************************
+ * FILE PURPOSE: Build configuration Script for the MCBSP LLD
+ ******************************************************************************
+ * FILE NAME: config.bld
+ *
+ * DESCRIPTION:
+ * This file contains the build configuration script for the MCBSP LLD
+ * and is responsible for configuration of the paths for the various
+ * tools required to build the LLD.
+ *
+ * Copyright (C) 2018, Texas Instruments, Inc.
+ *****************************************************************************/
+
+/* Get the Tools Base directory from the Environment Variable. */
+var toolsBaseDir = java.lang.System.getenv("C6X_GEN_INSTALL_PATH");
+var m4ToolsBaseDir = java.lang.System.getenv("TOOLCHAIN_PATH_M4");
+var a15ToolsBaseDir = java.lang.System.getenv("TOOLCHAIN_PATH_A15");
+var a9ToolsBaseDir = java.lang.System.getenv("TOOLCHAIN_PATH_A9");
+var arm9ToolsBaseDir = java.lang.System.getenv("TOOLCHAIN_PATH_ARM9");
+var a8ToolsBaseDir = java.lang.System.getenv("TOOLCHAIN_PATH_A8");
+
+/* Get the base directory for the McBSP LLD Driver Package */
+var driverPath = new java.io.File(".//").getPath();
+
+/* Include Path */
+var lldIncludePath = " -I" + driverPath + "/src" + " -I" + driverPath + " -I" + driverPath + "/include";
+
+/* Configure the McBSP Release Version Information */
+/* 3 steps: remove SPACE and TAB, convert to string and split to make array */
+var mcbspDriverReleaseVersion = (""+Pkg.version.replace(/\s/g, "")).split(',');
+
+/* Do not Print the Compiler Options */
+var pOpts = 0;
+
+/* List of all devices that needs to be build via XDC
+ * As the build happens through makefile, there is nothing to build via XDC
+ * using the below for packaging infrastructure
+ */
+var socs = [];
+var devices = [];
+var build_devices = [];
+Build.targets = []
+