Added bin2ccs
[keystone-rtos/mcsdk-tools.git] / bin2ccs / README.txt
1 Utility to convert binary file to TI CCS Format file
3 Usage:
5 Under Windows Command Prompt, run bin2ccs.bat or the following command:
6 bin2ccs <infile> <outfile>
8 Note: The infile is the input binary image or data file, the outfile is the generated output file 
9       in CCS data format that can be loaded into DSP memory using the CCS Memory Browser.
11 Example: bin2ccs app.out app.dat