]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - keystone-rtos/mcsdk-tools.git/blob - post/src/pa.c
Added EMAC loopback support and updated projects to use resource manager
[keystone-rtos/mcsdk-tools.git] / post / src / pa.c
1 /****************************************************************************************************
2  * FILE PURPOSE: The boot loader packet accelerator driver
3  ****************************************************************************************************
4  * FILE NAME: pa.c
5  *
6  * DESCRIPTION: The driver for the packet accelerator during boot
7  *
8  ****************************************************************************************************/
9 #include "types.h"
10 #include "platform.h"
11 #include "pa_loc.h"
12 #include "pa_api.h"
13 #include "target.h"
14 #include "hwpafw_bin.h"
15 #include <string.h>
17 /****************************************************************************************************
18  * FUNCTION PURPOSE: Initialize the PA sub-system
19  ****************************************************************************************************
20  * DESCRIPTION: Only PDSP 0 is used. All other PDSPs are put into reset. PDSP0 is downloaded
21  *              and started, then provided with the mac address configuration.
22  ****************************************************************************************************/
23 int16_t hwPaEnable (const paConfig_t *cfg)
24 {
25     uint32_t i;
26     uint32_t v;
27     BOOL   done;
29     /* Disable all PDSPs */
30     for (i = 0; i < DEVICE_PA_NUM_PDSPS; i++)
31         DEVICE_REG32_W (DEVICE_PA_BASE + PA_REG_PDSP_CTL(i), PA_REG_VAL_PDSP_CTL_DISABLE_PDSP);
33     /* Clear the mailbox registers for PDSP 0 */
34     for (i = 0; i < PA_NUM_MAILBOX_SLOTS; i++)
35         DEVICE_REG32_W (DEVICE_PA_BASE + PA_REG_MAILBOX_SLOT(0, i), 0);
38     /* Give a few cycles for the disable */
39     chipDelay32 (100);
41     /* download the firmware */
42     memcpy ((uint32_t *)(DEVICE_PA_BASE + PA_MEM_PDSP_IRAM(0)), PDSPcode, sizeof(PDSPcode));
44     /* Reset the PC and enable PDSP0 */
45     DEVICE_REG32_W (DEVICE_PA_BASE + PA_REG_PDSP_CTL(0), PA_REG_VAL_PDSP_CTL_ENABLE_PDSP(0));
48     /* Copy the two destination mac addresses to the mail box slots.
49      * Mailbox 4 must be written last since this write triggers the firmware to
50      * update the match information */
51     cfg->cmdBuf[0] = BOOT_READ_BITFIELD(cfg->mac0ms, 31, 24);
52     cfg->cmdBuf[1] = BOOT_READ_BITFIELD(cfg->mac0ms, 23, 16);
53     cfg->cmdBuf[2] = BOOT_READ_BITFIELD(cfg->mac0ms, 15,  8);
54     /* Cant use BOOT_READ_BITFIELD for 8 LSBs because it compiles with endian dependency */
55     cfg->cmdBuf[3] = chipLower8 (cfg->mac0ms);
56     cfg->cmdBuf[4] = BOOT_READ_BITFIELD(cfg->mac0ls, 31, 24);
57     cfg->cmdBuf[5] = BOOT_READ_BITFIELD(cfg->mac0ls, 23, 16);
58     cfg->cmdBuf[6] = cfg->cmdBuf[7] = 0;
60     cfg->cmdBuf[8]  = BOOT_READ_BITFIELD(cfg->mac1ms, 31, 24);
61     cfg->cmdBuf[9]  = BOOT_READ_BITFIELD(cfg->mac1ms, 23, 16);
62     cfg->cmdBuf[10] = BOOT_READ_BITFIELD(cfg->mac1ms, 15,  8);
63     /* Cant use BOOT_READ_BITFIELD for 8 LSBs because it compiles with endian dependency */
64     cfg->cmdBuf[11] = chipLower8 (cfg->mac1ms);
65     cfg->cmdBuf[12] = BOOT_READ_BITFIELD(cfg->mac1ls, 31, 24);
66     cfg->cmdBuf[13] = BOOT_READ_BITFIELD(cfg->mac1ls, 23, 16);
68     cfg->cmdBuf[14] = BOOT_READ_BITFIELD(cfg->rxQnum, 15, 8);
69     cfg->cmdBuf[15] = chipLower8 (cfg->rxQnum);
72     /* Give some delay then verify that the mailboxes have been cleared */
73     for (i = 0, done = FALSE; ((i < DEVICE_PA_RUN_CHECK_COUNT) && (done == FALSE)); i++)  {
74         chipDelay32 (100);
75         v = DEVICE_REG32_R (DEVICE_PA_BASE + PA_REG_MAILBOX_SLOT(0, 3));
76         if (v == 0)
77             done = TRUE;
78     }
80     if (done == FALSE)
81         return (-1);
83     return (0);
85 } /* hwPaEnable */
88 /***********************************************************************************************
89  * FUNCTION PURPOSE: Disable the PA firmware
90  ***********************************************************************************************
91  * DESCRIPTION: All PDSPs are disabled and all mailbox slots cleared
92  ***********************************************************************************************/
93 int16_t hwPaDisable (void)
94 {
95     uint32_t i, j;
97     /* Disable all pdsps, clear all mailboxes */
98     for (i = 0; i < DEVICE_PA_NUM_PDSPS; i++)  {
100         DEVICE_REG32_W (DEVICE_PA_BASE + PA_REG_PDSP_CTL(i), PA_REG_VAL_PDSP_CTL_DISABLE_PDSP);
102         for (j = 0; j < PA_NUM_MAILBOX_SLOTS; j++)
103             DEVICE_REG32_W (DEVICE_PA_BASE + PA_REG_MAILBOX_SLOT(i, j), 0);
105     }
107     return (0);
109 } /* hwPaDisable */