program_evm: Add gel files copied from emupack
[keystone-rtos/mcsdk-tools.git] / program_evm / gel / README.txt
1 Steps to update GELs for C66x EVMs
2 ----------------------------------
4 1: There are one or more GEL files provided in this directory
6 2: These GEL files needs to be copied to CCS installation
8 3: The following steps will assume the CCS is installed in <CCS_INSTALL_DIR> (which is typically C:\Program Files\Texas Instruments\ccsv5 for Windows XP and ~/ti/ccsv5 for Linux)
10 4: Close CCS if open
12 5: Replace the GEL file present in the <CCS_INSTALL_DIR>/ccs_base/emulation/boards/<BOARD_NAME>/gel directory with the <BOARD_NAME>.gel file present in this directory
14 6: Repeat step 5 for all gel files present in this directory