1 EEPROM Writer Utility
3 EEPROM Writer is a simple utility to program a CCS format image/data file to I2C EEPROM.
5 Steps to program the EEPROM:
7 1. Be sure to set the boot mode dip switch to no boot/EMIF16 boot mode on the EVM.
9 2. Copy the CCS format data file to writer\eeprom\evmc66xxl\bin directory, and rename it to app.dat.
11 3. Change the file_name, bus_addr, start_addr and swap_data in writer\eeprom\evmc66xxl\bin\eepromwriter_input.txt if necessary.
12 By default the EEPROM writer will load app.dat to DSP memory and write the data to I2C slave
13 bus address 81 (0x51) at EEPROM device start byte address 0 with data swap disabled (0).
15 4. Open CCSv5 and launch the evmc66xx emulator target configuration and connect to core 0.
17 5. Load the program writer\eeprom\evmc66xxl\bin\eepromwriter_evm66xxl.out to CCS, be sure evmc66xxl.gel is used in CCS
18 and DDR is intialized.
20 6. Open the Memory view (in CCSv5, view->Memory Browser), and view the memory address 0x80000000.
22 7. Load app.dat to 0x80000000:
23 * In CCSv5, right click mouse in memory window, select "load memory".
24 * Browse and select writer\eeprom\evmc66xxl\bin\app.dat.
25 * Select the option "Use the file header information to set the start address and size of the memory block to be
26 loaded" and click "next".
27 * Change the Start Address to "0x80000000" if it is not 0x80000000, and click "finish".
29 8.After the data file is loaded into the memory, run the program (in CCSv5, press F8), it will start to program the
30 EEPROM.
32 9.When programming is completed, the console will print "EEPROM programming completed successfully", if there
33 is any error, the console will show the error message.
36 Steps to re-build eepromwriter:
38 1. Uses CCS to build eepromwriter:
39 * Import the eepromwriter CCS project from writer\eeprom\evmc66xxl directory (in CCSv5, Project->Import Existing CCS/
40 CCE Eclipse Projects).
41 * Clean and build the eepromwriter project.
42 * After the project build is completed, eepromwriter_evm66xxl.out and eepromwriter_evm66xxl.map will be generated under
43 writer\eeprom\evmc66xxl\bin directory.
45 2. Uses Makefile to build eepromwriter:
46 NOTE FOR BUILDING ON WINDOWS ENVIRONMENT: For building on windows environment GNU utilities like
47 "make" would be required. The following build procedure should also work on MINGW-MSYS Bourne shell.
49 Before starting the build following environment setup has to be done
50 1) variable C_DIR should be set to the top directory of the Code Generation tools e.g.
51 Linux bash shell:
52 export C_DIR=/opt/TI/TI_CGT_C6000_7.2.0A10232/
53 MSYS bash shell:
54 export C_DIR='"C:/Program Files/Texas Instruments/ccsv5/tools/compiler/c6000"'
55 2) Code Generation tool binaries should be in the path e.g.
56 Linux bash shell:
57 export PATH=/opt/TI/TI_CGT_C6000_7.2.0A10232/bin:$PATH
58 MSYS bash shell:
59 export PATH=$PATH:/c/Program\ Files/Texas\ Instruments/ccsv5/tools/compiler/c6000/bin/
60 3) variable PFORM_LIB_DIR should be set the directory of the Platform Library root, e.g.
61 Linux bash shell:
62 export PFORM_LIB_DIR=pdk_C6670_1_0_0_10-rc1/packages/ti/platform
63 MSYS bash shell:
64 export PFORM_LIB_DIR='"C:/Program Files/Texas Instruments/pdk_C6670_1_0_0_10-rc1/packages/ti/platform"'
66 The makefile for building the eepromwriter is in the directory "tools/writer/eeprom/evmc66xxl"
67 Following are the steps to build eepromwriter, e.g.:
68 cd tools/writer/eeprom/evmc66xxl
69 make DEVICE=<device number>
70 supported device numbers are
71 C6678
72 C6670
74 Please refer to BIOS MCSDK 2.0 User's Guide (http://processors.wiki.ti.com/index.php/BIOS_MCSDK_2.0_User_Guide) for more details.