/****************************************************************************** * Copyright (c) 2011 Texas Instruments Incorporated - http://www.ti.com * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the * distribution. * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR * A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT * OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, * SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT * LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, * DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY * THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT * (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. * *****************************************************************************/ /************************************************************************************** * FILE PURPOSE: NAND writer utility ************************************************************************************** * FILE NAME: nandwriter.c * * DESCRIPTION: A simple nand writer using platform lib APIs to program the NAND flash * with an image that the ibl can read. * ***************************************************************************************/ #include #include #include #include "platform.h" #include "types.h" /* NAND writer utility version */ char version[] = "01.00.00.04"; /* The input file name is hard coded */ char *input_file = "nand_writer_input.txt"; uint32_t swap_byte = 0; /* Parameters defined in the input_file */ #define FILE_NAME "file_name" #define START_ADDR "start_addr" /* Memory address to store the write data */ #define WRITE_DATA_ADDRESS 0x80000000 /* NAND device specific definitions */ #define BAD_BLOCK_MARKER_VALUE 0xA5 /****************************************************************************** * Structure: NAND_WRITER_INFO_T * * NAND writer control data. This structure should be filled in * by the user before running ******************************************************************************/ #define MAX_LINE_LENGTH 40 typedef struct NAND_WRITER_INFO_tag { char file_name[MAX_LINE_LENGTH]; /* CCS format data file name */ uint32_t blockSizeBytes; /* The size of each sector */ uint32_t deviceTotalBytes; /* Total number of bytes available in the device */ uint32_t startAddr; /* Start address to write */ uint32_t writeBytes; /* Number of bytes to be written into the device */ uint8_t *writeData; /* Address to store the write data */ uint8_t *readData; /* Address to store the read data */ } NAND_WRITER_INFO_T; NAND_WRITER_INFO_T nandWriterInfo; /* OSAL functions for Platform Library */ uint8_t *Osal_platformMalloc (uint32_t num_bytes, uint32_t alignment) { return malloc(num_bytes); } void Osal_platformFree (uint8_t *dataPtr, uint32_t num_bytes) { /* Free up the memory */ if (dataPtr) { free(dataPtr); } } void Osal_platformSpiCsEnter(void) { return; } void Osal_platformSpiCsExit (void) { return; } /****************************************************************************** * Function: print_platform_errno ******************************************************************************/ void print_platform_errno ( void ) { printf ("Returned platform error number is %d\n", platform_errno); } /****************************************************************************** * Function: checkBadBlockMark * * Checks for the bad block mark. Returns TRUE if a block is marked bad. ******************************************************************************/ Bool checkBadBlockMark ( PLATFORM_DEVICE_info *p_device, uint32_t block ) { if (p_device->bblist[block] != 0xff) { return TRUE; } else { return FALSE; } } /****************************************************************************** * Function: markBlockBad * * Mark a block as bad. Byte 5 of the spare area data is * written as 0xA5. ******************************************************************************/ void markBlockBad ( PLATFORM_DEVICE_info *p_device, uint32_t block ) { uint8_t *spare_data; spare_data = malloc(p_device->spare_size); if (spare_data == NULL) { printf ("Can not allocate spare_data memory!\n"); return; } platform_device_read_spare_data(p_device->handle, block, 0, spare_data); /* Set all data bytes to 0xff, only set the user defined bad block mark value */ spare_data[p_device->bboffset] = BAD_BLOCK_MARKER_VALUE; /* Write the data to page */ platform_device_write_spare_data(p_device->handle, block, 0, spare_data); /* Save the user defined bad block mark in bblist */ p_device->bblist[block] = BAD_BLOCK_MARKER_VALUE; free (spare_data); } /****************************************************************************** * Function: form_block * * Form a block of data to write to the NOR. The block is * created as a byte stream from the 4 byte stream in which * the MSB is always sent first. ******************************************************************************/ void formBlock ( uint32_t *data, uint32_t blockSize, uint8_t *scratch ) { uint32_t i, j; /* Convert the data to a byte stream */ for (i = j = 0; j < blockSize; i++, j+=4) { scratch[j+0] = (data[i] >> 24) & 0xff; scratch[j+1] = (data[i] >> 16) & 0xff; scratch[j+2] = (data[i] >> 8) & 0xff; scratch[j+3] = (data[i] >> 0) & 0xff; } } /****************************************************************************** * Function: flashNand * * Write the image to flash. * Returns TRUE if the image is written successfully * FALSE if the image write fails ******************************************************************************/ Bool flash_nand ( PLATFORM_DEVICE_info *p_device ) { uint32_t wPos, wLen; uint32_t block, start_block; uint8_t *scrach_block; if (swap_byte) { scrach_block = malloc(nandWriterInfo.blockSizeBytes); if (scrach_block == NULL) { printf ("Can not allocate scratch block memory!\n"); return (FALSE); } } start_block = nandWriterInfo.startAddr / nandWriterInfo.blockSizeBytes; /* Program the NAND */ for (block = start_block, wPos = 0; wPos < nandWriterInfo.writeBytes; block++, wPos += nandWriterInfo.blockSizeBytes) { while(checkBadBlockMark(p_device, block)) { printf ("Bad block # %d detected, skipping block ... \n", block); if (++block == p_device->block_count) { printf ("Flash failed: End of device reached\n"); if (swap_byte) free (scrach_block); return (FALSE); } } printf ("Flashing block %d (%d bytes of %d)\n", block, wPos, nandWriterInfo.writeBytes); platform_device_erase_block(p_device->handle, block); wLen = nandWriterInfo.blockSizeBytes; if (nandWriterInfo.writeBytes - wPos < nandWriterInfo.blockSizeBytes) { wLen = nandWriterInfo.writeBytes - wPos; } if (swap_byte) { formBlock((uint32_t *)(&nandWriterInfo.writeData[wPos]), nandWriterInfo.blockSizeBytes, scrach_block); } else { scrach_block = &nandWriterInfo.writeData[wPos]; } if (platform_device_write(p_device->handle, block*nandWriterInfo.blockSizeBytes, scrach_block, wLen) != Platform_EOK) { printf ("platform_device_write block # %d failed!\n", block); print_platform_errno(); if (swap_byte) free (scrach_block); return (FALSE); } } if (swap_byte) free (scrach_block); return (TRUE); } /****************************************************************************** * Function: flashVerify * * Read back the data file that was just flashed. On errors mark the block as bad. * Returns TRUE if the image verified correctly. * FALSE if the image verification failed ******************************************************************************/ Bool flash_verify ( PLATFORM_DEVICE_info *p_device ) { uint32_t rPos, rLen; uint32_t i, j; uint32_t block, start_block; uint8_t *scrach_block; uint32_t *read_data_w; if (swap_byte) { scrach_block = malloc(nandWriterInfo.blockSizeBytes); if (scrach_block == NULL) { printf ("Can not allocate scratch block memory!\n"); return (FALSE); } } start_block = nandWriterInfo.startAddr / nandWriterInfo.blockSizeBytes; for (block = start_block, rPos = 0; rPos < nandWriterInfo.writeBytes; block++, rPos += nandWriterInfo.blockSizeBytes) { while(checkBadBlockMark(p_device, block)) { printf ("Bad block # %d detected, skipping block ... \n", block); if (++block == p_device->block_count) { printf ("Flash failed: End of device reached\n"); if (swap_byte) free (scrach_block); return (FALSE); } } printf ("Reading and verifying block %d (%d bytes of %d)\n", block, rPos, nandWriterInfo.writeBytes); if (!swap_byte) { scrach_block = &nandWriterInfo.readData[rPos]; } /* Read a block of data */ if(platform_device_read(p_device->handle, block*nandWriterInfo.blockSizeBytes, scrach_block, nandWriterInfo.blockSizeBytes) != Platform_EOK) { printf ("Failure in reading block %d\n", block); print_platform_errno(); if (platform_errno == PLATFORM_ERRNO_ECC_FAIL) { printf ("marking block %d as bad, re-flash attempted\n", block); markBlockBad (p_device, block); } if (swap_byte) free (scrach_block); return (FALSE); } /* Convert the packed data */ if (swap_byte) { read_data_w = (uint32_t *)(&nandWriterInfo.readData[rPos]); for (i = 0, j = 0; i < nandWriterInfo.blockSizeBytes; i += 4) read_data_w[j++] = (scrach_block[i+0] << 24) | (scrach_block[i+1] << 16) | (scrach_block[i+2] << 8) | scrach_block[i+3]; } rLen = nandWriterInfo.blockSizeBytes; if (nandWriterInfo.writeBytes - rPos < nandWriterInfo.blockSizeBytes) { rLen = nandWriterInfo.writeBytes - rPos; } /* Compare the data read with data programmed */ for (i = rPos; i < rLen; i++) { if (nandWriterInfo.readData[i] != nandWriterInfo.writeData[i]) { printf ("Failure in block %d, at byte %d, (at byte %d in the data file) expected 0x%08x, read 0x%08x\n", block, i, rPos, nandWriterInfo.writeData[i], nandWriterInfo.readData[i]); if (swap_byte) free (scrach_block); return (FALSE); } } } if (swap_byte) free (scrach_block); return (TRUE); } /****************************************************************************** * Function: parse_input_file ******************************************************************************/ static Bool parse_input_file ( FILE* fp ) { char line[MAX_LINE_LENGTH]; char tokens[] = " :=;\n\r"; char *key, *data; memset(line, 0, MAX_LINE_LENGTH); fgets(line, MAX_LINE_LENGTH, fp); key = (char *)strtok(line, tokens); data = (char *)strtok(NULL, tokens); if(strlen(data) == 0) { return FALSE; } if(strcmp(key, FILE_NAME) != 0) { return FALSE; } strcpy (nandWriterInfo.file_name, data); fgets(line, MAX_LINE_LENGTH, fp); key = (char *)strtok(line, tokens); data = (char *)strtok(NULL, tokens); if(strlen(data) == 0) { return FALSE; } if(strcmp(key, START_ADDR) != 0) { return FALSE; } nandWriterInfo.startAddr = (uint32_t)atoi(data); return TRUE; } /****************************************************************************** * Function: find_file_length ******************************************************************************/ static Bool find_file_length ( FILE* fp ) { char line[MAX_LINE_LENGTH]; char *pEnd; char *ext; uint32_t data_len, write_addr; memset(line, 0, MAX_LINE_LENGTH); ext = strrchr(nandWriterInfo.file_name, '.'); if (ext && (strcmp(ext, ".dat") == 0)) { fgets(line, MAX_LINE_LENGTH, fp); /* Read the write address from the CCS header */ strtoul (line,&pEnd,16); strtoul (pEnd,&pEnd,16); write_addr = strtoul (pEnd,&pEnd,16); strtoul (pEnd,&pEnd,16); /* Read the data length */ data_len = (strtoul (pEnd,NULL,16)) * 4; } else { /* find the data length by seeking to the end and getting position */ fseek(fp, 0, SEEK_END); data_len = ftell(fp); fseek(fp, 0, SEEK_SET); } if (data_len > (nandWriterInfo.deviceTotalBytes - nandWriterInfo.startAddr)) { printf ("The data file is too big to fit into the device.\n"); return FALSE; } nandWriterInfo.writeBytes = data_len; if (write_addr != WRITE_DATA_ADDRESS) write_addr = WRITE_DATA_ADDRESS; nandWriterInfo.writeData = (uint8_t *)write_addr; nandWriterInfo.readData = (uint8_t *)(write_addr + nandWriterInfo.deviceTotalBytes); return TRUE; } /****************************************************************************** * Function: main ******************************************************************************/ void main () { FILE *fp; platform_init_flags init_flags; platform_init_config init_config; PLATFORM_DEVICE_info *p_device; Bool ret; uint32_t rCount; printf("NAND Writer Utility Version %s\n\n", version); fp = fopen(input_file, "r"); if (fp == NULL) { printf("Error in opening %s input file\n", input_file); return; } ret = parse_input_file(fp); fclose (fp); if (ret == FALSE) { printf("Error in parsing %s input file\n", input_file); return; } /* Initialize main Platform lib */ memset(&init_config, 0, sizeof(platform_init_config)); memset(&init_flags, 1, sizeof(platform_init_flags)); if (platform_init(&init_flags, &init_config) != Platform_EOK) { printf ("Platform init failed!\n"); print_platform_errno(); return; } p_device = platform_device_open(PLATFORM_DEVID_NAND512R3A2D, 0); if (p_device == NULL) { printf ("NAND device open failed!\n"); print_platform_errno(); return; } nandWriterInfo.deviceTotalBytes = p_device->block_count * p_device->page_count * p_device->page_size; nandWriterInfo.blockSizeBytes = p_device->page_count * p_device->page_size; if ((nandWriterInfo.startAddr % nandWriterInfo.blockSizeBytes) != 0) { printf ("The start programming address 0x%8x set in %s is not at the beginning of a block, block size = 0x%4x\n", nandWriterInfo.startAddr, nandWriterInfo.file_name, nandWriterInfo.blockSizeBytes); return; } /* Open and find the length of the data file */ fp = fopen (nandWriterInfo.file_name, "rb"); if (fp == NULL) { printf ("Failed to open file %s\n", nandWriterInfo.file_name); platform_device_close(p_device->handle); return; } /* Parse the CCS format file */ ret = find_file_length(fp); fclose (fp); if (ret == FALSE) { printf("Error in parsing CCS file %s\n", nandWriterInfo.file_name); platform_device_close(p_device->handle); return; } /* Write the flash, verify the results. On read back failure mark * the block as bad and try rewriting again */ rCount = 0; do { if (flash_nand (p_device) == FALSE) { printf ("NAND write giving up\n"); return; } rCount += 1; } while ((flash_verify (p_device) == FALSE) && (rCount < 5)); if (rCount >= 5) { printf ("NAND write failed (maximum retries reached)\n"); } else { printf ("NAND programming completed successfully\n"); } platform_device_close(p_device->handle); return; }