Modified EMAC boot example readme
[keystone-rtos/mcsdk-tools.git] / boot_loader / examples / i2c / emac / docs / README.txt
index 46f520e7d508808980a3c8cbb2448a4c2e43cc04..380de22ba07c4ebf40c5c01f18cbf6d9e3392b98 100644 (file)
@@ -33,17 +33,13 @@ Steps to program i2cemacboot to EMAC:
 2. Be sure EMAC boot parameter table is progrommed to I2C EEPROM bus address 81 (0x51), if the table is not programmed, 
    refer to tools\boot_loader\ibl\doc\README.txt on how to program the boot parameter table to EEPROM. 
 
-3. Copy tools\boot_loader\examples\i2c\emac\evmc6xxxl\bin\i2cemacboot_evm6xxxl.out to tools\bin2ccs and rename
-   the file to app.out.
+3. Start a TFTP server (you can download a free, opensource application from http://tftpd32.jounin.net) and copy
+   tools\boot_loader\examples\i2c\emac\evmc6xxxl\bin\i2cemacboot_evm6xxxl.out to the TFTP base directory. Rename
+   i2cemacboot_evm6xxxl.out to app.out
 
-4. Double click bin2ccs.bat, which will convert app.out to a CCS format data file app.dat.
-
-5. Start a TFTP server (you can download a free, opensource application from http://tftpd32.jounin.net) and copy
-   app.dat to the TFTP base directory.
-
-6. Set the IP address of the PC that is running the TFTP server to 192.168.1.101, since by default IBL will set the EVM IP 
+4. Set the IP address of the PC that is running the TFTP server to 192.168.1.101, since by default IBL will set the EVM IP 
    address to 192.168.1.100 and the TFTP server IP address to 192.168.1.101. 
 
-7. Be sure the EVM and the PC are connected in the same subnet of a local network, after POR, the EVM will download the
+5. Be sure the EVM and the PC are connected in the same subnet of a local network, after POR, the EVM will download the
    boot image from TFTP server and boot from it.