diff --git a/post/docs/README.txt b/post/docs/README.txt
--- a/post/docs/README.txt
+++ b/post/docs/README.txt
Steps to build POST:
-1. Import the POST CCS project from tools\post\evmc66xxl directory. (in CCSv5, Project->Import Existing CCS/
+1. Import the POST CCS project from tools\post\evmxxxx directory. (in CCSv5, Project->Import Existing CCS/
CCE Eclipse Projects)
2. Be sure the lite version of the Platform Lib is pre-built:
- pdk_C66xx_1_x_x_x\packages\ti\platform\evmc66xxl\platform_lib\lib\debug\ti.platform.evm6670l.lite.lib
- If the lib is not pre-built, refer to Platform Lib User Guide under pdk_C66xx_x_x_x\packages\ti\platform\docs
+ pdk_xxxx_x_x_x_x\packages\ti\platform\evmxxxx\platform_lib\lib\debug\ti.platform.evmxxxx.lite.lib
+ If the lib is not pre-built, refer to Platform Lib User Guide under pdk_xxxx_x_x_x_x\packages\ti\platform\docs
on how to build the platform library.
Note that the lite version of platform lib only contains the functions that are required by the POST, so that
POST can be fit into the EEPROM.
-3. Clean the POST project and re-build the project, after build is completed, post_evm66xxl.out and post_evm66xxl.map
- will be generated under tools\post\evmc66xxl\bin directory.
+3. Clean the POST project and re-build the project, after build is completed, post_evmxxxx.out and post_evmxxxx.map
+ will be generated under tools\post\evmxxxx\bin directory.
Steps to run POST in CCSv5:
1. Be sure to set the boot mode dip switch to no boot/EMIF16 boot mode on the EVM
-2. Load the program tools\post\evmc66xxl\bin\post_evm66xxl.out to CCS.
+2. Load the program tools\post\evmxxxx\bin\post_evmxxxx.out to CCS.
3. Connect the 3-pin RS-232 cable from the EVM to the serial port of the PC, and start Hyper Terminal.
Steps to program POST to EEPROM:
-1. Copy tools\post\evmc66xxl\bin\post_i2crom.bin to tools\writer\eeprom\evmc66xxl\bin directory
+1. Copy tools\post\evmxxxx\bin\post_i2crom.bin to tools\writer\eeprom\evmxxxx\bin directory
-2. Navigate to tools\writer\eeprom\evmc66xxl\bin\ and open eepromwriter_input.txt. Make the following changes:
+2. Navigate to tools\writer\eeprom\evmxxxx\bin\ and open eepromwriter_input.txt. Make the following changes:
- Set the file_name to post_i2crom.bin
- Set the bus_addr to 0x50
- Set start_addr to 0
- Set swap_data to 0
Save and close eepromwriter_input.txt
-3. Refer to tools\writer\eeprom\evmc66xxl\docs\README.txt on how to program the raw binary file to EEPROM
+3. Refer to tools\writer\eeprom\evmxxxx\docs\README.txt on how to program the raw binary file to EEPROM
4. Once the programming is completed successfully, user can set the boot mode to I2C mode with bus address 0x50 and
boot the POST directly from the EEPROM after POR. The boot status and test result can be monitored using the Hyper
Terminal as mentioned in "Steps to run POST in CCSv5".
-Please refer to C6678L/C6670L EVM boot mode dip switch settings:
+Please refer to C6678L/C6670L/C6657L/TCI6634K2K EVM boot mode dip switch settings:
http://processors.wiki.ti.com/index.php/TMDXEVM6678L_EVM_Hardware_Setup#Boot_Mode_Dip_Switch_Settings
http://processors.wiki.ti.com/index.php/TMDXEVM6670L_EVM_Hardware_Setup#Boot_Mode_Dip_Switch_Settings
+http://processors.wiki.ti.com/index.php/TMDSEVM6657L_EVM_Hardware_Setup#Boot_Mode_Dip_Switch_Settings
+http://processors.wiki.ti.com/index.php/TMDSEVMK2K_EVM_Hardware_Setup#Boot_Mode_Dip_Switch_Settings (TBD)
and User's Guide for more details:
-http://processors.wiki.ti.com/index.php/BIOS_MCSDK_2.0_User_Guide
\ No newline at end of file
+http://processors.wiki.ti.com/index.php/BIOS_MCSDK_x.0_User_Guide
\ No newline at end of file