index 7049ef3866fd7f5272f44ea342f31ee9b8963075..90c81c6d0bd9d6d6e73691a8f92b440e13b665a3 100644 (file)
exe_file = "post.i2c.ccs"
}
-; The layout statement defines how the resulting I2C image is layed out. The base address
-; of this (given in the dev_addr) statement must be known to the initial IBL program
-; at compile time. The layout block is simple a group of 32 bit i2c addresses, so
-; the order of the exe_file and pad_file_id statements must be configured so as to
-; match the definition of struct iblI2cMap_t defined in ibl.h.
-layout
-{
- dev_addr = 0x420 ; Defined in iblcfg.h
- dev_addr_ext = 0x50
- file_align = 0x80
-
- exe_file = ""
- pad_file_id = 1
-
-
- exe_file = ""
- pad_file_id = 1
-}
-
-; The pad statements simply provide space for the IBL configuration structures. It is valid to
-; have a single configuration structure which is used for both endian values.
-pad
-{
- pad_file_id = 1
- dev_addr = 0x500
- dev_addr_ext = 0x50
- len = 0x300
-}