index 13ee9a046ce3aab7942473a946493ed966821e54..d943dc1055b880a9b47b25146fd2b97f4e357e98 100644 (file)
Steps to program the EEPROM:
-1. Be sure to set the boot mode dip switch to no boot/EMIF16 boot mode on the EVM (please refer to the EVM technical
- reference manual on how to set the boot mode dip switches)
+1. Be sure to set the boot mode dip switch to no boot/EMIF16 boot mode on the EVM.
2. Copy the CCS format data file to tools\writer\eeprom\evmc66xxl\bin directory, and rename it to app.dat.
-3. Change the file_name, bus_addr and start_addr in tools\writer\eeprom\evmc6xxxl\bin\eepromwriter_input.txt if necessary.
+3. Change the file_name, bus_addr and start_addr in tools\writer\eeprom\evmc66xxl\bin\eepromwriter_input.txt if necessary.
By default the EEPROM writer will load app.dat to DSP memory and write the data to I2C slave
- bus address 81 at EEPROM device start address 0.
+ bus address 81 (0x51) at EEPROM device start byte address 0.
4. Open CCSv5 and launch the evmc66xx emulator target configuration and connect to core 0.
-5. Load the program tools\writer\eeprom\evmc66xxl\bin\eepromwriter_evm66xxl.out to CCS, be sure evmc6xxxl.gel is used in CCS.
+5. Load the program tools\writer\eeprom\evmc66xxl\bin\eepromwriter_evm66xxl.out to CCS, be sure evmc66xxl.gel is used in CCS.
6. Open the Memory view (in CCSv5, view->Memory Browser), and view the memory address 0x80000000.
7. Load app.dat to 0x80000000:
* In CCSv5, right click mouse in memory window, select "load memory".
- * Browse and select tools\writer\eeprom\evmc6678l\bin\app.dat.
+ * Browse and select tools\writer\eeprom\evmc66xxl\bin\app.dat.
* Select the option "Use the file header information to set the start address and size of the memory block to be
loaded" and click "next".
* Change the Start Address to "0x80000000" if it is not 0x80000000, and click "finish".
2. Clean and build the eepromwriter project.
3. After the project build is completed, eepromwriter_evm66xxl.out and eepromwriter_evm66xxl.map will be generated under
- tools\writer\eeprom\evmc6678l\bin directory.
+ tools\writer\eeprom\evmc66xxl\bin directory.