index 26460dda18f5b34e48a88456620279be9a353f76..589c61d70e89c3bc71663ba598807cc9cb8aa032 100755 (executable)
1. Be sure to set the boot mode dip switch to no boot/EMIF16 boot mode on the EVM.
-2. Copy the binary file to writer\nand\evmc66xxl\bin directory, and rename it to app.bin.
+2. Copy the binary file to writer\nand\evmxxxx\bin directory, and rename it to app.bin.
-3. Change the file_name and start_addr in writer\nand\evmc66xxl\bin\nandwriter_input.txt if necessary.
+3. Change the file_name and start_addr in writer\nand\evmxxxx\bin\nandwriter_input.txt if necessary.
By default the NAND writer will load app.bin to DSP memory and write the data to NAND device start byte address 16384
(start address of block 1). The start_addr should always be set to the start byte addess of a block.
-4. Open CCSv5 and launch the evmc66xx emulator target configuration and connect to core 0.
+4. Open CCSv5 and launch the evmxxxx emulator target configuration and connect to core 0.
-5. Load the program writer\nand\evmc66xxl\bin\nandwriter_evm66xxl.out to CCS, be sure evmc66xxl.gel is used in CCS
+5. Load the program writer\nand\evmxxxx\bin\nandwriter_evmxxxx.out to CCS, be sure evmxxxx.gel is used in CCS
and DDR is intialized.
6. Open the Memory view (in CCSv5, view->Memory Browser), and view the memory address 0x80000000.
7. Load app.bin to 0x80000000:
* In CCSv5, right click mouse in memory window, select "load memory".
- * Browse and select writer\nand\evmc66xxl\bin\app.bin (raw data format), click "next"
+ * Browse and select writer\nand\evmxxxx\bin\app.bin (raw data format), click "next"
* Set the Start Address to "0x80000000", Type-size to 32-bits, leave swap unchecked, click "finish"
8. After the data file is loaded into the memory, run the program (in CCSv5, press F8), it will start to program the
Steps to re-build nandwriter:
1. Uses CCS to build nandwriter:
- * Import the nandwriter CCS project from writer\nand\evmc66xxl directory (in CCSv5, Project->Import Existing CCS/
+ * Import the nandwriter CCS project from writer\nand\evmxxxx directory (in CCSv5, Project->Import Existing CCS/
CCE Eclipse Projects).
* Clean and build the nandwriter project.
- * After the project build is completed, nandwriter_evm66xxl.out and nandwriter_evm66xxl.map will be generated under
- writer\nand\evmc66xxl\bin directory.
+ * After the project build is completed, nandwriter_evmxxxx.out and nandwriter_evmxxxx.map will be generated under
+ writer\nand\evmxxxx\bin directory.
2. Uses Makefile to build nandwriter:
NOTE FOR BUILDING ON WINDOWS ENVIRONMENT: For building on windows environment GNU utilities like
Linux bash shell:
export C_DIR=/opt/TI/TI_CGT_C6000_7.2.1/
MSYS bash shell:
- export C_DIR='"C:/Program Files/Texas Instruments/ccsv5/tools/compiler/c6000"'
+ export C_DIR='"C:/ti/ccsv5/tools/compiler/c6000"'
2) Code Generation tool binaries should be in the path e.g.
Linux bash shell:
export PATH=/opt/TI/TI_CGT_C6000_7.2.1/bin:$PATH
MSYS bash shell:
- export PATH=$PATH:/c/Program\ Files/Texas\ Instruments/ccsv5/tools/compiler/c6000/bin/
+ export PATH=$PATH:/c/ti/ccsv5/tools/compiler/c6000/bin/
3) variable PFORM_LIB_DIR should be set the directory of the Platform Library root, e.g.
Linux bash shell:
- export PFORM_LIB_DIR=pdk_C66xx_1_0_0_10/packages/ti/platform
+ export PFORM_LIB_DIR=pdk_xxxx_x_x_x_xx/packages/ti/platform
MSYS bash shell:
- export PFORM_LIB_DIR='"C:/Program Files/Texas Instruments/pdk_C66xx_1_0_0_10/packages/ti/platform"'
+ export PFORM_LIB_DIR='"C:/ti/pdk_xxxx_x_x_x_xx/packages/ti/platform"'
- The makefile for building the nandwriter is in the directory "tools/writer/nand/evmc66xxl"
+ The makefile for building the nandwriter is in the directory "tools/writer/nand/evmxxxx"
Following are the steps to build nandwriter, e.g.:
- cd tools/writer/nand/evmc66xxl
+ cd tools/writer/nand/evmxxxx
make DEVICE=<device number>
supported device numbers are
C6678
C6670
C6657
+ TCI6634K2K
-Please refer to BIOS MCSDK 2.0 User's Guide (http://processors.wiki.ti.com/index.php/BIOS_MCSDK_2.0_User_Guide) for more details.
\ No newline at end of file
+Please refer to BIOS MCSDK x.0 User's Guide (http://processors.wiki.ti.com/index.php/BIOS_MCSDK_x.0_User_Guide) for more details.
\ No newline at end of file