summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: abf260d)
raw | patch | inline | side by side (parent: abf260d)
author | Ivan Pang <i-pang@ti.com> | |
Fri, 21 Oct 2011 21:54:20 +0000 (17:54 -0400) | ||
committer | Ivan Pang <i-pang@ti.com> | |
Fri, 21 Oct 2011 21:54:20 +0000 (17:54 -0400) |
index 35fc35d7f419a139699edadfc523f23a50de1952..fb20f36123b967b5bc85d3b513e907b3b1f88cd4 100644 (file)
--- a/boot_loader/IBL_buildibl
+++ b/boot_loader/IBL_buildibl
cp -f ../util/i2cConfig/i2cConfig.gel ../../../i2cConfig.gel
cp -f ../util/btoccs/b2ccs.exe ../../../b2ccs.exe
cp -f ../util/btoccs/b2i2c.exe ../../../b2i2c.exe
+cp -f ../util/btoccs/ccs2bin.exe ../../../ccs2bin.exe
cp -f ../util/bconvert/bconvert64x.exe ../../../bconvert64x.exe
cp -f ../util/romparse/romparse.exe ../../../romparse.exe
mv -f ../../../i2cConfig.gel bin/i2cConfig.gel
mv -f ../../../b2ccs.exe ../util/btoccs/b2ccs.exe
mv -f ../../../b2i2c.exe ../util/btoccs/b2i2c.exe
+mv -f ../../../ccs2bin.exe ../util/btoccs/ccs2bin.exe
mv -f ../../../bconvert64x.exe ../util/bconvert/bconvert64x.exe
mv -f ../../../romparse.exe ../util/romparse/romparse.exe
index 765821fca0add009c1baa84d172d3c08d2d4d490..0414afa9e371586fa3a926a2d3f14e6649271dcc 100644 (file)
{
if (fputs(line, out) < 0)
{
- printf ("fputs %s error\n", fputs);
+ printf ("fputs %s error\n", line);
goto error;
}
}
if (fputs("};\n", out) < 0)
{
- printf ("fputs %s error\n", fputs);
+ printf ("fputs };\\n error\n");
goto error;
}
diff --git a/post/docs/README.txt b/post/docs/README.txt
index 82092e7f6de0ad995db49fd0c1160d33784b4bde..285d59c0100f6ef9fefe33bba62c715cf719ad96 100644 (file)
--- a/post/docs/README.txt
+++ b/post/docs/README.txt
Steps to program POST to EEPROM:
-1. Be sure that IBL romparse.exe is pre-built under tools\boot_loader\ibl\src\util\romparse, if IBL is not built,
- refer to tools\boot_loader\ibl\doc\README.txt on how to build IBL for EVMC66xxL.
+1. Copy tools\post\evmc66xxl\bin\post_i2crom.bin to tools\writer\eeprom\evmc66xxl\bin directory
-2. Go to the tools\post\evmc66xxl\bin directory in Windows Explorer and open the post_romparse.bat in a text editor,
- change "C6000_CG_DIR", "TARGET", "ENDIAN" and "IBL_ROOT_DIR" parameters accordingly.
+2. Navigate to tools\writer\eeprom\evmc66xxl\bin\ and open eepromwriter_input.txt. Make the following changes:
+ - Set the file_name to post_i2crom.bin
+ - Set the bus_addr to 0x50
+ - Set start_addr to 0
+ - Set swap_data to 0
+ Save and close eepromwriter_input.txt
-3. Double click post_romparse.bat. This will generate a CCS format image file "post_i2crom.dat", which can be programmed
- to I2C EEPROM slave bus address 0x50, below are the steps how to program the EEPROM using the EEPROM writer utility:
-
- * Copy post_i2crom.dat to tools\writer\eeprom\evmc66xxl\bin directory and rename it to "app.dat".
- * Change bus_addr to 0x50 and swap_data to "0" in tools\writer\eeprom\evmc66xxl\bin\eepromwriter_input.txt and save the file.
- * Refer to tools\writer\eeprom\evmc66xxl\docs\README.txt on how to program the CCS data file to EEPROM.
+3. Refer to tools\writer\eeprom\evmc66xxl\docs\README.txt on how to program the raw binary file to EEPROM
4. Once the programming is completed successfully, user can set the boot mode to I2C mode with bus address 0x50 and
boot the POST directly from the EEPROM after POR. The boot status and test result can be monitored using the Hyper
index cd42df0a84bcab7a647d634ec81e949e3432300d..92c9251180b5a3e17f6287fd1130798adc26acce 100644 (file)
echo Generating I2C ROM data ...
%IBL_ROOT_DIR%\src\util\romparse\romparse -rom_base 0x50 post_i2crom.map.pp
-mv i2crom.ccs post_i2crom.dat
+%IBL_ROOT_DIR%\src\util\btoccs\ccs2bin -swap i2crom.ccs post_i2crom.bin
rm -f *.ccs *.b
index 03d5e5860779a31d4d334a81159727a7fcf70ae5..a8378d4b07467ddc782ae964e858daa0b36774b7 100644 (file)
echo Generating I2C ROM data ...
%IBL_ROOT_DIR%\src\util\romparse\romparse -rom_base 0x50 post_i2crom.map.pp
-mv i2crom.ccs post_i2crom.dat
+%IBL_ROOT_DIR%\src\util\btoccs\ccs2bin -swap i2crom.ccs post_i2crom.bin
rm -f *.ccs *.b
index 9da0cb98412b737b5f2108434956ce6f5a8b196d..a456d3812a2558ebb30bb3cb1d6cf74c6345b6fe 100644 (file)
EEPROM Writer is a simple utility to program a CCS format image/data file to I2C EEPROM.
-Steps to program the EEPROM:
+Steps to program the EEPROM with a binary file:
1. Be sure to set the boot mode dip switch to no boot/EMIF16 boot mode on the EVM.
-2. Copy the CCS format data file to writer\eeprom\evmc66xxl\bin directory, and rename it to app.dat.
+2. Copy the binary file to writer\eeprom\evmc66xxl\bin directory.
3. Change the file_name, bus_addr, start_addr and swap_data in writer\eeprom\evmc66xxl\bin\eepromwriter_input.txt if necessary.
- By default the EEPROM writer will load app.dat to DSP memory and write the data to I2C slave
+ Make sure that file_name is set to the name of your binary file.
+
+ *By default the EEPROM writer will load app.bin to DSP memory and write the data to I2C slave
bus address 81 (0x51) at EEPROM device start byte address 0 with data swap disabled (0).
-
+
4. Open CCSv5 and launch the evmc66xx emulator target configuration and connect to core 0.
5. Load the program writer\eeprom\evmc66xxl\bin\eepromwriter_evm66xxl.out to CCS, be sure evmc66xxl.gel is used in CCS
7. Load app.dat to 0x80000000:
* In CCSv5, right click mouse in memory window, select "load memory".
- * Browse and select writer\eeprom\evmc66xxl\bin\app.dat.
- * Select the option "Use the file header information to set the start address and size of the memory block to be
- loaded" and click "next".
- * Change the Start Address to "0x80000000" if it is not 0x80000000, and click "finish".
+ * Browse and select your binary file.
+ - By default, the browse menu only displays .dat files. You will have to change the option
+ TI Data Format (*.dat) to Raw Data Format (*.bin) to find your binary file.
+ * Change the Start Address to "0x80000000" if it is not 0x80000000
+ * Change the Type-size to 32 bits if it is not 32 bits.
+ * click "finish".
8.After the data file is loaded into the memory, run the program (in CCSv5, press F8), it will start to program the
EEPROM.
9.When programming is completed, the console will print "EEPROM programming completed successfully", if there
is any error, the console will show the error message.
-
Steps to re-build eepromwriter:
1. Uses CCS to build eepromwriter:
diff --git a/writer/eeprom/evmc6670l/bin/eepromwriter_input.txt b/writer/eeprom/evmc6670l/bin/eepromwriter_input.txt
index 76b3dd90a7986ff08ea8b44d6600ab5e821834c6..d87d3c46e33dce4edb5df6db5af8a490e35c6c39 100644 (file)
-file_name = app.dat
+file_name = app.bin
bus_addr = 0x51
start_addr = 0
swap_data = 0
diff --git a/writer/eeprom/evmc6678l/bin/eepromwriter_input.txt b/writer/eeprom/evmc6678l/bin/eepromwriter_input.txt
index 76b3dd90a7986ff08ea8b44d6600ab5e821834c6..d87d3c46e33dce4edb5df6db5af8a490e35c6c39 100644 (file)
-file_name = app.dat
+file_name = app.bin
bus_addr = 0x51
start_addr = 0
swap_data = 0