summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 076ca09)
raw | patch | inline | side by side (parent: 076ca09)
author | Hao Zhang <hzhang@ti.com> | |
Thu, 21 Apr 2011 21:47:53 +0000 (17:47 -0400) | ||
committer | Hao Zhang <hzhang@ti.com> | |
Thu, 21 Apr 2011 21:47:53 +0000 (17:47 -0400) |
boot_loader/IBL_README.txt | patch | blob | history | |
boot_loader/examples/i2c/emac/docs/README.txt | patch | blob | history |
index 433ceb13d220e1cc16809107ba8acc202f70c4ca..9d9aa2547629f54b1be5c7114a082e8c1e5fd8c6 100644 (file)
window and select "Load GEL"
e. Run the GEL script EVMC66xx IBL->setConfig_c66xx_main, this will by default set the boot parameters for NOR boot over
- I2C. If the user wants to configure NAND boot or EMAC boot over I2C, he/she should run EVMC66xx IBL->setConfig_c66xx_main
+ I2C. Wait for 10 seconds to ensure that the script configuration is completed.
+
+ f. If the user wants to configure NAND boot or EMAC boot over I2C, he/she should run EVMC66xx IBL->setConfig_c66xx_main
followed by EVMC66xx IBL->setConfig_c66xx_nand or EVMC66xx IBL->setConfig_c66xx_emac.
- f. Press "Enter" in the CCS console window, and the program will write the boot configuration table to the EEPROM
+ g. Press "Enter" in the CCS console window, and the program will write the boot configuration table to the EEPROM
diff --git a/boot_loader/examples/i2c/emac/docs/README.txt b/boot_loader/examples/i2c/emac/docs/README.txt
index f5fe3d996eab76ceea94a55224fd6898894248eb..504328142082cd27c595d3e8dee8b2db417b642f 100644 (file)
5. Start a TFTP server (you can download a free, open source application from http://tftpd32.jounin.net) and copy
app.dat to the TFTP base directory.
-6. Set the IP address of the PC that is running the TFTP server to 192.168.1.101, since by default IBL will set the EVM IP
- address to 192.168.1.100 and the TFTP server IP address to 192.168.1.101.
+6. Set the IP address of the PC that is running the TFTP server to 192.168.2.101, since by default IBL will set the EVM IP
+ address to 192.168.2.100 and the TFTP server IP address to 192.168.2.101.
7. Be sure the EVM and the PC are connected in the same subnet of a local network, after POR, the EVM will download the
boot image from TFTP server and boot from it.