1 /***************************************************
2 * File: netcp_cfg.h
3 * Purpose: netcp config API
4 **************************************************************
5 * FILE: netcp_cfg.h
6 *
7 * DESCRIPTION: netapi NETCP configuration API header file
8 * for user space transport library
9 *
10 * REVISION HISTORY: rev 0.0.1
11 *
12 * Copyright (c) Texas Instruments Incorporated 2010-2011
13 *
14 * Redistribution and use in source and binary forms, with or without
15 * modification, are permitted provided that the following conditions
16 * are met:
17 *
18 * Redistributions of source code must retain the above copyright
19 * notice, this list of conditions and the following disclaimer.
20 *
21 * Redistributions in binary form must reproduce the above copyright
22 * notice, this list of conditions and the following disclaimer in the
23 * documentation and/or other materials provided with the
24 * distribution.
25 *
26 * Neither the name of Texas Instruments Incorporated nor the names of
27 * its contributors may be used to endorse or promote products derived
28 * from this software without specific prior written permission.
29 *
30 * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
31 * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
32 * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
33 * A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
34 * OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
35 * SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
36 * LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
37 * DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
38 * THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
39 * (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
40 * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
42 ***************************************************/
44 #ifndef __NETCP_CFG__H
45 #define __NETCP_CFG__H
47 #include "netapi.h"
48 #include "ti/drv/pa/pa.h"
49 #include "ti/runtime/pktlib/pktlib.h"
51 //NETCP FLOW
52 typedef struct NETCP_CFG_FLOW_Tag
53 {
54 int flowid;
55 } NETCP_CFG_FLOW_T;
56 typedef void * NETCP_CFG_FLOW_HANDLE_T;
59 //NETCP ROUTE
60 typedef struct NETCP_CFG_ROUTE_Tag
61 {
62 NETCP_CFG_FLOW_HANDLE_T p_flow;
63 PKTIO_HANDLE_T * p_dest_q;
64 int nextAction;
65 } NETCP_CFG_ROUTE_T;
66 typedef void * NETCP_CFG_ROUTE_HANDLE_T;
68 /*--------------flow management--------*/
69 NETCP_CFG_FLOW_HANDLE_T netcp_cfgAddFlow(NETAPI_T ,
70 int n,
71 Pktlib_HeapHandle handles[],
72 int * err );
73 void netcp_cfgDelFlow(NETAPI_T , NETCP_CFG_FLOW_HANDLE_T , int * err);
75 /*------------Routes------------------*/
76 NETCP_CFG_ROUTE_HANDLE_T netcp_cfgAddRoute(NETAPI_T ,int nh,
77 Pktlib_HeapHandle heaps[],
78 int *err );
79 void netcp_cfgDelRoute(NETAPI_T , NETCP_CFG_ROUTE_HANDLE_T, int *err );
81 /*-----------Actions----------*/
82 #define NETCP_CFG_ACTION_DISCARD 0
83 #define NETCP_CFG_ACTION_CONTINUE 1 //pass packet on to next classifier
84 #define NETCP_CFG_ACTION_TO_SW 2
86 /******************************************************************/
87 /***********************APP ids for rx meta data********************/
88 /******************************************************************/
89 // NWAL "AP ids" for PA Rules that are added
90 #define NETAPI_NETCP_MATCH_GENERIC_MAC 0x10000000 //lower byte==interface
91 #define NETAPI_NETCP_MATCH_GENERIC_IP 0x20000000 //lower byte==interface
92 #define NETAPI_NETCP_MATCH_CLASS 0x80000000 //or' in classifier #, lower byte==interface
95 /*---------MAC APPID------------------*/
96 typedef uint32_t NETCP_CFG_MACIF_T;
98 /*------------L2----------------------*/
99 typedef void * NETCP_CFG_VLAN_T;
101 /*---------------IP APPID-------------------*/
102 typedef uint32_t NETCP_CFG_IP_T;
104 /* del mac i/f */
105 void netcp_cfgDelMac(NETAPI_T h,int iface_no, int *err);
106 void netcp_cfgDelIp(NETAPI_T h, int iface_no, nwal_IpType ipType,
107 nwalIpAddr_t * ip_addr,
108 nwalIpOpt_t * ip_qualifiers, int *err);
111 /*****************************************************************
112 * Create a MAC interface
113 ****************************************************************/
114 /*
115 * @brief API Creates a MAC interface
116 *
117 * @details This api is used to create a MAC interface.
118 * Once it is created, the MAC interface can be used to receive packets. The API
119 * adds a rule to the NETCP 1st level lookup tables to route all packets with destination
120 * MAC matching supplied argument and not matching any other lookup entry (see @ref netcp_cfgAddIp) to
121 * the supplied route, @ref NETCP_CFG_ROUTE_T, (or default route).
122 * Packets arriving that match this rule are identified in meta data with Appid= NETAPI_NETCP_MATCH_GENERIC_MAC
123 * Note: The internal SOC switch must be "taught" that this mac
124 * address is present by transmitting a packet with destination mac = this interface mac address.
125 * @param[in] @ref NETAPI_T: NETAPI instance
126 * @param[in] char *: pointer to 6 byte MAC address for interface
127 * @param[in] int : interface number (0,1,..)
128 * @param[in] int : switch port (0 don't care, 1 switch port 1, 1 switch port 2) [only 0 supported]
129 * @param[in] @ref NETCP_CFG_ROUTE_HANDLE_T : [future] handle of a created route or NULL to use internal default route
130 * @oaram[in] @ref NETCP_CFG_VLAN_T : [future[ vlan configuration . Set to NULL
131 * @param[in] int : [future] interface state (0=down, 1= up)
132 * @param[out] int * err: pointer to error return
133 * @retval @ref NETCP_CFG_MACIF_T : returned AppID for interface (this is returned in meta data for
134 * received packets matching this rule an no others)
135 * @pre @ref netapi_init
136 */
137 NETCP_CFG_MACIF_T netcp_cfgCreateMacInterface(
138 NETAPI_T h, //
139 uint8_t *p_mac, //mac address associated with interface
140 int iface_no, //0,1, ..
141 int switch_port,//0=don't care, 1=switch port 1, 2=switch port 2 , ..
142 NETCP_CFG_ROUTE_HANDLE_T route, //NULL to use default
143 NETCP_CFG_VLAN_T vlan, //future
144 int state, //0=down, 1=up //FUTURE
145 int * err
146 );
148 /*****************************************************************
149 * Add IP address/qualifier to MAC interface
150 ****************************************************************/
151 /*
152 * @brief API attaches an IP adderess and qualifier to a MAC interface
153 *
154 * @details This api is used to add an IP address to a MAC interface along
155 * with optional IP qualifier. A route, @ref NETCP_CFG_ROUTE_HANDLE_T,or NULL for default
156 * may be specified to indicate where to send packets matching the MAC interface MAC address, the
157 * supplied IP address and any qualifier. This API adds a rule to the NETCP level 1 lookup tables
158 * Packets arriving that match this rule are identified in meta data with Appid= NETAPI_NETCP_MATCH_GENERIC_IP
159 * Note: An IP address must be attached to enable NETCP Recevie Checksum offload feature
160 * @param[in] @ref NETAPI_T: NETAPI instance
161 * @param[in] int : interface number (0,1,..)
162 * @param[in] @ref nwal_IpType : type of IP address (V4 for V6)
163 * @oaram[in] @ref nwalIpAddr_t : ip_address
164 * @param[in] @ref nwalIpOpt_t : ip_qualifiers (all 0 for no qualifiers). This can be used to apply special handling for
165 * diffserv category for example
166 * @param[in] @ref NETCP_CFG_ROUTE_HANDLE_T : [future] handle of a created route or NULL to use internal default route
167 * @param[out] int * err: pointer to error return
168 * @retval @ref NETCP_CFG_IP_T : returned AppID for attached rule. This is returned in RX meta data for
169 * packets matching this rule and no other.
170 * @pre @ref netapi_init , @ref netcp_cfgAddMac
171 */
172 NETCP_CFG_IP_T netcp_AddIp(
173 NETAPI_T h,
174 int iface_no,
175 nwal_IpType ipType,
176 nwalIpAddr_t * ip_addr,
177 nwalIpOpt_t * ip_qualifiers,
178 NETCP_CFG_ROUTE_HANDLE_T route, //NULL for default
179 int * err
180 );
182 /*------------------classification [FUTURE]-------------------*/
183 typedef void *NETCP_CFG_CLASS_T;
185 //add classifier
186 typedef struct NETCP_CFG_CLASSIFIER_Tag
187 {
188 //tbd a classisfier
190 } NETCP_CFG_CLASSIFIER_T;
192 NETCP_CFG_CLASS_T netcp_cfgAddClass(NETAPI_T h,
193 NETCP_CFG_CLASSIFIER_T *p_class,
194 NETCP_CFG_ROUTE_HANDLE_T p_route,
195 int action, int * err);
196 //del classifier
197 void netcp_cfgDelClass(NETAPI_T h,
198 NETCP_CFG_CLASS_T p_class,
199 int *err);
203 /***************************************************************************
204 ********************************STATS**************************************
205 **************************************************************************/
207 /*
208 * @brief This is the callback function that is used to return statistics from NETCP
209 *
210 * @details The application provides a callback function that NETAPI uses to report statistics.
211 * The request for stats is generated from the @ref netcp_cfgReqStats API.
212 * Note: to receive ths stats callback, the @ref netapi_netcpPoll funcition must be called
213 * @param[in] @ref NETAPI_T: NETAPI instance
214 * @param[in] @ref paSysStats_t * : the PA (NETCP packet accelerator subsystem) statistics block
215 * @retval none
216 * @pre @ref netapi_init , @ref netapi_cfgReqStats, @ref netapi_netcpPoll
217 */
218 //stats CB
219 typedef void (*NETCP_CFG_STATS_CB)( NETAPI_T h, paSysStats_t* pPaStats);
222 //stats request
223 /*
224 * @brief API request statistics from NETCP
225 *
226 * @details This api is used to request a statistics from NETCP. This will generate a stats request
227 * command to NETCP. Sometime later, the statistics result will arrive and will be passed to
228 * the caller via the asynchronus callback @ref NETCP_CFG_STATS_CB that is registered in this call.
229 * Note: to receive the stats callback, the @ref netapi_netcpPoll funcition must be called
230 * @param[in] @ref NETAPI_T: NETAPI instance
231 * @param[in] @ref NETCP_CFG_STATS_CB : the function to call with the resulting statistics block
232 * @param[in] int : clear the stats in NETCP after the report (0=no, 1=yes)
233 * @param[out] int * err: pointer to error return
234 * @retval none
235 * @pre @ref netapi_init
236 */
237 void netcp_cfgReqStats(NETAPI_T h, //NEAPI instance
238 NETCP_CFG_STATS_CB c, //stats report callback function
239 int doClear, //0: don't clear, 1 clear
240 int *err);
242 #endif