/***************************************** * file: netapi_loc.h * purpose: internal netapi stuff ****************************************/ #ifndef __NETAPI_LOC__H #define __NETAPI_LOC__H /*************************************** * INTERNAL HANDLE STRUCTURE DEFINITION ****************************************/ /*********************************************** * GLOBAL AREA * short term: this is global to process * (multi-process not supported) * long term: this structure gets put in shared memory ***********************************************/ /* list of global pktio channels that have been created (NETCP_TX, RX are intrinsic so won't be here) */ typedef struct PKTIO_ENTRY_tag { char name[PKTIO_MAX_NAME+1]; Qmss_Queue qn; // -1 => slot is free } PKTIO_ENTRY_T; /* to hold an IP on an interface */ typedef struct NETCP_INTERFACE_IP_Tag { int in_use; void * nwal_handle; nwal_IpType ip_type; nwalIpAddr_t ip_addr; nwalIpOpt_t ip_qualifiers; } NETCP_INTERFACE_IP_T; /* to hold a classifier */ typedef struct NETCP_INTERFACE_CLASSIFIER_Tag { int in_use; int class_type; //see netcp_cfg.h void * nwal_L2_handle; void * nwal_L3_handle; void * nwal_L4_handle; } NETCP_INTERFACE_CLASSIFIER_T; /* to hold an ipsec rx policy */ typedef struct NETCP_IPSEC_POLICY_Tag { int in_use; int tunnel; //associated tunnel void * nwal_handle; //handle associated with this RX Policy } NETCP_IPSEC_POLICY_T; /* to hold a tunnel */ typedef struct NETCP_IPSEC_SA_Tag { int in_use; int inbound; //true if inbound int sa_mode; //mode we are going to use #define NETCP_IPSEC_SA_MODE_INFLOW 0 #define NETCP_IPSEC_SA_MODE_SIDEBAND 1 void * sa_handle_inflow; //for inflow mode void * sa_handle_sideband; //for sideband mode int iface; //associated interface } NETCP_IPSEC_SA_T; /* to hold a netcp 'interface' */ typedef struct NETCP_INTERFACE_Tag { int in_use; /* 1 for valid */ int state; /* 0=down, 1=up, future.. */ void * nwal_handle; //handle associated with this interface unsigned char mac[6]; // mac address unsigned int vlan; //future } NETCP_INTERFACE_T; /*to keep track of netcp config transactions */ typedef struct { nwal_Bool_t inUse; uint16_t transType; #define NETAPI_NWAL_HANDLE_TRANS_NONE 0 #define NETAPI_NWAL_HANDLE_TRANS_MAC 1 #define NETAPI_NWAL_HANDLE_TRANS_IP 2 #define NETAPI_NWAL_HANDLE_TRANS_PORT 3 #define NETAPI_NWAL_HANDLE_TRANS_SA 4 #define NETAPI_NWAL_HANDLE_TRANS_SA_POLICY 5 #define NETAPI_NWAL_HANDLE_STAT_REQUEST 6 uint16_t state; #define NETAPI_NWAL_HANDLE_STATE_IDLE 0 #define NETAPI_NWAL_HANDLE_STATE_OPEN_PENDING 1 #define NETAPI_NWAL_HANDLE_STATE_OPEN 2 #define NETAPI_NWAL_HANDLE_STATE_CLOSE_PENDING 3 #define NETAPI_NWAL_HANDLE_STATE_ERR 4 nwal_Handle handle; uint64_t transId; NETAPI_T netapi_handle; //the thread making the transaction } NetapiNwalTransInfo_t; /* to hold user defined flows */ typedef struct NETCP_REGISTERED_FLOWS_Tag { int in_use; //1=> in use void * handle; //cppi handle to resource (internal) NETCP_CFG_FLOW_T flow; } NETCP_REGISTERED_FLOWS_T; /****************************** * nwal global context * (shared over all instances) *******************************/ typedef struct { int state; #define NETAPI_NW_CXT_GLOB_INACTIVE 0x0 #define NETAPI__CXT_GLOB_ACTIVE 0x1 #define NETAPI_NW_CXT_GLOB_RES_ALLOC_COMPLETE 0x3 nwal_Handle nwalInstHandle; //internal heaps used just by netcp (sa<->pa). SW doesn't touch these Pktlib_HeapHandle sa2pa_heap; Pktlib_HeapHandle pa2sa_heap; //stats paSysStats_t paStats; int numCmdPass; int numCmdFail; int numBogusTransIds; NetapiNwalTransInfo_t transInfos[TUNE_NETAPI_MAX_NUM_TRANS]; //transactions NETCP_INTERFACE_T interfaces[TUNE_NETAPI_MAX_NUM_MAC]; //interfaces NETCP_INTERFACE_CLASSIFIER_T classi[TUNE_NETAPI_MAX_CLASSIFIERS]; //classifiers NETCP_REGISTERED_FLOWS_T flows[TUNE_NETAPI_MAX_FLOWS]; //flows NETCP_IPSEC_SA_T tunnel[TUNE_NETAPI_MAX_SA]; //tunnels NETCP_IPSEC_POLICY_T policy[TUNE_NETAPI_MAX_POLICY]; //policies NETCP_INTERFACE_IP_T ips[TUNE_NETAPI_MAX_NUM_IP]; //ips } NETAPI_NWAL_GLOBAL_CONTEXT_T; /* NWAL Local context (per core/thread) */ typedef struct { //void * nwalLocInstance; #define NETAPI_NW_CXT_LOC_INACTIVE 0x0 #define NETAPI_NW_CXT_LOC_ACTIVE 0x2 int state; int numPendingCfg; NETCP_CFG_STATS_CB stats_cb; /* stats */ int numL2PktsRecvd; int numL3PktsRecvd; int numL4PktsRecvd; int numL4PktsSent; int TxErrDrop; /* local config */ nwalLocCfg_t nwalLocCfg; } NETAPI_NWAL_LOCAL_CONTEXT_T; /* the global */ typedef struct NETAPI_GLOBAL_tag { #define NETAPI_MAX_PKTIO (TUNE_NETAPI_MAX_PKTIO) PKTIO_ENTRY_T pktios[NETAPI_MAX_PKTIO]; /* configuration */ NETAPI_CFG_T cfg; /* global timers */ /* nwal context */ NETAPI_NWAL_GLOBAL_CONTEXT_T nwal_context; NETAPI_T p_master; //DALMT save p'masters handle } NETAPI_GLOBAL_T; /************************************ * this is a per thread structure. * It contains stuff local to thread * and pointer to global stuff * that is shared over all threads, **************************************/ typedef struct NETAPI_HANDLE_Tag { int master; //master type void * global; /* pointer to the global area */ /* heap handles */ Pktlib_HeapHandle netcp_heap; /* internal default */ Pktlib_HeapHandle netcp_control_rx_heap; /* for control messages */ Pktlib_HeapHandle netcp_control_tx_heap; /* for control messages */ Pktlib_HeapHandle createdHeaps[TUNE_NETAPI_MAX_HEAPS]; /* created by app and registered */ /* pktios defined */ int n_pktios; /* #of pktios that are active for this instance */ void* pktios[NETAPI_MAX_PKTIO]; /* the list of pktios */ /* scheduler stuff. unallocated if NETAPI_INCLUDE_SCHED not set */ void * p_sched; /* nwal local context */ NETAPI_NWAL_LOCAL_CONTEXT_T nwal_local; /* security stuff */ /* timer stuff */ /* thread cookie */ void * cookie; /*set by calling thread */ } NETAPI_HANDLE_T; //internal initialization routines */ int netapi_init_qm(int max_descriptors); int netapi_init_cppi(void); int netapi_start_qm(void); int netapi_init_nwal( int region2use, Pktlib_HeapIfTable * p_table, NETAPI_NWAL_GLOBAL_CONTEXT_T * p_nwal_context, NETAPI_CFG_T *p_cfg ); int netapi_start_nwal(Pktlib_HeapHandle pkt_heap, Pktlib_HeapHandle cmd_heapRx, Pktlib_HeapHandle cmd_heapTx, NETAPI_NWAL_LOCAL_CONTEXT_T *p , NETAPI_CFG_T *p_cfg, NETAPI_NWAL_GLOBAL_CONTEXT_T * p_nwal_glob_context ); int netapi_init_timer(void); int netapi_qm_setup_mem_region( unsigned int numDesc, unsigned int descSize, unsigned int* pDescMemBase, int memRegion); //for above #define NETAPI_GLOBAL_REGION TUNE_NETAPI_QM_GLOBAL_REGION #define NETAPI_LOCAL_REGION ((NETAPI_GLOBAL_REGION)+1) //nwal callbacks void netapi_NWALRxPktCallback (uint32_t appCookie, uint16_t numPkts, nwalRxPktInfo_t* pPktInfo, uint64_t timestamp, nwal_Bool_t* pFreePkt); void netapi_NWALCmdCallBack (nwal_AppId appHandle, uint16_t trans_id, nwal_RetValue ret); void netapi_NWALCmdPaStatsReply (nwal_AppId appHandle, nwal_TransID_t trans_id, paSysStats_t *stats); void netapi_NWALSBPktCallback (uint32_t appCookie, uint16_t numPkts, nwalDmRxPayloadInfo_t* pDmRxPktInfo, nwal_Bool_t* pFreePkt); //*********************************** //internal utilities //************************************* //return the list of pktios for this instance static inline void ** netapi_get_pktio_list(NETAPI_T p) { NETAPI_HANDLE_T *pp = (NETAPI_HANDLE_T *) p; return &pp->pktios[0]; } //get scheduler block handle static inline void * netapi_get_scheduler(NETAPI_T p) { NETAPI_HANDLE_T *pp = (NETAPI_HANDLE_T *) p; return pp->p_sched; } /* return pointer to global area */ NETAPI_GLOBAL_T * netapi_get_global(void); //add a pktio name (and queue) to global list static inline int netapi_add_global_pktio(NETAPI_T p, char *name, Qmss_Queue * qn) { NETAPI_HANDLE_T *pp = (NETAPI_HANDLE_T *) p; PKTIO_ENTRY_T *pe; int i; //find a free slot pe = &((NETAPI_GLOBAL_T *)(pp->global))->pktios[0]; for(i=0;iqn.qNum == -1) { pe->qn.qNum=qn->qNum; pe->qn.qMgr=qn->qMgr; strncpy(pe->name, name, PKTIO_MAX_NAME); return 1; } pe+=1; } return 0; //no room } //delete a pktio name (and queue) to global list static inline int netapi_del_global_pktio(NETAPI_T p, char *name) { NETAPI_HANDLE_T *pp = (NETAPI_HANDLE_T *) p; PKTIO_ENTRY_T *pe; int i; //find slot pe = &((NETAPI_GLOBAL_T *)(pp->global))->pktios[0]; for(i=0;iqn.qNum == -1) continue; if (!strncmp(name, pe->name, PKTIO_MAX_NAME)) { pe->qn.qNum=-1; pe->name[0]='\0'; return 1; } pe+=1; } return 0; //no room } /* get list of global pktios that have been created */ static inline Qmss_Queue* netapi_find_global_pktio(NETAPI_T p, char *name) { NETAPI_HANDLE_T *pp = (NETAPI_HANDLE_T *) p; PKTIO_ENTRY_T *pe; int i; //find slot pe = &((NETAPI_GLOBAL_T *)(pp->global))->pktios[0]; for(i=0;iqn.qNum == -1) continue; if (!strncmp(name, pe->name, PKTIO_MAX_NAME)) { return &pe->qn; } pe +=1; } return NULL; //not found } /* return the nwal global instance handle */ static inline nwal_Handle netapi_return_nwal_instance_handle(NETAPI_T p) { NETAPI_HANDLE_T *pp = (NETAPI_HANDLE_T *) p; return ((NETAPI_GLOBAL_T *)(pp->global))->nwal_context.nwalInstHandle; } //utility to clear out a queue void netapi_zapQ(int queueNum); void netcp_cfgp_build_route(NETCP_CFG_ROUTE_T * p_route, int16_t * p_flow, Qmss_QueueHnd * p_q); //database utilities int netcp_cfgp_find_saslot( NETAPI_NWAL_GLOBAL_CONTEXT_T *p, int iface); void netcp_cfgp_delete_sa(NETAPI_NWAL_GLOBAL_CONTEXT_T *p,int sa_slot); void netcp_cfgp_insert_sa(NETAPI_NWAL_GLOBAL_CONTEXT_T *p, int sa_slot, //we 'reserved it already' int dir, int mode, void * temp1, void * temp2, void * handle_inflow, void * handle_sideband); void *netcp_cfgp_get_sa_handles( NETAPI_NWAL_GLOBAL_CONTEXT_T *p, int sa_slot, void ** p_sideband); void* netcp_cfgp_get_mac_handle(NETAPI_NWAL_GLOBAL_CONTEXT_T *p,int iface_no); NetapiNwalTransInfo_t * netapip_GetFreeTransInfo(NETAPI_GLOBAL_T *p_global, nwal_TransID_t *pTransId); void netapip_FreeTransInfo(NetapiNwalTransInfo_t* pTransInfo); void *netcp_cfgp_get_policy( NETAPI_NWAL_GLOBAL_CONTEXT_T *p, int policy_slot); #endif