]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - keystone-rtos/netapi.git/blobdiff - ti/runtime/netapi/build/netapi_doxygen.cfg
Update location of doxygen output folder, config file changes, setup script changes
[keystone-rtos/netapi.git] / ti / runtime / netapi / build / netapi_doxygen.cfg
index 557adbbf940979bcc1f80af12103ea0cbaf2d3fa..9eff4f52695988731899275ca6575584b958c6dd 100755 (executable)
@@ -38,7 +38,7 @@ PROJECT_NUMBER         =
 # If a relative path is entered, it will be relative to the location
 # where doxygen was started. If left blank the current directory will be used.
 
-OUTPUT_DIRECTORY       = ../docs
+OUTPUT_DIRECTORY       = ../docs/doxygen
 
 # If the CREATE_SUBDIRS tag is set to YES, then doxygen will create
 # 4096 sub-directories (in 2 levels) under the output directory of each output