diff --git a/ti/runtime/netapi/build/netapi_doxygen.cfg b/ti/runtime/netapi/build/netapi_doxygen.cfg
index 557adbbf940979bcc1f80af12103ea0cbaf2d3fa..9eff4f52695988731899275ca6575584b958c6dd 100755 (executable)
# If a relative path is entered, it will be relative to the location
# where doxygen was started. If left blank the current directory will be used.
-OUTPUT_DIRECTORY = ../docs
+OUTPUT_DIRECTORY = ../docs/doxygen
# If the CREATE_SUBDIRS tag is set to YES, then doxygen will create
# 4096 sub-directories (in 2 levels) under the output directory of each output