diff --git a/ti/runtime/netapi/build/netapi_doxygen.cfg b/ti/runtime/netapi/build/netapi_doxygen.cfg
index 7a5de9e509e5a910c7541ff24258db0b3a07779e..9eff4f52695988731899275ca6575584b958c6dd 100755 (executable)
# If a relative path is entered, it will be relative to the location
# where doxygen was started. If left blank the current directory will be used.
-OUTPUT_DIRECTORY = ../docs
+OUTPUT_DIRECTORY = ../docs/doxygen
# If the CREATE_SUBDIRS tag is set to YES, then doxygen will create
# 4096 sub-directories (in 2 levels) under the output directory of each output
# directories like "/usr/src/myproject". Separate the files or directories
# with spaces.
-INPUT = ../netapi.h ../netcp_cfg.h ../netapi_sec.h ../netapi_tune.h ../netapi_sched.h ../pktio.h
+INPUT = ../netapi.h ../netcp_cfg.h ../netapi_sec.h ../netapi_tune.h ../netapi_sched.h ../pktio.h ../netapi_types.h ../netapi_ver.h
# This tag can be used to specify the character encoding of the source files
# that doxygen parses. Internally doxygen uses the UTF-8 encoding, which is
# each generated HTML page. If it is left blank doxygen will generate a
# standard header.
-HTML_HEADER =
+HTML_HEADER = ../docs/tiheader.htm
# The HTML_FOOTER tag can be used to specify a personal HTML footer for
# each generated HTML page. If it is left blank doxygen will generate a
# standard footer.
-HTML_FOOTER =
+HTML_FOOTER = ../docs/tifooter.htm
# The HTML_STYLESHEET tag can be used to specify a user-defined cascading
# style sheet that is used by each HTML page. It can be used to
# the various graphs.
DOT_CLEANUP = YES
+#---------------------------------------------------------------------------
+# Configuration::additions related to the search engine
+#---------------------------------------------------------------------------
+SEARCHENGINE = NO