index 8a61e16967db74b6b6290c1211e99b1afac73bb7..672d2b486b66010c4ead5000f8b9499a6284f0ad 100755 (executable)
/**
- * @ingroup netapi_structures
+ * @ingroup cfg_structures
* @brief CPPI flow ID for default case, use NETCP_DEFAULT_FLOW
*/
typedef struct NETCP_CFG_FLOW_Tag
} NETCP_CFG_FLOW_T;
+/**
+ * @ingroup cfg_structures
+ * @brief NETAPI configuration information
+ *
+ * @details The parameters in this structure are used to configure NETAPI.
+ */
+typedef struct NETAPI_CFG_Tag
+{
+ int def_mem_size; /**< Bytes of CMA memory we have allocated */
+ int def_flow_pkt_rx_offset; /**< Offset in pkt buffer for hw to start RX */
+ int def_max_descriptors; /**< Number of descriptors in system (must be power of 2), 2^14 max */
+ int def_tot_descriptors_for_us; /**< Number of descriptors to create in our region (must be power of 2)*/
+ int def_heap_n_descriptors; /**< Number of descriptor plus buffers in default heap*/
+ int def_heap_n_zdescriptors; /**< Number of zero len descriptors in defaut heap*/
+ int def_heap_buf_size; /**< Size of buffers in default heap, max amount of area for packet data */
+ int def_heap_tailroom_size; /**< Size of tailroom in reserve */
+ int def_heap_extra_size; /**< Size of extra space at end of buffer */
+} NETAPI_CFG_T;
+
+/* @note:
+ each buffer will be allocated: def_heap_buf_size+def_heap_extra_size bytes
+ each descriptor attached to these buffers will have rigBufferLen of:
+ def_heap_buf_size.
+ for default RX flow, for rx packet, the bufptr will be def_flow_pkt_rx_offset.
+ for detault RX flow, threshold (ie max # of bytes in buffer) will be:
+ def_heap_buf_size - def_heap_tailroom_size-def_flow_pkt_rx_offset
+
+
+ RX Packet from NetCP
+
+Headroom [Application] Packet [HW] Tailroom [Application] Extra Space [Application]
+<-----------------------><--------------------------><------------------------><----------------------->
+
+Cppi_HostDesc->origBufferLen
+<----------------------------------------------------------------------------->
+Cppi_HostDesc->origBuffPtr
+|
+\/
+|------------def_heap_buf_size-------------------------------------------------|--def_heap_extra_size--|
+| def_flow_pkt_rx_offset| max Cppi_HostDesc->buffLen | def_heap_tailroom_size | Extra Size |
+ ^
+ |
+ Cppi_HostDesc->buffPtr
+
+
+*/
+
/**
- * @ingroup netapi_constants
+ * @ingroup cfg_constants
* @brief This defines the handle to NETCP configuration flow.
*/
typedef void * NETCP_CFG_FLOW_HANDLE_T;
/**
- * @ingroup netapi_constants
+ * @ingroup cfg_constants
* @def NETCP_DEFAULT_FLOW
* This defines the NETCP default FLOW to be NULL.
*/
/**
- * @ingroup nwal_api_constants
+ * @ingroup cfg_constants
* @brief Handle to the default NETCP route.
* @details Application to use this handle to identify default NETCP route.
*/
/**
- * @ingroup netapi_structures
+ * @ingroup cfg_structures
* @brief NETCP application defined route information.
*
*/
typedef struct NETCP_CFG_ROUTE_Tag
{
NETCP_CFG_FLOW_T * p_flow; /**< NULL or NETCP_DEFAULT_FLOW for default flow, @ref NETCP_CFG_FLOW_T */
- PKTIO_HANDLE_T * p_dest_q;/**<NULL for default destination queue */
+ PKTIO_HANDLE_T * p_dest_q; /**<NULL for default destination queue */
} NETCP_CFG_ROUTE_T;
/**
- * @ingroup netapi_constants
+ * @ingroup cfg_constants
* @def NETCP_CFG_ACTION_DISCARD
* This defines the NETCP action to discard packet.
*/
#define NETCP_CFG_ACTION_DISCARD 0
/**
- * @ingroup netapi_constants
+ * @ingroup cfg_constants
* @def NETCP_CFG_ACTION_CONTINUE
* This defines the NETCP action to pass packet ono the next classifier
*/
#define NETCP_CFG_ACTION_CONTINUE 1
/**
- * @ingroup netapi_constants
+ * @ingroup cfg_constants
* @def NETCP_CFG_ACTION_TO_SW
* This defines the NETCP action to pass packet to User space application
*/
/**
- * @ingroup nwal_api_constants
+ * @ingroup cfg_constants
* @brief Handle to the default NETCP route.
* @details Application to use this handle to identify default NETCP route.
*/
typedef void * NETCP_CFG_VLAN_T;
/**
- * @ingroup nwal_api_constants
+ * @ingroup cfg_constants
* @brief AppID for MAC interface
*/
typedef uint32_t NETCP_CFG_MACIF_T;
/**
- * @ingroup nwal_api_constants
+ * @ingroup cfg_constants
* @brief AppID for IP interface
*/
typedef uint32_t NETCP_CFG_IP_T;
/**
- * @ingroup nwal_api_constants
+ * @ingroup cfg_constants
* @brief This define is used to identify the application id associated with a created SA
*/
typedef uint32_t NETCP_CFG_SA_T;
/**
- * @ingroup nwal_api_constants
+ * @ingroup cfg_constants
* @brief AppId used to identify NETCP IPSEC policy
*/
typedef uint32_t NETCP_CFG_IPSEC_POLICY_T;
/**
- * @ingroup nwal_api_constants
+ * @ingroup cfg_constants
* @def NETCP_CFG_NO_INTERFACE
* This define is to be used in AddIp, AddClassifier to indicate any MAC address.
*/
*/
/**
- * @ingroup netapi_constants
+ * @ingroup cfg_constants
* @def NETAPI_NETCP_MATCH_GENERIC_MAC
- * This define is used to indicate that apacket matched a MAC entry. Entry # (logical interface) is in byte 0 of APPID.
+ * This define is used to indicate that apacket matched a MAC entry. Entry # (logical interface) is in byte 0 of APPID.
* Packet did not match any other rule
*/
#define NETAPI_NETCP_MATCH_GENERIC_MAC 0x10000000 //lower byte==interface
/**
- * @ingroup netapi_constants
+ * @ingroup cfg_constants
* @def NETAPI_NETCP_MATCH_GENERIC_IP
* This define is used to indicate that a packet matched a MAC entry. Entry # (logical interface) is in byte 0 of APPID
* packet matched a generic IP rule attached to that interface. The IP rule # for the interface
/**
- * @ingroup netapi_constants
+ * @ingroup cfg_constants
* @def NETAPI_NETCP_MATCH_CLASS
* This define is used to indicate that a packet matched a MAC entry. Entry # (logical interface) is in byte 0 of APPID
* packet matched a generic IP rule attached to that interface OR a general IP rule added as part of
#define NETAPI_NETCP_MATCH_CLASS 0x80000000 //FULL MATCH or' in classifier (16 bits), lower byte==interface
/**
- * @ingroup netapi_constants
+ * @ingroup cfg_constants
* @def NETAPI_NETCP_MATCH_CLASS_L3
* This define is used to indicate that a packet matched a MAC entry. Entry # (logical interface) is in byte 0 of APPID
* packet matched a general IP rule added as part of a classifier. But it not match a
#define NETAPI_NETCP_MATCH_CLASS_L3 0x40000000 //MATCHED L3 but not L4. lower byte==interface
/**
- * @ingroup netapi_constants
+ * @ingroup cfg_constants
* @def NETAPI_NETCP_MATCH_IPSEC
* This define is used to indicate that a packet matched a MAC entry. Entry # (logical interface) is in byte 0 of APPID
* packet matched an IPSEC SA rule (matched proto, dest ip and SPI). The SA id is in
#define NETAPI_NETCP_MATCH_IPSEC 0x01000000 //lower byte==interface, Or' in SA id (16 bits)
/**
- * @ingroup netapi_constants
+ * @ingroup cfg_constants
* @def NETAPI_NETCP_MATCH_IPSEC_POLICY
* This define is used to indicate that a packet matched a MAC entry. Entry # (logical interface) is in byte 0 of APPID
* packet matched an IPSEC SA rule (matched proto, dest ip and SPI). Packet matched
/**
- * @ingroup netapi_cfg_functions
+ * @ingroup cfg_functions
* @brief netcp_cfgAddFlow API to add a flow
*
* @details This api is used to add a flow
/**
- * @ingroup netapi_cfg_functions
+ * @ingroup cfg_functions
* @brief netcp_cfgDelFlow API to delete a flow
*
* @details This api is used to delete a flow
int * err);
/**
- * @ingroup netapi_cfg_functions
+ * @ingroup cfg_functions
* @brief netcp_cfgDelMac API to delete MAC interface
*
* @details This api is used to delete a MAC interface
/**
- * @ingroup netapi_cfg_functions
+ * @ingroup cfg_functions
* @brief API attaches an IP adderess and qualifier to a MAC interface
*
* @details This api is used to add an IP address to a MAC interface along
);
/**
- * @ingroup netapi_cfg_functions
+ * @ingroup cfg_functions
* @brief netcp_cfgDelIp API to delete IP interface
*
* @details This api is used to delete an IP interface
/**
- * @ingroup netapi_cfg_functions
+ * @ingroup cfg_functions
* @brief netcp_cfgCreateMacInterface API to create a MAC interface
*
* @details This api is used to create a MAC interface.
/**
- * @ingroup netapi_structures
+ * @ingroup cfg_structures
* @brief NETAPI Class L4 Configuration
*
* @details This structure contains Class L4 Configuration. L2,L3 implied by iface, ip
/**
- * @ingroup netapi_structures
+ * @ingroup cfg_structures
* @brief NETAPI Classifier L4 plus IPSEC policy configuration
*
* @details This structure contains Class L4 plus IPSEC policy configuration. L2,L3 implied by iface, ip
/**
- * @ingroup netapi_structures
+ * @ingroup cfg_structures
* @brief NETAPI Classifier L4/L3 configuration
*
* @details This structure contains Class L4 and Class L3 configuration. L2 implied by iface
} NETCP_CFG_CLASS_L3_L4_T;
/**
- * @ingroup netapi_structures
+ * @ingroup cfg_structures
* @brief NETAPI Classifier configuration
*
* @details This structure contains the NETAPI classifer configuration
*/
typedef struct NETCP_CFG_CLASSIFIER_Tag
{
- int classType; /**< Classifier type */
+
+/**
+ * Classifer type which can be set to one of the following defines:
+ * <br>
+ * @ref NETCP_CFG_CLASS_TYPE_L4 , @ref NETCP_CFG_CLASS_TYPE_L3_L4
+ */
+ int classType;
+
/**
* @def NETCP_CFG_CLASS_TYPE_L4
- * This defines classifier type to be Class L4
+ * @ingroup cfg_constants
+ * This defines classifier type to be Class L4 TBD
*/
#define NETCP_CFG_CLASS_TYPE_L4 0
/**
* @def NETCP_CFG_CLASS_TYPE_L3_L4
- * This defines classifier type to be Class L4 and L3
+ * @ingroup cfg_constants
+ * This defines classifier type to be Class L4/L3 TBD
*/
#define NETCP_CFG_CLASS_TYPE_L3_L4 1
+
union
{
NETCP_CFG_CLASS_L3_L4_T c_l3_l4; /**< @ref NETCP_CFG_CLASS_L3_L4_T */
/**
- * @ingroup netapi_cfg_functions
+ * @ingroup cfg_functions
* @brief netcp_cfgAddClass API can be used to route a packet flow to a specific PKTIO channel
*
* @details This api can be used to route a packet flow to a particular PktIO channel, use a specific
/**
- * @ingroup netapi_cfg_functions
+ * @ingroup cfg_functions
* @brief netcp_cfgDelClass API can be used to delete a preconfigured classifier
*
* @details This API can be used to delete a preconfigured classifier
paSysStats_t* pPaStats);
/**
- * @ingroup netapi_cfg_functions
+ * @ingroup cfg_functions
* @brief netcp_cfgReqStats API to request statistics from NETCP
*
* @details This api is used to request a statistics from NETCP. This will generate a stats request