index bad13f42d881fc1caa22aa71c6f502123504644f..69934e7d51adc28cd6e9974de552e73e3693d206 100755 (executable)
-/************************************************
+/****************************************************************************
* FILE: netapi_init.c
-* Global, local initialization of NETAPI
+* Global, Private initialization and cleanup routines and defines of NETAPI
*
- * DESCRIPTION: Functions to initialize framework resources for running NETAPI
+ * DESCRIPTION: Functions to initialize and cleanup framework resources
+ * for running NETAPI
*
* REVISION HISTORY:
*
- * Copyright (c) Texas Instruments Incorporated 2010-2011
+ * Copyright (c) Texas Instruments Incorporated 2013
*
* Redistribution and use in source and binary forms, with or without
* modification, are permitted provided that the following conditions
* (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
* OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
*
- ***********************************************/
-#include <stdint.h>
-#include <stdio.h>
-#include <string.h>
+ ***************************************************************************/
+
+#include "netapi.h"
+#include "netapi_loc.h"
#include <sys/types.h>
#include <sys/stat.h>
#include <fcntl.h>
#include <errno.h>
#include <unistd.h>
-#include <ti/drv/nwal/nwal.h>
-#include "netapi.h"
-#include "netapi_loc.h"
#include "ti/drv/nwal/nwal.h"
/* CSL RL includes */
#include <ti/csl/csl_xmcAux.h>
#include <ti/drv/qmss/qmss_qm.h>
+
+/* Global variablesto hold virtual address of various subsystems */
+extern hplib_virtualAddrInfo_T netapi_VM_VirtAddr[];
+
+/* Global variables which needs to be populated with memory pool attributes
+ which is passed to HPLIB for memory pool initialization*/
+extern hplib_memPoolAttr_T netapi_VM_MempoolAttr[];
+extern unsigned char *netapi_VM_QMemLocalDescRam;
+extern unsigned char *netapi_VM_QMemGlobalDescRam;
+extern unsigned char *netapi_VM_SaContextVaddr;
+
+extern Pktlib_HeapIfTable netapi_pktlib_ifTable;
+extern NETAPI_GLOBAL_T netapi_global;
+
+
/* TODO verify: */
#define CACHE_LINESZ 64
-#define System_printf printf
+
#define ALIGN(x) __attribute__((aligned (x)))
/*****************************************************************************
uint8_t *cppiMemTxCtlLinkBuf = NULL;
-//****************************************************
-// Set up QM memory region (per SOC)
-//***************************************************
-int netapi_qm_setup_mem_region(
+/********************************************************************
+ * FUNCTION PURPOSE: Internal NETAPI function to setup the QM memory region
+ ********************************************************************
+ * DESCRIPTION: Internal NETAPI function to setup the QM memory region,
+ * once per SOC
+ ********************************************************************/
+int netapip_qmSetupMemRegion(
uint32_t numDesc,
uint32_t descSize,
uint32_t* pDescMemBase,
Qmss_MemRegion memRegion)
{
- Qmss_MemRegInfo memInfo;
- Int32 result;
- Int n;
- static int netapi_qm_region_index=0;
-
- memset(&memInfo,0,sizeof(Qmss_MemRegInfo));
- memInfo.descBase = pDescMemBase;
- memInfo.descSize = descSize;
- memInfo.descNum = numDesc;
- memInfo.manageDescFlag = Qmss_ManageDesc_MANAGE_DESCRIPTOR;
- memInfo.memRegion = memRegion;
-
- if(memRegion == NETAPI_GLOBAL_REGION)
- {
- memInfo.startIndex = TUNE_NETAPI_QM_START_INDEX; //was 0
- netapi_qm_region_index += numDesc;
- }else if(memRegion ==NETAPI_LOCAL_REGION)
- {
- /* 2nd region for descriptors (perhaps private?) */
- memInfo.startIndex = netapi_qm_region_index;
- }
- else
- {
- return -1 ;
- }
-
- memset (pDescMemBase, 0, (descSize * numDesc));
-
- result = Qmss_insertMemoryRegion (&memInfo);
- if (result < QMSS_SOK)
- {
- printf (">function setup_qm_region: Qmss_insertMemoryRegion returned error code %d\n", result);
- return (-1);
- }
-
- return 1;
+ Qmss_MemRegInfo memInfo;
+ Int32 result;
+ Int n;
+ static int netapi_qm_region_index=0;
+
+ memset(&memInfo,0,sizeof(Qmss_MemRegInfo));
+ memInfo.descBase = pDescMemBase;
+ memInfo.descSize = descSize;
+ memInfo.descNum = numDesc;
+ memInfo.manageDescFlag = Qmss_ManageDesc_MANAGE_DESCRIPTOR;
+ memInfo.memRegion = memRegion;
+
+ if(memRegion == TUNE_NETAPI_QM_GLOBAL_REGION)
+ {
+ memInfo.startIndex = TUNE_NETAPI_QM_START_INDEX; //was 0
+ netapi_qm_region_index += numDesc;
+ }else if(memRegion ==NETAPI_LOCAL_REGION)
+ {
+ /* 2nd region for descriptors (perhaps private?) */
+ memInfo.startIndex = netapi_qm_region_index;
+ }
+ else
+ {
+ return -1 ;
+ }
+
+ memset (pDescMemBase, 0, (descSize * numDesc));
+
+ result = Qmss_insertMemoryRegion (&memInfo);
+ if (result < QMSS_SOK)
+ {
+ netapi_Log ("netapip_qmSetupMemRegion: Qmss_insertMemoryRegion returned error code %d\n", result);
+ return (-1);
+ }
+ return 1;
}
-//****************************************************
-// Start QM (per thread)
-//***************************************************
-int netapi_start_qm(void)
+/********************************************************************
+ * FUNCTION PURPOSE: Internal NETAPI function to start QM
+ ********************************************************************
+ * DESCRIPTION: Internal NETAPI function to start QM
+ * once per thread/core
+ ********************************************************************/
+int netapip_startQm(void)
{
int32_t result;
result = Qmss_start();
if (result != QMSS_SOK)
{
- System_printf (">start_qm: Qmss_start failed with error code %d\n", result);
+ netapi_Log ("netapip_startQm: Qmss_start failed with error code %d\n", result);
return (-1);
}
return 1;
}
-//*************************************************
-//initialize NWAL (one per soc)
-//*************************************************
+
/*** NWAL Memory Buffer Configuration ***/
#define NETAPI_NWAL_CONFIG_BUFSIZE_NWAL_HANDLE 3400
uint8_t nwalInstMem[NETAPI_NWAL_CONFIG_BUFSIZE_NWAL_HANDLE]ALIGN(CACHE_LINESZ);
#define NETAPI_NWAL_CONFIG_BUFSIZE_PA_BUF1 128 * TUNE_NETAPI_MAX_NUM_MAC
uint8_t paBuf1[NETAPI_NWAL_CONFIG_BUFSIZE_PA_BUF1]ALIGN(CACHE_LINESZ);
-//#define NETAPI_NWAL_CONFIG_BUFSIZE_PA_BUF2 768
-//#define NETAPI_NWAL_CONFIG_BUFSIZE_PA_BUF2 6144
-#define NETAPI_NWAL_CONFIG_BUFSIZE_PA_BUF2 12288
+#define NETAPI_NWAL_CONFIG_BUFSIZE_PA_BUF2 13824
uint8_t paBuf2[NETAPI_NWAL_CONFIG_BUFSIZE_PA_BUF2]ALIGN(CACHE_LINESZ);
/* Memory used for SA LLD global Handle */
-#define NETAPI_NWAL_CONFIG_BUFSIZE_SA_LLD_HANDLE 384
+#define NETAPI_NWAL_CONFIG_BUFSIZE_SA_LLD_HANDLE 512
uint8_t salldHandle[NETAPI_NWAL_CONFIG_BUFSIZE_SA_LLD_HANDLE]ALIGN(CACHE_LINESZ);
#if 0 //need to alloc this since we need phy addr also
@@ -214,14 +228,25 @@ uint8_t saContext[NETAPI_NWAL_CONFIG_BUFSIZE_SA_CONTEXT_PER_CHAN * TUNE_NETAPI_M
uint8_t salldChanHandle[NETAPI_NWAL_CONFIG_BUFSIZE_SA_LLD_HANDLE_PER_CHAN * TUNE_NETAPI_MAX_NUM_IPSEC_CHANNELS*2]ALIGN(CACHE_LINESZ);
-/*******************************************
- * Initialize the nwal subsystem for NETAPI use
- ***********************************************/
-int netapi_init_nwal(
- int region2use,
- Pktlib_HeapIfTable * p_table,
- NETAPI_NWAL_GLOBAL_CONTEXT_T * p_nwal_context,
- NETAPI_CFG_T*p_cfg )
+/********************************************************************
+* FUNCTION PURPOSE: NETAPI internal function to gracefully cleanup when startup
+* issue occurs.
+ ********************************************************************
+ * DESCRIPTION: NETAPI internal function to gracefully cleanup when startup
+* issue occurs.
+ ********************************************************************/
+void netapipErrTeardown() { netapip_cleanupAtStart(); exit(-99); }
+
+/********************************************************************
+ * FUNCTION PURPOSE: Internal NETAPI function to initialize NWAL subsystem
+ ********************************************************************
+ * DESCRIPTION: Internal NETAPI function to initialize NWAL subsytem
+ ********************************************************************/
+int netapip_initNwal(
+ int region2use,
+ Pktlib_HeapIfTable * p_table,
+ NETAPI_NWAL_GLOBAL_CONTEXT_T * p_nwal_context,
+ NETAPI_CFG_T*p_cfg )
{
nwalSizeInfo_t nwalSizeInfo;
nwal_RetValue nwalRetVal;
Pktlib_createHeap(&heapCfg, &errCode);
if(nwalGlobCfg.pa2SaBufPool.bufPool[0].heapHandle == NULL)
{
- printf (">Pktlib_createHeap:Heap Creation Failed for PA to SA Buffer Pool , Error Code: %d\n",errCode);
- netapi_err_teardown();
+ netapi_Log ("netapip_initNwal: Pktlib_createHeap:Heap Creation Failed for PA to SA Buffer Pool, Error Code: %d\n",
+ errCode);
+ netapipErrTeardown();
return -1;
}
Pktlib_createHeap(&heapCfg, &errCode);
if(nwalGlobCfg.sa2PaBufPool.bufPool[0].heapHandle == NULL)
{
- printf (">Pktlib_createHeap:Heap Creation Failed for SA to PA Buffer Pool , Error Code: %d\n",errCode);
- netapi_err_teardown();
+ netapi_Log ("netapip_initNwal: Pktlib_createHeap:Heap Creation Failed for SA to PA Buffer Pool, Error Code: %d\n",
+ errCode);
+ netapipErrTeardown();
return -1;
}
aligns);
if(nwalRetVal != nwal_OK)
{
- printf (">netapi: init_nwal - nwal_getBufferReq Failed %d\n", nwalRetVal);
+ netapi_Log ("netapip_initNwal: nwal_getBufferReq Failed %d\n", nwalRetVal);
return nwal_FALSE;
}
bases[nwal_BUF_INDEX_INT_HANDLES] = (uint32_t *)Osal_nwalLocToGlobAddr((uint32_t)nwalHandleMem);
if(NWAL_CHAN_HANDLE_SIZE < sizes[nwal_BUF_INDEX_INT_HANDLES])
{
- printf("one\n");
/* Resize Memory */
while(1);
}
if((NETAPI_NWAL_CONFIG_BUFSIZE_PA_BUF0) < sizes[nwal_BUF_INDEX_PA_LLD_BUF0])
{
/* Resize Memory */
- printf("two\n");
while(1);
}
count++;
bases[nwal_BUF_INDEX_PA_LLD_BUF1] = (uint32_t *)Osal_nwalLocToGlobAddr((uint32_t)paBuf1);
- printf("NETAPI_NWAL_CONFIG_BUFSIZE_PA_BUF1 %d, size[nwal_BUF_INDEX_PA_LLD_BUF1] %d\n",
- NETAPI_NWAL_CONFIG_BUFSIZE_PA_BUF1, sizes[nwal_BUF_INDEX_PA_LLD_BUF1]);
if((NETAPI_NWAL_CONFIG_BUFSIZE_PA_BUF1) < sizes[nwal_BUF_INDEX_PA_LLD_BUF1])
{
- printf("NETAPI_NWAL_CONFIG_BUFSIZE_PA_BUF1 %d, size[nwal_BUF_INDEX_PA_LLD_BUF1] %d\n",
- NETAPI_NWAL_CONFIG_BUFSIZE_PA_BUF1, sizes[nwal_BUF_INDEX_PA_LLD_BUF1]);
/* Resize Memory */
while(1);
}
bases[nwal_BUF_INDEX_PA_LLD_BUF2] = (uint32_t *)Osal_nwalLocToGlobAddr((uint32_t)paBuf2);
if((NETAPI_NWAL_CONFIG_BUFSIZE_PA_BUF2) < sizes[nwal_BUF_INDEX_PA_LLD_BUF2])
{
- printf("four\n");
/* Resize Memory */
while(1);
}
bases[nwal_BUF_INDEX_SA_LLD_HANDLE] = (uint32_t *)Osal_nwalLocToGlobAddr((uint32_t)salldHandle);
if((NETAPI_NWAL_CONFIG_BUFSIZE_SA_LLD_HANDLE) < sizes[nwal_BUF_INDEX_SA_LLD_HANDLE])
{
- printf("five\n");
/* Resize Memory */
while(1);
}
if((NETAPI_NWAL_CONFIG_BUFSIZE_SA_LLD_HANDLE_PER_CHAN * TUNE_NETAPI_MAX_NUM_IPSEC_CHANNELS*2) <
sizes[nwal_BUF_INDEX_SA_LLD_CHAN_HANDLE])
{
- printf("netapi_init_nwal: sizes[nwal_BUF_INDEX_SA_LLD_CHAN_HANDLE] %d\n", sizes[nwal_BUF_INDEX_SA_LLD_CHAN_HANDLE]);
/* Resize Memory */
while(1);
}
&p_nwal_context->nwalInstHandle);
if(nwalRetVal != nwal_OK)
{
- printf (">netapi: init_nwal- nwal_create Failed %d\n",nwalRetVal);
+ netapi_Log ("netapip_initNwal: nwal_create Failed %d\n",nwalRetVal);
while(1);
}
- printf(">netapi: init_nwal - Global and Local Network initialization Successful \n");
+ netapi_Log("netapip_initNwal- Global and Local Network initialization Successful \n");
return 1;
}
-//*************************************************
-//* Local (per thread/core) nwal initialization0
-//**************************************************
-int netapi_start_nwal(Pktlib_HeapHandle pkt_heap,
+/********************************************************************
+ * FUNCTION PURPOSE: Internal NETAPI function to start NWAL
+ ********************************************************************
+ * DESCRIPTION: Internal NETAPI function to start NWAL, per thread/core
+ ********************************************************************/
+int netapip_startNwal(Pktlib_HeapHandle pkt_heap,
Pktlib_HeapHandle cmd_rx_heap,
Pktlib_HeapHandle cmd_tx_heap,
NETAPI_NWAL_LOCAL_CONTEXT_T *p,
NETAPI_NWAL_GLOBAL_CONTEXT_T * p_nwal_glob_context )
{
nwalLocCfg_t nwalLocCfg;
- int count;
+ int count=0;
+ static int first_time = 0;
nwal_RetValue nwalRetVal;
memset(&nwalLocCfg,0,sizeof(nwalLocCfg));
- /* Common Initialization for all cores */
- while(count < TUNE_NETAPI_MAX_NUM_TRANS)
- {
- p_nwal_glob_context->transInfos[count].transId = count;
- count++;
- }
-
/* Update the Start of Packet Offset for the default flows created
* by NWAL
*/
nwalLocCfg.rxPktTailRoomSz = p_cfg->def_heap_tailroom_size;
/* Call back registration for the core */
- nwalLocCfg.pRxPktCallBack = netapi_NWALRxPktCallback;
- nwalLocCfg.pCmdCallBack = netapi_NWALCmdCallBack;
- nwalLocCfg.pPaStatsCallBack = netapi_NWALCmdPaStatsReply;
- nwalLocCfg.pRxDmCallBack= netapi_NWALSBPktCallback; //sideband mode callback
+ nwalLocCfg.pRxPktCallBack = netapip_pktioNWALRxPktCallback;
+ nwalLocCfg.pCmdCallBack = netapip_netcpCfgNWALCmdCallBack;
+ nwalLocCfg.pPaStatsCallBack = netapip_netcpCfgNWALCmdPaStatsReply;
+
+ nwalLocCfg.pRxDmCallBack= netapip_pktioNWALSBPktCallback; //sideband mode callback
/* Initialize Buffer Pool for Control packets from NetCP to Host */
nwalLocCfg.rxCtlPool.numBufPools = 1;
if(nwalRetVal != nwal_OK)
{
- printf (">nwal_start:Failed ->err %d !!!\n", nwalRetVal);
+ netapi_Log (">nwal_start:Failed ->err %d !!!\n", nwalRetVal);
return -1;
}
p->state = NETAPI_NW_CXT_LOC_ACTIVE;
}
-//***************************************************
-// intialize timer
-//***************************************************
-int netapi_init_timer(void)
+/***********************************************************************
+ * FUNCTION PURPOSE: Internal NETAPI function to initialize the 64 bit timer.
+ ***********************************************************************
+ * DESCRIPTION: Internal NETAPI function to initialize the 64 bit timer. for tci6614 ONLY
+ **********************************************************************/
+int netapip_initTimer(void)
{
#ifdef CORTEX_A8
return t64_start();
}
+
+
+/***************************************************************************
+* FUNCTION PURPOSE: NETAPI internal function for virtual memory allocation.
+ ***************************************************************************
+ * DESCRIPTION: NETAPI internal function for virtual memory allocation.
+ **************************************************************************/
+
+static uint8_t* netapip_sharedMemoryMalloc(uint32_t size)
+{
+return (uint8_t *)hplib_vmMemAlloc(size +netapi_global.cfg.def_heap_extra_size , 128, 0);
+}
+
+/********************************************************************
+* FUNCTION PURPOSE: NETAPI internal function for virtual memory free.
+ ********************************************************************
+ * DESCRIPTION: NETAPI internal function for virtual memory free.
+ ********************************************************************/
+static void netapip_sharedMemoryFree(uint8_t* ptr, uint32_t size)
+{
+ /* Do Nothing. */
+ netapi_Log("netapi Unexpected. need to provide a free () for some reason!! \n");
+ return;
+}
+
+//defensive: clean out stuff hanging around
+//
+// open a bunch of free queues and zap them
+#define NQUEUES2CLEAR 35
+static Qmss_QueueHnd tempQH[NQUEUES2CLEAR];
+void netapip_cleanupAtStart(void)
+{
+ int i;
+ uint8_t isAllocated;
+
+ for(i=0;i<NQUEUES2CLEAR;i++)
+ {
+ tempQH[i] = Qmss_queueOpen(Qmss_QueueType_GENERAL_PURPOSE_QUEUE,
+ QMSS_PARAM_NOT_SPECIFIED, &isAllocated);
+ netapip_zapQ(tempQH[i]);
+ }
+
+ for(i=0;i<NQUEUES2CLEAR;i++)
+ {
+ Qmss_queueClose(tempQH[i]);
+ }
+}
+
+
+/********************************************************************
+* FUNCTION PURPOSE: NETAPI internal function system initialization
+ ********************************************************************
+ * DESCRIPTION: NETAPI internal function system initialization
+ ********************************************************************/
+int netapip_systemInit(NETAPI_HANDLE_T * handle)
+{
+ int32_t result;
+ Pktlib_HeapHandle sharedHeapHandle;
+ Pktlib_HeapHandle controlRxHeapHandle,controlTxHeapHandle;
+ Pktlib_HeapCfg heapCfg;
+ int32_t errCode;
+ int count=0;
+
+#ifdef NETAPI_USE_DDR
+ /* Init attributes for DDR */
+ netapi_VM_MempoolAttr[0].attr = HPLIB_ATTR_KM_CACHED0;
+ netapi_VM_MempoolAttr[0].phys_addr = 0;
+ netapi_VM_MempoolAttr[0].size = 0;
+
+ /* Init attributes for un-cached MSMC */
+ netapi_VM_MempoolAttr[1].attr = HPLIB_ATTR_UN_CACHED;
+ netapi_VM_MempoolAttr[1].phys_addr = CSL_MSMC_SRAM_REGS;
+ netapi_VM_MempoolAttr[1].size = TUNE_NETAPI_PERM_MEM_SZ;
+#else
+ netapi_VM_MempoolAttr[1].attr = HPLIB_ATTR_KM_CACHED0;
+ netapi_VM_MempoolAttr[1].phys_addr = 0;
+ netapi_VM_MempoolAttr[1].size = 0;
+
+ /* Init attributes for un-cached MSMC */
+ netapi_VM_MempoolAttr[0].attr = HPLIB_ATTR_UN_CACHED;
+ netapi_VM_MempoolAttr[0].phys_addr = CSL_MSMC_SRAM_REGS;
+ netapi_VM_MempoolAttr[0].size = TUNE_NETAPI_PERM_MEM_SZ;
+#endif
+ /* initialize all the memory we are going to use
+ - chunk for buffers, descriptors
+ - memory mapped peripherals we use, such as QMSS, PA, etc */
+ result = hplib_vmInit(&netapi_VM_VirtAddr[0], 2, &netapi_VM_MempoolAttr[0]);
+
+
+ if (result == hplib_OK) netapi_Log("netapip_systemInit: - memory set up OK\n");
+ else {netapi_Log("netapip_systemInit: - memory set up failed\n"); return -1;}
+
+
+#ifdef NETAPI_ENABLE_SECURITY
+#define SEC_CONTEXT_SZ 384 //not tunable
+/* allocate 2x number of tunnels since we need one for inflow and one for data mode */
+ netapi_VM_SaContextVaddr = hplib_vmMemAlloc((TUNE_NETAPI_MAX_NUM_IPSEC_CHANNELS*2 *
+ SEC_CONTEXT_SZ), 128, 0);
+ if (!netapi_VM_SaContextVaddr)
+ {
+ netapi_Log("netapip_systemInit: Failed to map SA context memory region\n");
+ return (-1);
+ }
+ netapi_Log("netapip_systemInit: SA Memory mapped/allocated at address %p.\n", netapi_VM_SaContextVaddr);
+
+#else
+ netapi_VM_SaContextVaddr= (char *) NULL;
+#endif
+
+/* TODO: the QM regions is application specific and needs to be moved
+ since number of regions created is appliction specific, put this in netapip_systemInit */
+ /* (3) Allocate 2 QM regions from continguous chunk above */
+ netapi_VM_QMemGlobalDescRam =
+ (void *)hplib_vmMemAlloc((TUNE_NETAPI_NUM_GLOBAL_DESC *
+ TUNE_NETAPI_DESC_SIZE),
+ 128, 0);
+
+ netapi_VM_QMemLocalDescRam =
+ (void *)hplib_vmMemAlloc((TUNE_NETAPI_NUM_LOCAL_DESC *
+ TUNE_NETAPI_DESC_SIZE),
+ 128, 0);
+ netapi_Log("netapip_systemInit: desc region=%x global desc region=%x\n", netapi_VM_QMemLocalDescRam, netapi_VM_QMemGlobalDescRam);
+
+ //get timer running
+#ifdef CORTEX_A8
+ netapip_initTimer();
+ netapi_Log("netapip_systemInit: returned from netapip_initTimer\n");
+#endif
+
+ /* Initialize Queue Manager Sub System */
+ result = netapip_initQm (netapi_global.cfg.def_max_descriptors);
+
+ if (result != 1)
+ {
+ netapi_Log("netapip_systemInit: returned from netapip_initQm with failure\n");
+ return -1;
+ }
+
+ /* Start the QMSS. */
+ if (netapip_startQm() != 1)
+ {
+ netapi_Log("netapip_systemInit: returned from netapip_startQm with failure\n");
+ return -1;
+ }
+
+
+ //clean our old junk in 1st bunch of queues that will be allocated to us
+ netapip_cleanupAtStart();
+ netapi_Log("netapip_systemInit: returned from netapip_cleanupAtStart\n");
+ /* Initialize the global descriptor memory region. */
+ result= netapip_qmSetupMemRegion(
+ netapi_global.cfg.def_tot_descriptors_for_us,
+ TUNE_NETAPI_DESC_SIZE,
+ (unsigned int *) netapi_VM_QMemGlobalDescRam,
+ TUNE_NETAPI_QM_GLOBAL_REGION);
+ if(result <0) {netapi_Log("netapip_systemInit: can't setup QM shared region\n"); return -1;}
+
+netapi_Log("netapip_systemInit: returned from netapip_qmSetupMemRegion\n");
+#if 0 //todo setup 2nd region
+/* Initialize the local memory region configuration. */
+ result= netapip_qmSetupMemRegion(
+ NUM_HOST_DESC,
+ SIZE_LOCAL_DESC,
+ netapi_VM_QMemLocalDescRam,
+ NETAPI_LOCAL_REGION);
+ if(result <0) {netapi_Log("can't setup local region\n"); return -1;}
+#endif
+ /* Initialize CPPI CPDMA */
+
+ result = netapip_initCppi ();
+ netapi_Log("netapip_systemInit: returned from netapip_initCppi\n");
+ if (result != 1)
+ {
+ netapi_Log ("netapi: Error initializing CPPI SubSystem error code : %d\n",result);
+ return -1;
+ }
+
+ /* CPPI and Queue Manager are initialized. */
+ netapi_Log ("netapi: Queue Manager and CPPI are initialized.\n");
+
+ /* create main pkt heap */
+ /* Initialize the Shared Heaps. */
+ Pktlib_sharedHeapInit();
+ netapi_Log("netapip_systemInit: returned from Pktlib_sharedHeapInit\n");
+ /* Populate the heap interface table. */
+ netapi_pktlib_ifTable.data_malloc = netapip_sharedMemoryMalloc;
+ netapi_pktlib_ifTable.data_free = netapip_sharedMemoryFree;
+
+ /* Initialize the heap configuration. */
+ memset ((void *)&heapCfg, 0, sizeof(Pktlib_HeapCfg));
+ /* Populate the heap configuration */
+ heapCfg.name = "netapi";
+ heapCfg.memRegion = TUNE_NETAPI_QM_GLOBAL_REGION;
+ heapCfg.sharedHeap = 1;
+ heapCfg.useStarvationQueue = 0;
+ heapCfg.dataBufferSize = netapi_global.cfg.def_heap_buf_size;
+ heapCfg.numPkts = netapi_global.cfg.def_heap_n_descriptors;
+ heapCfg.numZeroBufferPackets= netapi_global.cfg.def_heap_n_zdescriptors;
+ heapCfg.heapInterfaceTable.data_malloc = netapi_pktlib_ifTable.data_malloc;
+ heapCfg.heapInterfaceTable.data_free = netapi_pktlib_ifTable.data_free;
+ heapCfg.dataBufferPktThreshold = 0;
+ heapCfg.zeroBufferPktThreshold = 0;
+
+ /* Create Shared Heap with specified configuration. */
+ sharedHeapHandle = Pktlib_createHeap(&heapCfg, &errCode);
+ netapi_Log("netapip_systemInit: returned from Pktlib_createHeap1\n");
+ //todo -> cleanup on failure
+ if (!sharedHeapHandle) { netapi_Log(">'netapi' heap create failed, Error Code: %d\n",errCode); return -1;}
+ handle->netcp_heap= sharedHeapHandle;
+
+ /* Update for Control */
+ heapCfg.name = "netapi_control_rx";
+ heapCfg.sharedHeap = 1;
+ heapCfg.dataBufferSize = TUNE_NETAPI_CONFIG_MAX_CTL_RXTX_BUF_SIZE;
+ heapCfg.numPkts = TUNE_NETAPI_CONFIG_NUM_CTL_RX_BUF;
+ heapCfg.numZeroBufferPackets= 0;
+
+ controlRxHeapHandle = Pktlib_createHeap(&heapCfg, &errCode);
+ netapi_Log("netapip_systemInit: returned from Pktlib_createHeap2\n");
+ //todo -> cleanup on failure
+ if (!controlRxHeapHandle) { netapi_Log("netapi -'netapi_control_rx' heap create failed, Error Code: %d\n",errCode); return -1;}
+ handle->netcp_control_rx_heap= controlRxHeapHandle;
+
+
+ heapCfg.name = "netapi_control_tx";
+ heapCfg.numPkts = TUNE_NETAPI_CONFIG_NUM_CTL_TX_BUF;
+
+ controlTxHeapHandle = Pktlib_createHeap(&heapCfg, &errCode);
+ netapi_Log("netapip_systemInit: returned from Pktlib_createHeap3\n");
+ //todo -> cleanup on failure
+ if (!controlTxHeapHandle) { netapi_Log("netapi -'netapi_control_tx' heap create failed, Error Code: %d\n",errCode); return -1;}
+ handle->netcp_control_tx_heap= controlTxHeapHandle;
+
+ /* now NWAL */
+ result = netapip_initNwal(
+ TUNE_NETAPI_QM_GLOBAL_REGION,
+ &netapi_pktlib_ifTable,
+ &netapi_global.nwal_context,
+ &netapi_global.cfg);
+ if (result<0) {netapi_Log("netapi init_nwal() failed\n"); return -1; }
+ netapi_Log("netapip_systemInit: returned from netapip_initNwal\n");
+ /* start NWAL */
+
+
+ /* Common Initialization for all cores */
+ while(count < TUNE_NETAPI_MAX_NUM_TRANS)
+ {
+ netapi_global.nwal_context.transInfos[count].transId = count;
+ count++;
+ }
+ result = netapip_startNwal(sharedHeapHandle,
+ controlRxHeapHandle,
+ controlTxHeapHandle,
+ &handle->nwal_local,
+ &netapi_global.cfg,
+ &netapi_global.nwal_context);
+ if (result<0) {netapi_Log("netapi start_nwal() failed\n"); return -1; }
+ netapi_Log("netapip_systemInit: returned from netapip_startNwal\n");
+ return 0;
+}
+
+
+/****************************************************************************
+* FUNCTION PURPOSE: NETAPI internal function which performs clean for linux user space
+ ****************************************************************************
+ * DESCRIPTION: NETAPI internal function which performs clean for linux user space
+ ***************************************************************************/
+void netapip_zapQ(int queueNum)
+{
+ char * descPtr;
+ int i;
+ if (!queueNum)
+ {
+ return;
+ }
+ for (i=0;;i+=1 )
+ {
+ /* Pop descriptor from source queue */
+ if ((descPtr = (char *)pktio_mQmssQueuePopRaw(queueNum)) == NULL)
+ {
+ break;
+ }
+ }
+ if(i)
+ {
+ netapi_Log("netapip_zapQ: @recovery - %d descriptors cleaned from qn %d\n",i, queueNum);
+ }
+}
+
+
+/****************************************************************************
+* FUNCTION PURPOSE: NETAPI internal function to display internal heap stats.
+ ****************************************************************************
+ * DESCRIPTION: NETAPI internal function to display internal heap stats.
+ ***************************************************************************/
+void netapi_dump_internal_heap_stats(void)
+{
+ Pktlib_HeapStats pktLibHeapStats;
+ Pktlib_getHeapStats(netapi_get_global()->nwal_context.pa2sa_heap,&pktLibHeapStats);
+ printf("PA2SA(ingress) stats> #free=%d #zb=%d #garbage=%d\n", pktLibHeapStats.numFreeDataPackets,
+ pktLibHeapStats.numZeroBufferPackets, pktLibHeapStats.numPacketsinGarbage);
+ printf(" > #dataBufThreshStatus=%d #dataBufStarvCounter=%d #zBufThreshStatus=%d #zBufStarvCounter=%d \n",
+ pktLibHeapStats.dataBufferThresholdStatus,pktLibHeapStats.dataBufferStarvationCounter,
+ pktLibHeapStats.zeroDataBufferThresholdStatus, pktLibHeapStats.zeroDataBufferStarvationCounter);
+#if 0
+Pktlib_getHeapStats(netapi_get_global()->nwal_context.pa2saTX_heap,&pktLibHeapStats);
+netapi_Log("PA2SA(egress) stats> #free=%d #zb=%d #garbage=%d\n", pktLibHeapStats.numFreeDataPackets,
+ pktLibHeapStats.numZeroBufferPackets, pktLibHeapStats.numPacketsinGarbage);
+netapi_Log(" > #dataBufThreshStatus=%d #dataBufStarvCounter=%d #zBufThreshStatus=%d #zBufStarvCounter=%d \n",
+ pktLibHeapStats.dataBufferThresholdStatus,pktLibHeapStats.dataBufferStarvationCounter,
+ pktLibHeapStats.zeroDataBufferThresholdStatus, pktLibHeapStats.zeroDataBufferStarvationCounter);
+#endif
+ Pktlib_getHeapStats(netapi_get_global()->nwal_context.sa2pa_heap,&pktLibHeapStats);
+ printf("SA2PA stats> #free=%d #zb=%d #garbage=%d\n", pktLibHeapStats.numFreeDataPackets,
+ pktLibHeapStats.numZeroBufferPackets, pktLibHeapStats.numPacketsinGarbage);
+ printf(" > #dataBufThreshStatus=%d #dataBufStarvCounter=%d #zBufThreshStatus=%d #zBufStarvCounter=%d \n",
+ pktLibHeapStats.dataBufferThresholdStatus,pktLibHeapStats.dataBufferStarvationCounter,
+ pktLibHeapStats.zeroDataBufferThresholdStatus, pktLibHeapStats.zeroDataBufferStarvationCounter);
+
+}
+