index b7244aa7760fe9a2eed809df884297ba343b041d..ce7d4f7ee9c2c75a94fa1f13428ae7c2a28c8202 100755 (executable)
-/*****************************************\r
- * file: netapi_loc.h\r
- * purpose: internal netapi stuff\r
- ****************************************/\r
-\r
-#ifndef __NETAPI_LOC__H\r
-#define __NETAPI_LOC__H\r
-/***************************************\r
-* INTERNAL HANDLE STRUCTURE DEFINITION\r
-****************************************/\r
-\r
-/***********************************************\r
- * GLOBAL AREA\r
- * short term: this is global to process\r
- * (multi-process not supported)\r
- * long term: this structure gets put in shared memory \r
- ***********************************************/\r
-\r
-/* list of global pktio channels that have been created\r
- (NETCP_TX, RX are intrinsic so won't be here) */\r
-typedef struct PKTIO_ENTRY_tag\r
-{\r
- char name[PKTIO_MAX_NAME+1];\r
- Qmss_Queue qn; // -1 => slot is free\r
-} PKTIO_ENTRY_T;\r
-\r
-/* to hold an IP on an interface */\r
-typedef struct NETCP_INTERFACE_IP_Tag\r
-{\r
- int in_use;\r
- void * nwal_handle;\r
- nwal_IpType ip_type;\r
- nwalIpAddr_t ip_addr;\r
- nwalIpOpt_t ip_qualifiers;\r
-} NETCP_INTERFACE_IP_T;\r
-\r
-/* to hold a classifier */\r
-typedef struct NETCP_INTERFACE_CLASSIFIER_Tag\r
-{\r
- int in_use;\r
- int class_type; //see netcp_cfg.h\r
- void * nwal_L2_handle;\r
- void * nwal_L3_handle;\r
- void * nwal_L4_handle;\r
-} NETCP_INTERFACE_CLASSIFIER_T;\r
-\r
-/* to hold an ipsec rx policy */\r
-typedef struct NETCP_IPSEC_POLICY_Tag\r
-{\r
- int in_use;\r
- int tunnel; //associated tunnel\r
- void * nwal_handle; //handle associated with this RX Policy \r
-} NETCP_IPSEC_POLICY_T;\r
-\r
-/* to hold a tunnel */\r
-typedef struct NETCP_IPSEC_SA_Tag\r
-{\r
- int in_use;\r
- int inbound; //true if inbound\r
- \r
- int sa_mode; //mode we are going to use \r
-#define NETCP_IPSEC_SA_MODE_INFLOW 0\r
-#define NETCP_IPSEC_SA_MODE_SIDEBAND 1\r
- \r
- void * sa_handle_inflow; //for inflow mode\r
- void * sa_handle_sideband; //for sideband mode\r
- int iface; //associated interface\r
-} NETCP_IPSEC_SA_T;\r
-\r
-/* to hold a netcp 'interface' */\r
-typedef struct NETCP_INTERFACE_Tag\r
-{\r
- int in_use; /* 1 for valid */\r
- int state; /* 0=down, 1=up, future.. */\r
- void * nwal_handle; //handle associated with this interface\r
- unsigned char mac[6]; // mac address\r
- unsigned int vlan; //future\r
-} NETCP_INTERFACE_T;\r
-\r
-/*to keep track of netcp config transactions */\r
-typedef struct {\r
- nwal_Bool_t inUse;\r
- uint16_t transType;\r
-#define NETAPI_NWAL_HANDLE_TRANS_NONE 0\r
-#define NETAPI_NWAL_HANDLE_TRANS_MAC 1\r
-#define NETAPI_NWAL_HANDLE_TRANS_IP 2\r
-#define NETAPI_NWAL_HANDLE_TRANS_PORT 3\r
-#define NETAPI_NWAL_HANDLE_TRANS_SA 4\r
-#define NETAPI_NWAL_HANDLE_TRANS_SA_POLICY 5\r
-#define NETAPI_NWAL_HANDLE_STAT_REQUEST 6\r
-\r
- uint16_t state;\r
-#define NETAPI_NWAL_HANDLE_STATE_IDLE 0\r
-#define NETAPI_NWAL_HANDLE_STATE_OPEN_PENDING 1\r
-#define NETAPI_NWAL_HANDLE_STATE_OPEN 2\r
-#define NETAPI_NWAL_HANDLE_STATE_CLOSE_PENDING 3\r
- nwal_Handle handle;\r
- uint64_t transId;\r
- NETAPI_T netapi_handle; //the thread making the transaction\r
-} NetapiNwalTransInfo_t;\r
-\r
-/* to hold user defined flows */\r
-typedef struct NETCP_REGISTERED_FLOWS_Tag\r
-{\r
- int in_use; //1=> in use\r
- void * handle; //cppi handle to resource (internal)\r
- NETCP_CFG_FLOW_T flow;\r
-} NETCP_REGISTERED_FLOWS_T;\r
-\r
-/******************************\r
- * nwal global context \r
- * (shared over all instances)\r
- *******************************/\r
-typedef struct\r
-{\r
- int state;\r
-#define NETAPI_NW_CXT_GLOB_INACTIVE 0x0\r
-#define NETAPI__CXT_GLOB_ACTIVE 0x1\r
-#define NETAPI_NW_CXT_GLOB_RES_ALLOC_COMPLETE 0x3\r
-\r
- nwal_Handle nwalInstHandle;\r
- //internal heaps used just by netcp (sa<->pa). SW doesn't touch these\r
- Pktlib_HeapHandle sa2pa_heap;\r
- Pktlib_HeapHandle pa2sa_heap;\r
- //stats\r
- paSysStats_t paStats;\r
- int numCmdPass;\r
- int numCmdFail;\r
- int numBogusTransIds;\r
- NetapiNwalTransInfo_t transInfos[TUNE_NETAPI_MAX_NUM_TRANS]; //transactions\r
- NETCP_INTERFACE_T interfaces[TUNE_NETAPI_MAX_INTERFACES]; //interfaces\r
- NETCP_INTERFACE_CLASSIFIER_T classi[TUNE_NETAPI_MAX_CLASSIFIERS]; //classifiers\r
- NETCP_REGISTERED_FLOWS_T flows[TUNE_NETAPI_MAX_FLOWS]; //flows\r
- NETCP_IPSEC_SA_T tunnel[TUNE_NETAPI_MAX_SA]; //tunnels\r
- NETCP_IPSEC_POLICY_T policy[TUNE_NETAPI_MAX_POLICY]; //policies\r
- NETCP_INTERFACE_IP_T ips[TUNE_NETAPI_MAX_IP]; //ips\r
-} NETAPI_NWAL_GLOBAL_CONTEXT_T;\r
-\r
-/* NWAL Local context (per core/thread) */\r
-typedef struct\r
-{\r
- //void * nwalLocInstance;\r
-#define NETAPI_NW_CXT_LOC_INACTIVE 0x0\r
-#define NETAPI_NW_CXT_LOC_ACTIVE 0x2\r
- int state;\r
-\r
- int numPendingCfg;\r
- NETCP_CFG_STATS_CB stats_cb;\r
-\r
-/* stats */\r
- int numL2PktsRecvd;\r
- int numL3PktsRecvd;\r
- int numL4PktsRecvd;\r
- int numL4PktsSent;\r
- int TxErrDrop;\r
-\r
- /* local config */\r
- nwalLocCfg_t nwalLocCfg;\r
-} NETAPI_NWAL_LOCAL_CONTEXT_T;\r
-\r
-/* the global */\r
-typedef struct NETAPI_GLOBAL_tag\r
-{\r
-#define NETAPI_MAX_PKTIO (TUNE_NETAPI_MAX_PKTIO) \r
-PKTIO_ENTRY_T pktios[NETAPI_MAX_PKTIO];\r
-\r
-/* configuration */\r
-NETAPI_CFG_T cfg;\r
-\r
-/* global timers */\r
-\r
-/* nwal context */\r
-NETAPI_NWAL_GLOBAL_CONTEXT_T nwal_context;\r
-\r
-} NETAPI_GLOBAL_T;\r
-\r
-\r
-/************************************\r
- * this is a per thread structure.\r
- * It contains stuff local to thread\r
- * and pointer to global stuff\r
- * that is shared over all threads,\r
- **************************************/\r
-typedef struct NETAPI_HANDLE_Tag\r
-{\r
-int master; //master type\r
-\r
-void * global; /* pointer to the global area */\r
-\r
-/* heap handles */\r
-Pktlib_HeapHandle netcp_heap; /* internal default */\r
-Pktlib_HeapHandle netcp_control_heap; /* for control messages */\r
-Pktlib_HeapHandle createdHeaps[TUNE_NETAPI_MAX_HEAPS]; /* created by app and registered */\r
-\r
-/* pktios defined */\r
-int n_pktios; /* #of pktios that are active for this instance */\r
-void* pktios[NETAPI_MAX_PKTIO]; /* the list of pktios */\r
-\r
-/* scheduler stuff. unallocated if NETAPI_INCLUDE_SCHED not set */\r
-void * p_sched;\r
-\r
-/* nwal local context */\r
-NETAPI_NWAL_LOCAL_CONTEXT_T nwal_local;\r
-\r
-/* security stuff */\r
-\r
-/* timer stuff */\r
-\r
-/* thread cookie */\r
-void * cookie; /*set by calling thread */\r
-\r
-} NETAPI_HANDLE_T;\r
-\r
-\r
-//internal initialization routines */\r
-int netapi_init_qm(int max_descriptors);\r
-int netapi_init_cppi(void);\r
-int netapi_init_cpsw(void);\r
-int netapi_start_qm(void);\r
-int netapi_init_nwal(\r
- int region2use,\r
- Pktlib_HeapIfTable * p_table,\r
- NETAPI_NWAL_GLOBAL_CONTEXT_T * p_nwal_context,\r
- NETAPI_CFG_T *p_cfg );\r
-int netapi_start_nwal(Pktlib_HeapHandle pkt_heap,\r
- Pktlib_HeapHandle cmd_heap,\r
- NETAPI_NWAL_LOCAL_CONTEXT_T *p ,\r
- NETAPI_NWAL_GLOBAL_CONTEXT_T * p_nwal_glob_context );\r
-\r
-int netapi_init_timer(void);\r
-int netapi_qm_setup_mem_region(\r
- unsigned int numDesc,\r
- unsigned int descSize,\r
- unsigned int* pDescMemBase,\r
- int memRegion);\r
-//for above\r
-#define NETAPI_GLOBAL_REGION TUNE_NETAPI_QM_GLOBAL_REGION \r
-#define NETAPI_LOCAL_REGION ((NETAPI_GLOBAL_REGION)+1) \r
-\r
-int netapi_VM_memory_setup(void);\r
-void netapi_VM_memory_teardown(void);\r
-\r
-//nwal callbacks\r
-void netapi_NWALRxPktCallback (uint32_t appCookie,\r
- uint16_t numPkts,\r
- nwalRxPktInfo_t* pPktInfo,\r
- uint64_t timestamp,\r
- nwal_Bool_t* pFreePkt);\r
-\r
-void netapi_NWALCmdCallBack (nwal_AppId appHandle,\r
- uint16_t trans_id,\r
- nwal_RetValue ret);\r
-\r
-void netapi_NWALCmdPaStatsReply (nwal_AppId appHandle,\r
- nwal_TransID_t trans_id,\r
- paSysStats_t *stats);\r
-\r
-void netapi_NWALSBPktCallback (uint32_t appCookie,\r
- uint16_t numPkts,\r
- nwalDmRxPayloadInfo_t* pDmRxPktInfo,\r
- nwal_Bool_t* pFreePkt);\r
-\r
-\r
-//***********************************\r
-//internal utilities\r
-//*************************************\r
-\r
-//return the list of pktios for this instance\r
-static inline void ** netapi_get_pktio_list(NETAPI_T p)\r
-{\r
-NETAPI_HANDLE_T *pp = (NETAPI_HANDLE_T *) p;\r
-return &pp->pktios[0];\r
-}\r
-\r
-//get scheduler block handle\r
-static inline void * netapi_get_scheduler(NETAPI_T p)\r
-{\r
-NETAPI_HANDLE_T *pp = (NETAPI_HANDLE_T *) p;\r
-return pp->p_sched;\r
-}\r
-\r
-/* return pointer to global area */\r
-NETAPI_GLOBAL_T * netapi_get_global(void);\r
-\r
-//add a pktio name (and queue) to global list\r
-static inline int netapi_add_global_pktio(NETAPI_T p, char *name, Qmss_Queue * qn)\r
-{\r
-NETAPI_HANDLE_T *pp = (NETAPI_HANDLE_T *) p;\r
-PKTIO_ENTRY_T *pe;\r
-int i;\r
-//find a free slot\r
-pe = &((NETAPI_GLOBAL_T *)(pp->global))->pktios[0];\r
-\r
-for(i=0;i<NETAPI_MAX_PKTIO; i++,pe++)\r
- {\r
- if (pe->qn.qNum == -1)\r
- {\r
- pe->qn.qNum=qn->qNum;\r
- pe->qn.qMgr=qn->qMgr;\r
- strncpy(pe->name, name, PKTIO_MAX_NAME);\r
- return 1;\r
- }\r
- pe+=1;\r
- }\r
- return 0; //no room\r
-}\r
-\r
-//delete a pktio name (and queue) to global list\r
-static inline int netapi_del_global_pktio(NETAPI_T p, char *name)\r
-{\r
-NETAPI_HANDLE_T *pp = (NETAPI_HANDLE_T *) p;\r
-PKTIO_ENTRY_T *pe;\r
-int i;\r
-//find slot\r
-pe = &((NETAPI_GLOBAL_T *)(pp->global))->pktios[0];\r
-\r
-for(i=0;i<NETAPI_MAX_PKTIO; i++,pe++)\r
- {\r
- if (pe->qn.qNum == -1) continue;\r
- if (!strncmp(name, pe->name, PKTIO_MAX_NAME))\r
- {\r
- pe->qn.qNum=-1;\r
- pe->name[0]='\0';\r
- return 1;\r
- }\r
- pe+=1;\r
- }\r
- return 0; //no room\r
-}\r
-\r
-\r
-/* get list of global pktios that have been created */\r
-static inline Qmss_Queue* netapi_find_global_pktio(NETAPI_T p, char *name)\r
-{\r
-NETAPI_HANDLE_T *pp = (NETAPI_HANDLE_T *) p;\r
-PKTIO_ENTRY_T *pe;\r
-int i;\r
-//find slot\r
-pe = &((NETAPI_GLOBAL_T *)(pp->global))->pktios[0];\r
-\r
-for(i=0;i<NETAPI_MAX_PKTIO; i++,pe++)\r
- {\r
- if (pe->qn.qNum == -1) continue;\r
- if (!strncmp(name, pe->name, PKTIO_MAX_NAME))\r
- {\r
- return &pe->qn;\r
- }\r
- pe +=1;\r
- }\r
- return NULL; //not found\r
-}\r
-\r
-/* return the nwal global instance handle */\r
-static inline nwal_Handle netapi_return_nwal_instance_handle(NETAPI_T p)\r
-{\r
-\r
-NETAPI_HANDLE_T *pp = (NETAPI_HANDLE_T *) p;\r
-return ((NETAPI_GLOBAL_T *)(pp->global))->nwal_context.nwalInstHandle;\r
-}\r
-\r
-//utility to clear out a queue\r
-void netapi_zapQ(int queueNum);\r
-void netcp_cfgp_build_route(NETCP_CFG_ROUTE_T * p_route, int16_t * p_flow, Qmss_QueueHnd * p_q);\r
-\r
-//database utilities\r
-int netcp_cfgp_find_saslot( NETAPI_NWAL_GLOBAL_CONTEXT_T *p, int iface);\r
-void netcp_cfgp_delete_sa(NETAPI_NWAL_GLOBAL_CONTEXT_T *p,int sa_slot);\r
-void netcp_cfgp_insert_sa(NETAPI_NWAL_GLOBAL_CONTEXT_T *p,\r
- int sa_slot, //we 'reserved it already'\r
- int dir,\r
- int mode,\r
- void * temp1,\r
- void * temp2,\r
- void * handle_inflow,\r
- void * handle_sideband);\r
-void *netcp_cfgp_get_sa_handles( NETAPI_NWAL_GLOBAL_CONTEXT_T *p,\r
- int sa_slot, void ** p_sideband);\r
-void* netcp_cfgp_get_mac_handle(NETAPI_NWAL_GLOBAL_CONTEXT_T *p,int iface_no);\r
-NetapiNwalTransInfo_t * netapip_GetFreeTransInfo(NETAPI_GLOBAL_T *p_global, nwal_TransID_t *pTransId);\r
-void *netcp_cfgp_get_policy( NETAPI_NWAL_GLOBAL_CONTEXT_T *p,\r
- int policy_slot);\r
-#endif\r
+/*****************************************
+ * file: netapi_loc.h
+ * purpose: internal netapi stuff
+ ****************************************/
+
+#ifndef __NETAPI_LOC__H
+#define __NETAPI_LOC__H
+
+
+//#include "ti/runtime/netapi/netapi.h"
+#include "ti/drv/nwal/nwal_util.h"
+#include "ti/runtime/netapi/pktio.h"
+#include "ti/drv/nwal/nwal.h"
+#include "ti/drv/nwal/nwal_util.h"
+
+
+
+extern hplib_virtualAddrInfo_T netapi_VM_VirtAddr[HPLIB_MAX_MEM_POOLS];
+extern unsigned char *netapi_VM_SaContextVaddr;
+/***********************************************
+ * GLOBAL AREA
+ * short term: this is global to process
+ * (multi-process not supported)
+ * long term: this structure gets put in shared memory
+ ***********************************************/
+
+/* list of global pktio channels that have been created
+ (NETCP_TX, RX are intrinsic so won't be here) */
+typedef struct PKTIO_ENTRY_tag
+{
+ char name[PKTIO_MAX_NAME+1];
+ Qmss_Queue qn; // -1 => slot is free
+} PKTIO_ENTRY_T;
+
+/* to hold an IP on an interface */
+typedef struct NETCP_INTERFACE_IP_Tag
+{
+ int in_use;
+ void * nwal_handle;
+ nwal_IpType ip_type;
+ nwalIpAddr_t ip_addr;
+ nwalIpOpt_t ip_qualifiers;
+ void * user_data;
+} NETCP_INTERFACE_IP_T;
+
+/* to hold a classifier */
+typedef struct NETCP_INTERFACE_CLASSIFIER_Tag
+{
+ int in_use;
+ int class_type; //see netcp_cfg.h
+ void * nwal_L2_handle;
+ void * nwal_L3_handle;
+ void * nwal_L4_handle;
+ void * user_data;
+} NETCP_INTERFACE_CLASSIFIER_T;
+
+/* to hold an ipsec rx policy */
+typedef struct NETCP_IPSEC_POLICY_Tag
+{
+ int in_use;
+ int tunnel; //associated tunnel
+ void * nwal_handle; //handle associated with this RX Policy
+ void * user_data; // user data associtaed with this RX Policy
+} NETCP_IPSEC_POLICY_T;
+
+/* to hold a tunnel */
+typedef struct NETCP_IPSEC_SA_Tag
+{
+ int in_use;
+ int inbound; //true if inbound
+
+ int sa_mode; //mode we are going to use
+#define NETCP_IPSEC_SA_MODE_INFLOW 0
+#define NETCP_IPSEC_SA_MODE_SIDEBAND 1
+
+ void * sa_handle_inflow; //for inflow mode
+ void * sa_handle_sideband; //for sideband mode
+ int iface; //associated interface
+ nwalTxDmPSCmdInfo_t dmPSCmdInfo;
+ uint32_t swInfo0;
+ uint32_t swInfo1;
+ void* user_data;
+} NETCP_IPSEC_SA_T;
+
+/* to hold a netcp 'interface' */
+typedef struct NETCP_INTERFACE_Tag
+{
+ int in_use; /* 1 for valid */
+ int state; /* 0=down, 1=up, future.. */
+ void * nwal_handle; //handle associated with this interface
+ unsigned char mac[6]; // mac address
+ unsigned int vlan; //future
+} NETCP_INTERFACE_T;
+
+/*to keep track of netcp config transactions */
+typedef struct {
+ nwal_Bool_t inUse;
+ uint16_t transType;
+#define NETAPI_NWAL_HANDLE_TRANS_NONE 0
+#define NETAPI_NWAL_HANDLE_TRANS_MAC 1
+#define NETAPI_NWAL_HANDLE_TRANS_IP 2
+#define NETAPI_NWAL_HANDLE_TRANS_PORT 3
+#define NETAPI_NWAL_HANDLE_TRANS_SA 4
+#define NETAPI_NWAL_HANDLE_TRANS_SA_POLICY 5
+#define NETAPI_NWAL_HANDLE_STAT_REQUEST 6
+
+ uint16_t state;
+#define NETAPI_NWAL_HANDLE_STATE_IDLE 0
+#define NETAPI_NWAL_HANDLE_STATE_OPEN_PENDING 1
+#define NETAPI_NWAL_HANDLE_STATE_OPEN 2
+#define NETAPI_NWAL_HANDLE_STATE_CLOSE_PENDING 3
+#define NETAPI_NWAL_HANDLE_STATE_ERR 4
+ nwal_Handle handle;
+ uint64_t transId;
+ NETAPI_T netapi_handle; //the thread making the transaction
+} NetapiNwalTransInfo_t;
+
+/* to hold user defined flows */
+typedef struct NETCP_REGISTERED_FLOWS_Tag
+{
+ int in_use; //1=> in use
+ void* handle; //cppi handle to resource (internal)
+ NETCP_CFG_FLOW_T flow;
+} NETCP_REGISTERED_FLOWS_T;
+
+/******************************
+ * nwal global context
+ * (shared over all instances)
+ *******************************/
+typedef struct
+{
+ int state;
+#define NETAPI_NW_CXT_GLOB_INACTIVE 0x0
+#define NETAPI__CXT_GLOB_ACTIVE 0x1
+#define NETAPI_NW_CXT_GLOB_RES_ALLOC_COMPLETE 0x3
+
+ nwal_Handle nwalInstHandle;
+ //internal heaps used just by netcp (sa<->pa). SW doesn't touch these
+ Pktlib_HeapHandle sa2pa_heap;
+ Pktlib_HeapHandle pa2sa_heap;
+ //stats
+ paSysStats_t paStats;
+ int numCmdPass;
+ int numCmdFail;
+ int numBogusTransIds;
+ NetapiNwalTransInfo_t transInfos[TUNE_NETAPI_MAX_NUM_TRANS]; //transactions
+ NETCP_INTERFACE_T interfaces[TUNE_NETAPI_MAX_NUM_MAC]; //interfaces
+ NETCP_INTERFACE_CLASSIFIER_T classi[TUNE_NETAPI_MAX_CLASSIFIERS]; //classifiers
+ NETCP_REGISTERED_FLOWS_T flows[TUNE_NETAPI_MAX_FLOWS]; //flows
+ NETCP_IPSEC_SA_T tunnel[TUNE_NETAPI_MAX_SA]; //tunnels
+ NETCP_IPSEC_POLICY_T policy[TUNE_NETAPI_MAX_POLICY]; //policies
+ NETCP_INTERFACE_IP_T ips[TUNE_NETAPI_MAX_NUM_IP]; //ips
+} NETAPI_NWAL_GLOBAL_CONTEXT_T;
+
+/* NWAL Local context (per core/thread) */
+typedef struct
+{
+#define NETAPI_NW_CXT_LOC_INACTIVE 0x0
+#define NETAPI_NW_CXT_LOC_ACTIVE 0x2
+ int state;
+
+ int numPendingCfg;
+ NETCP_CFG_STATS_CB stats_cb;
+
+/* stats */
+ int numL2PktsRecvd;
+ int numL3PktsRecvd;
+ int numL4PktsRecvd;
+ int numL4PktsSent;
+ int TxErrDrop;
+
+ /* local config */
+ nwalLocCfg_t nwalLocCfg;
+} NETAPI_NWAL_LOCAL_CONTEXT_T;
+
+/* the global */
+typedef struct NETAPI_GLOBAL_tag
+{
+#define NETAPI_MAX_PKTIO (TUNE_NETAPI_MAX_PKTIO)
+ PKTIO_ENTRY_T pktios[NETAPI_MAX_PKTIO];
+ /* configuration */
+ NETAPI_CFG_T cfg;
+ /* nwal context */
+ NETAPI_NWAL_GLOBAL_CONTEXT_T nwal_context;
+ NETAPI_T p_master; // save p'masters handle
+} NETAPI_GLOBAL_T;
+
+
+/************************************
+ * this is a per thread structure.
+ * It contains stuff local to thread
+ * and pointer to global stuff
+ * that is shared over all threads,
+ **************************************/
+typedef struct NETAPI_HANDLE_Tag
+{
+ int master; //master type
+
+ void* global; /* pointer to the global area */
+
+ /* heap handles */
+ Pktlib_HeapHandle netcp_heap; /* internal default */
+ Pktlib_HeapHandle netcp_control_rx_heap; /* for control messages */
+ Pktlib_HeapHandle netcp_control_tx_heap; /* for control messages */
+ Pktlib_HeapHandle createdHeaps[TUNE_NETAPI_MAX_HEAPS]; /* created by app and registered */
+
+ /* pktios defined */
+ int n_pktios; /* #of pktios that are active for this instance */
+ void* pktios[NETAPI_MAX_PKTIO]; /* the list of pktios */
+
+ /* scheduler stuff. unallocated if NETAPI_INCLUDE_SCHED not set */
+ void* p_sched;
+
+ /* nwal local context */
+ NETAPI_NWAL_LOCAL_CONTEXT_T nwal_local;
+
+ /* thread cookie */
+ void* cookie; /*set by calling thread */
+} NETAPI_HANDLE_T;
+
+//internal initialization routines */
+int netapip_initQm(int max_descriptors);
+int netapip_initCppi(void);
+int netapip_startQm(void);
+int netapip_initNwal(int region2use,
+ Pktlib_HeapIfTable * p_table,
+ NETAPI_NWAL_GLOBAL_CONTEXT_T * p_nwal_context,
+ NETAPI_CFG_T *p_cfg );
+
+int netapip_startNwal(Pktlib_HeapHandle pkt_heap,
+ Pktlib_HeapHandle cmd_heapRx,
+ Pktlib_HeapHandle cmd_heapTx,
+ NETAPI_NWAL_LOCAL_CONTEXT_T* p,
+ NETAPI_CFG_T* p_cfg,
+ NETAPI_NWAL_GLOBAL_CONTEXT_T* p_nwal_glob_context );
+
+int netapip_initTimer(void);
+int netapip_qmSetupMemRegion(unsigned int numDesc,
+ unsigned int descSize,
+ unsigned int* pDescMemBase,
+ int memRegion);
+
+#define NETAPI_GLOBAL_REGION TUNE_NETAPI_QM_GLOBAL_REGION
+#define NETAPI_LOCAL_REGION ((NETAPI_GLOBAL_REGION)+1)
+
+
+//nwal callbacks
+void netapip_pktioNWALRxPktCallback(uint32_t appCookie,
+ uint16_t numPkts,
+ nwalRxPktInfo_t* pPktInfo,
+ uint64_t timestamp,
+ nwal_Bool_t* pFreePkt);
+
+void netapip_netcpCfgNWALCmdCallBack (nwal_AppId appHandle,
+ uint16_t trans_id,
+ nwal_RetValue ret);
+
+void netapip_netcpCfgNWALCmdPaStatsReply (nwal_AppId appHandle,
+ nwal_TransID_t trans_id,
+ paSysStats_t *stats);
+
+void netapip_pktioNWALSBPktCallback (uint32_t appCookie,
+ uint16_t numPkts,
+ nwalDmRxPayloadInfo_t* pDmRxPktInfo,
+ nwal_Bool_t* pFreePkt);
+
+
+//***********************************
+//internal utilities
+//*************************************
+
+//return the list of pktios for this instance
+static inline void ** netapi_get_pktio_list(NETAPI_T p)
+{
+NETAPI_HANDLE_T *pp = (NETAPI_HANDLE_T *) p;
+return &pp->pktios[0];
+}
+
+//get scheduler block handle
+static inline void * netapi_get_scheduler(NETAPI_T p)
+{
+ NETAPI_HANDLE_T *pp = (NETAPI_HANDLE_T *) p;
+ return pp->p_sched;
+}
+
+/* return pointer to global area */
+NETAPI_GLOBAL_T * netapi_get_global(void);
+
+//add a pktio name (and queue) to global list
+static inline int netapip_addGlobalPktio(NETAPI_T p, char *name, Qmss_Queue * qn)
+{
+NETAPI_HANDLE_T *pp = (NETAPI_HANDLE_T *) p;
+PKTIO_ENTRY_T *pe;
+int i;
+//find a free slot
+pe = &((NETAPI_GLOBAL_T *)(pp->global))->pktios[0];
+
+for(i=0;i<NETAPI_MAX_PKTIO; i++,pe++)
+ {
+ if (pe->qn.qNum == -1)
+ {
+ pe->qn.qNum=qn->qNum;
+ pe->qn.qMgr=qn->qMgr;
+ strncpy(pe->name, name, PKTIO_MAX_NAME);
+ return 1;
+ }
+ pe+=1;
+ }
+ return 0; //no room
+}
+
+//delete a pktio name (and queue) to global list
+static inline int netapi_del_global_pktio(NETAPI_T p, char *name)
+{
+NETAPI_HANDLE_T *pp = (NETAPI_HANDLE_T *) p;
+PKTIO_ENTRY_T *pe;
+int i;
+//find slot
+pe = &((NETAPI_GLOBAL_T *)(pp->global))->pktios[0];
+
+for(i=0;i<NETAPI_MAX_PKTIO; i++,pe++)
+ {
+ if (pe->qn.qNum == -1) continue;
+ if (!strncmp(name, pe->name, PKTIO_MAX_NAME))
+ {
+ pe->qn.qNum=-1;
+ pe->name[0]='\0';
+ return 1;
+ }
+ pe+=1;
+ }
+ return 0; //no room
+}
+
+
+/* get list of global pktios that have been created */
+static inline Qmss_Queue* netapip_findGlobalPktio(NETAPI_T p, char *name)
+{
+NETAPI_HANDLE_T *pp = (NETAPI_HANDLE_T *) p;
+PKTIO_ENTRY_T *pe;
+int i;
+//find slot
+pe = &((NETAPI_GLOBAL_T *)(pp->global))->pktios[0];
+
+for(i=0;i<NETAPI_MAX_PKTIO; i++,pe++)
+ {
+ if (pe->qn.qNum == -1) continue;
+ if (!strncmp(name, pe->name, PKTIO_MAX_NAME))
+ {
+ return &pe->qn;
+ }
+ pe +=1;
+ }
+ return NULL; //not found
+}
+
+/* return the nwal global instance handle */
+static inline nwal_Handle netapip_returnNwalInstanceHandle(NETAPI_T p)
+{
+
+NETAPI_HANDLE_T *pp = (NETAPI_HANDLE_T *) p;
+return ((NETAPI_GLOBAL_T *)(pp->global))->nwal_context.nwalInstHandle;
+}
+
+
+
+//utility to clear out a queue
+void netapip_zapQ(int queueNum);
+void netapip_netcpCfgBuildRoute(NETCP_CFG_ROUTE_T * p_route, int16_t * p_flow, Qmss_QueueHnd * p_q);
+
+//database utilities
+void netapip_netcpCfgDeleteSa(NETAPI_NWAL_GLOBAL_CONTEXT_T *p,int sa_slot);
+void netapip_netcpCfgInsertSa(NETAPI_NWAL_GLOBAL_CONTEXT_T *p,
+ int sa_slot, //we 'reserved it already'
+ int dir,
+ int mode,
+ void * temp1,
+ void * temp2,
+ void * handle_inflow,
+ void * handle_sideband,
+ nwalTxDmPSCmdInfo_t *dmPSCmdInfo;);
+void *netapip_netcpCfgGetSaHandles( NETAPI_NWAL_GLOBAL_CONTEXT_T *p,
+ int sa_slot, void ** p_sideband);
+void* netapip_netcpCfgGetMacHandle(NETAPI_NWAL_GLOBAL_CONTEXT_T *p,int iface_no);
+NetapiNwalTransInfo_t * netapip_getFreeTransInfo(NETAPI_GLOBAL_T *p_global, nwal_TransID_t *pTransId);
+void netapip_freeTransInfo(NetapiNwalTransInfo_t* pTransInfo);
+void *netapip_netcpCfgGetPolicy( NETAPI_NWAL_GLOBAL_CONTEXT_T *p,
+ int policy_slot);
+nwalTxDmPSCmdInfo_t* netapip_netcpCfgGetSaSBInfo(NETAPI_NWAL_GLOBAL_CONTEXT_T *p,
+ NETCP_CFG_SA_T sa_app_id);
+int netapip_netcpCfgGetSaInflowInfo(NETAPI_NWAL_GLOBAL_CONTEXT_T *p,
+ NETCP_CFG_SA_T sa_app_id,
+ uint32_t *swInfo0,
+ uint32_t *swInfo1);
+
+int netapip_systemInit(NETAPI_HANDLE_T *);
+void netapip_cleanupAtStart(void);
+#endif