summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: f4654cc)
raw | patch | inline | side by side (parent: f4654cc)
author | David Lide <a0216552@gtudci01.(none)> | |
Thu, 26 Jan 2012 22:29:54 +0000 (17:29 -0500) | ||
committer | David Lide <a0216552@gtudci01.(none)> | |
Thu, 26 Jan 2012 22:29:54 +0000 (17:29 -0500) |
netapi_timer.h -> added comments, minor changs to api
timlist.c -> bug in recovering cancelled timer, added unit test code
netapi_timer.c -> minor api changes\
timlist.c -> bug in recovering cancelled timer, added unit test code
netapi_timer.c -> minor api changes\
index 63dd2ecb90437ddea7aa67781899fcc134ceeb69..ae05a1198ec5e82f407854d316a0b504ec610020 100644 (file)
%.o: %.c
$(CC) -c $(CFLAGS) $< -o $@
-api: $(NETAPI_LIB_DIR)/api_lib.a
+api: $(NETAPI_LIB_DIR)/ti.runtime.netapi.aearmv7.a
-$(NETAPI_LIB_DIR)/api_lib.a: $(API_OBJS)
- rm -f $(NETAPI_LIB_DIR)/api_lib.a
- $(AR) rcv $(NETAPI_LIB_DIR)/api_lib.a $(API_OBJS)
+$(NETAPI_LIB_DIR)/ti.runtime.netapi.aearmv7.a: $(API_OBJS)
+ rm -f $(NETAPI_LIB_DIR)/ti.runtime.netapi.aearmv7.a
+ $(AR) rcv $(NETAPI_LIB_DIR)/ti.runtime.netapi.aearmv7.a $(API_OBJS)
index a74294c20ecb9f440a725636ce13169e01f24fa5..213974c6deb2c8d0bad729b01b797e1715d8b0dd 100644 (file)
* OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
***********************************************/
+
+/** @mainpage Netapi Timer Lib
+ *
+ * @section intro Introduction
+ *
+ * The network API provides a user space interface to timers
+ * - a function to read a hw provided 64bit time stamp, @ref netapi_getTimestamp
+ * This returns a tick running at 1/6 cpu frequency
+ * - functions to create or open timer groups: @ref netapi_TimerGroupCreateTimer
+ * and @ref netapi_TimerGroupOpenTimer. A timer group
+ * is a group of timers with the same characteristics:
+ * -> local or global
+ * -> timer resolution (msc, 10 msc, etc)
+ * -> expect to fire or expect to cancel
+ * -> the same call back function for fired timers
+ * - functions to close or delete timer groups
+ * - function to start a timer, @ref netapi_TimerGroupStartTimer
+ * - function to cancel a timer, @ref netapi_TimerGroupCancelTimer
+ * - function to poll a timer group, or all timer groups registered to a NETAPI
+ * instance
+ * \par
+ * NOTE:
+ * (C) Copyright 2010-2011 Texas Instruments, Inc.
+ * \par
+ */
+
+
#ifndef __NETAPI_TIMER__H
#define __NETAPI_TIMER__H
#include "netapi.h"
extern volatile unsigned long * t64_virt_addr;
extern unsigned int cpu_cycles_sec;
-//return clock ticks per second
+//return hw timer clock ticks per second
unsigned long t64_ticks_sec(void);
#define netapi_getTicksPerSec t64_ticks_sec
-//return 64 bit timestamp
+
+/** @ingroup netapi_api_functions */
+
+/*
+ * @brief API returns a 64bit h/w timestamp
+ *
+ * @details reads a h/w timer (TIMER64 on Appleton SOC) and returns a 64 bit time stamp
+ * timer runs at @ref t64_ticks_sec. Nominally this should be 1/6 CPU clk (@ref cpu_cycles_sec)
+ *
+ * @param[in] none
+ * @retval unsigned long long timestamp (64 buts)
+ * @pre @ref netapi_init
+ */
+//return 64 bit timestamp from hw timer
static inline unsigned long long netapi_getTimestamp(void)
{
volatile unsigned long long t1;
typedef void * NETAPI_TIMER_GROUP_HANDLE_T;
typedef void * NETAPI_TIMER_T;
typedef void * NETAPI_TIMER_LIST_T;
+
+/* timer filter values */
typedef int NETAPI_TIMER_FILTER_T;
#define NETAPI_TIMER_NA (void*) NULL
#define NETAPI_TIMER_FILTER_GLOBAL 0x1
@@ -83,13 +125,46 @@ NETAPI_TIMER_T netapi_TimerGetNext( NETAPI_TIMER_LIST_T list,NETAPI_TIMER_T prev
void * netapi_TimerGetCookie(NETAPI_TIMER_T timer);
unsigned long long netapi_TimerGetTs(NETAPI_TIMER_T timer); //debug
+/*
+ * @brief API callback for timer expiration
+ *
+ * @details this function, provided by application, is registered by application
+ * when timer group is created. It is called by timer library when a timer or set of timers
+ * expire. The timer list can be walled with iterators: @ref netapi_TimerGetFirst,
+ * @ref netapi_TimerGetNext. The timer id or "cookie" can be accessed via @ref netapi_TimerGetCookie
+ * NOTE: callback should check for cookie==NULL since timer could be cancelled as it is being fired
+ * @param[in] @ref NETAPI_TIMER_GROUP_HANDLE_T : the handle to the timer group
+ * @param[in] int : the number of timers that have fired
+ * @param[in] @ref NETAPI_TIMER_LIST_T : the list of timers that hace expired
+ * @param[in] uint64_t : the current time
+ * @retval none
+ * @pre @ref netapi_init , @ref netapi_TimerGroupCreate, @ref netapi_TimerGroupStartTimer
+ */
//timer callback
typedef void (*NETAPI_TIMER_CB_T) (
- NETAPI_TIMER_GROUP_HANDLE_T th,
+ NETAPI_TIMER_GROUP_HANDLE_T th, //timer group
int n_fired, //# timers fired
- NETAPI_TIMER_LIST_T fired_list,
- uint64_t currentTime);
+ NETAPI_TIMER_LIST_T fired_list, //the list of fired timers. Access via iterators above
+ uint64_t currentTime); //current timestamp
+/*
+* @brief API for Timer Group Creation
+ *
+ * @details this function is used to create a timer group. A timer group is a block of timers
+ * that share the same characteristics.
+ * @param[in] @ref NETAPI_T : the handle to the NETAPI Instance
+ * @param[in] char * : the name of the timer
+ * @param[in] @ref NETAPI_TIMER_CB_T : the callback function
+ * @param[in] int : local (=1 if this timer group is local to this netapi instance, =0 if global)
+ * @param[in] int : exp2cancel. (=1 if this timer group is expected to be cancelled, =0 otherwise))
+ * @param[in] int : the timer group 'tick'. This is the group timer resolution in hw timestamp units.
+ * Eg for 10 msc , enter @ref netapi_getTicksPerSec()/100
+ * @param[in] int : timerTolerence in hw timestamp ticks. This is FUTURE.
+ * @param[in] int : maxTimers - the max number of timers that can be handled by the group.
+ * @param[in] int* : pointer to error return
+ * @retval @ref NETAPI_TIMER_GROUP_HANDLE_T : handle for this timer group
+ * @pre @ref netapi_init
+ */
//create a timer group
NETAPI_TIMER_GROUP_HANDLE_T netapi_TimerGroupCreate(
NETAPI_T netHandle, //netapi instance
NETAPI_TIMER_CB_T cb, //the callback function
int local, //1 if timers local to thread
int exp2cancel,//1 if expect to cancel
- int timerTicksPerGroupTick, //resolution for this timer block, in timer ticks
+ int timerTicksPerGroupTick, //resolution for this timer block, in hw timer ticks
+ int timerTolerence, //tolerence for this timer block, in hw timer ticksi [FUTURE]
int maxTimers, //max # of timer objects for this group
int *pErr);
-//open a [global] timer group
+//open a [global] timer group [FUTURE]
NETAPI_TIMER_GROUP_HANDLE_T netapi_TimerGroupOpen(
NETAPI_T netHandle,
+ char * name,
NETAPI_TIMER_CB_T cb,
int *pErr);
+/*
+* @brief API for Start a Timer
+ *
+ * @details this function is used to start a timer. When it expires, the @ref NETAPI_TIMER_CB_T
+ * will be called.
+ * @param[in] @ref NATAPI_TIMER_GROUP_HANDLE_T : the handle to the timer group
+ * @param[in] void * : application provided timer id or cookie. MUST NOT BE NULL!!!
+ * @param[in] uint64_t : offset from current time when to fire this timer. This offset MUST be in
+ * units of timer group ticks (set at create time). Eg. For 10 msc timer group,
+ * offset2fire =1 => timer is to fire in 10 msc.
+ * @param[in] int* : pointer to error return
+ * @retval @ref NETAPI_TIMER_T : handle for this timer. Used to reference the timer for cancel
+ * @pre @ref netapi_init , @ref netapi_TimerGroupCreate
+ */
//start an individual timer
-NETAPI_TIMER_T netapi_TimerGroupStartiTimer(
- NETAPI_TIMER_GROUP_HANDLE_T th,
- void * cookie,
+NETAPI_TIMER_T netapi_TimerGroupStartTimer(
+ NETAPI_TIMER_GROUP_HANDLE_T th, //the group handle
+ void * cookie, //user id -> CANNONT BE NULL
uint64_t offs2fire, //offset in timerGroup ticks (eg msc)
- int * pErr);
+ int * pErr); //error return
+/*
+* @brief API for Cancel a Timer
+ *
+ * @details this function is used to cancel a timer. When it expires, the @ref NETAPI_TIMER_CB_T
+ * will be called.
+ * @param[in] @ref NATAPI_TIMER_GROUP_HANDLE_T : the handle to the timer group
+ * @param[in] @ref NATAPI_TIMER_T : the handle to the individual timer to cancel
+ * @param[in] int* : pointer to error return
+ * @retval none
+ * @pre @ref netapi_TimerGroupStartTimer
+ */
//Cancel a timer
void netapi_TimerGroupCancel(
NETAPI_TIMER_GROUP_HANDLE_T th,
//poll a specific timer group
int netapi_TimerGroupPoll(NETAPI_TIMER_GROUP_HANDLE_T th, int maxTimers);
+/*
+* @brief API for Polling all timer groups attached to an instance
+ *
+ * @details this function is used to poll all or a specified subset of the timer groups of an
+ * instance. A mask can be set to filter which categories of timer groups (local vs global etc)
+ * to poll. The approximate max # of timers to process can also be set.
+ * @param[in] @ref NATAPI_T : the handle of the netapi instance.
+ * @param[in] @ref NATAPI_TIMER_FILTER_T : the bit mask of timer group types to poll
+ * @param[in] int : approximate max number of timers to process. NOTE: this can be used to
+ * coarsely control how many timers to process. In general, all timers that have been
+ * hashed into the same cell and have expired will be processed regardless of the
+ * maxTmers setting.. [FUTURE]
+ * @retval none
+ * @pre @ref netapi_init, @ref netapi_TimerGroupCreate
+ */
+
//poll all timers
int netapi_TimerGroupPollAll(NETAPI_T nh, NETAPI_TIMER_FILTER_T f, int maxTimers);
index 2565089e33fef05b19abdbe0e6d7fa956971d77d..21d5cdd946c114db584c3a7db7a2d6ca3a9f7798 100644 (file)
NETAPI_TIMER_CB_T cb,
int local, //1 if timers local to thread
int exp2cancel,//1 if expect to cancel
- int cell_width,
+ int cell_width, //in ticks
+ int tol, //in ticks
int maxTimers,
int *pErr)
{
temp_g.local = local;
temp_g.exp2cancel= exp2cancel;
temp_g.cell_width=cell_width;
+ temp_g.tol=tol;
temp_g.h = netHandle;
temp_g.last_polled=(netapi_getTimestamp()/cell_width) * cell_width + (cell_width-1);
printf(">timer group %s created. width = %d (ticks)\n", name, cell_width);
//open a [global] timer group
NETAPI_TIMER_GROUP_HANDLE_T netapi_TimerGroupOpen(
NETAPI_T netHandle,
+ char * name,
NETAPI_TIMER_CB_T cb,
int *pErr)
{
tim_return_fired_list(&((TIMER_GROUP_T*) th)->cells[cell],
&res,
&((TIMER_GROUP_T*) th)->free,
- i,
+ i,
&n);
if (n)
{
int netapi_TimerGroupPollAll(NETAPI_T nh, NETAPI_TIMER_FILTER_T f, int maxTimers)
{
//todo: use filters and poll global, local lists in nh
- netapi_TimerGroupPoll(&temp_g, maxTimers);
+ if (temp_g.h)
+ netapi_TimerGroupPoll(&temp_g, maxTimers);
return 0;
}
index dcea6e9364737d0f7afdba458b15989ba6c06347..9b086de91b77813f176486a6eb5b3991122f99b1 100644 (file)
* OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
***************************************/
-#include "netapi_timer.h"
+//#define TEST_DRIVER
+#ifdef TEST_DRIVER
+typedef void * NETAPI_T;
+typedef void * NETAPI_TIMER_CB_T;
+#else
+#include "../netapi_timer.h"
+#endif
#include "timer_loc.h"
-#include "netapi_err.h"
+#include "../netapi_err.h"
#ifndef NULL
#define NULL 0
}
else //skip over cancelled timer..
{
- //skip & free
+ //skip & free. make sure we adjust head or tail if necessary
if (p_last){
p_last->next=p->next;
}
else {
- tl->head = p->next;
+ tl->head = p->next; /* we are freeing old head..*/
}
+ if (tl->tail ==p) tl->tail=p_last; /* we are freeing old tail */
temp_p_next=p->next;
tim_return_single_free(ftl,p);
p=temp_p_next;
else {
tl->head = p->next;
}
+ if (tl->tail ==p) tl->tail=p_last; /* we are freeing old tail */
temp_p_next=p->next;
tim_return_single_free(ftl,p);
p=temp_p_next;
return p;
}
-//#define TEST_DRIVER
#ifdef TEST_DRIVER
TIM_LIST_T the_base={NULL,NULL};
TIM_LIST_T cell_base={NULL,NULL};
@@ -340,7 +347,23 @@ tim_return_fired_list(&cell_base, &res, &the_base, (unsigned long long) i, &n);
printf("at %d got %d\n", i, n);
if (n) tim_return_free(&the_base,&res,n);
}
+
+//special cases..
+
+ timers[0]=tim_set(&cell_base, &the_base, 106LL, (void *)10, &err);
+ tim_cancel(timers[0],&err);
+ tim_return_fired_list(&cell_base, &res, &the_base, (unsigned long long) 106, &n);
+ timers[0]=tim_set(&cell_base, &the_base, 106LL, (void *)10, &err);
+ timers[1]=tim_set(&cell_base, &the_base, 106LL, (void *)10, &err);
+ tim_cancel(timers[0],&err);
+ tim_return_fired_list(&cell_base, &res, &the_base, (unsigned long long) 106, &n);
+
+ timers[0]=tim_set(&cell_base, &the_base, 106LL, (void *)10, &err);
+ timers[1]=tim_set(&cell_base, &the_base, 106LL, (void *)10, &err);
+ tim_cancel(timers[0],&err);
+ tim_cancel(timers[1],&err);
+ tim_return_fired_list(&cell_base, &res, &the_base, (unsigned long long) 106, &n);
}
#endif
index b98c38a2a57aa967841dcf1b79ea29fd3b9324bd..21c2edefe257c062db8d16074d2ff1cb31479f4e 100644 (file)
%.o: %.c
$(CC) -c $(CFLAGS) $< -o $@
-$(NETAPI_LIB_DIR)/api_lib.a:
+$(NETAPI_LIB_DIR)/ti.runtime.netapi.aearmv7.a:
make -C $(NETAPI_BUILD_DIR)
-net_test: $(NT_OBJS) $(TRIE_OBJS) $(NETAPI_LIB_DIR)/api_lib.a
- $(CC) $(LDFLAGS) $(NT_OBJS) $(TRIE_OBJS) $(NETAPI_LIB_DIR)/api_lib.a $(PKTLIB_LIB) $(QMSS_LIB) $(CPPI_LIB) $(NWAL_LIB) $(PA_LIB) -o net_test
+net_test: $(NT_OBJS) $(TRIE_OBJS) $(NETAPI_LIB_DIR)/ti.runtime.netapi.aearmv7.a
+ $(CC) $(LDFLAGS) $(NT_OBJS) $(TRIE_OBJS) $(NETAPI_LIB_DIR)/ti.runtime.netapi.aearmv7.a $(PKTLIB_LIB) $(QMSS_LIB) $(CPPI_LIB) $(NWAL_LIB) $(PA_LIB) -o net_test
synchtest: ../synchtest.o
index 188890e6c45c0679f5419a783008bee2d19cb31d..8d147d0d24987f9f4645ce0551fa6cf5653f3f8a 100755 (executable)
200LL, //every second
&err);
else
+ {
t3 = netapi_TimerGroupStartTimer(
th,
(void *) 3,
300LL, //every second
&err);
+ //cancel 1 and restart 1
+ netapi_TimerGroupCancel(th,t1,&err);
+ t1 = netapi_TimerGroupStartTimer(
+ th,
+ (void *) 1,
+ 100LL, //every second
+ &err);
+
+
+ }
tx = netapi_TimerGetNext(fired_list,tx);
0, //1 if timers local to thread
0, //1 if expect to cancel
netapi_getTicksPerSec()/100, /* 10 msc resolution for these timers */
+ netapi_getTicksPerSec()/1000, /* would like 1msc tolerence */
100,
&err);
if (err) {printf("timergroupcreate failed %d\n",err); exit(1);}