Update location of doxygen output folder, config file changes, setup script changes
authorTinku Mannan <tmannan@ti.com>
Thu, 25 Apr 2013 15:23:53 +0000 (11:23 -0400)
committerTinku Mannan <tmannan@ti.com>
Thu, 25 Apr 2013 15:23:53 +0000 (11:23 -0400)
ti/runtime/netapi/build/netapi_doxygen.cfg
ti/runtime/netapi/test/net_test_config.txt
ti/runtime/netapi/test/net_test_setup.sh

index 557adbbf940979bcc1f80af12103ea0cbaf2d3fa..9eff4f52695988731899275ca6575584b958c6dd 100755 (executable)
@@ -38,7 +38,7 @@ PROJECT_NUMBER         =
 # If a relative path is entered, it will be relative to the location
 # where doxygen was started. If left blank the current directory will be used.
 
-OUTPUT_DIRECTORY       = ../docs
+OUTPUT_DIRECTORY       = ../docs/doxygen
 
 # If the CREATE_SUBDIRS tag is set to YES, then doxygen will create
 # 4096 sub-directories (in 2 levels) under the output directory of each output
index f24bf63c97e9ce5c307e8da9909fb8260bf79d31..598dfe5755669c9883c72870e8bb57411a93ae23 100755 (executable)
@@ -1,7 +1,8 @@
 #sp0 thread-number start-core end-core
 sp0 = 1 0-0
-fp0 = 2 0-0 
-fp1 = 3 0-0
+fp0 = 2 1-1 
+fp1 = 3 2-2
+fp2 = 4 3-3
 #mac0 = mac-address switch-port
 mac0 = 00-01-02-03-05-05 sp0
 #mac1 = 00-01-02-03-05-06 sp1
index 8fe90af90b850dd14f6768ea424a749c10cb5553..7d680062af9bbd0ae0cf1e1549de7f5e689f965b 100644 (file)
@@ -1,9 +1,13 @@
 #!/bin/sh
 
-#modprobe hplibmod
+#install kernel module
+insmod /lib/modules/3.8.4-rt2/extra/hplibmod.ko
 #
-#cat /proc/netapi
+cat /proc/netapi
 #
 devmem2 0x2090804 w 0x4
-/usr/bin/net_test
+#
+# run net_test applicaton, default location of config file is in /etc/netapi, 
+# default config file name is net_test_config.txt
+/usr/bin/net_test /etc/netapi/net_test_config.txt
 #