SDOCM00115593: Re-size max control rx/tx buf size to sync with latest PA LLD
Update version
Update makefile for parallel build issue
Add offload support for SA_EALG_AES_GCM
Update to sync with latest version of PA-LLD
Update release version
Fix for SDOCM00114893
7 years agoSDOCM00113252: transportnetlib queue clean up logic does not work when RM is used DEV.NETAPI.01.01.00.04
SDOCM00113252: transportnetlib queue clean up logic does not work when RM is used
SDOCM00113322: kernel RX UDP/TCP checksum offload to NETCP breaks user space tranportnetlib sample applications
Removed RM OSAL functions, now part of hplib, coverity cleanup
Adding stub functions for RM OSAL multi-thread critical section enter and exit
Resolve Coverity warnings
SDOCM00112879: There needs to be a definitive way to determine if you are using IPSEC inflow mode for the ipsec manager/kernel module
Resolve coverity warning in pktio.c
SDOCM00113664: The default exception handler setup inside netapi_int should be made configurable
SDOCM00112200: Making NETAPI tuneable parameters configurable in code
SDOCM00112354: Require support for start/stop offloading of policies sharing signle CHILD_SA
SDOCM00113075: DPI demo: typo on main page
SDOCM00112355: Need multi-instance support of IPSecMgr library
Fix in netapi_pktioOpen when calling Qmss_queueOpen
SDOCM00113227: transportnetlib K2H: nt_bridge_setup application minor bugs
Update eqos config files
Version Update
Update install to include nt_bridge_setup.sh
NETAPI changes for EQOS mode support
Remove subtraction of MAC trailer from the packet len being sent for DPI
SDOCM00112691: Fix setup scripts for loopback and router appliations
dpi demo updates to collect memory stats per core/thread,
makefile update to install gif files.
makefile update to install gif files.
some changes to scripts
modified demo script and Make file to include new .awk files, and .gifs
added awk file to process packet stats
Fix clear stats for transport_dpi_demo application
Merge branch 'master' of gtgit01.gt.design.ti.com:git/projects/netapi
some updates to scripts/web pages
Update config file paths to point to new location on filesystem
Integrate transport_dpi_demo with RM
Merge remote branch 'origin/dpi_demo'
Multi-proc changes for integration with latest NWAL
Merge branch 'multi-proc'
Conflicts:
ti/runtime/netapi/src/netapi_init.c
ti/runtime/netapi/src/netapi_loc.h
ti/runtime/netapi/test/net_test_bench.c
ti/runtime/netapi/test/net_test_router.c
Conflicts:
ti/runtime/netapi/src/netapi_init.c
ti/runtime/netapi/src/netapi_loc.h
ti/runtime/netapi/test/net_test_bench.c
ti/runtime/netapi/test/net_test_router.c
Updates to transport_dpi_demo_setup to restart thttpd with ability to run cgi scripts, other minor updates.
Updates to transport_dpi_demo_setup.sh
Update net_test setup scripts to reflect new path to config files
Makefile updates for install
Adding demo setup files
Update calls to netapi_netcpCfgCreateMacInterface with etherType field
Renaming demo files to reflect transport, fix stats collection for multi-proc
Updates for stats collection across processes
Adding netapi dpi demo files
Add support for etherType field for netapi_netcpCfgCraeteMacInterface
Additional fix for SDOCM00107974: Add support for hmac-sha256 in netapi ipsecmgr daemon
Integrate net_test_router with RM.
Update version to 01.01.00.02
SDOCM00112119,SDOCM00108231: Added option for stop_offload command to not expire SA
DOCM00112138: Resolve issue with NETAPI ipsecmgr delete Sa interface API.
Remove printf from pktio send functions.
Resolve NETAPI library coverity warnings.
net_test_loopback: only teardown DSP fastpath classifier and pktio channel if NETAPI_SYS_MASTER
Fix delete and find pktio internal functions
Test application updates for Multi-process support in NETAPI
Multi-proc support in NETAPI
Upate pktio.c to include csl_qm_queue.h
Fix compilation issues
Update release version
Release spinlock in case of sock_send failure to RM server
SDOCM00107974: Add support for hmac-sha2-256 in netapi ipsecmgr daemon
NETAPI ipsecmgr daemon changes to integrate with Resource Manager(RM)
NETAPI library and test changes to integrate with Resource Manager(RM)
SDOCM00107645: ipsecmgr sampe application needs to provide option for user to give flow to use for egress offload
SDOCM00107645: ipsecmgr sampe application needs to provide option for user to give flow to use for egress offload
NETAPI changes to support device specific libraries
NETAPI makefile updates to sync with yocto recipes
Merge remote-tracking branch 'origin/lamarr'
Conflicts:
ti/runtime/netapi/src/netapi_loc.h
Conflicts:
ti/runtime/netapi/src/netapi_loc.h
8 years agoFix for SDOCM00107501:Compilation issues observed when compiling with C++ DEV.NETAPI.01.00.00.11
Fix for SDOCM00107501:Compilation issues observed when compiling with C++
Fix makefile_armv7 to build shared libraries
Integration changes with latest NWAL
Fix for SDOCM00106989: Additional fix for K2E settings
Fix for SDOCM00107104: NETAPI changes to support new mechanism for PA stats collection for K2L/K2E.
Fix for SDOCM00106989: Need to update netapi ipsecmgr with K2L/K2E device-tree paths for netrx completion queue and flow
NETAPI changes for MCSDK3.1, cleanup
Change back paFwActive flag to nwal_TRUE, fix of previous commit
Resize PA_ BUFFER2 configuration size for k2l/k2e
mFix install rule for ipsecmgr_daemon.out
Makefile udpates to build device specific test applications
NETAPI test application changes for MCSDK 3.1 which supports k2l/k2e
NETAPI library changes for MCSDK 3.1 which supports k2l/k2e
some minor changes to test code:
- bug in net_test_router double counting rx pkts
- handle other crypto modes in router.c
- support NULL crypto/auth combinations in net_test_sa_utils.c
-
- bug in net_test_router double counting rx pkts
- handle other crypto modes in router.c
- support NULL crypto/auth combinations in net_test_sa_utils.c
-
Updated version to 01.00.00.10
This commit adds the following:
1. SDOCM0090624: Fix for Delete Classifer API will try and delete the same
ad hoc IP rule if it is used in multiple classifiers.
2. Incorporated NETAPI code review comments.
1. SDOCM0090624: Fix for Delete Classifer API will try and delete the same
ad hoc IP rule if it is used in multiple classifiers.
2. Incorporated NETAPI code review comments.
Added back rule for netapi shared object compilation
General cleanup to remove collection of debug stats
SDOCM00090624:Delete Classifer API will try and delete the same ad hoc IP rule if it is used in multiple classifiers
Multiple interface routing support updates.
Added support for routeType configurtion for exception rules.
Added support for remote/source IP configuration for IP rules.
Added support for remote/source IP configuration for IP rules.
NETAPI updates to support enhanced route types.
Integration with latest version of HPLIB
Added IPV6 and bridge interface support
Fix for SDOCM00103887- resized TUNE_NETAPI_CONFIG_MAX_SA_TO_PA_DESC to 200.
Added shared object library support, updated release version.
Multi-proc support in NETAPI changes
Fix for SDOCM00103116: netapi_init() error codes not checked in right place.