keystone-rtos/netapi.git
2014-08-05 Tinku MannanAdd support for etherType field for netapi_netcpCfgCrae...
2014-07-28 Tinku MannanAdditional fix for SDOCM00107974: Add support for hmac...
2014-07-25 Tinku MannanIntegrate net_test_router with RM. DEV.NETAPI.01.01.00.02
2014-07-24 Tinku MannanUpdate version to 01.01.00.02
2014-07-23 Tinku MannanSDOCM00112119,SDOCM00108231: Added option for stop_offl...
2014-07-19 Tinku MannanDOCM00112138: Resolve issue with NETAPI ipsecmgr delete...
2014-07-18 Tinku MannanRemove printf from pktio send functions.
2014-07-18 Tinku MannanResolve NETAPI library coverity warnings.
2014-06-04 Tinku MannanUpate pktio.c to include csl_qm_queue.h DEV.NETAPI.01.01.00.01
2014-06-03 Tinku MannanFix compilation issues
2014-05-22 Tinku MannanUpdate release version
2014-05-22 Tinku MannanRelease spinlock in case of sock_send failure to RM...
2014-05-22 Tinku MannanSDOCM00107974: Add support for hmac-sha2-256 in netapi...
2014-05-14 Tinku MannanNETAPI ipsecmgr daemon changes to integrate with Resour...
2014-05-14 Tinku MannanNETAPI library and test changes to integrate with Resou...
2014-05-08 Tinku MannanSDOCM00107645: ipsecmgr sampe application needs to...
2014-05-06 Tinku MannanSDOCM00107645: ipsecmgr sampe application needs to...
2014-04-30 Tinku MannanNETAPI changes to support device specific libraries
2014-04-29 Tinku MannanNETAPI makefile updates to sync with yocto recipes
2014-04-24 Tinku MannanMerge remote-tracking branch 'origin/lamarr'
2014-04-22 Tinku MannanFix for SDOCM00107501:Compilation issues observed when... DEV.NETAPI.01.00.00.11
2014-04-22 Tinku MannanFix makefile_armv7 to build shared libraries
2014-04-21 Tinku MannanIntegration changes with latest NWAL
2014-03-27 Tinku Mannan Fix for SDOCM00106989: Additional fix for K2E settings
2014-03-24 Tinku MannanFix for SDOCM00107104: NETAPI changes to support new...
2014-03-18 Tinku MannanFix for SDOCM00106989: Need to update netapi ipsecmgr...
2014-02-18 Tinku MannanNETAPI changes for MCSDK3.1, cleanup DEV.NETAPI.01.01.00.00
2014-02-03 Tinku MannanChange back paFwActive flag to nwal_TRUE, fix of previo...
2014-01-24 Tinku MannanResize PA_ BUFFER2 configuration size for k2l/k2e
2014-01-24 Tinku MannanmFix install rule for ipsecmgr_daemon.out
2014-01-23 Tinku MannanMakefile udpates to build device specific test applications
2014-01-23 Tinku MannanNETAPI test application changes for MCSDK 3.1 which...
2014-01-23 Tinku MannanNETAPI library changes for MCSDK 3.1 which supports...
2013-11-14 David Lidesome minor changes to test code: DEV.NETAPI.01.00.00.10
2013-11-13 Tinku MannanUpdated version to 01.00.00.10
2013-11-13 Tinku MannanThis commit adds the following:
2013-11-12 Tinku MannanAdded back rule for netapi shared object compilation
2013-11-12 Tinku MannanGeneral cleanup to remove collection of debug stats
2013-11-08 Tinku MannanSDOCM00090624:Delete Classifer API will try and delete...
2013-11-05 Tinku MannanMultiple interface routing support updates.
2013-11-04 Tinku MannanAdded support for routeType configurtion for exception...
2013-10-24 Tinku MannanNETAPI updates to support enhanced route types.
2013-10-15 Tinku MannanIntegration with latest version of HPLIB
2013-09-20 Tinku MannanAdded IPV6 and bridge interface support DEV.NETAPI.01.00.00.09
2013-09-18 Tinku MannanFix for SDOCM00103887- resized TUNE_NETAPI_CONFIG_MAX_S...
2013-09-17 Tinku MannanAdded shared object library support, updated release...
2013-09-04 Tinku MannanMulti-proc support in NETAPI changes
2013-09-04 Tinku MannanFix for SDOCM00103116: netapi_init() error codes not...
2013-09-04 Tinku MannanFix for SDOCM00103205: scheduler cycle counts are not...
2013-09-04 Tinku MannanFix for SDOCM00103115: ARM user space transport: net...
2013-07-24 Tinku MannanSDOCM00102718: Offload support for AEX_XCBC DEV.NETAPI.01.00.00.08
2013-07-23 Tinku MannanChanging netapi_secGetChanCtxInfo API definition and...
2013-07-22 Tinku MannanThis commit adds the following:
2013-07-20 Tinku MannanMulti-proc changes
2013-07-20 Tinku MannanSupport for multiple interfaces
2013-07-17 Tinku MannanThis commit adds the following:
2013-07-12 Tinku MannanThis commit adds the following:
2013-07-10 Tinku MannanMakfile updates for yocto
2013-07-10 Tinku MannanNETAPI integration with ipsecmgr
2013-05-28 Tinku MannanConfiguration updates for router application DEV.NETAPI.01.00.00.07
2013-05-22 Tinku MannanFix DSP load issue for DSP cores 0 and 1
2013-05-22 Tinku MannanRemoved IPSEC_TOOLS dir and contents
2013-05-21 Tinku MannanAdding scripts/configuration files to test IPSEC wit...
2013-05-21 Tinku Mannan fix for SDOCM00101400- sp config file parameter is...
2013-05-17 Tinku MannanChanges for yocto build env.
2013-05-16 Tinku MannanUpdates to net_test_bench application, removed net_test...
2013-05-16 Tinku MannanSet qmQueMgmtProxyDataReg to NULL for k1, k2h
2013-05-15 Tinku MannanAdding net_test_bench application, scripts to set irq...
2013-05-13 Tinku MannanThis commit adds the following:
2013-05-13 Tinku MannanFix for SDOCM00101269: call netapi_netcpCfgException...
2013-05-03 Tinku MannanChanges to compile with devkit
2013-04-28 Raghu NambiathUpdate for nightly build fix. Incorrect typo in the... DEV.NETAPI.01.00.00.06
2013-04-26 Tinku Mannanfix for net_test_setup.sh script for hplibmod.ko path...
2013-04-25 Tinku MannanUpdate version info to 01.00.00.06
2013-04-25 Tinku MannanMakefile cleanup: removed dependency on CORTEX_A15...
2013-04-25 Tinku MannanUpdate location of doxygen output folder, config file...
2013-04-24 Tinku MannanMakefile updates for yocto: fixed make install for...
2013-04-24 Tinku MannanNETAPI net test application updates
2013-04-24 Tinku MannanUpdated the netapi build infrastructure to align for...
2013-04-16 Tinku MannanFixed issue with running and gracefully terminating...
2013-03-26 Tinku MannanUpdated netapi makefile to use correct DEVICE define... DEV.NETAPI.01.00.00.05
2013-03-25 Tinku MannanThis commits adds the following:
2013-03-13 Tinku MannanThis commit adds the following:
2013-02-22 David Lideone more fix
2013-02-22 David Lidechanges for ifdma mode. some fixes to previous merge
2013-02-22 Tinku MannanThis commit adds the following:
2013-02-22 Tinku MannanThis commit adds the following:
2013-02-20 Tinku MannanThis commit adds the following:
2013-02-20 Tinku MannanThis commit adds the following:
2013-02-15 Tinku MannanThis commit adds the following:
2013-02-14 Tinku MannanThis commit includes the following changes:
2013-02-08 Tinku MannanNETAPI: This commit addes the following functionality:
2013-02-05 Tinku MannanAdding soure file for net_test SA utilities, adding...
2013-01-31 Tinku MannanMoved SA configuration parameters to confile file,...
2013-01-21 Tinku MannanIncorporated code review comments, source file cleanup...
2013-01-15 Tinku MannanAdding netcp_cfgExceptions API and related changes...
2013-01-10 Tinku MannanMerge remote branch 'origin/master' into netapi-keystone2
2013-01-08 Tinku Mannan Support IPSEC AH mode, additional cleanup
2012-12-28 Tinku MannanImplemented multi-core/thread protections, implemented...
2012-12-18 Tinku MannanImplemented per core net_test stats, integration with...
next