diff --git a/pasahost.h b/pasahost.h
--- a/pasahost.h
+++ b/pasahost.h
#ifdef __cplusplus
extern "C" {
#endif
-
/** @defgroup pasaho_if_module PA/SA/Host Interface
* @{
*/
*/
-
/**
* @defgroup pasahoCommands PA/SA/Host Commands
* @ingroup pasaho_if_constants
#define PASAHO_PAMOD_NROUTE 3
+
+/**
+ * @def PASAHO_PAMOD_EF_OP
+ * Instruct PDSP to perform egress flow operation
+ */
+
+#define PASAHO_PAMOD_EF_OP 5
+
/**
* @def PASAHO_PAMOD_REPORT_TIMESTAMP
* Instruct PDSP to report the system timestamp at the timestamp field of the packet descriptor
* Instruct PDSP to perform message length patching after IPv4 fragmentation operation. This command is
* valid only if it is in conjunction with the PASAHO_PAMOD_IP_FRAGMENT command.
*/
-#define PASAHO_PAMOD_PATCH_MSG_LEN PASAHO_PAMOD_GROUP_7
+#define PASAHO_PAMOD_PATCH_MSG_LEN PASAHO_PAMOD_GROUP_7
+
+/**
+ * @def PASAHO_PAMOD_EMAC_CRC_VERIFY
+ * Instruct PDSP to perform Ethernet CRC verification for egress traffic. This command is provided as a workarond
+ * for the following GbE errata at some keystone devices. (Gen1 support only)
+ *
+ * The GbE switch may drop packets in TX path when:
+ * - full gigabit speeds are sustained and
+ * - the packet size is not a 32 bit multiple (1499, 1498, 1497, 1495, etc.) and
+ * - Ethernet CRC is included in the last 4 bytes of the packet sent to the switch
+ *
+ * @note The Ethernet CRC Verify command can not be combined with any other tx commands, all other commands will be ignored
+ * by PASS when this command is processed.
+ */
+
+#define PASAHO_PAMOD_EMAC_CRC_VERIFY PASAHO_PAMOD_GROUP_7
+
+/**
+ * @def PASAHO_PAMOD_PATCH_MSG_TIME
+ * Instruct PDSP to perform message time insert for packets such as Ethernet OAM. (Gen2 support only)
+ */
+#define PASAHO_PAMOD_PATCH_MSG_TIME PASAHO_PAMOD_GROUP_7
+
+/**
+ * @def PASAHO_PAMOD_PATCH_MSG_COUNT
+ * Instruct PDSP to perform message count insert for packets such as Ethernet OAM.
+ */
+#define PASAHO_PAMOD_PATCH_MSG_COUNT PASAHO_PAMOD_GROUP_7
/* SA commands */
/**
PASAHO_HDR_ESP_DECODED, /**< Decoded Encapsulating Security Payload header */
PASAHO_HDR_AUTH, /**< Authentication header */
PASAHO_HDR_CUSTOM_C1, /**< Custom classify 1 header */
- PASAHO_HDR_FORCE_LOOKUP, /**< A contrived header type used with custom SRIO to force
- * a parse after looking at only the SRIO L0-L2 */
+ PASAHO_HDR_PPPoE, /**< PPPoE Header */
+ PASAHO_HDR_SCTP, /**< SCTP Header */
PASAHO_HDR_UNKNOWN, /**< Next header type is unknown */
PASAHO_HDR_UDP, /**< User Datagram Protocol header */
PASAHO_HDR_UDP_LITE, /**< Lightweight User Datagram Protocol header */
PASAHO_HDR_TCP, /**< Transmission Control Protocol header */
+ PASAHO_HDR_GTPU, /**< GTPU header */
+ PASAHO_HDR_ESP_DECODED_C2, /**< Decoded Encapsulating Security Payload header at Classifyer2 */
PASAHO_HDR_CUSTOM_C2 /**< Custom classify 2 header */
} pasaho_HeaderType_e;
typedef enum {
- PASAHO_SUB_CMD_DUMMY = 0, /**< Dummy */
- PASAHO_SUB_CMD_IP_FRAG, /**< IPv4 fragmentation */
- PASAHO_SUB_CMD_PATCH_MSG_LEN /**< Message length Patching */
+ PASAHO_SUB_CMD_DUMMY = 0, /**< Dummy */
+ PASAHO_SUB_CMD_IP_FRAG = 1, /**< IPv4 fragmentation */
+ PASAHO_SUB_CMD_PATCH_MSG_LEN = 2, /**< Message length Patching */
+ PASAHO_SUB_CMD_INS_TIME = 3, /**< Ethernet EOAM insert time at specified offset (Gen2 only) */
+ PASAHO_SUB_CMD_INS_COUNT = 4, /**< Ethernet EOAM insert count at specified offset (Gen2 only) */
+ PASAHO_SUB_CMD_EMAC_CRC_VERIFY = 3 /**< Ethernet CRC Verification (Gen1 only)*/
} pasaho_SubCmdCode_e;
/*@}*/
/** @} */
uint32_t word3; /**< Control block word 3 */
uint32_t word4; /**< Control block word 4 */
uint32_t word5; /**< Control block word 5 */
-
+ uint32_t word6; /**< Control block word 6 */
+ uint32_t word7; /**< Control block word 7 */
+ uint32_t word8; /**< Control block word 8 */
+ uint32_t word9; /**< Control block word 9 */
+ uint32_t word10; /**< Control block word 10 (optional) */
+ uint32_t word11; /**< Control block word 11 (optional) */
+ uint32_t word12; /**< Control block word 12 (optional) */
+ uint32_t word13; /**< Control block word 13 (optional) */
} pasahoLongInfo_t;
+/**
+ * @defgroup PASAHO_long_info_command_gen1_macros PASAHO Long Info Command Macros For First Generation PASS
+ * @ingroup pasaho_if_macros
+ * @{
+ * @name PASAHO Long Info Command Macros For First Generation PASS
+ * Macros used by the PASAHO Long Info Command
+ */
+/*@{*/
+
+#define PASAHO_LINFO_READ_CMDID_GEN1(x) PASAHO_READ_BITFIELD((x)->word0,29,3) /**< Extract the command ID defined at @ref pasahoCommands (PASS Gen1)*/
+#define PASAHO_LINFO_READ_RECLEN_GEN1(x) PASAHO_READ_BITFIELD((x)->word0,24,5) /**< Extract the block length (PASS Gen1)*/
+#define PASAHO_LINFO_READ_START_OFFSET_GEN1(x) PASAHO_READ_BITFIELD((x)->word0,0,16) /**< Extract the next parse start offset (PASS Gen1)*/
+
+#define PASAHO_LINFO_IS_MAC_BROADCAST_GEN1(x) PASAHO_READ_BITFIELD((x)->word0,16,1) /**< Indicate whether it is a broadcast MAC packet (PASS Gen1)*/
+#define PASAHO_LINFO_IS_MAC_MULTICAST_GEN1(x) PASAHO_READ_BITFIELD((x)->word0,17,1) /**< Indicate whether it is a multicast MAC packet (PASS Gen1)*/
+#define PASAHO_LINFO_READ_MAC_PKTTYPE_GEN1(x) PASAHO_READ_BITFIELD((x)->word0,16,2) /**< Extract the MAC packet type (PASS Gen1)*/
+
+#define PASAHO_LINFO_IS_IP_BROADCAST_GEN1(x) PASAHO_READ_BITFIELD((x)->word0,18,1) /**< Indicate whether it is a broadcast IP packet (PASS Gen1)*/
+#define PASAHO_LINFO_IS_IP_MULTICAST_GEN1(x) PASAHO_READ_BITFIELD((x)->word0,19,1) /**< Indicate whether it is a multicast IP packet (PASS Gen1)*/
+#define PASAHO_LINFO_READ_IP_PKTTYPE_GEN1(x) PASAHO_READ_BITFIELD((x)->word0,18,2) /**< Extract the IP packet type (PASS Gen1)*/
+
+#define PASAHO_LINFO_READ_END_OFFSET_GEN1(x) PASAHO_READ_BITFIELD((x)->word1,16,16) /**< Extract the end of packet parse offset (PASS Gen1)*/
+#define PASAHO_LINFO_READ_EIDX_GEN1(x) PASAHO_READ_BITFIELD((x)->word1,11,5) /**< Extract the error index (PASS Gen1)*/
+#define PASAHO_LINFO_READ_PMATCH_GEN1(x) PASAHO_READ_BITFIELD((x)->word1,10,1) /**< Extract the previous match flag (PASS Gen1)*/
+#define PASAHO_LINFO_READ_L1_PDSP_ID_GEN1(x) PASAHO_READ_BITFIELD((x)->word1,6,3) /**< Extract the first parse module ID (PASS Gen1)*/
+#define PASAHO_LINFO_READ_L1_IDX_GEN1(x) PASAHO_READ_BITFIELD((x)->word1,0,6) /**< Extract the first parse module match index (PASS Gen1)*/
+
+#define PASAHO_LINFO_READ_L3_OFFSET_GEN1(x) PASAHO_READ_BITFIELD((x)->word2,24,8) /**< Extract the offset to the level 3 header (PASS Gen1)*/
+#define PASAHO_LINFO_READ_L4_OFFSET_GEN1(x) PASAHO_READ_BITFIELD((x)->word2,16,8) /**< Extract the offset to the level 4 header (PASS Gen1)*/
+#define PASAHO_LINFO_READ_L5_OFFSET_GEN1(x) PASAHO_READ_BITFIELD((x)->word2,8,8) /**< Extract the offset to the level 5 header (PASS Gen1)*/
+#define PASAHO_LINFO_READ_ESP_AH_OFFSET_GEN1(x) PASAHO_READ_BITFIELD((x)->word2,0,8) /**< Extract the offset to the security header (PASS Gen1)*/
+
+#define PASAHO_LINFO_READ_HDR_BITMASK_GEN1(x) PASAHO_READ_BITFIELD((x)->word3,21,11) /**< Extract the bitmask of parsed header types (PASS Gen1)*/
+#define PASAHO_LINFO_READ_HDR_BITMASK2_GEN1(x) PASAHO_READ_BITFIELD((x)->word3, 4,4) /**< Extract the bitmask2 of parsed header types (PASS Gen1)*/
+#define PASAHO_LINFO_READ_NXT_HDR_TYPE_GEN1(x) PASAHO_READ_BITFIELD((x)->word3,16,5) /**< Extract the next header to parse type (PASS Gen1)*/
+#define PASAHO_LINFO_READ_VLAN_COUNT_GEN1(x) PASAHO_READ_BITFIELD((x)->word3,14,2) /**< Extract the number of VLAN tags found (PASS Gen1)*/
+#define PASAHO_LINFO_READ_IP_COUNT_GEN1(x) PASAHO_READ_BITFIELD((x)->word3,8,3) /**< Extract the number of IP headers found (PASS Gen1)*/
+#define PASAHO_LINFO_READ_GRE_COUNT_GEN1(x) PASAHO_READ_BITFIELD((x)->word3,11,3) /**< Extract the number of GRE headers found (PASS Gen1)*/
+#define PASAHO_LINFO_READ_FLAG_FRAG_GEN1(x) PASAHO_READ_BITFIELD((x)->word3,3,1) /**< Extract the fragmentation found flag (PASS Gen1)*/
+#define PASAHO_LINFO_READ_INPORT_GEN1(x) PASAHO_READ_BITFIELD((x)->word3,0,3) /**< Extract the (1-based) input EMAC port number
+ 0: Indicates that the packet does not enter PASS
+ through CPSW (PASS Gen1)*/
+#define PASAHO_LINFO_READ_INNER_IP_OFFSET_GEN1(x) PASAHO_READ_BITFIELD((x)->word4,16,8) /**< Extract the offset to the most inner IP header (PASS Gen1)*/
+#define PASAHO_LINFO_READ_TSTAMP_MSB_GEN1(x) (x)->word6 /**< Extract the most significant 32-bit of the 64-bit timestamp */
+#define PASAHO_LINFO_READ_TSTAMP_MSB2_GEN1(x) (x)->word8 /**< Extract the most significant 32-bit of the 64-bit timestamp
+ where the paylaod data has been copied to word6/7 within
+ pasahoLongInfo_t by using PASS command pa_CMD_COPY_DATA_TO_PSINFO */
+
+/*@}*/ /* PASAHO_long_info_command_gen1_macros */
+/** @}*/ /* @name PASAHO Long Info Command Macros For First Generation PASS */
+
+/**
+ * @defgroup PASAHO_long_info_command_gen2_macros PASAHO Long Info Command Macros For Second Generation PASS
+ * @ingroup pasaho_if_macros
+ * @{
+ * @name PASAHO Long Info Command Macros For Second Generation PASS
+ * Macros used by the PASAHO Long Info Command
+ */
+/*@{*/
+
+#define PASAHO_LINFO_READ_CMDID_GEN2(x) PASAHO_READ_BITFIELD((x)->word0,29,3) /**< Extract the command ID defined at @ref pasahoCommands (PASS Gen2)*/
+#define PASAHO_LINFO_READ_RECLEN_GEN2(x) PASAHO_READ_BITFIELD((x)->word0,24,5) /**< Extract the block length (PASS Gen2)*/
+#define PASAHO_LINFO_READ_START_OFFSET_GEN2(x) PASAHO_READ_BITFIELD((x)->word0,0,8) /**< Extract the next parse start offset (PASS Gen2)*/
+
+#define PASAHO_LINFO_IS_MAC_BROADCAST_GEN2(x) PASAHO_READ_BITFIELD((x)->word0,16,1) /**< Indicate whether it is a broadcast MAC packet (PASS Gen2)*/
+#define PASAHO_LINFO_IS_MAC_MULTICAST_GEN2(x) PASAHO_READ_BITFIELD((x)->word0,17,1) /**< Indicate whether it is a multicast MAC packet (PASS Gen2)*/
+#define PASAHO_LINFO_READ_MAC_PKTTYPE_GEN2(x) PASAHO_READ_BITFIELD((x)->word0,16,2) /**< Extract the MAC packet type (PASS Gen2)*/
+
+#define PASAHO_LINFO_IS_IP_BROADCAST_GEN2(x) PASAHO_READ_BITFIELD((x)->word0,16,1) /**< Indicate whether it is a broadcast IP packet (PASS Gen2)*/
+#define PASAHO_LINFO_IS_IP_MULTICAST_GEN2(x) PASAHO_READ_BITFIELD((x)->word0,17,1) /**< Indicate whether it is a multicast IP packet (PASS Gen2)*/
+#define PASAHO_LINFO_READ_IP_PKTTYPE_GEN2(x) PASAHO_READ_BITFIELD((x)->word0,16,2) /**< Extract the IP packet type (PASS Gen2)*/
+
+#define PASAHO_LINFO_READ_PMATCH_GEN2(x) PASAHO_READ_BITFIELD((x)->word0,23,1) /**< Extract the previous match flag (PASS Gen2)*/
+#define PASAHO_LINFO_READ_FLAG_FRAG_GEN2(x) PASAHO_READ_BITFIELD((x)->word0,19,1) /**< Extract the fragmentation found flag (PASS Gen2)*/
+
+#define PASAHO_LINFO_READ_END_OFFSET_GEN2(x) PASAHO_READ_BITFIELD((x)->word1,16,16) /**< Extract the end of packet parse offset (PASS Gen2)*/
+#define PASAHO_LINFO_READ_EIDX_GEN2(x) PASAHO_READ_BITFIELD((x)->word1,10,6) /**< Extract the exception index (PASS Gen2)*/
+#define PASAHO_LINFO_READ_NXT_HDR_TYPE_GEN2(x) PASAHO_READ_BITFIELD((x)->word1,0,6) /**< Extract the next header to parse type (PASS Gen2)*/
+#define PASAHO_LINFO_READ_INPORT_GEN2(x) PASAHO_READ_BITFIELD((x)->word1,6,4) /**< Extract the (1-based) input EMAC port number
+ through CPSW (PASS Gen2)*/
+
+#define PASAHO_LINFO_READ_L3_OFFSET_GEN2(x) PASAHO_READ_BITFIELD((x)->word2,24,8) /**< Extract the offset to the level 3 header (PASS Gen2)*/
+#define PASAHO_LINFO_READ_L4_OFFSET_GEN2(x) PASAHO_READ_BITFIELD((x)->word2,16,8) /**< Extract the offset to the level 4 header (PASS Gen2)*/
+#define PASAHO_LINFO_READ_L5_OFFSET_GEN2(x) PASAHO_READ_BITFIELD((x)->word2,8,8) /**< Extract the offset to the level 5 header (PASS Gen2)*/
+#define PASAHO_LINFO_READ_ESP_AH_OFFSET_GEN2(x) PASAHO_READ_BITFIELD((x)->word2,0,8) /**< Extract the offset to the security header (PASS Gen2)*/
+
+#define PASAHO_LINFO_READ_L1_PDSP_ID_GEN2(x) PASAHO_READ_BITFIELD((x)->word3,26,6) /**< Extract the first parse module ID (PASS Gen2)*/
+#define PASAHO_LINFO_READ_L1_IDX_GEN2(x) PASAHO_READ_BITFIELD((x)->word3,16,10) /**< Extract the first parse module match index (PASS Gen2)*/
+#define PASAHO_LINFO_READ_HDR_BITMASK_GEN2(x) PASAHO_READ_BITFIELD((x)->word3,0,16) /**< Extract the bitmask of parsed header types (PASS Gen2)*/
+#define PASAHO_LINFO_READ_HDR_BITMASK2_GEN2(x) 0 /**< Extract the bitmask2 of parsed header types (PASS Gen2)*/
+#define PASAHO_LINFO_READ_VLAN_COUNT_GEN2(x) PASAHO_READ_BITFIELD((x)->word4,6,2) /**< Extract the number of VLAN tags found (PASS Gen2)*/
+#define PASAHO_LINFO_READ_IP_COUNT_GEN2(x) PASAHO_READ_BITFIELD((x)->word4,0,3) /**< Extract the number of IP headers found (PASS Gen2)*/
+#define PASAHO_LINFO_READ_GRE_COUNT_GEN2(x) PASAHO_READ_BITFIELD((x)->word4,3,3) /**< Extract the number of GRE headers found (PASS Gen2)*/
+
+#define PASAHO_LINFO_READ_INNER_IP_OFFSET_GEN2(x) PASAHO_READ_BITFIELD((x)->word5,24,8) /**< Extract the offset to the inner IP header (PASS Gen2)*/
+#define PASAHO_LINFO_READ_TSTAMP_MSB_GEN2(x) (x)->word6 /**< Extract the most significant 32-bit of the 64-bit timestamp */
+#define PASAHO_LINFO_READ_TSTAMP_MSB2_GEN2(x) (x)->word8 /**< Extract the most significant 32-bit of the 64-bit timestamp
+ where the paylaod data has been copied to word6/7 within
+ pasahoLongInfo_t by using PASS command pa_CMD_COPY_DATA_TO_PSINFO */
+#define PASAHO_LINFO_READ_PATSTAMP_LSW_GEN2(x) (x)->word9 /**< Extract the most significant 32-bit of the 64-bit PA timestamp */
+#define PASAHO_LINFO_READ_PATSTAMP_MSW_GEN2(x) (x)->word8 /**< Extract the least significant 32-bit of the 64-bit PA timestamp */
+
+#define PASAHO_LINFO_READ_PATSTAMP_LSW2_GEN2(x) (x)->word11 /**< Extract the most significant 32-bit of the 64-bit PA timestamp
+ where the paylaod data has been copied to word6/7 within
+ pasahoLongInfo_t by using PASS command pa_CMD_COPY_DATA_TO_PSINFO */
+#define PASAHO_LINFO_READ_PATSTAMP_MSW2_GEN2(x) (x)->word10 /**< Extract the most significant 32-bit of the 64-bit PA timestamp
+ where the paylaod data has been copied to word6/7 within
+ pasahoLongInfo_t by using PASS command pa_CMD_COPY_DATA_TO_PSINFO */
+
+#define PASAHO_LINFO_READ_EOAM_TF_MATCH_CNT_GEN2(x) (x)->word5 /**< Extract the Ethernet OAM target flow match count, valid during
+ EOAM mode on LMM/LMR control packts only (PASS Gen2)*/
+#define PASAHO_LINFO_READ_EOAM_PKT_MEG_LEVEL_GEN2(x) PASAHO_READ_BITFIELD((x)->word2,24,8) /**< Extract the MEG Level during a valid EOAM packet measurement, valid during
+ EOAM mode only (PASS Gen2)*/
+#define PASAHO_LINFO_READ_EOAM_PKT_OPCODE_GEN2(x) PASAHO_READ_BITFIELD((x)->word2,16,8) /**< Extract the MEG Level during a valid EOAM packet measurement, valid during
+ EOAM mode only (PASS Gen2)*/
+
+
+/*@}*/ /* PASAHO_long_info_command_gen2 macros */
+/** @}*/ /* @name PASAHO Long Info Command Macros For Second Generation PASS */
+
/**
* @defgroup PASAHO_long_info_command_macros PASAHO Long Info Command Macros
* @ingroup pasaho_if_macros
*/
/*@{*/
-#define PASAHO_LINFO_READ_CMDID(x) PASAHO_READ_BITFIELD((x)->word0,29,3) /**< Extract the command ID defined at @ref pasahoCommands */
-#define PASAHO_LINFO_READ_RECLEN(x) PASAHO_READ_BITFIELD((x)->word0,24,5) /**< Extract the block length */
-#define PASAHO_LINFO_READ_START_OFFSET(x) PASAHO_READ_BITFIELD((x)->word0,0,16) /**< Extract the next parse start offset */
-
-#define PASAHO_LINFO_IS_MAC_BROADCAST(x) PASAHO_READ_BITFIELD((x)->word0,16,1) /**< Indicate whether it is a broadcast MAC packet */
-#define PASAHO_LINFO_IS_MAC_MULTICAST(x) PASAHO_READ_BITFIELD((x)->word0,17,1) /**< Indicate whether it is a multicast MAC packet */
-#define PASAHO_LINFO_READ_MAC_PKTTYPE(x) PASAHO_READ_BITFIELD((x)->word0,16,2) /**< Extract the MAC packet type */
-
-#define PASAHO_LINFO_IS_IP_BROADCAST(x) PASAHO_READ_BITFIELD((x)->word0,18,1) /**< Indicate whether it is a broadcast IP packet */
-#define PASAHO_LINFO_IS_IP_MULTICAST(x) PASAHO_READ_BITFIELD((x)->word0,19,1) /**< Indicate whether it is a multicast IP packet */
-#define PASAHO_LINFO_READ_IP_PKTTYPE(x) PASAHO_READ_BITFIELD((x)->word0,18,2) /**< Extract the IP packet type */
-
-#define PASAHO_LINFO_READ_END_OFFSET(x) PASAHO_READ_BITFIELD((x)->word1,16,16) /**< Extract the end of packet parse offset */
-#define PASAHO_LINFO_READ_EIDX(x) PASAHO_READ_BITFIELD((x)->word1,11,5) /**< Extract the error index */
-#define PASAHO_LINFO_READ_PMATCH(x) PASAHO_READ_BITFIELD((x)->word1,10,1) /**< Extract the previous match flag */
-#define PASAHO_LINFO_READ_L1_PDSP_ID(x) PASAHO_READ_BITFIELD((x)->word1,6,3) /**< Extract the first parse module ID */
-#define PASAHO_LINFO_READ_L1_IDX(x) PASAHO_READ_BITFIELD((x)->word1,0,6) /**< Extract the first parse module match index */
-
-#define PASAHO_LINFO_READ_L3_OFFSET(x) PASAHO_READ_BITFIELD((x)->word2,24,8) /**< Extract the offset to the level 3 header */
-#define PASAHO_LINFO_READ_L4_OFFSET(x) PASAHO_READ_BITFIELD((x)->word2,16,8) /**< Extract the offset to the level 4 header */
-#define PASAHO_LINFO_READ_L5_OFFSET(x) PASAHO_READ_BITFIELD((x)->word2,8,8) /**< Extract the offset to the level 5 header */
-#define PASAHO_LINFO_READ_ESP_AH_OFFSET(x) PASAHO_READ_BITFIELD((x)->word2,0,8) /**< Extract the offset to the security header */
-
-#define PASAHO_LINFO_READ_HDR_BITMASK(x) PASAHO_READ_BITFIELD((x)->word3,21,11) /**< Extract the bitmask of parsed header types */
-#define PASAHO_LINFO_READ_HDR_BITMASK2(x) PASAHO_READ_BITFIELD((x)->word3, 4,4) /**< Extract the bitmask2 of parsed header types */
-#define PASAHO_LINFO_READ_NXT_HDR_TYPE(x) PASAHO_READ_BITFIELD((x)->word3,16,5) /**< Extract the next header to parse type */
-#define PASAHO_LINFO_READ_VLAN_COUNT(x) PASAHO_READ_BITFIELD((x)->word3,14,2) /**< Extract the number of VLAN tags found */
-#define PASAHO_LINFO_READ_IP_COUNT(x) PASAHO_READ_BITFIELD((x)->word3,8,3) /**< Extract the number of IP headers found */
-#define PASAHO_LINFO_READ_GRE_COUNT(x) PASAHO_READ_BITFIELD((x)->word3,11,3) /**< Extract the number of GRE headers found */
-#define PASAHO_LINFO_READ_FLAG_FRAG(x) PASAHO_READ_BITFIELD((x)->word3,3,1) /**< Extract the fragmentation found flag */
-#define PASAHO_LINFO_READ_INPORT(x) PASAHO_READ_BITFIELD((x)->word3,0,3) /**< Extract the (1-based) input EMAC port number
- 0: Indicates that the packet does not enter PASS
- through CPSW */
-#define PASAHO_LINFO_READ_PSEUDO_CHKSM(x) PASAHO_READ_BITFIELD((x)->word4,16,16) /**< Extract the last pseudo-header checksum computed */
-#define PASAHO_LINFO_READ_TSTAMP_MSB(x) PASAHO_READ_BITFIELD((x)->word5,0,16) /**< Extract the most significant 16-bit of the 48-bit timestamp */
+#ifdef NSS_GEN2
+#define PASAHO_LINFO_READ_CMDID(x) PASAHO_LINFO_READ_CMDID_GEN2(x) /**< Extract the command ID defined at @ref pasahoCommands */
+#define PASAHO_LINFO_READ_RECLEN(x) PASAHO_LINFO_READ_RECLEN_GEN2(x) /**< Extract the block length */
+#define PASAHO_LINFO_READ_START_OFFSET(x) PASAHO_LINFO_READ_START_OFFSET_GEN2(x) /**< Extract the next parse start offset */
+
+#define PASAHO_LINFO_IS_MAC_BROADCAST(x) PASAHO_LINFO_IS_MAC_BROADCAST_GEN2(x) /**< Indicate whether it is a broadcast MAC packet */
+#define PASAHO_LINFO_IS_MAC_MULTICAST(x) PASAHO_LINFO_IS_MAC_MULTICAST_GEN2(x) /**< Indicate whether it is a multicast MAC packet */
+#define PASAHO_LINFO_READ_MAC_PKTTYPE(x) PASAHO_LINFO_READ_MAC_PKTTYPE_GEN2(x) /**< Extract the MAC packet type */
+
+#define PASAHO_LINFO_IS_IP_BROADCAST(x) PASAHO_LINFO_IS_IP_BROADCAST_GEN2(x) /**< Indicate whether it is a broadcast IP packet */
+#define PASAHO_LINFO_IS_IP_MULTICAST(x) PASAHO_LINFO_IS_IP_MULTICAST_GEN2(x) /**< Indicate whether it is a multicast IP packet */
+#define PASAHO_LINFO_READ_IP_PKTTYPE(x) PASAHO_LINFO_READ_IP_PKTTYPE_GEN2(x) /**< Extract the IP packet type */
+
+#define PASAHO_LINFO_READ_PMATCH(x) PASAHO_LINFO_READ_PMATCH_GEN2(x) /**< Extract the previous match flag */
+#define PASAHO_LINFO_READ_FLAG_FRAG(x) PASAHO_LINFO_READ_FLAG_FRAG_GEN2(x) /**< Extract the fragmentation found flag */
+
+#define PASAHO_LINFO_READ_END_OFFSET(x) PASAHO_LINFO_READ_END_OFFSET_GEN2(x) /**< Extract the end of packet parse offset */
+#define PASAHO_LINFO_READ_EIDX(x) PASAHO_LINFO_READ_EIDX_GEN2(x) /**< Extract the exception index */
+#define PASAHO_LINFO_READ_NXT_HDR_TYPE(x) PASAHO_LINFO_READ_NXT_HDR_TYPE_GEN2(x) /**< Extract the next header to parse type */
+#define PASAHO_LINFO_READ_INPORT(x) PASAHO_LINFO_READ_INPORT_GEN2(x) /**< Extract the (1-based) input EMAC port number
+ through CPSW */
+
+#define PASAHO_LINFO_READ_L3_OFFSET(x) PASAHO_LINFO_READ_L3_OFFSET_GEN2(x) /**< Extract the offset to the level 3 header */
+#define PASAHO_LINFO_READ_L4_OFFSET(x) PASAHO_LINFO_READ_L4_OFFSET_GEN2(x) /**< Extract the offset to the level 4 header */
+#define PASAHO_LINFO_READ_L5_OFFSET(x) PASAHO_LINFO_READ_L5_OFFSET_GEN2(x) /**< Extract the offset to the level 5 header */
+#define PASAHO_LINFO_READ_ESP_AH_OFFSET(x) PASAHO_LINFO_READ_ESP_AH_OFFSET_GEN2(x) /**< Extract the offset to the security header */
+
+#define PASAHO_LINFO_READ_L1_PDSP_ID(x) PASAHO_LINFO_READ_L1_PDSP_ID_GEN2(x) /**< Extract the first parse module ID */
+#define PASAHO_LINFO_READ_L1_IDX(x) PASAHO_LINFO_READ_L1_IDX_GEN2(x) /**< Extract the first parse module match index */
+#define PASAHO_LINFO_READ_HDR_BITMASK(x) PASAHO_LINFO_READ_HDR_BITMASK_GEN2(x) /**< Extract the bitmask of parsed header types */
+#define PASAHO_LINFO_READ_HDR_BITMASK2(x) PASAHO_LINFO_READ_HDR_BITMASK2_GEN2(x) /**< Extract the bitmask2 of parsed header types */
+#define PASAHO_LINFO_READ_VLAN_COUNT(x) PASAHO_LINFO_READ_VLAN_COUNT_GEN2(x) /**< Extract the number of VLAN tags found */
+#define PASAHO_LINFO_READ_IP_COUNT(x) PASAHO_LINFO_READ_IP_COUNT_GEN2(x) /**< Extract the number of IP headers found */
+#define PASAHO_LINFO_READ_GRE_COUNT(x) PASAHO_LINFO_READ_GRE_COUNT_GEN2(x) /**< Extract the number of GRE headers found */
+
+#define PASAHO_LINFO_READ_INNER_IP_OFFSET(x)PASAHO_LINFO_READ_INNER_IP_OFFSET_GEN2(x) /**< Extract the offset to the inner IP header */
+#define PASAHO_LINFO_READ_TSTAMP_MSB(x) PASAHO_LINFO_READ_TSTAMP_MSB_GEN2(x) /**< Extract the most significant 32-bit of the 64-bit timestamp */
+#define PASAHO_LINFO_READ_TSTAMP_MSB2(x) PASAHO_LINFO_READ_TSTAMP_MSB2_GEN2(x) /**< Extract the most significant 32-bit of the 64-bit timestamp
+ where the paylaod data has been copied to word6/7 within
+ pasahoLongInfo_t by using PASS command pa_CMD_COPY_DATA_TO_PSINFO */
+#define PASAHO_LINFO_READ_EOAM_TF_MATCH_CNT(x) PASAHO_LINFO_READ_EOAM_TF_MATCH_CNT_GEN2(x) /**< Extract the EOAM target flow match count for LMM/LMR packets */
+#define PASAHO_LINFO_READ_EOAM_PKT_MEG_LEVEL(x) PASAHO_LINFO_READ_EOAM_PKT_MEG_LEVEL_GEN2(x) /**< Extract the EOAM MEG level for that packet */
+#define PASAHO_LINFO_READ_EOAM_PKT_OPCODE(x) PASAHO_LINFO_READ_EOAM_PKT_OPCODE_GEN2(x) /**< Extract the EOAM Opcode for that packet */
+
+#else
+#define PASAHO_LINFO_READ_CMDID(x) PASAHO_LINFO_READ_CMDID_GEN1(x) /**< Extract the command ID defined at @ref pasahoCommands */
+#define PASAHO_LINFO_READ_RECLEN(x) PASAHO_LINFO_READ_RECLEN_GEN1(x) /**< Extract the block length */
+#define PASAHO_LINFO_READ_START_OFFSET(x) PASAHO_LINFO_READ_START_OFFSET_GEN1(x) /**< Extract the next parse start offset */
+
+#define PASAHO_LINFO_IS_MAC_BROADCAST(x) PASAHO_LINFO_IS_MAC_BROADCAST_GEN1(x) /**< Indicate whether it is a broadcast MAC packet */
+#define PASAHO_LINFO_IS_MAC_MULTICAST(x) PASAHO_LINFO_IS_MAC_MULTICAST_GEN1(x) /**< Indicate whether it is a multicast MAC packet */
+#define PASAHO_LINFO_READ_MAC_PKTTYPE(x) PASAHO_LINFO_READ_MAC_PKTTYPE_GEN1(x) /**< Extract the MAC packet type */
+
+#define PASAHO_LINFO_IS_IP_BROADCAST(x) PASAHO_LINFO_IS_IP_BROADCAST_GEN1(x) /**< Indicate whether it is a broadcast IP packet */
+#define PASAHO_LINFO_IS_IP_MULTICAST(x) PASAHO_LINFO_IS_IP_MULTICAST_GEN1(x) /**< Indicate whether it is a multicast IP packet */
+#define PASAHO_LINFO_READ_IP_PKTTYPE(x) PASAHO_LINFO_READ_IP_PKTTYPE_GEN1(x) /**< Extract the IP packet type */
+
+#define PASAHO_LINFO_READ_END_OFFSET(x) PASAHO_LINFO_READ_END_OFFSET_GEN1(x) /**< Extract the end of packet parse offset */
+#define PASAHO_LINFO_READ_EIDX(x) PASAHO_LINFO_READ_EIDX_GEN1(x) /**< Extract the error index */
+#define PASAHO_LINFO_READ_PMATCH(x) PASAHO_LINFO_READ_PMATCH_GEN1(x) /**< Extract the previous match flag */
+#define PASAHO_LINFO_READ_L1_PDSP_ID(x) PASAHO_LINFO_READ_L1_PDSP_ID_GEN1(x) /**< Extract the first parse module ID */
+#define PASAHO_LINFO_READ_L1_IDX(x) PASAHO_LINFO_READ_L1_IDX_GEN1(x) /**< Extract the first parse module match index */
+
+#define PASAHO_LINFO_READ_L3_OFFSET(x) PASAHO_LINFO_READ_L3_OFFSET_GEN1(x) /**< Extract the offset to the level 3 header */
+#define PASAHO_LINFO_READ_L4_OFFSET(x) PASAHO_LINFO_READ_L4_OFFSET_GEN1(x) /**< Extract the offset to the level 4 header */
+#define PASAHO_LINFO_READ_L5_OFFSET(x) PASAHO_LINFO_READ_L5_OFFSET_GEN1(x) /**< Extract the offset to the level 5 header */
+#define PASAHO_LINFO_READ_ESP_AH_OFFSET(x) PASAHO_LINFO_READ_ESP_AH_OFFSET_GEN1(x) /**< Extract the offset to the security header */
+
+#define PASAHO_LINFO_READ_HDR_BITMASK(x) PASAHO_LINFO_READ_HDR_BITMASK_GEN1(x) /**< Extract the bitmask of parsed header types */
+#define PASAHO_LINFO_READ_HDR_BITMASK2(x) PASAHO_LINFO_READ_HDR_BITMASK2_GEN1(x) /**< Extract the bitmask2 of parsed header types */
+#define PASAHO_LINFO_READ_NXT_HDR_TYPE(x) PASAHO_LINFO_READ_NXT_HDR_TYPE_GEN1(x) /**< Extract the next header to parse type */
+#define PASAHO_LINFO_READ_VLAN_COUNT(x) PASAHO_LINFO_READ_VLAN_COUNT_GEN1(x) /**< Extract the number of VLAN tags found */
+#define PASAHO_LINFO_READ_IP_COUNT(x) PASAHO_LINFO_READ_IP_COUNT_GEN1(x) /**< Extract the number of IP headers found */
+#define PASAHO_LINFO_READ_GRE_COUNT(x) PASAHO_LINFO_READ_GRE_COUNT_GEN1(x) /**< Extract the number of GRE headers found */
+#define PASAHO_LINFO_READ_FLAG_FRAG(x) PASAHO_LINFO_READ_FLAG_FRAG_GEN1(x) /**< Extract the fragmentation found flag */
+#define PASAHO_LINFO_READ_INPORT(x) PASAHO_LINFO_READ_INPORT_GEN1(x) /**< Extract the (1-based) input EMAC port number
+ 0: Indicates that the packet does not enter PASS
+ through CPSW */
+#define PASAHO_LINFO_READ_INNER_IP_OFFSET(x)PASAHO_LINFO_READ_INNER_IP_OFFSET_GEN1(x) /**< Extract the offset to the inner IP header */
+#define PASAHO_LINFO_READ_TSTAMP_MSB(x) PASAHO_LINFO_READ_TSTAMP_MSB_GEN1(x) /**< Extract the most significant 32-bit of the 64-bit timestamp */
+#define PASAHO_LINFO_READ_TSTAMP_MSB2(x) PASAHO_LINFO_READ_TSTAMP_MSB2_GEN1(x) /**< Extract the most significant 32-bit of the 64-bit timestamp
+ where the paylaod data has been copied to word6/7 within
+ pasahoLongInfo_t by using PASS command pa_CMD_COPY_DATA_TO_PSINFO */
+#endif
+
/* Extract Protocol Information */
/*@}*/ /* PASAHO_long_info_command_macros */
/** @}*/ /* @name PASAHO Long Info Command Macros */
+/**
+ * @defgroup PASAHO_long_info_proto_ind_gen1_macros PASAHO Long Info Protocol Indication Macros For First Generation PASS
+ * @ingroup pasaho_if_macros
+ * @{
+ * @name PASAHO Long Info Protocol Indication Macros For First Generation PASS
+ */
+#define PASAHO_LINFO_IS_MAC_GEN1(x) PASAHO_READ_BITFIELD((x)->word3,21,1) /**< Indicate whether it is a MAC packet (Pass Gen1)*/
+#define PASAHO_LINFO_IS_802_3_GEN1(x) PASAHO_READ_BITFIELD((x)->word3,7,1) /**< Indicate whether it is a 802.3 packet (Pass Gen1)*/
+#define PASAHO_LINFO_IS_WITH_VLAN_GEN1(x) PASAHO_LINFO_READ_VLAN_COUNT(x) /**< Indicate whether it is a MAC packet with VLAN (Pass Gen1)*/
+#define PASAHO_LINFO_IS_WITH_MPLS_GEN1(x) PASAHO_READ_BITFIELD((x)->word3,23,1) /**< Indicate whether it is a MAC packet with MPLS (Pass Gen1)*/
+#define PASAHO_LINFO_IS_PPPoE_GEN1(x) PASAHO_READ_BITFIELD((x)->word3,6,1) /**< Indicate whether it is a PPPoE packet (Pass Gen1)*/
+#define PASAHO_LINFO_IS_IP_GEN1(x) PASAHO_LINFO_READ_IP_COUNT(x) /**< Indicate whether it is an IP packet (Pass Gen1)*/
+#define PASAHO_LINFO_IS_IPSEC_ESP_GEN1(x) PASAHO_READ_BITFIELD((x)->word3,25,1) /**< Indicate whether it is an IPSEC ESP packet (Pass Gen1)*/
+#define PASAHO_LINFO_IS_IPSEC_AH_GEN1(x) PASAHO_READ_BITFIELD((x)->word3,26,1) /**< Indicate whether it is an IPSEC AH packet (Pass Gen1)*/
+#define PASAHO_LINFO_IS_UDP_GEN1(x) PASAHO_READ_BITFIELD((x)->word3,27,1) /**< Indicate whether it is an UDP packet (Pass Gen1)*/
+#define PASAHO_LINFO_IS_UDP_LITE_GEN1(x) PASAHO_READ_BITFIELD((x)->word3,28,1) /**< Indicate whether it is an UDP Lite packet (Pass Gen1)*/
+#define PASAHO_LINFO_IS_TCP_GEN1(x) PASAHO_READ_BITFIELD((x)->word3,29,1) /**< Indicate whether it is a TCP packet (Pass Gen1)*/
+#define PASAHO_LINFO_IS_GRE_GEN1(x) PASAHO_LINFO_READ_GRE_COUNT(x) /**< Indicate whether it is a GRE packet (Pass Gen1)*/
+#define PASAHO_LINFO_IS_GTPU_GEN1(x) PASAHO_READ_BITFIELD((x)->word3,30,1) /**< Indicate whether it is a GTPU packet (Pass Gen1)*/
+#define PASAHO_LINFO_IS_CUSTOM_GEN1(x) PASAHO_READ_BITFIELD((x)->word3,31,1) /**< Indicate whether it is a Custom packet (Pass Gen1)*/
+#define PASAHO_LINFO_IS_SCTP_GEN1(x) PASAHO_READ_BITFIELD((x)->word3,4,1) /**< Indicate whether it is a SCTP packet (Pass Gen1)*/
+#define PASAHO_LINFO_IS_IPSEC_NAT_T_GEN1(x) PASAHO_READ_BITFIELD((x)->word3,5,1) /**< Indicate whether it is an IPSEC NAT-T packet (Pass Gen1)*/
+
+/*@}*/ /* PASAHO_long_info_proto_ind_gen1_macross */
+/** @}*/ /* @name PASAHO Long Info Protocol Indication Macross For First Generation PASS */
+
+/**
+ * @defgroup PASAHO_long_info_proto_ind_gen2_macros PASAHO Long Info Protocol Indication Macros For Second Generation PASS
+ * @ingroup pasaho_if_macros
+ * @{
+ * @name PASAHO Long Info Protocol Indication Macros For Second Generation PASS
+ */
+#define PASAHO_LINFO_IS_MAC_GEN2(x) PASAHO_READ_BITFIELD((x)->word3,0,1) /**< Indicate whether it is a MAC packet (Pass Gen2)*/
+#define PASAHO_LINFO_IS_WITH_VLAN_GEN2(x) PASAHO_LINFO_READ_VLAN_COUNT(x) /**< Indicate whether it is a MAC packet with VLAN (Pass Gen2)*/
+#define PASAHO_LINFO_IS_WITH_MPLS_GEN2(x) PASAHO_READ_BITFIELD((x)->word3,2,1) /**< Indicate whether it is a MAC packet with MPLS (Pass Gen2)*/
+#define PASAHO_LINFO_IS_802_3_GEN2(x) PASAHO_READ_BITFIELD((x)->word3,3,1) /**< Indicate whether it is a 802.3 packet (Pass Gen2)*/
+#define PASAHO_LINFO_IS_PPPoE_GEN2(x) PASAHO_READ_BITFIELD((x)->word3,4,1) /**< Indicate whether it is a PPPoE packet (Pass Gen2)*/
+#define PASAHO_LINFO_IS_IP_GEN2(x) PASAHO_LINFO_READ_IP_COUNT(x) /**< Indicate whether it is an IP packet (Pass Gen2)*/
+#define PASAHO_LINFO_IS_IPv4_GEN2(x) PASAHO_READ_BITFIELD((x)->word3,5,1) /**< Indicate whether it is an IPv4 packet (Pass Gen2)*/
+#define PASAHO_LINFO_IS_IPv6_GEN2(x) PASAHO_READ_BITFIELD((x)->word3,6,1) /**< Indicate whether it is an IPv4 packet (Pass Gen2)*/
+#define PASAHO_LINFO_IS_IP_OPTIONS_GEN2(x) PASAHO_READ_BITFIELD((x)->word3,7,1) /**< Indicate whether there are IPV4 options or IPv6 extention headers (Pass Gen2)*/
+#define PASAHO_LINFO_IS_IPSEC_ESP_GEN2(x) PASAHO_READ_BITFIELD((x)->word3,8,1) /**< Indicate whether it is an IPSEC ESP packet (Pass Gen2)*/
+#define PASAHO_LINFO_IS_IPSEC_AH_GEN2(x) PASAHO_READ_BITFIELD((x)->word3,9,1) /**< Indicate whether it is an IPSEC AH packet (Pass Gen2)*/
+#define PASAHO_LINFO_IS_SCTP_GEN2(x) PASAHO_READ_BITFIELD((x)->word3,10,1) /**< Indicate whether it is a SCTP packet (Pass Gen2)*/
+#define PASAHO_LINFO_IS_UDP_GEN2(x) PASAHO_READ_BITFIELD((x)->word3,11,1) /**< Indicate whether it is an UDP packet (Pass Gen2)*/
+#define PASAHO_LINFO_IS_UDP_LITE_GEN2(x) PASAHO_READ_BITFIELD((x)->word3,11,1) /**< Indicate whether it is an UDP Lite packet (Pass Gen2)*/
+#define PASAHO_LINFO_IS_TCP_GEN2(x) PASAHO_READ_BITFIELD((x)->word3,12,1) /**< Indicate whether it is a TCP packet (Pass Gen2)*/
+#define PASAHO_LINFO_IS_GRE_GEN2(x) PASAHO_LINFO_READ_GRE_COUNT(x) /**< Indicate whether it is a GRE packet (Pass Gen2)*/
+#define PASAHO_LINFO_IS_GTPU_GEN2(x) PASAHO_READ_BITFIELD((x)->word3,13,1) /**< Indicate whether it is a GTPU packet (Pass Gen2)*/
+#define PASAHO_LINFO_IS_CUSTOM_GEN2(x) PASAHO_READ_BITFIELD((x)->word3,14,1) /**< Indicate whether it is a Custom packet (Pass Gen2)*/
+#define PASAHO_LINFO_IS_IPSEC_NAT_T_GEN2(x) PASAHO_READ_BITFIELD((x)->word3,15,1) /**< Indicate whether it is an IPSEC NAT-T packet (Pass Gen2)*/
+
+/*@}*/ /* PASAHO_long_info_proto_ind_macross */
+/** @}*/ /* @name PASAHO Long Info Protocol Indication Macross For Second Generation PASS */
+
/**
* @defgroup PASAHO_long_info_proto_ind_macros PASAHO Long Info Protocol Indication Macros
* @ingroup pasaho_if_macros
* @{
* @name PASAHO Long Info Protocol Indication Macros
*/
-
-#define PASAHO_LINFO_IS_MAC(x) PASAHO_READ_BITFIELD((x)->word3,21,1) /**< Indicate whether it is a MAC packet */
-#define PASAHO_LINFO_IS_802_3(x) PASAHO_READ_BITFIELD((x)->word3,7,1) /**< Indicate whether it is a 802.3 packet */
-#define PASAHO_LINFO_IS_WITH_VLAN(x) PASAHO_LINFO_READ_VLAN_COUNT(x) /**< Indicate whether it is a MAC packet with VLAN */
-#define PASAHO_LINFO_IS_WITH_MPLS(x) PASAHO_READ_BITFIELD((x)->word3,23,1) /**< Indicate whether it is a MAC packet with MPLS */
-#define PASAHO_LINFO_IS_PPPoE(x) PASAHO_READ_BITFIELD((x)->word3,6,1) /**< Indicate whether it is a PPPoE packet */
-#define PASAHO_LINFO_IS_IP(x) PASAHO_LINFO_READ_IP_COUNT(x) /**< Indicate whether it is an IP packet */
-#define PASAHO_LINFO_IS_IPSEC_ESP(x) PASAHO_READ_BITFIELD((x)->word3,25,1) /**< Indicate whether it is an IPSEC ESP packet */
-#define PASAHO_LINFO_IS_IPSEC_AH(x) PASAHO_READ_BITFIELD((x)->word3,26,1) /**< Indicate whether it is an IPSEC AH packet */
-#define PASAHO_LINFO_IS_UDP(x) PASAHO_READ_BITFIELD((x)->word3,27,1) /**< Indicate whether it is an UDP packet */
-#define PASAHO_LINFO_IS_UDP_LITE(x) PASAHO_READ_BITFIELD((x)->word3,28,1) /**< Indicate whether it is an UDP Lite packet */
-#define PASAHO_LINFO_IS_TCP(x) PASAHO_READ_BITFIELD((x)->word3,29,1) /**< Indicate whether it is a TCP packet */
-#define PASAHO_LINFO_IS_GRE(x) PASAHO_LINFO_READ_GRE_COUNT(x) /**< Indicate whether it is a GRE packet */
-#define PASAHO_LINFO_IS_GTPU(x) PASAHO_READ_BITFIELD((x)->word3,30,1) /**< Indicate whether it is a GTPU packet */
-#define PASAHO_LINFO_IS_CUSTOM(x) PASAHO_READ_BITFIELD((x)->word3,31,1) /**< Indicate whether it is a Custom packet */
-#define PASAHO_LINFO_IS_SCTP(x) PASAHO_READ_BITFIELD((x)->word3,4,1) /**< Indicate whether it is a SCTP packet */
-#define PASAHO_LINFO_IS_IPSEC_NAT_T(x) PASAHO_READ_BITFIELD((x)->word3,5,1) /**< Indicate whether it is an IPSEC NAT-T packet */
+#ifdef NSS_GEN2
+#define PASAHO_LINFO_IS_MAC(x) PASAHO_LINFO_IS_MAC_GEN2(x) /**< Indicate whether it is a MAC packet */
+#define PASAHO_LINFO_IS_WITH_VLAN(x) PASAHO_LINFO_IS_WITH_VLAN_GEN2(x) /**< Indicate whether it is a MAC packet with VLAN */
+#define PASAHO_LINFO_IS_WITH_MPLS(x) PASAHO_LINFO_IS_WITH_MPLS_GEN2(x) /**< Indicate whether it is a MAC packet with MPLS */
+#define PASAHO_LINFO_IS_802_3(x) PASAHO_LINFO_IS_802_3_GEN2(x) /**< Indicate whether it is a 802.3 packet */
+#define PASAHO_LINFO_IS_PPPoE(x) PASAHO_LINFO_IS_PPPoE_GEN2(x) /**< Indicate whether it is a PPPoE packet */
+#define PASAHO_LINFO_IS_IP(x) PASAHO_LINFO_IS_IP_GEN2(x) /**< Indicate whether it is an IP packet */
+#define PASAHO_LINFO_IS_IPv4(x) PASAHO_LINFO_IS_IPv4_GEN2(x) /**< Indicate whether it is an IPv4 packet */
+#define PASAHO_LINFO_IS_IPv6(x) PASAHO_LINFO_IS_IPv6_GEN2(x) /**< Indicate whether it is an IPv4 packet */
+#define PASAHO_LINFO_IS_IP_OPTIONS(x) PASAHO_LINFO_IS_IP_OPTIONS_GEN2(x) /**< Indicate whether there are IPV4 options or IPv6 extention headers */
+#define PASAHO_LINFO_IS_IPSEC_ESP(x) PASAHO_LINFO_IS_IPSEC_ESP_GEN2(x) /**< Indicate whether it is an IPSEC ESP packet */
+#define PASAHO_LINFO_IS_IPSEC_AH(x) PASAHO_LINFO_IS_IPSEC_AH_GEN2(x) /**< Indicate whether it is an IPSEC AH packet */
+#define PASAHO_LINFO_IS_SCTP(x) PASAHO_LINFO_IS_SCTP_GEN2(x) /**< Indicate whether it is a SCTP packet */
+#define PASAHO_LINFO_IS_UDP(x) PASAHO_LINFO_IS_UDP_GEN2(x) /**< Indicate whether it is an UDP packet */
+#define PASAHO_LINFO_IS_UDP_LITE(x) PASAHO_LINFO_IS_UDP_LITE_GEN2(x) /**< Indicate whether it is an UDP Lite packet */
+#define PASAHO_LINFO_IS_TCP(x) PASAHO_LINFO_IS_TCP_GEN2(x) /**< Indicate whether it is a TCP packet */
+#define PASAHO_LINFO_IS_GRE(x) PASAHO_LINFO_IS_GRE_GEN2(x) /**< Indicate whether it is a GRE packet */
+#define PASAHO_LINFO_IS_GTPU(x) PASAHO_LINFO_IS_GTPU_GEN2(x) /**< Indicate whether it is a GTPU packet */
+#define PASAHO_LINFO_IS_CUSTOM(x) PASAHO_LINFO_IS_CUSTOM_GEN2(x) /**< Indicate whether it is a Custom packet */
+#define PASAHO_LINFO_IS_IPSEC_NAT_T(x) PASAHO_LINFO_IS_IPSEC_NAT_T_GEN2(x) /**< Indicate whether it is an IPSEC NAT-T packet */
+#else
+#define PASAHO_LINFO_IS_MAC(x) PASAHO_LINFO_IS_MAC_GEN1(x) /**< Indicate whether it is a MAC packet */
+#define PASAHO_LINFO_IS_802_3(x) PASAHO_LINFO_IS_802_3_GEN1(x) /**< Indicate whether it is a 802.3 packet */
+#define PASAHO_LINFO_IS_WITH_VLAN(x) PASAHO_LINFO_IS_WITH_VLAN_GEN1(x) /**< Indicate whether it is a MAC packet with VLAN */
+#define PASAHO_LINFO_IS_WITH_MPLS(x) PASAHO_LINFO_IS_WITH_MPLS_GEN1(x) /**< Indicate whether it is a MAC packet with MPLS */
+#define PASAHO_LINFO_IS_PPPoE(x) PASAHO_LINFO_IS_PPPoE_GEN1(x) /**< Indicate whether it is a PPPoE packet */
+#define PASAHO_LINFO_IS_IP(x) PASAHO_LINFO_IS_IP_GEN1(x) /**< Indicate whether it is an IP packet */
+#define PASAHO_LINFO_IS_IPSEC_ESP(x) PASAHO_LINFO_IS_IPSEC_ESP_GEN1(x) /**< Indicate whether it is an IPSEC ESP packet */
+#define PASAHO_LINFO_IS_IPSEC_AH(x) PASAHO_LINFO_IS_IPSEC_AH_GEN1(x) /**< Indicate whether it is an IPSEC AH packet */
+#define PASAHO_LINFO_IS_UDP(x) PASAHO_LINFO_IS_UDP_GEN1(x) /**< Indicate whether it is an UDP packet */
+#define PASAHO_LINFO_IS_UDP_LITE(x) PASAHO_LINFO_IS_UDP_LITE_GEN1(x) /**< Indicate whether it is an UDP Lite packet */
+#define PASAHO_LINFO_IS_TCP(x) PASAHO_LINFO_IS_TCP_GEN1(x) /**< Indicate whether it is a TCP packet */
+#define PASAHO_LINFO_IS_GRE(x) PASAHO_LINFO_IS_GRE_GEN1(x) /**< Indicate whether it is a GRE packet */
+#define PASAHO_LINFO_IS_GTPU(x) PASAHO_LINFO_IS_GTPU_GEN1(x) /**< Indicate whether it is a GTPU packet */
+#define PASAHO_LINFO_IS_CUSTOM(x) PASAHO_LINFO_IS_CUSTOM_GEN1(x) /**< Indicate whether it is a Custom packet */
+#define PASAHO_LINFO_IS_SCTP(x) PASAHO_LINFO_IS_SCTP_GEN1(x) /**< Indicate whether it is a SCTP packet */
+#define PASAHO_LINFO_IS_IPSEC_NAT_T(x) PASAHO_LINFO_IS_IPSEC_NAT_T_GEN1(x) /**< Indicate whether it is an IPSEC NAT-T packet */
+#endif
/*@}*/ /* PASAHO_long_info_proto_ind_macross */
/** @}*/ /* @name PASAHO Long Info Protocol Indication Macross */
+/**
+ * @defgroup PASAHO_long_info_ipReassm_gen1_macros PASAHO Long Info IP Reassembly Macros For First Generation PASS
+ * @ingroup pasaho_if_macros
+ * @{
+ * @name PASAHO Long Info IpReassm Macros For First Generation PASS
+ * Macros used by the PASAHO PASS-assisted IP Reassembly Operation
+ *
+ */
+#define PASAHO_LINFO_READ_TFINDEX_GEN1(x) PASAHO_READ_BITFIELD((x)->word4,24,8) /**< Extract the IP Reassembly Traffic Flow Index (PASS Gen1)*/
+#define PASAHO_LINFO_READ_FRANCNT_GEN1(x) PASAHO_READ_BITFIELD((x)->word4,16,8) /**< Extract the IP Reassembly Fragment count (PASS Gen1)*/
+
+#define PASAHO_LINFO_SET_TFINDEX_GEN1(x, v) PASAHO_SET_BITFIELD((x)->word4,(v),24,8) /**< Set the IP Reassembly Traffic Flow Index (PASS Gen1)*/
+#define PASAHO_LINFO_SET_FRANCNT_GEN1(x, v) PASAHO_SET_BITFIELD((x)->word4,(v),16,8) /**< Set the IP Reassembly Fragment count (PASS Gen1)*/
+
+#define PASAHO_LINFO_IS_IPSEC_GEN1(x) PASAHO_READ_BITFIELD((x)->word3,25,2) /**< Indicate whether it is an IPSEC packet (PASS Gen1)*/
+#define PASAHO_LINFO_CLR_IPSEC_GEN1(x) PASAHO_SET_BITFIELD((x)->word3,0,25,2) /**< Clear IPSEC indication bits (PASS Gen1)*/
+#define PASAHO_LINFO_CLR_IPSEC_ESP_GEN1(x) PASAHO_SET_BITFIELD((x)->word3,0,26,1) /**< Clear IPSEC ESP indication bit (PASS Gen1)*/
+#define PASAHO_LINFO_CLR_IPSEC_AH_GEN1(x) PASAHO_SET_BITFIELD((x)->word3,0,25,1) /**< Claer IPSEC AH indication bit (PASS Gen1)*/
+#define PASAHO_LINFO_CLR_FLAG_FRAG_GEN1(x) PASAHO_SET_BITFIELD((x)->word3,0,3,1) /**< Clear the fragmentation found flag (PASS Gen1)*/
+
+
+#define PASAHO_LINFO_SET_START_OFFSET_GEN1(x, v) PASAHO_SET_BITFIELD((x)->word0,(v),0,16) /**< Update the next parse start offset (PASS Gen1)*/
+#define PASAHO_LINFO_SET_END_OFFSET_GEN1(x, v) PASAHO_SET_BITFIELD((x)->word1,(v),16,16) /**< Update the end of packet parse offset (PASS Gen1)*/
+
+#define PASAHO_LINFO_SET_NULL_PKT_IND_GEN1(x, v) PASAHO_SET_BITFIELD((x)->word0,(v),21,1) /**< Set the null packet flag which indicates that the packet should be dropped.
+ This flag should be set for the null packet to be delivered to PASS when
+ the reassembly timeout occurs (PASS Gen1)*/
+
+/*@}*/ /* PASAHO_long_info_ipReassm_gen1_macros */
+/** @}*/ /* @name PASAHO Long Info IpReassm Macros For First Generation PASS */
+
+/**
+ * @defgroup PASAHO_long_info_ipReassm_gen2_macros PASAHO Long Info IP Reassembly Macros For Second Generation PASS
+ * @ingroup pasaho_if_macros
+ * @{
+ * @name PASAHO Long Info IpReassm Macros
+ * Macros used by the PASAHO PASS-assisted IP Reassembly Operation For Second Generation PASS
+ *
+ */
+#define PASAHO_LINFO_READ_TFINDEX_GEN2(x) PASAHO_READ_BITFIELD((x)->word5,24,8) /**< Extract the IP Reassembly Traffic Flow Index (Pass Gen2)*/
+#define PASAHO_LINFO_READ_FRANCNT_GEN2(x) PASAHO_READ_BITFIELD((x)->word5,16,8) /**< Extract the IP Reassembly Fragment count (Pass Gen2)*/
+
+#define PASAHO_LINFO_SET_TFINDEX_GEN2(x, v) PASAHO_SET_BITFIELD((x)->word5,(v),24,8) /**< Set the IP Reassembly Traffic Flow Index (Pass Gen2)*/
+#define PASAHO_LINFO_SET_FRANCNT_GEN2(x, v) PASAHO_SET_BITFIELD((x)->word5,(v),16,8) /**< Set the IP Reassembly Fragment count (Pass Gen2)*/
+
+#define PASAHO_LINFO_IS_IPSEC_GEN2(x) PASAHO_READ_BITFIELD((x)->word3,8,2) /**< Indicate whether it is an IPSEC packet (Pass Gen2)*/
+#define PASAHO_LINFO_CLR_IPSEC_GEN2(x) PASAHO_SET_BITFIELD((x)->word3,0,8,2) /**< Clear IPSEC indication bits (Pass Gen2)*/
+#define PASAHO_LINFO_CLR_IPSEC_ESP_GEN2(x) PASAHO_SET_BITFIELD((x)->word3,0,8,1) /**< Clear IPSEC ESP indication bit (Pass Gen2)*/
+#define PASAHO_LINFO_CLR_IPSEC_AH_GEN2(x) PASAHO_SET_BITFIELD((x)->word3,0,9,1) /**< Claer IPSEC AH indication bit (Pass Gen2)*/
+#define PASAHO_LINFO_CLR_FLAG_FRAG_GEN2(x) PASAHO_SET_BITFIELD((x)->word1,0,19,1) /**< Clear the fragmentation found flag (Pass Gen2)*/
+
+
+#define PASAHO_LINFO_SET_START_OFFSET_GEN2(x, v) PASAHO_SET_BITFIELD((x)->word0,(v),0,8) /**< Update the next parse start offset (Pass Gen2)*/
+#define PASAHO_LINFO_SET_END_OFFSET_GEN2(x, v) PASAHO_SET_BITFIELD((x)->word1,(v),16,16) /**< Update the end of packet parse offset (Pass Gen2)*/
+#define PASAHO_LINFO_SET_NXT_HDR_TYPE_GEN2(x, v) PASAHO_SET_BITFIELD((x)->word1,(v),0,6) /**< Update the next header to parse type (Pass Gen2)*/
+
+#define PASAHO_LINFO_SET_NULL_PKT_IND_GEN2(x, v) PASAHO_SET_BITFIELD((x)->word0,(v),13,1) /**< Set the null packet flag which indicates that the packet should be dropped.
+ This flag should be set for the null packet to be delivered to PASS when
+ the reassembly timeout occurs (Pass Gen2)*/
+/*@}*/ /* PASAHO_long_info_ipReassm_gen2_macros */
+/** @}*/ /* @name PASAHO Long Info IpReassm Macros For Second Generation PASS */
+
/**
* @defgroup PASAHO_long_info_ipReassm_macros PASAHO Long Info IP Reassembly Macros
* @ingroup pasaho_if_macros
* Macros used by the PASAHO PASS-assisted IP Reassembly Operation
*
*/
-#define PASAHO_LINFO_READ_TFINDEX(x) PASAHO_READ_BITFIELD((x)->word4,24,8) /**< Extract the IP Reassembly Traffic Flow Index */
-#define PASAHO_LINFO_READ_FRANCNT(x) PASAHO_READ_BITFIELD((x)->word4,16,8) /**< Extract the IP Reassembly Fragment count */
+#ifdef NSS_GEN2
+#define PASAHO_LINFO_READ_TFINDEX(x) PASAHO_LINFO_READ_TFINDEX_GEN2(x) /**< Extract the IP Reassembly Traffic Flow Index */
+#define PASAHO_LINFO_READ_FRANCNT(x) PASAHO_LINFO_READ_FRANCNT_GEN2(x) /**< Extract the IP Reassembly Fragment count */
+
+#define PASAHO_LINFO_SET_TFINDEX(x, v) PASAHO_LINFO_SET_TFINDEX_GEN2(x, v) /**< Set the IP Reassembly Traffic Flow Index */
+#define PASAHO_LINFO_SET_FRANCNT(x, v) PASAHO_LINFO_SET_FRANCNT_GEN2(x, v) /**< Set the IP Reassembly Fragment count */
+
+#define PASAHO_LINFO_IS_IPSEC(x) PASAHO_LINFO_IS_IPSEC_GEN2(x) /**< Indicate whether it is an IPSEC packet */
+#define PASAHO_LINFO_CLR_IPSEC(x) PASAHO_LINFO_CLR_IPSEC_GEN2(x) /**< Clear IPSEC indication bits */
+#define PASAHO_LINFO_CLR_IPSEC_ESP(x) PASAHO_LINFO_CLR_IPSEC_ESP_GEN2(x) /**< Clear IPSEC ESP indication bit */
+#define PASAHO_LINFO_CLR_IPSEC_AH(x) PASAHO_LINFO_CLR_IPSEC_AH_GEN2(x) /**< Claer IPSEC AH indication bit */
+#define PASAHO_LINFO_CLR_FLAG_FRAG(x) PASAHO_LINFO_CLR_FLAG_FRAG_GEN2(x) /**< Clear the fragmentation found flag */
-#define PASAHO_LINFO_SET_TFINDEX(x, v) PASAHO_SET_BITFIELD((x)->word4,(v),24,8) /**< Set the IP Reassembly Traffic Flow Index */
-#define PASAHO_LINFO_SET_FRANCNT(x, v) PASAHO_SET_BITFIELD((x)->word4,(v),16,8) /**< Set the IP Reassembly Fragment count */
-#define PASAHO_LINFO_IS_IPSEC(x) PASAHO_READ_BITFIELD((x)->word3,25,2) /**< Indicate whether it is an IPSEC packet */
-#define PASAHO_LINFO_CLR_IPSEC(x) PASAHO_SET_BITFIELD((x)->word3,0,25,2) /**< Clear IPSEC indication bits */
-#define PASAHO_LINFO_CLR_IPSEC_ESP(x) PASAHO_SET_BITFIELD((x)->word3,0,26,1) /**< Clear IPSEC ESP indication bit */
-#define PASAHO_LINFO_CLR_IPSEC_AH(x) PASAHO_SET_BITFIELD((x)->word3,0,25,1) /**< Claer IPSEC AH indication bit */
-#define PASAHO_LINFO_CLR_FLAG_FRAG(x) PASAHO_SET_BITFIELD((x)->word3,0,3,1) /**< Clear the fragmentation found flag */
+#define PASAHO_LINFO_SET_START_OFFSET(x, v) PASAHO_LINFO_SET_START_OFFSET_GEN2(x, v) /**< Update the next parse start offset */
+#define PASAHO_LINFO_SET_END_OFFSET(x, v) PASAHO_LINFO_SET_END_OFFSET_GEN2(x, v) /**< Update the end of packet parse offset */
+#define PASAHO_LINFO_SET_NXT_HDR_TYPE(x, v) PASAHO_LINFO_SET_NXT_HDR_TYPE_GEN2(x, v) /**< Update the next header to parse type */
+#define PASAHO_LINFO_SET_NULL_PKT_IND(x, v) PASAHO_LINFO_SET_NULL_PKT_IND_GEN2(x, v) /**< Set the null packet flag which indicates that the packet should be dropped.
+ This flag should be set for the null packet to be delivered to PASS when
+ the reassembly timeout occurs */
+#else
+#define PASAHO_LINFO_READ_TFINDEX(x) PASAHO_LINFO_READ_TFINDEX_GEN1(x) /**< Extract the IP Reassembly Traffic Flow Index */
+#define PASAHO_LINFO_READ_FRANCNT(x) PASAHO_LINFO_READ_FRANCNT_GEN1(x) /**< Extract the IP Reassembly Fragment count */
+
+#define PASAHO_LINFO_SET_TFINDEX(x, v) PASAHO_LINFO_SET_TFINDEX_GEN1(x, v) /**< Set the IP Reassembly Traffic Flow Index */
+#define PASAHO_LINFO_SET_FRANCNT(x, v) PASAHO_LINFO_SET_FRANCNT_GEN1(x, v) /**< Set the IP Reassembly Fragment count */
+
+#define PASAHO_LINFO_IS_IPSEC(x) PASAHO_LINFO_IS_IPSEC_GEN1(x) /**< Indicate whether it is an IPSEC packet */
+#define PASAHO_LINFO_CLR_IPSEC(x) PASAHO_LINFO_CLR_IPSEC_GEN1(x) /**< Clear IPSEC indication bits */
+#define PASAHO_LINFO_CLR_IPSEC_ESP(x) PASAHO_LINFO_CLR_IPSEC_ESP_GEN1(x) /**< Clear IPSEC ESP indication bit */
+#define PASAHO_LINFO_CLR_IPSEC_AH(x) PASAHO_LINFO_CLR_IPSEC_AH_GEN1(x) /**< Claer IPSEC AH indication bit */
+#define PASAHO_LINFO_CLR_FLAG_FRAG(x) PASAHO_LINFO_CLR_FLAG_FRAG_GEN1(x) /**< Clear the fragmentation found flag */
-#define PASAHO_LINFO_SET_START_OFFSET(x, v) PASAHO_SET_BITFIELD((x)->word0,(v),0,16) /**< Update the next parse start offset */
-#define PASAHO_LINFO_SET_END_OFFSET(x, v) PASAHO_SET_BITFIELD((x)->word1,(v),16,16) /**< Update the end of packet parse offset */
-#define PASAHO_LINFO_SET_NULL_PKT_IND(x, v) PASAHO_SET_BITFIELD((x)->word0,(v),21,1) /**< Set the null packet flag which indicates that the packet should be dropped.
+#define PASAHO_LINFO_SET_START_OFFSET(x, v) PASAHO_LINFO_SET_START_OFFSET_GEN1(x, v) /**< Update the next parse start offset */
+#define PASAHO_LINFO_SET_END_OFFSET(x, v) PASAHO_LINFO_SET_END_OFFSET_GEN1(x, v) /**< Update the end of packet parse offset */
+
+#define PASAHO_LINFO_SET_NULL_PKT_IND(x, v) PASAHO_LINFO_SET_NULL_PKT_IND_GEN1(x, v) /**< Set the null packet flag which indicates that the packet should be dropped.
This flag should be set for the null packet to be delivered to PASS when
the reassembly timeout occurs */
+
+#endif
/*@}*/ /* PASAHO_long_info_ipReassm_macros */
/** @}*/ /* @name PASAHO Long Info IpReassm Macros */
*
*/
/*@{*/
-
#define PASAHO_SINFO_READ_CMDID(x) PASAHO_READ_BITFIELD((x)->word0,29,3) /**< Extract the command ID defined at @ref pasahoCommands */
#define PASAHO_SINFO_RESD_PAYLOAD_OFFSET(x) PASAHO_READ_BITFIELD((x)->word0,16,8) /**< Extract the offset to the packet payload */
#define PASAHO_SINFO_READ_PAYLOAD_LENGTH(x) PASAHO_READ_BITFIELD((x)->word0,0,16) /**< Extract the byte length of the payload */
/*@}*/ /* PASAHO_short_info_command_macros */
/** @}*/ /* @name PASAHO Short Info Command Macros */
+/* Header bitmask bits */
+/**
+ * @defgroup pasahoHeaderBitmapGen1 PA/SA/HO Header Bitmap Bit Definitions For First Generation PASS
+ * @ingroup pasaho_if_constants
+ * @{
+ *
+ * @name PA/SA/HO Header Bitmap Bit Definitions For First Generation PASS
+ * Bitmap definition of the protocol header bitmask at the long info of First Generation PASS.
+ */
+/*@{*/
+#define PASAHO_HDR_BITMASK_MAC_GEN1 (1 << 0) /**< MAC present (PASS Gen1)*/
+#define PASAHO_HDR_BITMASK_VLAN_GEN1 (1 << 1) /**< VLAN present (PASS Gen1)*/
+#define PASAHO_HDR_BITMASK_MPLS_GEN1 (1 << 2) /**< MPLS present (PASS Gen1)*/
+#define PASAHO_HDR_BITMASK_IP_GEN1 (1 << 3) /**< IP present (PASS Gen1)*/
+#define PASAHO_HDR_BITMASK_ESP_GEN1 (1 << 4) /**< IPSEC/ESP present (PASS Gen1)*/
+#define PASAHO_HDR_BITMASK_AH_GEN1 (1 << 5) /**< IPSEC/AH present (PASS Gen1)*/
+#define PASAHO_HDR_BITMASK_UDP_GEN1 (1 << 6) /**< UDP present (PASS Gen1)*/
+#define PASAHO_HDR_BITMASK_UDPLITE_GEN1 (1 << 7) /**< UDPLITE present (PASS Gen1)*/
+#define PASAHO_HDR_BITMASK_TCP_GEN1 (1 << 8) /**< TCP present (PASS Gen1)*/
+#define PASAHO_HDR_BITMASK_GTPU_GEN1 (1 << 9) /**< GTPU present (PASS Gen1)*/
+#define PASAHO_HDR_BITMASK_CUSTOM_GEN1 (1 << 10) /**< Custom header present (PASS Gen1)*/
+
+#define PASAHO_HDR_BITMASK2_SCTP_GEN1 (1 << 0) /**< SCTP present (PASS Gen1)*/
+#define PASAHO_HDR_BITMASK2_IPSEC_NAT_T_GEN1 (1 << 1) /**< IPSEC NAT-T present (PASS Gen1)*/
+#define PASAHO_HDR_BITMASK2_PPPoE_GEN1 (1 << 2) /**< PPPoE present (PASS Gen1)*/
+#define PASAHO_HDR_BITMASK2_802_3_GEN1 (1 << 3) /**< 802.3 present (PASS Gen1)*/
+
+/*@}*/
+/** @} */
+
+/* Header bitmask bits */
+/**
+ * @defgroup pasahoHeaderBitmapGen2 PA/SA/HO Header Bitmap Bit Definitions For Second Generation PASS
+ * @ingroup pasaho_if_constants
+ * @{
+ *
+ * @name PA/SA/HO Header Bitmap Bit Definitions For Second Generation PASS
+ * Bitmap definition of the protocol header bitmask at the long info For Second Generation PASS.
+ */
+/*@{*/
+#define PASAHO_HDR_BITMASK_MAC_GEN2 (1 << 0) /**< MAC present (PASS Gen2)*/
+#define PASAHO_HDR_BITMASK_VLAN_GEN2 (1 << 1) /**< VLAN present (PASS Gen2)*/
+#define PASAHO_HDR_BITMASK_MPLS_GEN2 (1 << 2) /**< MPLS present (PASS Gen2)*/
+#define PASAHO_HDR_BITMASK_802_3_GEN2 (1 << 3) /**< 802.3 present (PASS Gen2)*/
+#define PASAHO_HDR_BITMASK_PPPoE_GEN2 (1 << 4) /**< PPPoE present (PASS Gen2)*/
+#define PASAHO_HDR_BITMASK_IPv4_GEN2 (1 << 5) /**< IPv4 present (PASS Gen2)*/
+#define PASAHO_HDR_BITMASK_IPv6_GEN2 (1 << 6) /**< IPv6 present (PASS Gen2)*/
+#define PASAHO_HDR_BITMASK_IP_OPTS_GEN2 (1 << 7) /**< IPv4 options or IPv6 extension headers present (PASS Gen2)*/
+#define PASAHO_HDR_BITMASK_ESP_GEN2 (1 << 8) /**< IPSEC/ESP present (PASS Gen2)*/
+#define PASAHO_HDR_BITMASK_AH_GEN2 (1 << 9) /**< IPSEC/AH present (PASS Gen2)*/
+#define PASAHO_HDR_BITMASK_SCTP_GEN2 (1 << 10) /**< SCTP present (PASS Gen2)*/
+#define PASAHO_HDR_BITMASK_UDP_GEN2 (1 << 11) /**< UDP present (PASS Gen2)*/
+#define PASAHO_HDR_BITMASK_UDPLITE_GEN2 (1 << 11) /**< UDPLITE present (PASS Gen2)*/
+#define PASAHO_HDR_BITMASK_TCP_GEN2 (1 << 12) /**< TCP present (PASS Gen2)*/
+#define PASAHO_HDR_BITMASK_GTPU_GEN2 (1 << 13) /**< GTPU present (PASS Gen2)*/
+#define PASAHO_HDR_BITMASK_CUSTOM_GEN2 (1 << 14) /**< Custom header present (PASS Gen2)*/
+#define PASAHO_HDR_BITMASK_IPSEC_NAT_T_GEN2 (1 << 15) /**< IPSEC NAT-T present (PASS Gen2)*/
+
+/*@}*/
+/** @} */
/* Header bitmask bits */
/**
* Bitmap definition of the protocol header bitmask at the long info.
*/
/*@{*/
-
-#define PASAHO_HDR_BITMASK_MAC (1 << 0) /**< MAC present */
-#define PASAHO_HDR_BITMASK_VLAN (1 << 1) /**< VLAN present */
-#define PASAHO_HDR_BITMASK_MPLS (1 << 2) /**< MPLS present */
-#define PASAHO_HDR_BITMASK_IP (1 << 3) /**< IP present */
-#define PASAHO_HDR_BITMASK_ESP (1 << 4) /**< IPSEC/ESP present */
-#define PASAHO_HDR_BITMASK_AH (1 << 5) /**< IPSEC/AH present */
-#define PASAHO_HDR_BITMASK_UDP (1 << 6) /**< UDP present */
-#define PASAHO_HDR_BITMASK_UDPLITE (1 << 7) /**< UDPLITE present */
-#define PASAHO_HDR_BITMASK_TCP (1 << 8) /**< TCP present */
-#define PASAHO_HDR_BITMASK_GTPU (1 << 9) /**< GTPU present */
-#define PASAHO_HDR_BITMASK_CUSTOM (1 << 10) /**< Custom header present */
-
-#define PASAHO_HDR_BITMASK2_SCTP (1 << 0) /**< SCTP present */
-#define PASAHO_HDR_BITMASK2_IPSEC_NAT_T (1 << 1) /**< IPSEC NAT-T present */
-#define PASAHO_HDR_BITMASK2_PPPoE (1 << 2) /**< PPPoE present */
-#define PASAHO_HDR_BITMASK2_802_3 (1 << 3) /**< 802.3 present */
+#ifdef NSS_GEN2
+#define PASAHO_HDR_BITMASK_MAC PASAHO_HDR_BITMASK_MAC_GEN2 /**< MAC present */
+#define PASAHO_HDR_BITMASK_VLAN PASAHO_HDR_BITMASK_VLAN_GEN2 /**< VLAN present */
+#define PASAHO_HDR_BITMASK_MPLS PASAHO_HDR_BITMASK_MPLS_GEN2 /**< MPLS present */
+#define PASAHO_HDR_BITMASK_802_3 PASAHO_HDR_BITMASK_802_3_GEN2 /**< 802.3 present */
+#define PASAHO_HDR_BITMASK_PPPoE PASAHO_HDR_BITMASK_PPPoE_GEN2 /**< PPPoE present */
+#define PASAHO_HDR_BITMASK_IPv4 PASAHO_HDR_BITMASK_IPv4_GEN2 /**< IPv4 present */
+#define PASAHO_HDR_BITMASK_IPv6 PASAHO_HDR_BITMASK_IPv6_GEN2 /**< IPv6 present */
+#define PASAHO_HDR_BITMASK_IP_OPTS PASAHO_HDR_BITMASK_IP_OPTS_GEN2 /**< IPv4 options or IPv6 extension headers present */
+#define PASAHO_HDR_BITMASK_ESP PASAHO_HDR_BITMASK_ESP_GEN2 /**< IPSEC/ESP present */
+#define PASAHO_HDR_BITMASK_AH PASAHO_HDR_BITMASK_AH_GEN2 /**< IPSEC/AH present */
+#define PASAHO_HDR_BITMASK_SCTP PASAHO_HDR_BITMASK_SCTP_GEN2 /**< SCTP present */
+#define PASAHO_HDR_BITMASK_UDP PASAHO_HDR_BITMASK_UDP_GEN2 /**< UDP present */
+#define PASAHO_HDR_BITMASK_UDPLITE PASAHO_HDR_BITMASK_UDPLITE_GEN2 /**< UDPLITE present */
+#define PASAHO_HDR_BITMASK_TCP PASAHO_HDR_BITMASK_TCP_GEN2 /**< TCP present */
+#define PASAHO_HDR_BITMASK_GTPU PASAHO_HDR_BITMASK_GTPU_GEN2 /**< GTPU present */
+#define PASAHO_HDR_BITMASK_CUSTOM PASAHO_HDR_BITMASK_CUSTOM_GEN2 /**< Custom header present */
+#define PASAHO_HDR_BITMASK_IPSEC_NAT_T PASAHO_HDR_BITMASK_IPSEC_NAT_T_GEN2 /**< IPSEC NAT-T present */
+#else
+#define PASAHO_HDR_BITMASK_MAC PASAHO_HDR_BITMASK_MAC_GEN1 /**< MAC present */
+#define PASAHO_HDR_BITMASK_VLAN PASAHO_HDR_BITMASK_VLAN_GEN1 /**< VLAN present */
+#define PASAHO_HDR_BITMASK_MPLS PASAHO_HDR_BITMASK_MPLS_GEN1 /**< MPLS present */
+#define PASAHO_HDR_BITMASK_IP PASAHO_HDR_BITMASK_IP_GEN1 /**< IP present */
+#define PASAHO_HDR_BITMASK_ESP PASAHO_HDR_BITMASK_ESP_GEN1 /**< IPSEC/ESP present */
+#define PASAHO_HDR_BITMASK_AH PASAHO_HDR_BITMASK_AH_GEN1 /**< IPSEC/AH present */
+#define PASAHO_HDR_BITMASK_UDP PASAHO_HDR_BITMASK_UDP_GEN1 /**< UDP present */
+#define PASAHO_HDR_BITMASK_UDPLITE PASAHO_HDR_BITMASK_UDPLITE_GEN1 /**< UDPLITE present */
+#define PASAHO_HDR_BITMASK_TCP PASAHO_HDR_BITMASK_TCP_GEN1 /**< TCP present */
+#define PASAHO_HDR_BITMASK_GTPU PASAHO_HDR_BITMASK_GTPU_GEN1 /**< GTPU present */
+#define PASAHO_HDR_BITMASK_CUSTOM PASAHO_HDR_BITMASK_CUSTOM_GEN1 /**< Custom header present */
+
+#define PASAHO_HDR_BITMASK2_SCTP PASAHO_HDR_BITMASK2_SCTP_GEN1 /**< SCTP present */
+#define PASAHO_HDR_BITMASK2_IPSEC_NAT_T PASAHO_HDR_BITMASK2_IPSEC_NAT_T_GEN1/**< IPSEC NAT-T present */
+#define PASAHO_HDR_BITMASK2_PPPoE PASAHO_HDR_BITMASK2_PPPoE_GEN1 /**< PPPoE present */
+#define PASAHO_HDR_BITMASK2_802_3 PASAHO_HDR_BITMASK2_802_3_GEN1 /**< 802.3 present */
+#endif
/*@}*/
/** @} */
+
+
/* Next Route command */
+/**
+ * @defgroup pasahoNrDestGen1 PA/SA/HO Destination Types at NextRoute Command of First Generation PASS
+ * @ingroup pasaho_if_constants
+ * @{
+ *
+ * @name PA/SA/HO Destination Types at NextRoute Command of First Generation PASS
+ * Bitmap definition of the destination type at the nextRoute command of First Generation PASS.
+ */
+/*@{*/
+#define PASAHO_NR_DEST_PKTDMA_GEN1 6 /**< NextRoute Destination: PKTDMA (PASS Gen1)*/
+#define PASAHO_NR_DEST_ETH_GEN1 7 /**< NextRoute Destination: Ethernet Port (PASS Gen1)*/
+#define PASAHO_NR_DEST_SRIO_GEN1 0 /**< NextRoute Destination: SRIO (PASS Gen1)*/
+
+/*@}*/
+/** @} */
+
+/**
+ * @defgroup pasahoNrDestGen2 PA/SA/HO Destination Types at NextRoute Command of Second Generation PASS
+ * @ingroup pasaho_if_constants
+ * @{
+ *
+ * @name PA/SA/HO Destination Types at NextRoute Command of Second Generation PASS
+ * Bitmap definition of the destination type at the nextRoute command of Second Generation PASS.
+ */
+/*@{*/
+#define PASAHO_NR_DEST_PKTDMA_GEN2 0 /**< NextRoute Destination: PKTDMA (PASS Gen2)*/
+#define PASAHO_NR_DEST_ETH_GEN2 2 /**< NextRoute Destination: Ethernet Port (PASS Gen2)*/
+#define PASAHO_NR_DEST_SRIO_GEN2 7 /**< NextRoute Destination: SRIO (PASS Gen2)*/
+
+/*@}*/
+/** @} */
+
+/**
+ * @defgroup pasahoNrDest PA/SA/HO Destination Types at NextRoute Command
+ * @ingroup pasaho_if_constants
+ * @{
+ *
+ * @name PA/SA/HO Destination Types at NextRoute Command
+ * Bitmap definition of the destination type at the nextRoute command
+ */
+#ifdef NSS_GEN2
+#define PASAHO_NR_DEST_PKTDMA PASAHO_NR_DEST_PKTDMA_GEN2 /**< NextRoute Destination: PKTDMA */
+#define PASAHO_NR_DEST_ETH PASAHO_NR_DEST_ETH_GEN2 /**< NextRoute Destination: Ethernet Port */
+#define PASAHO_NR_DEST_SRIO PASAHO_NR_DEST_SRIO_GEN2 /**< NextRoute Destination: SRIO */
+#else
+#define PASAHO_NR_DEST_PKTDMA PASAHO_NR_DEST_PKTDMA_GEN1 /**< NextRoute Destination: PKTDMA */
+#define PASAHO_NR_DEST_ETH PASAHO_NR_DEST_ETH_GEN1 /**< NextRoute Destination: Ethernet Port */
+#define PASAHO_NR_DEST_SRIO PASAHO_NR_DEST_SRIO_GEN1 /**< NextRoute Destination: SRIO */
+#endif
+
+/*@}*/
+/** @} */
+
/**
* @ingroup pasaho_if_structures
* @brief pasahoNextRoute_t defines the next route command. The command structure is defined as 32 bit
#define PASAHO_SET_PKTTYPE(x,v) PASAHO_SET_BITFIELD((x)->word1, (v), 24, 8) /**< Specifies the packet type to use for packets send to the SRIO */
#define PASAHO_SET_TX_PADDING(x,v) PASAHO_SET_BITFIELD((x)->word1, (v), 0, 1) /**< Sets the tx padding bit which indicates PASS should check padding condition and provide L2 zero padding if required */
#define PASAHO_SET_TX_STATS(x,v) PASAHO_SET_BITFIELD((x)->word1, (v), 1, 1) /**< Sets the tx stats bit which indicates PASS should increment the user statistics chain pointed by the user statistics index */
+#define PASAHO_SET_RPT_TX_TIMESTAMP(x,v) PASAHO_SET_BITFIELD((x)->word1, (v), 2, 1) /**< Sets the report tx timestamp bit which indicates swInfo0 is required to configure CPTS Tx timestamp report */
#define PASAHO_SET_USR_STATS_INDEX(x,v) PASAHO_SET_BITFIELD((x)->word1, (v), 8, 16) /**< Specifies index of the first user-defined statistics to be updated */
/*@}*/ /* PASAHO_next_route_command_macros */
*/
/*@{*/
-
#define PASAHO_CHKCRC_SET_NEG0(x,v) PASAHO_SET_BITFIELD((x)->word0, (v), 23, 1) /**< Sets the negative 0 flag - if set a checksum computed as 0 will be sent as 0xffff */
#define PASAHO_CHKCRC_SET_CTRL(x,v) PASAHO_SET_BITFIELD((x)->word0, (v), 16, 4) /**< Sets the optional flags of the CRC/Checksum command */
-#define PASAHO_CHKCRC_SET_START(x,v) PASAHO_SET_BITFIELD((x)->word0, (v), 0, 16) /**< Sets the start offset of the checksum/crc */
+#define PASAHO_CHKCRC_SET_CRCSIZE(x,v) PASAHO_SET_BITFIELD((x)->word0, (v), 8, 8) /**< Sets the size of the crc in bytes (PASS Gen2 only) */
+#define PASAHO_CHKCRC_SET_START(x,v) PASAHO_SET_BITFIELD((x)->word0, (v), 0, 8) /**< Sets the start offset of the checksum/crc */
#define PASAHO_CHKCRC_SET_LEN(x,v) PASAHO_SET_BITFIELD((x)->word1, (v), 16, 16) /**< Sets the length of the checksum/crc */
#define PASAHO_CHKCRC_SET_RESULT_OFF(x,v) PASAHO_SET_BITFIELD((x)->word1, (v), 0, 16) /**< Sets the offset to where to paste the checksum/crc into the packet */
-#define PASAHO_CHKCRC_SET_INITVAL(x,v) PASAHO_SET_BITFIELD((x)->word2, (v), 16, 16) /**< Sets the initial value of the checksum/crc */
+#define PASAHO_CHKCRC_SET_INITVAL(x,v) PASAHO_SET_BITFIELD((x)->word2, (v), 16, 16) /**< Sets the initial value of the 16-bit checksum */
+#define PASAHO_CHKCRC_SET_INITVAL32(x,v) (x)->word2 = (v) /**< Sets the initial value of the 32-bit crc (PASS Gen2 only)*/
/*@}*/ /* @name PASAHO Checksum/CRC Command Macros */
/** @}*/ /* PASAHO_chksum_command_macros */
/*@}*/ /* @name PASAHO Message Length Patching Command Macros */
/** @}*/ /* PASAHO_patch_msg_len_command_macros */
+/* Compute checksum command */
+/**
+ * @ingroup pasaho_if_structures
+ * @brief pasahoEfOp_t defines the egress flow operation command which is used to instruct PASS to
+ * perform optional flow cache lookup and egress packet modification according to the associated
+ * egress flow records. The command structure is defined as 32 bit values to wrok with the hardware
+ * regardless of the device endianness.
+ *
+ * @details
+ */
+
+typedef struct pasahoEfOp_s {
+ uint32_t word0; /**< @ref PASAHO_ef_op_command_macros */
+ uint32_t word1; /**< @ref PASAHO_ef_op_command_macros */
+ uint32_t word2; /**< @ref PASAHO_ef_op_command_macros */
+ uint32_t word3; /**< @ref PASAHO_ef_op_command_macros */
+ uint32_t word4; /**< @ref PASAHO_ef_op_command_macros */
+ uint32_t word5; /**< @ref PASAHO_ef_op_command_macros */
+
+} pasahoComEfOp_t;
+
+/**
+ * @defgroup pasahoEfOpCtrlBitmap PA/SA/HO Egress Flow Opertaion Control Bitmap Bit Definitions
+ * @ingroup pasaho_if_constants
+ * @{
+ *
+ * @name PA/SA/HO Egress Flow Opertaion Control Bitmap Bit Definitions
+ * Bitmap definition of the control bitmap at the Egress Flow operation info.
+ */
+/*@{*/
+
+#define PASAHO_HDR_EF_OP_CTRL_FC (1 << 15) /**< Enable Flow Cache lookup */
+#define PASAHO_HDR_EF_OP_CTRL_LVL4_REC (1 << 7) /**< Level 4 record prespent */
+#define PASAHO_HDR_EF_OP_CTRL_LVL3_REC (1 << 6) /**< Level 3 record prespent */
+#define PASAHO_HDR_EF_OP_CTRL_LVL2_REC (1 << 5) /**< Level 2 record prespent */
+#define PASAHO_HDR_EF_OP_CTRL_LVL1_REC (1 << 4) /**< Level 1 record prespent */
+
+/*@}*/
+/** @} */
+
+
+/**
+ * @defgroup PASAHO_ef_op_command_macros PASAHO Egress Flow Operation Command Macros
+ * @ingroup pasaho_if_macros
+ * @{
+ * @name PASAHO Egress Flow Operation Command Macros
+ * Macros used by the PASAHO Egress Flow Operation Command
+ */
+/*@{*/
+#define PASAHO_EF_OP_SET_CTRL(x,v) PASAHO_SET_BITFIELD((x)->word0,(v), 8, 16) /**< Sets the control flags of the Flow Cache operation command */
+#define PASAHO_EF_OP_SET_CTRL_FC(x,v) PASAHO_SET_BITFIELD((x)->word0,(v), 23, 1) /**< Enable/Disable Flow Cache lookup */
+#define PASAHO_EF_OP_SET_CTRL_LVL4(x,v) PASAHO_SET_BITFIELD((x)->word0,(v), 15, 1) /**< Enable/Disable Level 4 Egress Flow record */
+#define PASAHO_EF_OP_SET_CTRL_LVL3(x,v) PASAHO_SET_BITFIELD((x)->word0,(v), 14, 1) /**< Enable/Disable Level 3 Egress Flow record */
+#define PASAHO_EF_OP_SET_CTRL_LVL2(x,v) PASAHO_SET_BITFIELD((x)->word0,(v), 13, 1) /**< Enable/Disable Level 2 Egress Flow record */
+#define PASAHO_EF_OP_SET_CTRL_LVL1(x,v) PASAHO_SET_BITFIELD((x)->word0,(v), 12, 1) /**< Enable/Disable Level 1 Egress Flow record */
+
+#define PASAHO_EF_OP_SET_L2_OFFSET(x, v) PASAHO_SET_BITFIELD((x)->word1,(v),8,8) /**< Set the l2 offset */
+#define PASAHO_EF_OP_SET_L3_OFFSET2(x, v) PASAHO_SET_BITFIELD((x)->word1,(v),0,8) /**< Set the l3 offset for inner or fisrt IP */
+#define PASAHO_EF_OP_SET_L3_OFFSET(x, v) PASAHO_SET_BITFIELD((x)->word2,(v),24,8) /**< Set the l3 offset for outer or fisrt IP */
+#define PASAHO_EF_OP_SET_IPSEC_OFFSET(x, v) PASAHO_SET_BITFIELD((x)->word2,(v),0, 8) /**< Set the IPSEC offset if the IPSEC header exists in the packet */
+#define PASAHO_EF_OP_SET_END_OFFSET(x, v) PASAHO_SET_BITFIELD((x)->word1,(v),16,16) /**< Set the end offset as end of L4 (UDP/UDPLite/TCP) payload */
+
+#define PASAHO_EF_OP_SET_LVL1_REC(x, v) PASAHO_SET_BITFIELD((x)->word3,(v),24, 8) /**< Set the index of Egress Flow level 1 record */
+#define PASAHO_EF_OP_SET_LVL2_REC(x, v) PASAHO_SET_BITFIELD((x)->word3,(v),16, 8) /**< Set the index of Egress Flow level 2 record */
+#define PASAHO_EF_OP_SET_LVL3_REC(x, v) PASAHO_SET_BITFIELD((x)->word3,(v), 8, 8) /**< Set the index of Egress Flow level 3 record */
+#define PASAHO_EF_OP_SET_LVL4_REC(x, v) PASAHO_SET_BITFIELD((x)->word3,(v), 0, 8) /**< Set the index of Egress Flow level 4 record */
+
+/*@}*/
+/** @} */
+
+
+/* EMAC CRC Verify command */
+/**
+ * @ingroup pasaho_if_structures
+ * @brief pasahoEmacCrcVerify_t defines the Ethernet CRC Verify command. The command structure is defined as 32 bit
+ * values to work with the hardware regardless of the device endianness.
+ *
+ * @details
+ */
+
+typedef struct pasahoEmacCrcVerify_s {
+ uint32_t word0; /**< Contains the Ethernet CRC Verify command information. @ref PASAHO_emac_crc_verify_command_macros */
+} pasahoEmacCrcVerify_t;
+
+/**
+ * @defgroup PASAHO_emac_crc_verify_command_macros PASAHO EMAC CRC Verify Command Macros
+ * @ingroup pasaho_if_macros
+ * @{
+ * @name PASAHO EMAC CRC Verify Command Macros
+ * Macros used by the PASAHO EMAC CRC Verify Command
+ *
+ */
+/*@{*/
+
+#define PASAHO_SET_SUB_CODE_EMAC_CRC_VERIFY(x) PASAHO_SET_BITFIELD((x)->word0, PASAHO_SUB_CMD_EMAC_CRC_VERIFY, 24, 5) /**< Set sub-command code to indicate EMAC CRC Verify command */
+#define PASAHO_SET_EMACPORT(x,v) PASAHO_SET_BITFIELD((x)->word0, (v), 20, 4) /**< Specifies the one-based destination EMAC port number
+ where 0 indicates standard ethernet switch forwarding */
+
+/*@}*/ /* @name PASAHO EMAC CRC Verify Command Macros */
+/** @}*/ /* PASAHO_emac_crc_verify_command_macros */
+
+/* Insert Message time command */
+/**
+ * @ingroup pasaho_if_structures
+ * @brief pasahoInsMsgTime_t defines the message time insert command. The command structure is defined as 32 bit
+ * values to work with the hardware regardless of the device endianness.
+ *
+ * @details
+ */
+
+typedef struct pasahoInsMsgTime_s {
+ uint32_t word0; /**< Contains the message time patching command information. @ref PASAHO_insert_msg_time_command_macros */
+} pasahoInsMsgTime_t;
+
+/**
+ * @defgroup PASAHO_insert_msg_time_command_macros PASAHO Message Time Insert Command Macros
+ * @ingroup pasaho_if_macros
+ * @{
+ * @name PASAHO Message Time Insert Command Macros
+ * Macros used by the PASAHO Message Time Insert Command
+ *
+ */
+/*@{*/
+
+#define PASAHO_SET_SUB_CODE_INS_MSG_TIME(x) PASAHO_SET_BITFIELD((x)->word0, PASAHO_SUB_CMD_INS_TIME, 24, 5) /**< Set sub-command code to indicate Message Time Insert command */
+#define PASAHO_SET_INS_OFFSET_MSG_TIME(x,offset) PASAHO_SET_BITFIELD((x)->word0, offset, 0, 16) /**< Set the offset from start of packet to insert the 8 byte time */
+
+/*@}*/ /* @name PASAHO Message Time Insert Command Macros */
+/** @}*/ /* PASAHO_insert_msg_time_command_macros */
+
+/* Insert Message Count command */
+/**
+ * @ingroup pasaho_if_structures
+ * @brief pasahoInsMsgCount_t defines the message count insert command. The command structure is defined as 32 bit
+ * values to work with the hardware regardless of the device endianness.
+ *
+ * @details
+ */
+
+typedef struct pasahoInsMsgCount_s {
+ uint32_t word0; /**< Contains the message count patching command information. @ref PASAHO_insert_msg_count_command_macros */
+ uint32_t word1; /**< Contains the message count patching command information. @ref PASAHO_insert_msg_count_command_macros */
+} pasahoInsMsgCount_t;
+
+/**
+ * @defgroup PASAHO_insert_msg_count_command_macros PASAHO Message Count Insert Command Macros
+ * @ingroup pasaho_if_macros
+ * @{
+ * @name PASAHO Message Count Insert Command Macros
+ * Macros used by the PASAHO Message Count Insert Command
+ *
+ */
+/*@{*/
+
+#define PASAHO_SET_SUB_CODE_INS_MSG_COUNT(x) PASAHO_SET_BITFIELD((x)->word0, PASAHO_SUB_CMD_INS_COUNT, 24, 5) /**< Set sub-command code to indicate Message Count Insert command */
+#define PASAHO_SET_INS_OFFSET_MSG_COUNT(x,offset) PASAHO_SET_BITFIELD((x)->word0, offset, 0, 16) /**< Set the offset from start of packet to insert the 4 byte count */
+#define PASAHO_SET_COUNTER_INDEX_FOR_MSG_COUNT(x,offset) PASAHO_SET_BITFIELD((x)->word1, offset, 16, 16) /**< Set the counter index to read from, to insert the 4 byte count */
+
+/*@}*/ /* @name PASAHO Message Count Insert Command Macros */
+/** @}*/ /* PASAHO_insert_msg_count_command_macros */
#ifdef __cplusplus
#endif
#endif /* _PASAHO_H */
-
-
-
-
-