2016-03-18 |
Suraj Das | final fix for IR SDOCM00121575 |
tree | commitdiff |
2016-03-17 |
Aravind Batni | Merge branch 'master' of gtgit01.gt.design.ti.com:git... |
tree | commitdiff |
2016-03-17 |
Aravind Batni | fix typo in RTSC cfg file devType to socType |
tree | commitdiff |
2016-03-17 |
Suraj Das | Adding i2c to A15 examples using board for k2e pcie |
tree | commitdiff |
2016-03-17 |
Aravind Batni | fix application RTSC cfg file to include i2c for board |
tree | commitdiff |
2016-03-17 |
Mahesh Radhakrishnan | Merge branch 'master' of gtgit01.gt.design.ti.com:git... |
tree | commitdiff |
2016-03-17 |
Mahesh Radhakrishnan | Adding I2C to A15 examples |
tree | commitdiff |
2016-03-17 |
Suraj Das | Adding i2c to A15 examples using board for k2e |
tree | commitdiff |
2016-03-16 |
Mahesh Radhakrishnan | Including I2C to the k2g a15 examples using board library |
tree | commitdiff |
2016-03-15 |
John Dowdal | sdocm 00121706: exception due to bad pcie data address |
tree | commitdiff |
2016-03-15 |
Suraj Das | fix for IR SDOCM00121689 |
tree | commitdiff |
2016-03-12 |
Suraj Das | fix for IR SDOCM00121575 version 2 |
tree | commitdiff |
2016-03-11 |
Suraj Das | fix for IR SDOCM00121575 |
tree | commitdiff |
2016-03-11 |
Suraj Das | copyright and crucible review updates |
tree | commitdiff |
2016-03-05 |
Suraj Das | needed changes for running k2e arm projects |
tree | commitdiff |
2016-03-05 |
Suraj Das | EDMA code clean & removed redundant files |
tree | commitdiff |
2016-03-04 |
Suraj Das | modified edma address range on all arm projects |
tree | commitdiff |
2016-03-04 |
Suraj Das | fixed file-names in all the project.txt files |
tree | commitdiff |
2016-03-04 |
Suraj Das | Changing the project name for k2g |
tree | commitdiff |
2016-03-04 |
John Dowdal | remove board from k2x for c66 as it doesn't use uart... |
tree | commitdiff |
2016-03-03 |
John Dowdal | add soclib/soc file to all projects, and k2x arm projects |
tree | commitdiff |
2016-03-03 |
John Dowdal | remove gpio_osal |
tree | commitdiff |
2016-03-03 |
John Dowdal | clean warnings |
tree | commitdiff |
2016-03-03 |
John Dowdal | remove gen2 for am57x |
tree | commitdiff |
2016-03-03 |
John Dowdal | use gpio to remove reset signal from bus so 3p cards... |
tree | commitdiff |
2016-03-02 |
John Dowdal | Merge branch 'pcie_gpioReset' |
tree | commitdiff |
2016-03-02 |
John Dowdal | Merge XBAR cleanup |
tree | commitdiff |
2016-03-02 |
Kiran, Madana Jyothi | PCIE: Use CSL xbar API to perform crossbar configuration |
tree | commitdiff |
2016-03-02 |
John Dowdal | Merge branch 'm4' |
tree | commitdiff |
2016-03-02 |
John Dowdal | K2G works with ARM and DSP using EDMA and CPU |
tree | commitdiff |
2016-02-26 |
Suraj Das | Enabling EDMA changes on all projects |
tree | commitdiff |
2016-02-26 |
John Dowdal | k2g hand merge works |
tree | commitdiff |
2016-02-22 |
John Dowdal | am5x changes broke v0 hw (k1/k2) : sdocm00121387 |
tree | commitdiff |
2016-02-16 |
John Dowdal | make m4 work |
tree | commitdiff |
2016-02-10 |
Benjamin Jayakumar | Updated based on Review feedback |
tree | commitdiff |
2016-01-28 |
Benjamin Jayakumar | Code fix for GPIO reset |
tree | commitdiff |
2016-01-28 |
Benjamin Jayakumar | Fix code for GPIO |
tree | commitdiff |
2016-01-28 |
Benjamin Jayakumar | Added AM572x PCIe Reset - PCIE_PERSTn using GPIO |
tree | commitdiff |
2016-01-20 |
Kiran, Madana Jyothi | PCIE: Cleanup of sys bios config files of AM572x |
tree | commitdiff |
2016-01-20 |
Kiran, Madana Jyothi | PCIE: Cleanup of sys bios config files of AM571x |
tree | commitdiff |
2016-01-11 |
Kiran, Madana Jyothi | PCIE: Update example source file to support M4 |
tree | commitdiff |
2016-01-11 |
Kiran, Madana Jyothi | PCIE: Update board specific file to support M4 |
tree | commitdiff |
2016-01-11 |
Kiran, Madana Jyothi | PCIE: Add new project text and config files to support M4 |
tree | commitdiff |
2015-12-11 |
Suraj Das | added task module into .cfg files for task hooks |
tree | commitdiff |
2015-12-10 |
Suraj Das | enabling benchmarking on pcie |
tree | commitdiff |
2015-12-04 |
John Dowdal | SDOCM00119656: replace delay function with one that... |
tree | commitdiff |
2015-11-30 |
John Dowdal | Merge branch 'master' of gtgit01.gt.design.ti.com:git... |
tree | commitdiff |
2015-11-30 |
John Dowdal | SDOCM00119119 add missing registers PM/MSI and remove... |
tree | commitdiff |
2015-11-30 |
John Dowdal | add sections for pinmux (needs to be internal) |
tree | commitdiff |
2015-11-24 |
Eric Ruei | pcie_sample.c: cleanup for K1 device support |
tree | commitdiff |
2015-11-12 |
Hao Zhang | pcie: example: revert PCIE_logPrintf back to System_printf |
tree | commitdiff |
2015-11-04 |
Suraj Das | Klocwork/Misra-C fixes |
tree | commitdiff |
2015-10-19 |
Aravind Batni | added CCS project files for C6678 and C6657 |
tree | commitdiff |
2015-09-17 |
Aravind Batni | rename Example Project to align to boardName_cpu name... |
tree | commitdiff |
2015-09-17 |
Aravind Batni | updated library search path to have BIOS search path... |
tree | commitdiff |
2015-09-15 |
John Dowdal | remove hack for bad csl defines |
tree | commitdiff |
2015-09-15 |
John Dowdal | Set up 2 projects per device/core, one that uses soc... |
tree | commitdiff |
2015-09-08 |
John Dowdal | sync with latest device library implementation from... |
tree | commitdiff |
2015-08-31 |
John Dowdal | clean some comments and add #ifdef example for gen... |
tree | commitdiff |
2015-08-27 |
John Dowdal | Merge branch 'releases/PROCESSOR-SDK.01.00.00' of gtgit... |
tree | commitdiff |
2015-08-27 |
John Dowdal | Use board_init where applicable, send printf() to uart... |
tree | commitdiff |
2015-08-20 |
John Dowdal | Merge remote-tracking branch 'origin' into releases... |
tree | commitdiff |
2015-08-20 |
John Dowdal | add msi/legacy interrupts to example, and add fast... |
tree | commitdiff |
2015-07-14 |
Aravind Batni | applied patch to fix k2e compilation issues DEV.PCIE_LLD.02.01.00.02 |
tree | commitdiff |
2015-07-09 |
Aravind Batni | updated the patch for SDOCM00114000-fix |
tree | commitdiff |
2015-05-29 |
Eric Ruei | Am57xx C66 example: use device-independent library |
tree | commitdiff |
2015-05-18 |
John Dowdal | both am571x and am572x work |
tree | commitdiff |
2015-05-13 |
John Dowdal | am572x a15 and c66 projects work |
tree | commitdiff |
2015-05-11 |
John Dowdal | sync to latest csl |
tree | commitdiff |
2015-05-11 |
John Dowdal | dsp example works on am572x |
tree | commitdiff |
2015-04-09 |
John Dowdal | refactor for v0/v1 and run on k2h |
tree | commitdiff |
2014-02-21 |
Eric Ruei | add K2E Serdes support DEV.PCIE_LLD.02.01.00.00 |
tree | commitdiff |
2014-01-29 |
Raghu Nambiath | Update to PCIe example to use SERDES configuration... |
tree | commitdiff |
2013-10-03 |
John Dowdal | add k2e and k2l |
tree | commitdiff |
2013-01-30 |
John Dowdal | fix Pcie_setMode so it doesn't depend on device |
tree | commitdiff |
2013-01-30 |
John Dowdal | remove requirement for cslr_device.h by using a device... |
tree | commitdiff |
2013-01-29 |
Raghu Nambiath | Update for SERDES configuration. Commit after board... |
tree | commitdiff |
2012-10-16 |
Murtaza Gaadiwala | Temporary workaround to fix PCIE errors as LLD is using... DEV.PCIE_LLD.02.00.00.03 |
tree | commitdiff |
2012-10-16 |
Murtaza Gaadiwala | Renaming device directories and adding Hawking (TCI6636... |
tree | commitdiff |
2012-07-27 |
Martin Qian | Commited by migration script DEV.PCIE_LLD.02.00.00.02 |
tree | commitdiff |
2012-07-25 |
Martin Qian | Commited by migration script DEV.PCIE_LLD.02.00.00.01 |
tree | commitdiff |
2012-07-22 |
Martin Qian | initial commit |
tree | commitdiff |
2012-07-03 |
Martin Qian | initial commit |
tree | commitdiff |
|