rm: keystone 2: add A15 library build for Keystone II devices.
[keystone-rtos/rm-lld.git] / package.bld
1 /******************************************************************************\r
2  * FILE PURPOSE: Build description for the RM Package\r
3  ******************************************************************************\r
4  * FILE NAME: package.bld\r
5  *\r
6  * DESCRIPTION: \r
7  *  This file contains the build specification and description for the RM\r
8  *  \r
9  *  The file takes the following parameters from the command line through the\r
10  *  XDCARGS variable.\r
11  *      XDCARGS[0] = RM Install Type \r
12  *      Valid Values are "TAR" or "SETUP"\r
13  *      DEFAULT is "SETUP"\r
14  *\r
15  *  Example for a valid command:\r
16  *      xdc XDCARGS="SETUP" release   \r
17  *\r
18  * Copyright (C) 2012-2015, Texas Instruments, Inc.\r
19  *****************************************************************************/\r
20 \r
21 /* List of all subdirectories that combine to make the RM Package. */\r
22 var subDirectories = ["src", "docs", "device", "include", "test", "util"];\r
23 \r
24 /* Generate rmver.h */\r
25 var tplt = xdc.loadTemplate("./rmver.h.xdt");\r
26 tplt.genFile("./rmver.h",lldReleaseVersion);   \r
27 \r
28 /* Determine if we need to create the InstallJammer Application or not? \r
29  * RM Deliverables be either of the following formats:\r
30  *  - TAR Ball Package\r
31  *  - Setup Executable \r
32  * DEFAULT is a TAR Executable. */\r
33 \r
34 if ((arguments[0] != "TAR") && (arguments[0] != "SETUP"))\r
35     lldInstallType = "TAR";\r
36 else\r
37     lldInstallType = arguments[0];\r
38 \r
39 /* Irrespective of the InstallType we always create a TAR Ball Package as a part\r
40  * of the RTSC Build. Here we determine the name of the TAR Ball Package\r
41  *  Format is as follows:\r
42  *      lld_<version> */\r
43 var lldRTSCFileName = "rm" + "_" + lldPartNumber + "_" +\r
44                       lldReleaseVersion[0] + "_" +  lldReleaseVersion[1] + "_" + \r
45                       lldReleaseVersion[2]  + "_" + lldReleaseVersion[3];\r
46 \r
47 /******************************************************************\r
48  ************************ Release Banner **************************\r
49  ******************************************************************/\r
50 \r
51 print ("*************** RM Build Information ****************");\r
52 print ("RM Install                 : " + lldInstallType);\r
53 print ("RM Version                 : " + lldReleaseVersion);\r
54 print ("C66 Tools Directory        : " + c66ToolsBaseDir);\r
55 print ("M4 Tools Directory         : " + m4ToolsBaseDir);\r
56 print ("A15 Tools Directory        : " + a15ToolsBaseDir);\r
57 print ("RTSC File Name             : " + lldRTSCFileName);\r
58 print ("RM Path                    : " + lldPath);\r
59 print ("Coverity Analysis          : " + (coverityAnalysis == "ON" ? "ON" : "OFF"));\r
60 print ("CC LE opts                 : " + C66LE.ccOpts.prefix);\r
61 print ("CC BE opts                 : " + C66BE.ccOpts.prefix);\r
62 print ("M4 LE opts                 : " + M4LE.ccOpts.prefix);\r
63 print ("A15 basic opts             : " + A15LE.ccOpts.prefix);\r
64 print ("***********************************************************");\r
65 \r
66 /* Create the release package for the RM */\r
67 Pkg.defaultRelease = Pkg.addRelease (lldRTSCFileName, {prefix: "./packages/"});\r
68 \r
69 /* Moving forward we need to set the Archiver of the package to be ZIP. This is currently\r
70  * not supported in the XDC tools being used. Currenly builds need to be done with the \r
71  * following options:-\r
72  *   xdc MK_FIXLISTOPTS=-t release \r
73  * ZIP is a better option as it works natively with INSTALL Jammer and we can remove the\r
74  * uncompression into a temporary directory. XDC Tools with xdc-rXX support the ZIP archiver. */\r
75 //Pkg.attrs = {archiver : "zip"};\r
76 \r
77 /* Cycle through all the sub-directories and build all the files */\r
78 for (var i = 0; i < subDirectories.length; i++) \r
79 {\r
80     /* Load the capsule in the sub directory. */\r
81     var caps = xdc.loadCapsule (subDirectories[i]+"/Module.xs");\r
82 \r
83     print ("Building directory " + subDirectories[i]);\r
84 \r
85     /* Build the capsule. */\r
86     caps.modBuild();\r
87 \r
88     /* Package the module.xs files for building via package */\r
89     Pkg.otherFiles[Pkg.otherFiles.length++] = subDirectories[i]+"/Module.xs";\r
90 }\r
91 \r
92 /* Package the remaining files */\r
93 Pkg.otherFiles[Pkg.otherFiles.length++] = "config.bld";\r
94 Pkg.otherFiles[Pkg.otherFiles.length++] = "package.bld";\r
95 Pkg.otherFiles[Pkg.otherFiles.length++] = "package.xdc";\r
96 Pkg.otherFiles[Pkg.otherFiles.length++] = "Settings.xdc";\r
97 Pkg.otherFiles[Pkg.otherFiles.length++] = "Settings.xdc.xdt";\r
98 Pkg.otherFiles[Pkg.otherFiles.length++] = "rm.h";\r
99 Pkg.otherFiles[Pkg.otherFiles.length++] = "rm_services.h";\r
100 Pkg.otherFiles[Pkg.otherFiles.length++] = "rm_transport.h";\r
101 Pkg.otherFiles[Pkg.otherFiles.length++] = "rm_server_if.h";\r
102 Pkg.otherFiles[Pkg.otherFiles.length++] = "rm_osal.h";\r
103 Pkg.otherFiles[Pkg.otherFiles.length++] = "rmver.h";\r
104 Pkg.otherFiles[Pkg.otherFiles.length++] = "rmver.h.xdt";\r
105 Pkg.otherFiles[Pkg.otherFiles.length++] = "docs/Doxyfile";\r
106 Pkg.otherFiles[Pkg.otherFiles.length++] = "docs/doxyfile.xdt";\r
107 Pkg.otherFiles[Pkg.otherFiles.length++] = "build/buildlib.xs";\r
108 Pkg.otherFiles[Pkg.otherFiles.length++] = "makefile";\r
109 Pkg.otherFiles[Pkg.otherFiles.length++] = "makefile_armv7";\r
110 Pkg.otherFiles[Pkg.otherFiles.length++] = "build/armv7/librm_aearmv7.mk";\r
111 \r
112 /* Generate Users Manual Doxyfile */\r
113 var tplt = xdc.loadTemplate("./docs/doxyfile.xdt");\r
114 tplt.genFile("./docs/Doxyfile",lldReleaseVersion); \r
115 \r
116 /* Generate Settings.xdc */\r
117 var tplt = xdc.loadTemplate("./Settings.xdc.xdt");\r
118 tplt.genFile("./Settings.xdc",lldReleaseVersion); \r
119 \r
120 /* Check if we need to create the mini package? */\r
121 var miniBuild = java.lang.System.getenv("MINI_PACKAGE");\r
122 \r
123 if (miniBuild == "ON")\r
124 {\r
125     /***************************************************************************\r
126      ********************************* MINI Package ****************************\r
127      ***************************************************************************/\r
128     /* Create the MINI RTSC Package */\r
129     var libUtility = xdc.loadCapsule ("build/buildlib.xs");\r
130     libUtility.createMiniPkg(lldRTSCFileName);\r
131 }\r
132 \r
133 /********************************************************************* \r
134  *********************** INSTALL-JAMMER Support **********************\r
135  * In order to create the InstallJammer Application; we need to UNTAR\r
136  * the package into a temporary directory. This is required because \r
137  * currently the InstallJammer does not support the TAR Files and thus\r
138  * creating an UNTAR of the file. So to work-around the problem we will\r
139  * do the following in the EPILOGUE Section:-\r
140  *  (a) Create a temporary directory called 'tmp'\r
141  *  (b) UNTAR the package into 'tmp'\r
142  *  (c) Run the INSTALL Jammer on 'tmp'\r
143  *  (d) Remove the 'tmp' directory.\r
144  *\r
145  * This can be done only after the 'release' package has been created.\r
146  * Thus all of this work is being done in the EPILOGUE.\r
147  *********************************************************************/\r
148 if (lldInstallType == "SETUP")\r
149 {\r
150     /* Create the Install Jammer Version Variable. This is used inside the \r
151      * MPI File to create the Final executable. \r
152      *  The format supported is as follows:-\r
153      *   - setupwin32_rm_<part_number>_<version>.exe \r
154      *      This is for RM Libraries and Header files\r
155      */\r
156     var InstallJammerVersion = "-DVersion " + lldPartNumber + "_" + lldReleaseVersion[0] + "_" +\r
157                                lldReleaseVersion[1] + "_" +  lldReleaseVersion[2]  + "_" + lldReleaseVersion[3];\r
158 \r
159     /* This is the location where the tmp directory is located; this is used as \r
160      * the input directory for the Install Jammer. */ \r
161     var PackageBaseDir = " -DPackageBaseDir " + lldPath + "./tmp";\r
162 \r
163     /* This is the location where the RM will be installed by default. */\r
164     var WinInstallDir = " -DWinInstallDir C:/ti/rm" + "_" + \r
165                             lldPartNumber + "_" + \r
166                             lldReleaseVersion[0] + "_" +  lldReleaseVersion[1] + "_" +  \r
167                             lldReleaseVersion[2]  + "_" + lldReleaseVersion[3];\r
168 \r
169     /* Create the actual EPILOGUE Section for the INSTALLER */\r
170     Pkg.makeEpilogue += "release: install_application\n";\r
171     Pkg.makeEpilogue += "install_application:\n";\r
172     Pkg.makeEpilogue += "\t @echo -------------------------------------------------------\n";\r
173     Pkg.makeEpilogue += "\t @echo Creating the Install\n";\r
174     Pkg.makeEpilogue += "\t @echo -------------------------------------------------------\n";\r
175     Pkg.makeEpilogue += "\t -$(MKDIR) tmp\n";\r
176     Pkg.makeEpilogue += "\t -$(MKDIR) tmp/packages\n";\r
177     Pkg.makeEpilogue += "\t -$(MKDIR) tmp/eclipse\n";\r
178     Pkg.makeEpilogue += "\t -$(CP) -R eclipse tmp\n";\r
179     Pkg.makeEpilogue += "\t tar -xf ./packages/" + lldRTSCFileName + ".tar" + " -Ctmp/packages \n";\r
180     Pkg.makeEpilogue += "\t installjammer " + InstallJammerVersion + PackageBaseDir + WinInstallDir + \r
181                         " --output-dir packages/ --build install/rm.mpi\n";\r
182     Pkg.makeEpilogue += "\t -$(RMDIR) /S /Q tmp\n\n";\r
183 }\r
184 \r
185 /* We need to clean after ourselves; extend the 'clean' target to take care of this. */\r
186 Pkg.makeEpilogue += "clean::\n";\r
187 Pkg.makeEpilogue += "\t -$(RM) docs/Doxyfile Settings.xdc rmver.h\n";\r
188 Pkg.makeEpilogue += "\t -$(RM) makefile\n";\r
189 Pkg.makeEpilogue += "\t -$(RMDIR) docs/doxygen\n";\r
190 if (lldInstallType == "SETUP")\r
191 {\r
192     Pkg.makeEpilogue += "\t -$(RM) packages/*.exe\n";\r
193     Pkg.makeEpilogue += "\t -$(RM) packages/*.bin\n";\r
194     Pkg.makeEpilogue += "\t -$(RMDIR) eclipse\n\n";\r
195 }\r
196 if (miniBuild == "ON")\r
197 {\r
198     Pkg.makeEpilogue += "\t -$(RM) simpleC66LE.mak\n";\r
199     Pkg.makeEpilogue += "\t -$(RM) simpleC66BE.mak\n";\r
200 }\r