69775ea8c6eb7175c9ef4a04e7439a5e96a943a9
1 /**
2 * @file rm.h
3 *
4 * @brief
5 * This is the Resource Manager include file.
6 *
7 * \par
8 * ============================================================================
9 * @n (C) Copyright 2012, Texas Instruments, Inc.
10 *
11 * Redistribution and use in source and binary forms, with or without
12 * modification, are permitted provided that the following conditions
13 * are met:
14 *
15 * Redistributions of source code must retain the above copyright
16 * notice, this list of conditions and the following disclaimer.
17 *
18 * Redistributions in binary form must reproduce the above copyright
19 * notice, this list of conditions and the following disclaimer in the
20 * documentation and/or other materials provided with the
21 * distribution.
22 *
23 * Neither the name of Texas Instruments Incorporated nor the names of
24 * its contributors may be used to endorse or promote products derived
25 * from this software without specific prior written permission.
26 *
27 * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
28 * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
29 * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
30 * A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
31 * OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
32 * SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
33 * LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
34 * DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
35 * THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
36 * (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
37 * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
38 *
39 * \par
40 */
42 #ifndef RM_H_
43 #define RM_H_
45 #ifdef __cplusplus
46 extern "C" {
47 #endif
49 /* RM version */
50 #include <ti/drv/rm/rmver.h>
52 /** @mainpage Resource Manager
53 *
54 * @section intro Introduction
55 *
56 * The Resource Manager low level driver (RM LLD) is designed to provide initialization and permissions checking
57 * for LLD resources. A system integrator can specify DSP permissions for LLD resources within the system.
58 * The resource permissions are stored in the RM LLD and used to validate resource requests from supported LLDs.
59 * Currently, the RM LLD supports permissions for the following LLDs
60 * - QMSS
61 * - CPPI
62 * - PA
63 * For information on the specific resources supported with each LLD please see @ref RM_LLD_RESOURCE_TABLE.
64 *
65 * The system integrator must specify the supported LLD resource permissions for all DSPs prior to compile time.
66 * An array of @ref Rm_Resource objects must be created. Each @ref Rm_Resource entry in the array specifies
67 * a resource type, start and end range for the resource, and the initialization and usage permissions for the
68 * resource for each DSP. For an example resource table definitions please see the @ref rmResourceTable array
69 * defined in the resource_table\ directory. This resource table assigns full initialization and usage permissions
70 * to all DSPs for all supported resources. Please note that the resouce table must start with the
71 * @ref RM_RESOURCE_MAGIC_NUMBER entry and end with the @ref RM_RESOURCE_FINAL_ENTRY. These
72 * first and last entries are used the RM LLD to validate and parse the resource table.
73 *
74 * The RM LLD must be initialized and started prior to all supported LLD initialization and start routines. The
75 * @ref Rm_init function should be invoked, and passed a pointer to the integrator defined resource table, on the
76 * master DSP core in the system. All other DSP cores should invoke the @ref Rm_start API. The @ref Rm_init
77 * function first initializes the internal permission tables to deny all DSPs access to all resources. Next the
78 * @ref Rm_init function parses the resource table provided and copies all specified permissions into the internal
79 * tables. When the permission transfer completes the @ref Rm_init function writes a global synchronization
80 * object which the @ref Rm_start functions are spinning on. The slave cores that have invoked @ref Rm_start
81 * will stop spinning once the global synchronization has been written. At this time @ref Rm_start will invalidate
82 * all internal permission tables so that no further cache invalidate operations need to be performed when
83 * checking resource permissions in the data path. The upfront cache invalidate operation is possible because
84 * the RM LLD does not allow dynamic resource permission modifications. The permissions defined by the system
85 * integrator and loaded during RM initialization are static throughout the system up-time.
86 *
87 * The RM LLD must be registered with a supported LLD in order for the supported LLD to perform resource
88 * permission checks. If the RM LLD is not registered with a supported LLD the LLD will operate as if the RM LLD
89 * is not there. This maintains full backwards compatability with existing applications not using the RM LLD. In order
90 * to register the RM LLD with supported LLDs the following steps should be taken
91 * - Get a @ref Rm_Handle via the @ref Rm_getHandle API on each DSP that uses the RM LLD.
92 * - Register the RM LLD with the supported LLDs by passing the @ref Rm_Handle to the
93 * LLD's <<LLD name>>_startCfg API. Again, this should be performed on all DSP cores using the RM LLD.
94 * Note: The master core for the QMSS LLD should have the @ref Rm_Handle registered via the Qmss_init API.
95 * After registering the RM LLD with supported LLDs all supported LLD resources covered by the RM LLD will invoke
96 * permission check callouts to the RM. A permission denied or approved response will be given back to the
97 * invoking LLD based on the permissions stored in the RM LLD for the resource.
98 *
99 * All internal RM LLD permission tables are placed into a single memory section called ".rm". This memory section
100 * MUST be placed in shared memory (MSMC or DDR). The permission tables are shared between all DSPs utilizing
101 * the RM LLD.
102 *
103 * In summary, the initialization flow if the RM LLD is to be utilized should look like the following:
104 *
105 * Master DSP Core:
106 * - Call @ref Rm_init passing in the system integrator defined resource table
107 * - Call @ref Rm_getHandle
108 * - Call supported LLD _init or _create functions (for QMSS pass the @ref Rm_Handle inside the
109 * Qmss_GlobalConfigParams structure)
110 * - Call supported LLD _startCfg functions passing the @ref Rm_Handle as an argument
111 *
112 * Slave DSP Cores:
113 * - Call @ref Rm_start
114 * - Call @ref Rm_getHandle
115 * - Call supported LLD _start functions (if supported)
116 * - Call supported LLD _startCfg functions passing the @ref Rm_Handle as an argument
117 *
118 */
120 /* Define RM_LLD_API as a master group in Doxygen format and add all RM LLD API
121 definitions to this group. */
122 /** @defgroup RM_LLD_API RM LLD Module API
123 * @{
124 */
125 /** @} */
127 /**
128 @defgroup RM_TRANSPORT_API RM Transport-Layer API
129 @ingroup RM_LLD_API
130 */
131 /**
132 @defgroup RM_SERVICES_API RM Registered Component Services API
133 @ingroup RM_LLD_API
134 */
135 /**
136 @defgroup RM_POLICY_API RM Policy modification API
137 @ingroup RM_LLD_API
138 */
140 /**
141 * @brief Maximum number of characters in a RM instance name
142 */
143 #define RM_INSTANCE_NAME_MAX_CHARS (24)
145 /**
146 * @brief RM Handle provided to application. The RM Handle is used by the
147 * application to distinquish between different RM instances running on
148 * the same core.
149 */
150 typedef void *Rm_Handle;
152 /**
153 * @brief RM Instance types
154 */
155 typedef enum {
156 /** RM Server */
157 Rm_instType_SERVER = 0,
158 /** RM Client Delegate */
159 Rm_instType_CLIENT_DELEGATE,
160 /** RM Client */
161 Rm_instType_CLIENT
162 } Rm_InstType;
164 /**
165 * @brief RM instance initialization structure
166 */
167 typedef struct {
168 /** Pointer to RM instance name character array. The name of the RM instance must
169 * be reflected exactly in the initial RM policies provided to the RM
170 * tree's Servers and Client Delegates. The RM instance name is
171 * used by the policy to map which instances are allowed defined
172 * privileges */
173 char *instName;
174 /** RM instance type. Defines whether the RM instance will be initialized
175 * as a RM Server, Client Delegate, or Client */
176 Rm_InstType instType;
177 /** [Server Parameter] Pointer to the device-wide resource list. The list
178 * contains all resources available on the device available for
179 * allocation. Servers running on ARM-Linux cores provide a subset
180 * of the global device list for allocation. The subset is formed from
181 * the global resources leftover after the Linux DTB is parsed for
182 * resources reserved by Linux.
183 *
184 * Note: This parameter will be ignored when the instance type is either
185 * Client Delegate or Client */
186 void *globalResourceList;
187 /** [Server Parameter When Running on ARM Linux] Pointer to the Linux DTB.
188 * The Linux DTB will be parsed for all tracked resources reserved for use
189 * by Linux.
190 *
191 * Note: This parameter will be ignored when the instance type is either
192 * Client Delegate or Client */
193 void *linuxDtb;
194 /** [Server/Client Delegate Paramter] Pointer to the startup allocation
195 * policy. RM Servers should be initialized with the global policy
196 * listing for all RM instances within the system. RM Client Delegates
197 * can be initialized with their local policy, must be a subset of the
198 * global policy provided to the Client Delegate's Server.
199 *
200 * Note: The core charged with the task of initializing the BIOS and IPC
201 * components must run an RM Client Delegate with an initial policy
202 * that allocates a system timer to BIOS and a HW semaphore to IPC
203 *
204 * Note: This parameter will be ignored when the instance type is a
205 * Client
206 */
207 void *startupPolicy;
208 } Rm_InitCfg;
210 /**
211 * @b Description
212 * @n
213 * This function initializes a RM instance.
214 *
215 * IMPORTANT: Rm_init must be called prior to any other component startup
216 * APIs (BIOS_start, Ipc_start, etc).
217 *
218 * @param[in] *initCfg
219 * Pointer to structure containing the initialization information for
220 * this RM instance.
221 *
222 * @retval
223 * Success - non-zero Rm_Handle returned.
224 * @retval
225 * Failure - NULL Rm_handle returned.
226 */
227 Rm_Handle Rm_init(Rm_InitCfg *initCfg);
229 /**
230 * @b Description
231 * @n
232 * The function is used to get the version information of the RM.
233 *
234 * @retval
235 * Version Information.
236 */
237 uint32_t Rm_getVersion (void);
239 /**
240 * @b Description
241 * @n
242 * The function is used to get the version string for the RM.
243 *
244 * @retval
245 * Version String.
246 */
247 const char* Rm_getVersionStr (void);
249 #ifdef __cplusplus
250 }
251 #endif
253 #endif /* RM_H_ */