]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - keystone-rtos/rm-lld.git/blob - rm_osal.h
update queues 4095/8191/12287/16383 to use "iue" instead of "u" permission per review...
[keystone-rtos/rm-lld.git] / rm_osal.h
1 /**
2  *   @file  rm_osal.h
3  *
4  *   @brief   
5  *      This is the sample OS Adaptation layer which is used by the Resource
6  *      Manager. The OSAL layer can be ported in either of the following
7  *      manners to a native OS:
8  *
9  *      <b> Approach 1: </b>
10  *      @n  Use Prebuilt Libraries
11  *           - Ensure that the provide an implementation of all
12  *             Osal_XXX API for their native OS.
13  *           - Link the prebuilt libraries with their application.
14  *           - Refer to the "example" directory for an example of this
15  *       @n <b> Pros: </b>
16  *           - Customers can reuse prebuilt TI provided libraries
17  *       @n <b> Cons: </b>
18  *           - Level of indirection in the API to get to the actual OS call
19  *
20  *      <b> Approach 2: </b>
21  *      @n  Rebuilt Library 
22  *           - Create a copy of this file and modify it to directly 
23  *             inline the native OS calls
24  *           - Rebuild the RM low level drivver library; ensure that the Include
25  *             path points to the directory where the copy of this file
26  *             has been provided.
27  *           - Please refer to the "test" directory for an example of this
28  *       @n <b> Pros: </b>
29  *           - Optimizations can be done to remove the level of indirection
30  *       @n <b> Cons: </b>
31  *           - RM LLD Libraries need to be rebuilt by the customer.
32  *
33  *  \par
34  *  NOTE:
35  *      (C) Copyright 2012-2015 Texas Instruments, Inc.
36  * 
37  *  Redistribution and use in source and binary forms, with or without
38  *  modification, are permitted provided that the following conditions
39  *  are met:
40  *
41  *    Redistributions of source code must retain the above copyright
42  *    notice, this list of conditions and the following disclaimer.
43  *
44  *    Redistributions in binary form must reproduce the above copyright
45  *    notice, this list of conditions and the following disclaimer in the
46  *    documentation and/or other materials provided with the
47  *    distribution.
48  *
49  *    Neither the name of Texas Instruments Incorporated nor the names of
50  *    its contributors may be used to endorse or promote products derived
51  *    from this software without specific prior written permission.
52  *
53  *  THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
54  *  "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
55  *  LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
56  *  A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
57  *  OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
58  *  SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
59  *  LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
60  *  DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
61  *  THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
62  *  (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
63  *  OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
64  *
65  *  \par
66 */
67 #ifndef RM_OSAL_H_
68 #define RM_OSAL_H_
70 /** @addtogroup RM_OSAL_API
71  @{
72  */
74 /**********************************************************************
75  ************************* Extern Declarations ************************
76  **********************************************************************/
78 extern void *Osal_rmMalloc (uint32_t num_bytes);
79 extern void  Osal_rmFree (void *ptr, uint32_t size);
80 extern void *Osal_rmCsEnter (void);
81 extern void  Osal_rmCsExit (void *CsHandle);
82 extern void *Osal_rmMtCsEnter (void *mtSemObj);
83 extern void  Osal_rmMtCsExit (void *mtSemObj, void *CsHandle);
84 extern void  Osal_rmBeginMemAccess (void *ptr, uint32_t size);
85 extern void  Osal_rmEndMemAccess (void *ptr, uint32_t size);
86 extern void *Osal_rmTaskBlockCreate (void);
87 extern void  Osal_rmTaskBlock (void *handle);
88 extern void  Osal_rmTaskUnblock (void *handle);
89 extern void  Osal_rmTaskBlockDelete (void *handle);
90 extern void  Osal_rmLog (char *fmt, ... );
92 /**
93  * @brief   The macro is used by RM to allocate memory of specified
94  *          size
95  *
96  * <b> Prototype: </b>
97  *  The following is the C prototype for the expected OSAL API.
98  *
99  *  @verbatim
100  *     void* Osal_rmMalloc (uint32_t numBytes)
101  *  @endverbatim
102  *
103  *  <b> Parameter </b>
104  *  @n  Number of bytes to be allocated
105  *
106  *  <b> Return Value </b>
107  *  @n  Pointer to the allocated block size
108  */
109 #define Rm_osalMalloc             Osal_rmMalloc
111 /**
112  * @brief   The macro is used by RM to free a allocated block of 
113  *          memory 
114  *
115  * <b> Prototype: </b>
116  *  The following is the C prototype for the expected OSAL API.
117  *
118  *  @verbatim
119  *     void Osal_rmFree (void *ptr, uint32_t size)
120  *  @endverbatim
121  *
122  *  <b> Parameter </b>
123  *  @n  Pointer to the block of memory to be cleaned up.
124  *  @n  Size of the allocated memory which is being freed.
125  *
126  *  <b> Return Value </b>
127  *  @n  Not applicable.
128  */
129 #define Rm_osalFree               Osal_rmFree
131 /**
132  * @brief   The function is used to enter a critical section.
133  *          Function protects against 
134  *
135  *          access from multiple cores 
136  *          and 
137  *          access from multiple threads on single core
138  *
139  * <b> Prototype: </b>
140  *  The following is the C prototype for the expected OSAL API.
141  *
142  *  @verbatim
143  *     void *Osal_rmCsEnter (void)
144  *  @endverbatim
145  *
146  *  <b> Parameter </b>
147  *  @n  Not applicable.
148  *
149  *  <b> Return Value </b>
150  *  @n  Handle used to lock critical section
151  */
152 #define Rm_osalCsEnter            Osal_rmCsEnter
154 /**
155  * @brief   The function is used to exit a critical section
156  *          protected using Osal_rmCsEnter() API.
157  *
158  * <b> Prototype: </b>
159  *  The following is the C prototype for the expected OSAL API.
160  *
161  *  @verbatim
162  *     void Osal_rmCsExit (void *CsHandle)
163  *  @endverbatim
164  *
165  *  <b> Parameter </b>
166  *  @n  Handle for unlocking critical section.
167  *
168  *  <b> Return Value </b>
169  *  @n  Not applicable.
170  */
171 #define Rm_osalCsExit             Osal_rmCsExit
173 /**
174  * @brief   The function is used to enter a multi-threaded critical
175  *          section.  Function protects against
176  *
177  *          access from multiple threads on single core
178  *
179  * <b> Prototype: </b>
180  *  The following is the C prototype for the expected OSAL API.
181  *
182  *  @verbatim
183  *     void *Osal_rmMtCsEnter (void *mtSemObj)
184  *  @endverbatim
185  *
186  *  <b> Parameter </b>
187  *  @n  Multi-threaded critical section object handle.
188  *
189  *  <b> Return Value </b>
190  *  @n  Handle used to lock the multi-threaded critical section
191  */
192 #define Rm_osalMtCsEnter          Osal_rmMtCsEnter
194 /**
195  * @brief   The function is used to exit a multi-threaded critical
196  *          section protected using Osal_rmMtCsEnter() API.
197  *
198  * <b> Prototype: </b>
199  *  The following is the C prototype for the expected OSAL API.
200  *
201  *  @verbatim
202  *     void Osal_rmMtCsExit (void *mtSemObj, void *CsHandle)
203  *  @endverbatim
204  *
205  *  <b> Parameter </b>
206  *  @n  Multi-threaded critical section object handle.
207  *
208  *  <b> Parameter </b>
209  *  @n  Handle for unlocking multi-threaded critical section.
210  *
211  *  <b> Return Value </b>
212  *  @n  Not applicable.
213  */
214 #define Rm_osalMtCsExit           Osal_rmMtCsExit
216 /**
217  * @brief   The function is used to indicate that a block of memory is 
218  *          about to be accessed. If the memory block is cached then this 
219  *          indicates that the application would need to ensure that the 
220  *          cache is updated with the data from the actual memory.
221  *
222  * <b> Prototype: </b>
223  *  The following is the C prototype for the expected OSAL API.
224  *
225  *  @verbatim
226  *     void Osal_rmBeginMemAccess (void *ptr, uint32_t size)
227  *  @endverbatim
228  *
229  *  <b> Parameter </b>
230  *  @n  Address of memory block
231  *  @n  Size of memory block
232  *
233  *  <b> Return Value </b>
234  *  @n  Not applicable.
235  */
236 #define Rm_osalBeginMemAccess     Osal_rmBeginMemAccess
238 /**
239  * @brief   The function is used to indicate that the block of memory has
240  *          finished being accessed. If the memory block is cached then the
241  *          application would need to ensure that the contents of the cache
242  *          are updated immediately to the actual memory.
243  *
244  * <b> Prototype: </b>
245  *  The following is the C prototype for the expected OSAL API.
246  *
247  *  @verbatim
248  *     void Osal_rmEndMemAccess (void *ptr, uint32_t size)
249  *  @endverbatim
250  *
251  *  <b> Parameter </b>
252  *  @n  Address of memory block
253  *  @n  Size of memory block
254  *
255  *  <b> Return Value </b>
256  *  @n  Not applicable.
257  */
258 #define Rm_osalEndMemAccess       Osal_rmEndMemAccess
260 /**
261  * @brief   The macro is used by RM to create a task blocking
262  *          mechanism allowing a RM instance to block when it
263  *          has not been provided a service callback function
264  *          and it must send a packet to remote RM instance
265  *          to complete a service.
266  *
267  * <b> Prototype: </b>
268  *  The following is the C prototype for the expected OSAL API.
269  *
270  *  @verbatim
271  *     void *Osal_rmTaskBlockCreate (void)
272  *  @endverbatim
273  *
274  *  <b> Parameter </b>
275  *  @n  Not applicable.
276  *
277  *  <b> Return Value </b>
278  *  @n  Task blocking mechanism handle cast as a void pointer
279  */
280 #define Rm_osalTaskBlockCreate    Osal_rmTaskBlockCreate
282 /**
283  * @brief   The macro is used by a RM instance to block when it
284  *          has not been provided a service callback function
285  *          and it must send a packet to remote RM instance
286  *          to complete a service.  The blocking operation
287  *          should block the current RM instance's task/thread
288  *          from executing until a task/thread from which the
289  *          RM receive code runs unblocks the RM instance
290  *
291  * <b> Prototype: </b>
292  *  The following is the C prototype for the expected OSAL API.
293  *
294  *  @verbatim
295  *     void  Osal_rmTaskBlock (void *handle)
296  *  @endverbatim
297  *
298  *  <b> Parameter </b>
299  *  @n  Task blocking mechanism handle cast as a void pointer
300  *
301  *  <b> Return Value </b>
302  *  @n  Not applicable.
303  */
304 #define Rm_osalTaskBlock          Osal_rmTaskBlock
306 /**
307  * @brief   The macro is used by a RM instance to unblock from
308  *          a previous block operation.
309  *
310  * <b> Prototype: </b>
311  *  The following is the C prototype for the expected OSAL API.
312  *
313  *  @verbatim
314  *     void  Osal_rmTaskUnblock (void *handle)
315  *  @endverbatim
316  *
317  *  <b> Parameter </b>
318  *  @n  Task blocking mechanism handle cast as a void pointer
319  *
320  *  <b> Return Value </b>
321  *  @n  Not applicable.
322  */
323 #define Rm_osalTaskUnblock        Osal_rmTaskUnblock
325 /**
326  * @brief   The macro is used by a RM instance to delete its
327  *          task blocking mechanism.
328  *
329  * <b> Prototype: </b>
330  *  The following is the C prototype for the expected OSAL API.
331  *
332  *  @verbatim
333  *     void  Osal_rmTaskBlockDelete (void *handle)
334  *  @endverbatim
335  *
336  *  <b> Parameter </b>
337  *  @n  Task blocking mechanism handle cast as a void pointer
338  *
339  *  <b> Return Value </b>
340  *  @n  Not applicable.
341  */
342 #define Rm_osalTaskBlockDelete    Osal_rmTaskBlockDelete
344 /**
345  * @brief   The macro is used by RM to log various 
346  *          messages.
347  *
348  * <b> Prototype: </b>
349  *  The following is the C prototype for the expected OSAL API.
350  *
351  *  @verbatim
352  *     void Osal_rmLog( char *fmt, ... )
353  *  @endverbatim
354  *
355  *  <b> Parameter </b>
356  *  @n  printf-style format string 
357  *
358  *  <b> Return Value </b>
359  *  @n  Not applicable.
360  */
361 #define Rm_osalLog                Osal_rmLog
363 /**
364 @}
365 */
367 #endif /* RM_OSAL_H_ */