Cleaned up test code to show clear PASS/FAIL
[keystone-rtos/rm-lld.git] / rm_osal.h
1 /**
2  *   @file  rm_osal.h
3  *
4  *   @brief   
5  *      This is the sample OS Adaptation layer which is used by the Resource
6  *      Manager. The OSAL layer can be ported in either of the following 
7  *      manners to a native OS:
8  *
9  *      <b> Approach 1: </b>
10  *      @n  Use Prebuilt Libraries
11  *           - Ensure that the provide an implementation of all 
12  *             Osal_XXX API for their native OS.
13  *           - Link the prebuilt libraries with their application.
14  *           - Refer to the "example" directory for an example of this
15  *       @n <b> Pros: </b>
16  *           - Customers can reuse prebuilt TI provided libraries
17  *       @n <b> Cons: </b>
18  *           - Level of indirection in the API to get to the actual OS call
19  *              
20  *      <b> Approach 2: </b>
21  *      @n  Rebuilt Library 
22  *           - Create a copy of this file and modify it to directly 
23  *             inline the native OS calls
24  *           - Rebuild the RM low level drivver library; ensure that the Include 
25  *             path points to the directory where the copy of this file 
26  *             has been provided.
27  *           - Please refer to the "test" directory for an example of this 
28  *       @n <b> Pros: </b>
29  *           - Optimizations can be done to remove the level of indirection
30  *       @n <b> Cons: </b>
31  *           - RM LLD Libraries need to be rebuilt by the customer.
32  *
33  *  \par
34  *  NOTE:
35  *      (C) Copyright 2012-2013 Texas Instruments, Inc.
36  * 
37  *  Redistribution and use in source and binary forms, with or without 
38  *  modification, are permitted provided that the following conditions 
39  *  are met:
40  *
41  *    Redistributions of source code must retain the above copyright 
42  *    notice, this list of conditions and the following disclaimer.
43  *
44  *    Redistributions in binary form must reproduce the above copyright
45  *    notice, this list of conditions and the following disclaimer in the 
46  *    documentation and/or other materials provided with the   
47  *    distribution.
48  *
49  *    Neither the name of Texas Instruments Incorporated nor the names of
50  *    its contributors may be used to endorse or promote products derived
51  *    from this software without specific prior written permission.
52  *
53  *  THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS 
54  *  "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT 
55  *  LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
56  *  A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT 
57  *  OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, 
58  *  SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT 
59  *  LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
60  *  DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
61  *  THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT 
62  *  (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE 
63  *  OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
64  *
65  *  \par
66 */
67 #ifndef RM_OSAL_H_
68 #define RM_OSAL_H_
70 /** @addtogroup RM_OSAL_API
71  @{ 
72  */
74 /**********************************************************************
75  ************************* Extern Declarations ************************
76  **********************************************************************/
78 extern void *Osal_rmMalloc (uint32_t num_bytes);
79 extern void  Osal_rmFree (void *ptr, uint32_t size);
80 extern void *Osal_rmLocalGateEnter (void);
81 extern void  Osal_rmLocalGateLeave (void *localGateKey);
82 extern void  Osal_rmLog (char *fmt, ... );
84 /**
85  * @brief   The macro is used by RM to allocate memory of specified
86  *          size
87  *
88  * <b> Prototype: </b>
89  *  The following is the C prototype for the expected OSAL API.
90  *
91  *  @verbatim
92        void* Osal_rmMalloc (uint32_t numBytes)
93     @endverbatim
94  *      
95  *  <b> Parameter </b>
96  *  @n  Number of bytes to be allocated
97  *
98  *  <b> Return Value </b>
99  *  @n  Pointer to the allocated block size
100  */
101 #define Rm_osalMalloc             Osal_rmMalloc
103 /**
104  * @brief   The macro is used by RM to free a allocated block of 
105  *          memory 
106  *
107  * <b> Prototype: </b>
108  *  The following is the C prototype for the expected OSAL API.
109  *
110  *  @verbatim
111        void Osal_rmFree (void *ptr, uint32_t size)
112     @endverbatim
113  *      
114  *  <b> Parameter </b>
115  *  @n  Pointer to the block of memory to be cleaned up.
116  *  @n  Size of the allocated memory which is being freed.
117  *
118  *  <b> Return Value </b>
119  *  @n  Not applicable.
120  */
121 #define Rm_osalFree               Osal_rmFree
124 #define Rm_osalLocalGateEnter     Osal_rmLocalGateEnter
126 #define Rm_osalLocalGateLeave     Osal_rmLocalGateLeave
128 /**
129  * @brief   The macro is used by RM to log various 
130  *          messages. 
131  *
132  * <b> Prototype: </b>
133  *  The following is the C prototype for the expected OSAL API.
134  *
135  *  @verbatim
136        void Osal_rmLog( char *fmt, ... ) 
137     @endverbatim
138  *
139  *  <b> Parameter </b>
140  *  @n  printf-style format string 
141  *
142  *  <b> Return Value </b>
143  *  @n  Not applicable.
144  */
145 #define Rm_osalLog                Osal_rmLog
147 /**
148 @}
149 */
151 #endif /* RM_OSAL_H_ */