]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - keystone-rtos/rm-lld.git/blob - rm_osal.h
c41032ddfbd193fc67dab039c28e98f667fd1f20
[keystone-rtos/rm-lld.git] / rm_osal.h
1 /**
2  *   @file  rm_osal.h
3  *
4  *   @brief   
5  *      This is the sample OS Adaptation layer which is used by the RM low level
6  *      driver. The OSAL layer can be ported in either of the following 
7  *      manners to a native OS:
8  *
9  *      <b> Approach 1: </b>
10  *      @n  Use Prebuilt Libraries
11  *           - Ensure that the provide an implementation of all 
12  *             Osal_XXX API for their native OS.
13  *           - Link the prebuilt libraries with their application.
14  *           - Refer to the "example" directory for an example of this
15  *       @n <b> Pros: </b>
16  *           - Customers can reuse prebuilt TI provided libraries
17  *       @n <b> Cons: </b>
18  *           - Level of indirection in the API to get to the actual OS call
19  *              
20  *      <b> Approach 2: </b>
21  *      @n  Rebuilt Library 
22  *           - Create a copy of this file and modify it to directly 
23  *             inline the native OS calls
24  *           - Rebuild the RM low level drivver library; ensure that the Include 
25  *             path points to the directory where the copy of this file 
26  *             has been provided.
27  *           - Please refer to the "test" directory for an example of this 
28  *       @n <b> Pros: </b>
29  *           - Optimizations can be done to remove the level of indirection
30  *       @n <b> Cons: </b>
31  *           - RM LLD Libraries need to be rebuilt by the customer.
32  *
33  *  \par
34  *  NOTE:
35  *      (C) Copyright 2012 Texas Instruments, Inc.
36  * 
37  *  Redistribution and use in source and binary forms, with or without 
38  *  modification, are permitted provided that the following conditions 
39  *  are met:
40  *
41  *    Redistributions of source code must retain the above copyright 
42  *    notice, this list of conditions and the following disclaimer.
43  *
44  *    Redistributions in binary form must reproduce the above copyright
45  *    notice, this list of conditions and the following disclaimer in the 
46  *    documentation and/or other materials provided with the   
47  *    distribution.
48  *
49  *    Neither the name of Texas Instruments Incorporated nor the names of
50  *    its contributors may be used to endorse or promote products derived
51  *    from this software without specific prior written permission.
52  *
53  *  THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS 
54  *  "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT 
55  *  LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
56  *  A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT 
57  *  OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, 
58  *  SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT 
59  *  LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
60  *  DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
61  *  THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT 
62  *  (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE 
63  *  OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
64  *
65  *  \par
66 */
67 #ifndef __RM_OSAL_H__
68 #define __RM_OSAL_H__
70 /** @addtogroup RM_LLD_OSAL
71  @{ */
73 /**********************************************************************
74  ************************* Extern Declarations ************************
75  **********************************************************************/
77 /* #include <string.h> is here because there used to be 
78  * memcpy/memset prototypes here.  This #include prevents warnings in 
79  * other code that unintentionally worked because of these prototypes
80  */
81 #include <string.h>
83 extern void* Osal_rmMalloc (uint32_t num_bytes);
84 extern void Osal_rmFree (void *ptr, uint32_t size);
85 extern void* Osal_rmCsEnter (void);
86 extern void Osal_rmCsExit (void *CsHandle);
87 extern void* Osal_rmMtCsEnter (void);
88 extern void Osal_rmMtCsExit (void *CsHandle);
89 extern void Osal_rmLog (char *fmt, ... );
90 extern void Osal_rmBeginMemAccess (void *ptr, uint32_t size);
91 extern void Osal_rmEndMemAccess (void *ptr, uint32_t size);
93 /**
94  * @brief   The macro is used by the RM LLD to allocate memory of specified
95  * size
96  *
97  * <b> Prototype: </b>
98  *  The following is the C prototype for the expected OSAL API.
99  *
100  *  @verbatim
101        void* Osal_rmMalloc (uint32_t numBytes)
102     @endverbatim
103  *      
104  *  <b> Parameter </b>
105  *  @n  Number of bytes to be allocated
106  *
107  *  <b> Return Value </b>
108  *  @n  Pointer to the allocated block size
109  */
111 #define Rm_osalMalloc             Osal_rmMalloc
113 /**
114  * @brief   The macro is used by the RM LLD to free a allocated block of 
115  * memory 
116  *
117  * <b> Prototype: </b>
118  *  The following is the C prototype for the expected OSAL API.
119  *
120  *  @verbatim
121        void Osal_rmFree (void *ptr, uint32_t size)
122     @endverbatim
123  *      
124  *  <b> Parameter </b>
125  *  @n  Pointer to the block of memory to be cleaned up.
126  *  @n  Size of the allocated memory which is being freed.
127  *
128  *  <b> Return Value </b>
129  *  @n  Not applicable.
130  */
132 #define Rm_osalFree               Osal_rmFree
134 /**
135  * @brief   The macro is used by the RM LLD to provide critical sections to 
136  * protect global and shared variables from
137  *
138  *      access from multiple cores 
139  *      and 
140  *      access from multiple threads on single core
141  *
142  * <b> Prototype: </b>
143  *  The following is the C prototype for the expected OSAL API.
144  *
145  *  @verbatim
146        void* Osal_rmCsEnter (void)
147     @endverbatim
148  *      
149  *  <b> Parameter </b>
150  *  @n  None.
151  *
152  *  <b> Return Value </b>
153  *  @n  Handle used to lock critical section.
154  */
155 #define Rm_osalCsEnter            Osal_rmCsEnter
157 /**
158  * @brief   The macro is used by the RM LLD to exit a critical section 
159  *      protected using Osal_rmCsEnter() API.
160  *
161  * <b> Prototype: </b>
162  *  The following is the C prototype for the expected OSAL API.
163  *
164  *  @verbatim
165        void Osal_rmCsExit (void *CsHandle)
166     @endverbatim
167  *      
168  *  <b> Parameter </b>
169  *  @n  Handle for unlocking critical section.
170  *
171  *  <b> Return Value </b>
172  *  @n  Not applicable.
173  */
174 #define Rm_osalCsExit             Osal_rmCsExit
176 /**
177  * @brief   The macro is used by the RM LLD to provide critical sections to 
178  * protect global and shared variables from
179  *
180  *      access from multiple threads on single core
181  *
182  * <b> Prototype: </b>
183  *  The following is the C prototype for the expected OSAL API.
184  *
185  *  @verbatim
186        void* Osal_rmMtCsEnter (void)
187     @endverbatim
188  *      
189  *  <b> Parameter </b>
190  *  @n  None.
191  *
192  *  <b> Return Value </b>
193  *  @n  Handle used to lock critical section.
194  */
195 #define Rm_osalMtCsEnter          Osal_rmMtCsEnter
197 /**
198  * @brief   The macro is used by the RM LLD to exit a critical section 
199  *      protected using Osal_rmMtCsEnter() API.
200  *
201  * <b> Prototype: </b>
202  *  The following is the C prototype for the expected OSAL API.
203  *
204  *  @verbatim
205        void Osal_rmMtCsExit (void *CsHandle)
206     @endverbatim
207  *      
208  *  <b> Parameter </b>
209  *  @n  Handle for unlocking critical section.
210  *
211  *  <b> Return Value </b>
212  *  @n  Not applicable.
213  */
214 #define Rm_osalMtCsExit           Osal_rmMtCsExit
216 /**
217  * @brief   The macro is used by the RM LLD to log various 
218  * messages. 
219  *
220  * <b> Prototype: </b>
221  *  The following is the C prototype for the expected OSAL API.
222  *
223  *  @verbatim
224        void Osal_rmLog( char *fmt, ... ) 
225     @endverbatim
226  *
227  *  <b> Parameter </b>
228  *  @n  printf-style format string 
229  *
230  *  <b> Return Value </b>
231  *  @n  Not applicable.
232  */
233 #define Rm_osalLog                Osal_rmLog
235 /**
236  * @brief   The macro is used by the RM LLD to indicate that a block
237  * of memory is about to be accessed. If the memory block is cached then
238  * this indicates that the application would need to ensure that the cache
239  * is updated with the data from the actual memory.
240  *
241  * <b> Prototype: </b>
242  *  The following is the C prototype for the expected OSAL API.
243  *
244  *  @verbatim
245        void Osal_rmBeginMemAccess (void *ptr, uint32_t size) 
246     @endverbatim
247  *
248  *  <b> Parameter </b>
249  *  @n  Address of memory block.
250  *  @n  Size of memory block.
251  *
252  *  <b> Return Value </b>
253  *  @n  Not applicable.
254  */
255 #define Rm_osalBeginMemAccess     Osal_rmBeginMemAccess
257 /**
258  * @brief   The macro is used by the RM LLD to indicate that the block of 
259  * memory has finished being accessed. If the memory block is cached then the 
260  * application would need to ensure that the contents of the cache are updated
261  * immediately to the actual memory.
262  *
263  * <b> Prototype: </b>
264  *  The following is the C prototype for the expected OSAL API.
265  *
266  *  @verbatim
267        void Osal_rmEndMemAccess (void *ptr, uint32_t size) 
268     @endverbatim
269  *
270  *  <b> Parameter </b>
271  *  @n  Address of memory block.
272  *  @n  Size of memory block.
273  *
274  *  <b> Return Value </b>
275  *  @n  Not applicable.
276  */
277 #define Rm_osalEndMemAccess       Osal_rmEndMemAccess
279 /**
280 @}
281 */
282 #endif /* __RM_OSAL_H__ */