]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - keystone-rtos/rm-lld.git/blob - rm_osal.h
Removed memory test project warning
[keystone-rtos/rm-lld.git] / rm_osal.h
1 /**
2  *   @file  rm_osal.h
3  *
4  *   @brief   
5  *      This is the sample OS Adaptation layer which is used by the Resource
6  *      Manager. The OSAL layer can be ported in either of the following 
7  *      manners to a native OS:
8  *
9  *      <b> Approach 1: </b>
10  *      @n  Use Prebuilt Libraries
11  *           - Ensure that the provide an implementation of all 
12  *             Osal_XXX API for their native OS.
13  *           - Link the prebuilt libraries with their application.
14  *           - Refer to the "example" directory for an example of this
15  *       @n <b> Pros: </b>
16  *           - Customers can reuse prebuilt TI provided libraries
17  *       @n <b> Cons: </b>
18  *           - Level of indirection in the API to get to the actual OS call
19  *              
20  *      <b> Approach 2: </b>
21  *      @n  Rebuilt Library 
22  *           - Create a copy of this file and modify it to directly 
23  *             inline the native OS calls
24  *           - Rebuild the RM low level drivver library; ensure that the Include 
25  *             path points to the directory where the copy of this file 
26  *             has been provided.
27  *           - Please refer to the "test" directory for an example of this 
28  *       @n <b> Pros: </b>
29  *           - Optimizations can be done to remove the level of indirection
30  *       @n <b> Cons: </b>
31  *           - RM LLD Libraries need to be rebuilt by the customer.
32  *
33  *  \par
34  *  NOTE:
35  *      (C) Copyright 2012-2013 Texas Instruments, Inc.
36  * 
37  *  Redistribution and use in source and binary forms, with or without 
38  *  modification, are permitted provided that the following conditions 
39  *  are met:
40  *
41  *    Redistributions of source code must retain the above copyright 
42  *    notice, this list of conditions and the following disclaimer.
43  *
44  *    Redistributions in binary form must reproduce the above copyright
45  *    notice, this list of conditions and the following disclaimer in the 
46  *    documentation and/or other materials provided with the   
47  *    distribution.
48  *
49  *    Neither the name of Texas Instruments Incorporated nor the names of
50  *    its contributors may be used to endorse or promote products derived
51  *    from this software without specific prior written permission.
52  *
53  *  THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS 
54  *  "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT 
55  *  LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
56  *  A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT 
57  *  OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, 
58  *  SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT 
59  *  LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
60  *  DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
61  *  THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT 
62  *  (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE 
63  *  OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
64  *
65  *  \par
66 */
67 #ifndef RM_OSAL_H_
68 #define RM_OSAL_H_
70 /** @addtogroup RM_OSAL_API
71  @{ 
72  */
74 /**********************************************************************
75  ************************* Extern Declarations ************************
76  **********************************************************************/
78 extern void *Osal_rmMalloc (uint32_t num_bytes);
79 extern void  Osal_rmFree (void *ptr, uint32_t size);
80 extern void *Osal_rmCsEnter (void);
81 extern void  Osal_rmCsExit (void *CsHandle);
82 extern void  Osal_rmBeginMemAccess (void *ptr, uint32_t size);
83 extern void  Osal_rmEndMemAccess (void *ptr, uint32_t size);
84 extern void *Osal_rmTaskBlockCreate (void);
85 extern void  Osal_rmTaskBlock (void *handle);
86 extern void  Osal_rmTaskUnblock (void *handle);
87 extern void  Osal_rmTaskBlockDelete (void *handle);
88 extern void  Osal_rmLog (char *fmt, ... );
90 /**
91  * @brief   The macro is used by RM to allocate memory of specified
92  *          size
93  *
94  * <b> Prototype: </b>
95  *  The following is the C prototype for the expected OSAL API.
96  *
97  *  @verbatim
98        void* Osal_rmMalloc (uint32_t numBytes)
99     @endverbatim
100  *      
101  *  <b> Parameter </b>
102  *  @n  Number of bytes to be allocated
103  *
104  *  <b> Return Value </b>
105  *  @n  Pointer to the allocated block size
106  */
107 #define Rm_osalMalloc             Osal_rmMalloc
109 /**
110  * @brief   The macro is used by RM to free a allocated block of 
111  *          memory 
112  *
113  * <b> Prototype: </b>
114  *  The following is the C prototype for the expected OSAL API.
115  *
116  *  @verbatim
117        void Osal_rmFree (void *ptr, uint32_t size)
118     @endverbatim
119  *      
120  *  <b> Parameter </b>
121  *  @n  Pointer to the block of memory to be cleaned up.
122  *  @n  Size of the allocated memory which is being freed.
123  *
124  *  <b> Return Value </b>
125  *  @n  Not applicable.
126  */
127 #define Rm_osalFree               Osal_rmFree
129 /**
130  * @brief   The function is used to enter a critical section.
131  *          Function protects against 
132  *      
133  *          access from multiple cores 
134  *          and 
135  *          access from multiple threads on single core
136  *
137  * <b> Prototype: </b>
138  *  The following is the C prototype for the expected OSAL API.
139  *
140  *  @verbatim
141        void *Osal_rmCsEnter (void)
142     @endverbatim
143  *      
144  *  <b> Parameter </b>
145  *  @n  Not applicable.
146  *
147  *  <b> Return Value </b>
148  *  @n  Handle used to lock critical section
149  */
150 #define Rm_osalCsEnter            Osal_rmCsEnter
152 /**
153  * @brief   The function is used to exit a critical section 
154  *          protected using Osal_rmCsEnter() API.
155  *
156  * <b> Prototype: </b>
157  *  The following is the C prototype for the expected OSAL API.
158  *
159  *  @verbatim
160        void Osal_rmCsExit (void *CsHandle)
161     @endverbatim
162  *      
163  *  <b> Parameter </b>
164  *  @n  Handle for unlocking critical section.
165  *
166  *  <b> Return Value </b>
167  *  @n  Not applicable.
168  */
169 #define Rm_osalCsExit             Osal_rmCsExit
171 /**
172  * @brief   The function is used to indicate that a block of memory is 
173  *          about to be accessed. If the memory block is cached then this 
174  *          indicates that the application would need to ensure that the 
175  *          cache is updated with the data from the actual memory.
176  *
177  * <b> Prototype: </b>
178  *  The following is the C prototype for the expected OSAL API.
179  *
180  *  @verbatim
181        void Osal_rmBeginMemAccess (void *ptr, uint32_t size)
182     @endverbatim
183  *      
184  *  <b> Parameter </b>
185  *  @n  Address of memory block
186  *  @n  Size of memory block
187  *
188  *  <b> Return Value </b>
189  *  @n  Not applicable.
190  */
191 #define Rm_osalBeginMemAccess     Osal_rmBeginMemAccess
193 /**
194  * @brief   The function is used to indicate that the block of memory has 
195  *          finished being accessed. If the memory block is cached then the 
196  *          application would need to ensure that the contents of the cache 
197  *          are updated immediately to the actual memory. 
198  *
199  * <b> Prototype: </b>
200  *  The following is the C prototype for the expected OSAL API.
201  *
202  *  @verbatim
203        void Osal_rmEndMemAccess (void *ptr, uint32_t size)
204     @endverbatim
205  *      
206  *  <b> Parameter </b>
207  *  @n  Address of memory block
208  *  @n  Size of memory block
209  *
210  *  <b> Return Value </b>
211  *  @n  Not applicable.
212  */
213 #define Rm_osalEndMemAccess       Osal_rmEndMemAccess
215 /**
216  * @brief   The macro is used by RM to create a task blocking
217  *          mechanism allowing a RM instance to block when it
218  *          has not been provided a service callback function
219  *          and it must send a packet to remote RM instance 
220  *          to complete a service.
221  *
222  * <b> Prototype: </b>
223  *  The following is the C prototype for the expected OSAL API.
224  *
225  *  @verbatim
226        void *Osal_rmTaskBlockCreate (void)
227     @endverbatim
228  *      
229  *  <b> Parameter </b>
230  *  @n  Not applicable.
231  *
232  *  <b> Return Value </b>
233  *  @n  Task blocking mechanism handle cast as a void pointer
234  */
235 #define Rm_osalTaskBlockCreate    Osal_rmTaskBlockCreate
237 /**
238  * @brief   The macro is used by a RM instance to block when it
239  *          has not been provided a service callback function
240  *          and it must send a packet to remote RM instance 
241  *          to complete a service.  The blocking operation
242  *          should block the current RM instance's task/thread
243  *          from executing until a task/thread from which the
244  *          RM receive code runs unblocks the RM instance
245  *
246  * <b> Prototype: </b>
247  *  The following is the C prototype for the expected OSAL API.
248  *
249  *  @verbatim
250        void  Osal_rmTaskBlock (void *handle)
251     @endverbatim
252  *      
253  *  <b> Parameter </b>
254  *  @n  Task blocking mechanism handle cast as a void pointer
255  *
256  *  <b> Return Value </b>
257  *  @n  Not applicable.
258  */
259 #define Rm_osalTaskBlock          Osal_rmTaskBlock
261 /**
262  * @brief   The macro is used by a RM instance to unblock from 
263  *          a previous block operation.
264  *
265  * <b> Prototype: </b>
266  *  The following is the C prototype for the expected OSAL API.
267  *
268  *  @verbatim
269        void  Osal_rmTaskUnblock (void *handle)
270     @endverbatim
271  *      
272  *  <b> Parameter </b>
273  *  @n  Task blocking mechanism handle cast as a void pointer
274  *
275  *  <b> Return Value </b>
276  *  @n  Not applicable.
277  */
278 #define Rm_osalTaskUnblock        Osal_rmTaskUnblock
280 /**
281  * @brief   The macro is used by a RM instance to delete its
282  *          task blocking mechanism.
283  *
284  * <b> Prototype: </b>
285  *  The following is the C prototype for the expected OSAL API.
286  *
287  *  @verbatim
288        void  Osal_rmTaskBlockDelete (void *handle)
289     @endverbatim
290  *      
291  *  <b> Parameter </b>
292  *  @n  Task blocking mechanism handle cast as a void pointer
293  *
294  *  <b> Return Value </b>
295  *  @n  Not applicable.
296  */
297 #define Rm_osalTaskBlockDelete    Osal_rmTaskBlockDelete
299 /**
300  * @brief   The macro is used by RM to log various 
301  *          messages. 
302  *
303  * <b> Prototype: </b>
304  *  The following is the C prototype for the expected OSAL API.
305  *
306  *  @verbatim
307        void Osal_rmLog( char *fmt, ... ) 
308     @endverbatim
309  *
310  *  <b> Parameter </b>
311  *  @n  printf-style format string 
312  *
313  *  <b> Return Value </b>
314  *  @n  Not applicable.
315  */
316 #define Rm_osalLog                Osal_rmLog
318 /**
319 @}
320 */
322 #endif /* RM_OSAL_H_ */