/** * @file rm_osal.h * * @brief * This is the sample OS Adaptation layer which is used by the Resource * Manager. The OSAL layer can be ported in either of the following * manners to a native OS: * * Approach 1: * @n Use Prebuilt Libraries * - Ensure that the provide an implementation of all * Osal_XXX API for their native OS. * - Link the prebuilt libraries with their application. * - Refer to the "example" directory for an example of this * @n Pros: * - Customers can reuse prebuilt TI provided libraries * @n Cons: * - Level of indirection in the API to get to the actual OS call * * Approach 2: * @n Rebuilt Library * - Create a copy of this file and modify it to directly * inline the native OS calls * - Rebuild the RM low level drivver library; ensure that the Include * path points to the directory where the copy of this file * has been provided. * - Please refer to the "test" directory for an example of this * @n Pros: * - Optimizations can be done to remove the level of indirection * @n Cons: * - RM LLD Libraries need to be rebuilt by the customer. * * \par * NOTE: * (C) Copyright 2012-2013 Texas Instruments, Inc. * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the * distribution. * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR * A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT * OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, * SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT * LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, * DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY * THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT * (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. * * \par */ #ifndef RM_OSAL_H_ #define RM_OSAL_H_ /** @addtogroup RM_OSAL_API @{ */ /********************************************************************** ************************* Extern Declarations ************************ **********************************************************************/ extern void *Osal_rmMalloc (uint32_t num_bytes); extern void Osal_rmFree (void *ptr, uint32_t size); extern void *Osal_rmCsEnter (void); extern void Osal_rmCsExit (void *CsHandle); extern void Osal_rmBeginMemAccess (void *ptr, uint32_t size); extern void Osal_rmEndMemAccess (void *ptr, uint32_t size); extern void *Osal_rmTaskBlockCreate (void); extern void Osal_rmTaskBlock (void *handle); extern void Osal_rmTaskUnblock (void *handle); extern void Osal_rmTaskBlockDelete (void *handle); extern void Osal_rmLog (char *fmt, ... ); /** * @brief The macro is used by RM to allocate memory of specified * size * * Prototype: * The following is the C prototype for the expected OSAL API. * * @verbatim void* Osal_rmMalloc (uint32_t numBytes) @endverbatim * * Parameter * @n Number of bytes to be allocated * * Return Value * @n Pointer to the allocated block size */ #define Rm_osalMalloc Osal_rmMalloc /** * @brief The macro is used by RM to free a allocated block of * memory * * Prototype: * The following is the C prototype for the expected OSAL API. * * @verbatim void Osal_rmFree (void *ptr, uint32_t size) @endverbatim * * Parameter * @n Pointer to the block of memory to be cleaned up. * @n Size of the allocated memory which is being freed. * * Return Value * @n Not applicable. */ #define Rm_osalFree Osal_rmFree /** * @brief The function is used to enter a critical section. * Function protects against * * access from multiple cores * and * access from multiple threads on single core * * Prototype: * The following is the C prototype for the expected OSAL API. * * @verbatim void *Osal_rmCsEnter (void) @endverbatim * * Parameter * @n Not applicable. * * Return Value * @n Handle used to lock critical section */ #define Rm_osalCsEnter Osal_rmCsEnter /** * @brief The function is used to exit a critical section * protected using Osal_rmCsEnter() API. * * Prototype: * The following is the C prototype for the expected OSAL API. * * @verbatim void Osal_rmCsExit (void *CsHandle) @endverbatim * * Parameter * @n Handle for unlocking critical section. * * Return Value * @n Not applicable. */ #define Rm_osalCsExit Osal_rmCsExit /** * @brief The function is used to indicate that a block of memory is * about to be accessed. If the memory block is cached then this * indicates that the application would need to ensure that the * cache is updated with the data from the actual memory. * * Prototype: * The following is the C prototype for the expected OSAL API. * * @verbatim void Osal_rmBeginMemAccess (void *ptr, uint32_t size) @endverbatim * * Parameter * @n Address of memory block * @n Size of memory block * * Return Value * @n Not applicable. */ #define Rm_osalBeginMemAccess Osal_rmBeginMemAccess /** * @brief The function is used to indicate that the block of memory has * finished being accessed. If the memory block is cached then the * application would need to ensure that the contents of the cache * are updated immediately to the actual memory. * * Prototype: * The following is the C prototype for the expected OSAL API. * * @verbatim void Osal_rmEndMemAccess (void *ptr, uint32_t size) @endverbatim * * Parameter * @n Address of memory block * @n Size of memory block * * Return Value * @n Not applicable. */ #define Rm_osalEndMemAccess Osal_rmEndMemAccess /** * @brief The macro is used by RM to create a task blocking * mechanism allowing a RM instance to block when it * has not been provided a service callback function * and it must send a packet to remote RM instance * to complete a service. * * Prototype: * The following is the C prototype for the expected OSAL API. * * @verbatim void *Osal_rmTaskBlockCreate (void) @endverbatim * * Parameter * @n Not applicable. * * Return Value * @n Task blocking mechanism handle cast as a void pointer */ #define Rm_osalTaskBlockCreate Osal_rmTaskBlockCreate /** * @brief The macro is used by a RM instance to block when it * has not been provided a service callback function * and it must send a packet to remote RM instance * to complete a service. The blocking operation * should block the current RM instance's task/thread * from executing until a task/thread from which the * RM receive code runs unblocks the RM instance * * Prototype: * The following is the C prototype for the expected OSAL API. * * @verbatim void Osal_rmTaskBlock (void *handle) @endverbatim * * Parameter * @n Task blocking mechanism handle cast as a void pointer * * Return Value * @n Not applicable. */ #define Rm_osalTaskBlock Osal_rmTaskBlock /** * @brief The macro is used by a RM instance to unblock from * a previous block operation. * * Prototype: * The following is the C prototype for the expected OSAL API. * * @verbatim void Osal_rmTaskUnblock (void *handle) @endverbatim * * Parameter * @n Task blocking mechanism handle cast as a void pointer * * Return Value * @n Not applicable. */ #define Rm_osalTaskUnblock Osal_rmTaskUnblock /** * @brief The macro is used by a RM instance to delete its * task blocking mechanism. * * Prototype: * The following is the C prototype for the expected OSAL API. * * @verbatim void Osal_rmTaskBlockDelete (void *handle) @endverbatim * * Parameter * @n Task blocking mechanism handle cast as a void pointer * * Return Value * @n Not applicable. */ #define Rm_osalTaskBlockDelete Osal_rmTaskBlockDelete /** * @brief The macro is used by RM to log various * messages. * * Prototype: * The following is the C prototype for the expected OSAL API. * * @verbatim void Osal_rmLog( char *fmt, ... ) @endverbatim * * Parameter * @n printf-style format string * * Return Value * @n Not applicable. */ #define Rm_osalLog Osal_rmLog /** @} */ #endif /* RM_OSAL_H_ */