/** * @file rm_services.h * * @brief * This is the RM include file for services provided to components that * register a RM instance * * \par * ============================================================================ * @n (C) Copyright 2012-2015, Texas Instruments, Inc. * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the * distribution. * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR * A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT * OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, * SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT * LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, * DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY * THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT * (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. * * \par */ #ifndef RM_SERVICES_H_ #define RM_SERVICES_H_ #ifdef __cplusplus extern "C" { #endif /* RM includes */ #include /** @addtogroup RM_SERVICES_API @{ */ /** * @brief RM service types */ typedef enum { /** RM resource allocate for initialization service */ Rm_service_RESOURCE_ALLOCATE_INIT = 0, /** RM resource allocate for use service */ Rm_service_RESOURCE_ALLOCATE_USE, /** RM resource free service */ Rm_service_RESOURCE_FREE, /** RM resource status service - returns the reference count for specified * resource. */ Rm_service_RESOURCE_STATUS, /** RM NameServer map resource to name service */ Rm_service_RESOURCE_MAP_TO_NAME, /** RM NameServer get resource by name service */ Rm_service_RESOURCE_GET_BY_NAME, /** RM NameServer unmap resource from name service */ Rm_service_RESOURCE_UNMAP_NAME, /** DO NOT USE: Last type */ Rm_service_LAST } Rm_ServiceType; /** * @brief RM service response information used by RM to provide service * request results back to the application components */ typedef struct { /** RM instance handle from which the service request that spawned this * result originated. Used by application to sort responses, received * via callback function, from RM instances located on the same core. */ Rm_Handle rmHandle; /** Service request state. State values can be found in rm.h starting * with #RM_SERVICE_PROCESSING, #RM_SERVICE_DENIED_BASE, and * #RM_ERROR_LIBFDT_START */ int32_t serviceState; /** The service ID is returned to the application in order to match service * responses received at a later time via the provided callback function * because RM required a blocking operation in order to satisfy the * resource request.

The service ID will never have a value of * zero. */ uint32_t serviceId; /** Affected resource name */ char resourceName[RM_NAME_MAX_CHARS]; /** The resource base value allocated, freed, or mapped to NameServer * name. */ int32_t resourceBase; /** The resource length starting at base allocated, freed, or mapped to * NameServer name. */ uint32_t resourceLength; /** resourceNumOwners is not valid unless >= 0 */ #define RM_RESOURCE_NUM_OWNERS_INVALID (-1) /** Current number of owners for the returned resource. A value greater * than one means the resource is being shared. This value is only valid * if the serviceState is RM_SERVICE_APPROVED or * RM_SERVICE_APPROVED_STATIC. */ int32_t resourceNumOwners; /** instAllocCount is not valid unless >= 0 */ #define RM_INST_ALLOC_COUNT_INVALID (-1) /** Number of times the requesting instance has allocated the returned * resource. This value is only valid if the serviceState is * RM_SERVICE_APPROVED or RM_SERVICE_APPROVED_STATIC */ int32_t instAllocCount; } Rm_ServiceRespInfo; /** * @brief RM service callback function */ typedef struct { /** Component callback function. RM calls this function when a blocking * resource service request is complete. The callback function supplied * for this parameter must match the function pointer prototype. */ void (*serviceCallback) (Rm_ServiceRespInfo *serviceResponse); } Rm_ServiceCallback; /** * @brief RM service request information */ typedef struct { /** The type of service requested */ Rm_ServiceType type; /** Pointer to an array containing the resource name affected by * the request. The resource name must match a resource node name * defined in the GRL and global/static policy. The request will be * denied if the resource name does not match any resource node names * in the policy */ const char *resourceName; /** Informs RM to find the next available resource block of length * resourceLength and alignment resourceAlignment for allocation. This * parameter is only valid for resource allocate service types. */ #define RM_RESOURCE_BASE_UNSPECIFIED (-1) /** The base value of the resource affected by the service request. * #RM_RESOURCE_BASE_UNSPECIFIED can be substituted. */ int32_t resourceBase; /** The resource length, starting from #resourceBase affected by the * service request. */ uint32_t resourceLength; /** Informs RM to find the next available resource block with length * resourceLength and the alignment specified in * a) The resource node in the policy if it has the "allocation-alignment" * property defined. * b) The default alignment of 1 if no alignment is specified in the policy * for the resource. * This value is only valid if resourceBase is set to * #RM_RESOURCE_BASE_UNSPECIFIED */ #define RM_RESOURCE_ALIGNMENT_UNSPECIFIED (-1) /** Alignment of the resource affected by the service request. Only valid * if resourceBase is set to #RM_RESOURCE_BASE_UNSPECIFIED. * #RM_RESOURCE_ALIGNMENT_UNSPECIFIED can be substituted. */ int32_t resourceAlignment; /** The NameServer name associated, or to be associated, with a resource. * The NameServer name has precedence over #resourceBase and * #resourceLength for all resource modification service types as well as * #Rm_service_RESOURCE_GET_BY_NAME. If the NameServer name and the base * and length are not NULL the resource information retrieved from the * NameServer entry for the name will replace the values present in * #resourceBase and #resourceLength */ const char *resourceNsName; /** Callback function used by RM to provide responses back to application * components after a service request resulted in a blocking operation. * If no callback function is provided the RM instance will block until * the service response is ready. */ Rm_ServiceCallback callback; } Rm_ServiceReqInfo; /** * @brief RM service handle provided to application components for requesting * services */ typedef struct { /** RM instance handle from which the service handle was allocated from. */ void *rmHandle; /** * @b Description * @n * Processes service requests from application components. Responses * are returned immediately if the service request could be satisfied * without blocking. If the service request requires a blocking * operation, such as forwarding the service request to another * instance for validation, the response will be received via the * Rm_ServerCallback * * @param[in] rmHandle * RM instance handle specifies the instance that handles the service * request. The request's result, if policy checks are involved, will * be based on the permissions assigned to the rmHandle's instance * name within global/static policy. * * @param[in] serviceRequest * Pointer to the service request structure * * @param[out] serviceResponse * Pointer to a service response structure. */ void (*Rm_serviceHandler)(void *rmHandle, const Rm_ServiceReqInfo *serviceRequest, Rm_ServiceRespInfo *serviceResponse); } Rm_ServiceHandle; /** * @b Description * @n * This function returns a RM service handle to the application to * provide services to software components (LLDs, BIOS, etc) that want to * use RM for resource management. Only one service handle can be opened * from each RM instance. * * @param[in] rmHandle * RM instance handle from which the service handle will be opened * * @param[out] result * Pointer to a signed int used to return any errors encountered during * the instance initialization process. * * @retval * Success - Rm_ServiceHandle and result = #RM_OK * @retval * Failure - NULL Rm_ServiceHandle and * result = #RM_ERROR_SERVICE_HANDLE_MEM_ALLOC_FAILED */ Rm_ServiceHandle *Rm_serviceOpenHandle(Rm_Handle rmHandle, int32_t *result); /** * @b Description * @n * This function closes a RM instance's service handle * * @param[in] rmServiceHandle * RM instance service handle to be closed. * * @retval * Success - #RM_OK * @retval * Failure - #RM_ERROR_SERVICE_HANDLE_ALREADY_CLOSED */ int32_t Rm_serviceCloseHandle(Rm_ServiceHandle *rmServiceHandle); /** @} */ #ifdef __cplusplus } #endif #endif /* RM_SERVICES_H_ */