/** * @file rm_transport.h * * @brief * This is the RM include file for the generic transport interface * used by RM to exchange RM control signals and data between RM instances * * \par * ============================================================================ * @n (C) Copyright 2012-2013, Texas Instruments, Inc. * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the * distribution. * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR * A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT * OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, * SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT * LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, * DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY * THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT * (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. * * \par */ #ifndef RM_TRANSPORT_H_ #define RM_TRANSPORT_H_ #ifdef __cplusplus extern "C" { #endif /* Standard includes */ #include /* RM includes */ #include /** @addtogroup RM_TRANSPORT_API @{ */ /** * @brief Maximum size of RM transport packet */ #define RM_TRANSPORT_PACKET_MAX_SIZE_BYTES (256) /** * @brief RM transport handle */ typedef void *Rm_TransportHandle; /** * @brief Application transport handle. Void casted application transport * data structure. The Rm_AppTransportHandle provided by the * application could be anything from a queue number to a pointer * to an application transport data structure. RM will provide * a Rm_AppTransportHandle to the application any time RM * wants to alloc or send a packet via the transport callouts */ typedef void *Rm_AppTransportHandle; /** * @brief A void pointer to the start of a registered application transport * packet buffer. The Rm_PacketHandle may be different from the * Rm_Packet pointer based on the application transport. For example, * for a QMSS based transport the Rm_PacketHandle may point to the * beginning of a Host descriptor where as the Rm_Packet pointer would * point to the beginning of the data buffer linked with the Host * descriptor. */ typedef void *Rm_PacketHandle; /** * @brief RM packet types */ typedef enum { /** Allocate/Free request packet */ Rm_pktType_RESOURCE_REQUEST = 0, /** Allocate/Free response packet */ Rm_pktType_RESOURCE_RESPONSE, /** RM NameServer mapping request */ Rm_pktType_NAMESERVER_REQUEST, /** RM NameServer mapping response */ Rm_pktType_NAMESERVER_RESPONSE } Rm_pktType; /** * @brief RM transport layer packet */ typedef struct { /** Packet length in bytes. Written by application when allocated */ uint32_t pktLenBytes; /** Type of RM packet contained in data byte array */ Rm_pktType pktType; /** Byte array containing RM packet data */ char data[RM_TRANSPORT_PACKET_MAX_SIZE_BYTES]; } Rm_Packet; /** * @brief RM transport callout functions used by RM to allocate and send * RM packets via the application data paths between RM instances */ typedef struct { /** * @b Description * @n * This function pointer describes the RM transport layer packet * allocation function. The application must supply an alloc function * to RM instances at transport registration if the RM instance is * intended to communicate with other RM instances. The function * provided by the application must match this prototype. The provided * function implements the allocation of packet buffers from the * application data path that the RM transport will use to send messages * between RM instances. The Rm_Packet pointer will point to start of * the data buffer containing the RM packet data. The pktHandle will * point to the start of the application data path "packet" data * structure. The Rm_Packet pointer and pktHandle cannot be NULL. They * will either be different or the same value based on the application * transport. * * @param[in] appTransport * Application transport handle to allocate packet from. This value * is provided by the application at transport registration. * * @param[in] pktSize * Size of buffer needed by RM for the RM packet. The application * must place this value in the pktLenBytes field of the Rm_Packet. * after the buffer has been allocated. * * @param[out] pktHandle * Pointer to the start of the application's transport "packet". * Could be the pointer to the start of a QMSS descriptor, * network packet, etc. * * @retval * Success - Pointer to allocated packet buffer. * @retval * Failure - NULL */ Rm_Packet *(*rmAllocPkt)(Rm_AppTransportHandle appTransport, uint32_t pktSize, Rm_PacketHandle *pktHandle); /** * @b Description * @n * This function pointer describes the RM transport layer packet * send function. The application must supply a send function * to RM instances at transport registration if the RM instance is * intended to communicate with other RM instances. The function * provided by the application must match this prototype. The provided * function implements the sending of application data path packets, * encapsulating RM packets, between RM instances. The pktHandle will * point to the start of the application data path "packet" data * structure. * * RM assumes that the application will free application data * path packet and the buffer containing the Rm_Packet after * the send operation. * * @param[in] appTransport * Application transport handle to send packet on. This value * is provided by the application at transport registration. * * @param[in] pktHandle * Pointer to the start of the application's transport "packet". * Could be the pointer to the start of a QMSS descriptor, * network packet, etc. * * @retval * 0 - Packet sent okay. * @retval * < 0 - Packet send failed. */ int32_t (*rmSendPkt)(Rm_AppTransportHandle appTransport, Rm_PacketHandle pktHandle); } Rm_TransportCallouts; /** * @brief RM transport registration configuration structure */ typedef struct { /** RM Handle for which the transport is being registered */ Rm_Handle rmHandle; /** Application transport handle associated with the registered * transport. This value can be anything that helps the application * identify the application transport "pipe" for which a RM packet * should be sent on. For example, a QMSS queue number, network * port data structure, etc. */ Rm_AppTransportHandle appTransportHandle; /** Remote RM instance type at other end of the application transport * "pipe". */ Rm_InstType remoteInstType; /** Pointers to application implemented transport APIs. The APIs for the * provided functions must match the prototypes defined in the * #Rm_TransportCallouts structure. Callouts need to be defined * for each registered transport. However, based on the application's * implementation of transport code the same function can be provided * for each transport registration. In these cases, the transport * must mux/demux the packets it receives from RM based on the * #Rm_TransportHandle. */ Rm_TransportCallouts transportCallouts; } Rm_TransportCfg; /** * @brief RM transport reconfiguration structure */ typedef struct { /** Application transport handle associated with the registered * transport. This value can be anything that helps the application * identify the application transport "pipe" for which a RM packet * should be sent on. For example, a QMSS queue number, network * port data structure, etc. */ Rm_AppTransportHandle appTransportHandle; /** Pointers to application implemented transport APIs. The APIs for the * provided functions must match the prototypes defined in the * #Rm_TransportCallouts structure. Callouts need to be defined * for each registered transport. However, based on the application's * implementation of transport code the same function can be provided * for each transport registration. In these cases, the transport * must mux/demux the packets it receives from RM based on the * #Rm_TransportHandle. */ Rm_TransportCallouts transportCallouts; } Rm_TransportReCfg; /** * @b Description * @n * This function is used to register transports with RM for sending and * receiving packets between RM instances over application transport * data paths. * * RM Transport Restrictions: * a) RM Servers cannot register with other Servers * b) RM CDs cannot register with other CDs * c) RM Clients cannot register with other Clients * d) Clients cannot register with more than one CD or Server * e) Clients cannot register with both a CD and Server (either or) * f) CDs cannot register with more than one Server * * @param[in] transportCfg * Pointer to the transport registration configuration structure. * * @param[out] result * Pointer to a signed int used to return any errors encountered during * the transport registration process. * * @retval * Success - RM_TransportHandle and result = #RM_OK * @retval * Failure - NULL RM_TransportHandle and result = #RM_ERROR_INVALID_REMOTE_INST_TYPE * @retval * Failure - NULL RM_TransportHandle and result = #RM_ERROR_ALREADY_REGD_SERVER_OR_CD * @retval * Failure - NULL RM_TransportHandle and result = #RM_ERROR_TRANSPORT_ALLOC_PKT_NOT_REGD * @retval * Failure - NULL RM_TransportHandle and result = #RM_ERROR_TRANSPORT_SEND_NOT_REGD */ Rm_TransportHandle Rm_transportRegister(const Rm_TransportCfg *transportCfg, int32_t *result); /** * @b Description * @n * This function reconfigures an existing transport handle using the * provided transport configurations * * @param[in] transportHandle * Transport handle to unregister. The RM instance that the handle will * be unregistered from is contained within the transportHandle. * * @param[in] transportReCfg * Pointer to the transport registration configuration structure. * * @retval * Success - #RM_OK * @retval * Failure - #RM_ERROR_TRANSPORT_HANDLE_DOES_NOT_EXIST */ int32_t Rm_transportReconfig (Rm_TransportHandle transportHandle, const Rm_TransportReCfg *transportReCfg); /** * @b Description * @n * This function unregisters the provided transportHandle from the * RM instance * * @param[in] transportHandle * Transport handle to unregister. The RM instance that the handle will * be unregistered from is contained within the transportHandle. * * @retval * Success - #RM_OK * @retval * Failure - #RM_ERROR_TRANSPORT_HANDLE_DOES_NOT_EXIST */ int32_t Rm_transportUnregister (Rm_TransportHandle transportHandle); /** * @b Description * @n * This function is called by the application when it has received a RM * packet for processing. The application provides the transportHandle * associated with the RM instance that should receive the packet and * a pointer to the data buffer containing the Rm_Packet. * * RM assumes that the application will free the data buffer containing * the Rm_Packet after RM has finished processing the packet. * * @param[in] transportHandle * RM transportHandle containing the instance that should process the * received packet. * * @param[in] pkt * Pointer to the data buffer containing the Rm_Packet * * @retval * Success - #RM_OK * @retval * Failure - < #RM_OK */ int32_t Rm_receivePacket(Rm_TransportHandle transportHandle, const Rm_Packet *pkt); /** @} */ #ifdef __cplusplus } #endif #endif /* RM_TRANSPORT_H_ */